]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - ti-u-boot/ti-u-boot.git/blob - include/serial.h
Prepare v2024.04
[ti-u-boot/ti-u-boot.git] / include / serial.h
1 #ifndef __SERIAL_H__
2 #define __SERIAL_H__
4 #include <post.h>
6 struct serial_device {
7         /* enough bytes to match alignment of following func pointer */
8         char    name[16];
10         int     (*start)(void);
11         int     (*stop)(void);
12         void    (*setbrg)(void);
13         int     (*getc)(void);
14         int     (*tstc)(void);
15         void    (*putc)(const char c);
16         void    (*puts)(const char *s);
17 #if CONFIG_POST & CONFIG_SYS_POST_UART
18         void    (*loop)(int);
19 #endif
20         struct serial_device    *next;
21 };
23 void default_serial_puts(const char *s);
25 extern struct serial_device serial_smc_device;
26 extern struct serial_device serial_scc_device;
27 extern struct serial_device *default_serial_console(void);
29 #if     defined(CONFIG_MPC83xx) || defined(CONFIG_MPC85xx) || \
30         defined(CONFIG_MPC86xx) || \
31         defined(CONFIG_ARCH_TEGRA) || defined(CONFIG_SYS_COREBOOT) || \
32         defined(CONFIG_MICROBLAZE)
33 extern struct serial_device serial0_device;
34 extern struct serial_device serial1_device;
35 #endif
37 extern struct serial_device eserial1_device;
38 extern struct serial_device eserial2_device;
39 extern struct serial_device eserial3_device;
40 extern struct serial_device eserial4_device;
41 extern struct serial_device eserial5_device;
42 extern struct serial_device eserial6_device;
44 extern void serial_register(struct serial_device *);
45 extern void serial_stdio_init(void);
46 extern int serial_assign(const char *name);
47 extern void serial_reinit_all(void);
48 int serial_initialize(void);
50 /* For usbtty */
51 #ifdef CONFIG_USB_TTY
53 struct stdio_dev;
55 int usbtty_getc(struct stdio_dev *dev);
56 void usbtty_putc(struct stdio_dev *dev, const char c);
57 void usbtty_puts(struct stdio_dev *dev, const char *str);
58 int usbtty_tstc(struct stdio_dev *dev);
60 #else
62 /* stubs */
63 #define usbtty_getc(dev) 0
64 #define usbtty_putc(dev, a)
65 #define usbtty_puts(dev, a)
66 #define usbtty_tstc(dev) 0
68 #endif /* CONFIG_USB_TTY */
70 struct udevice;
72 enum serial_par {
73         SERIAL_PAR_NONE,
74         SERIAL_PAR_ODD,
75         SERIAL_PAR_EVEN
76 };
78 #define SERIAL_PAR_SHIFT        0
79 #define SERIAL_PAR_MASK         (0x03 << SERIAL_PAR_SHIFT)
80 #define SERIAL_SET_PARITY(parity) \
81         ((parity << SERIAL_PAR_SHIFT) & SERIAL_PAR_MASK)
82 #define SERIAL_GET_PARITY(config) \
83         ((config & SERIAL_PAR_MASK) >> SERIAL_PAR_SHIFT)
85 enum serial_bits {
86         SERIAL_5_BITS,
87         SERIAL_6_BITS,
88         SERIAL_7_BITS,
89         SERIAL_8_BITS
90 };
92 #define SERIAL_BITS_SHIFT       2
93 #define SERIAL_BITS_MASK        (0x3 << SERIAL_BITS_SHIFT)
94 #define SERIAL_SET_BITS(bits) \
95         ((bits << SERIAL_BITS_SHIFT) & SERIAL_BITS_MASK)
96 #define SERIAL_GET_BITS(config) \
97         ((config & SERIAL_BITS_MASK) >> SERIAL_BITS_SHIFT)
99 enum serial_stop {
100         SERIAL_HALF_STOP,       /* 0.5 stop bit */
101         SERIAL_ONE_STOP,        /*   1 stop bit */
102         SERIAL_ONE_HALF_STOP,   /* 1.5 stop bit */
103         SERIAL_TWO_STOP         /*   2 stop bit */
104 };
106 #define SERIAL_STOP_SHIFT       4
107 #define SERIAL_STOP_MASK        (0x3 << SERIAL_STOP_SHIFT)
108 #define SERIAL_SET_STOP(stop) \
109         ((stop << SERIAL_STOP_SHIFT) & SERIAL_STOP_MASK)
110 #define SERIAL_GET_STOP(config) \
111         ((config & SERIAL_STOP_MASK) >> SERIAL_STOP_SHIFT)
113 #define SERIAL_CONFIG(par, bits, stop) \
114                      (par << SERIAL_PAR_SHIFT | \
115                       bits << SERIAL_BITS_SHIFT | \
116                       stop << SERIAL_STOP_SHIFT)
118 #define SERIAL_DEFAULT_CONFIG \
119                         (SERIAL_PAR_NONE << SERIAL_PAR_SHIFT | \
120                          SERIAL_8_BITS << SERIAL_BITS_SHIFT | \
121                          SERIAL_ONE_STOP << SERIAL_STOP_SHIFT)
123 enum serial_chip_type {
124         SERIAL_CHIP_UNKNOWN = -1,
125         SERIAL_CHIP_16550_COMPATIBLE,
126 };
128 enum adr_space_type {
129         SERIAL_ADDRESS_SPACE_MEMORY = 0,
130         SERIAL_ADDRESS_SPACE_IO,
131 };
133 /**
134  * struct serial_device_info - structure to hold serial device info
135  *
136  * @type:       type of the UART chip
137  * @addr_space: address space to access the registers
138  * @addr:       physical address of the registers
139  * @reg_width:  size (in bytes) of the IO accesses to the registers
140  * @reg_offset: offset to apply to the @addr from the start of the registers
141  * @reg_shift:  quantity to shift the register offsets by
142  * @clock:      UART base clock speed in Hz
143  * @baudrate:   baud rate
144  */
145 struct serial_device_info {
146         enum serial_chip_type type;
147         enum adr_space_type addr_space;
148         ulong addr;
149         u8 reg_width;
150         u8 reg_offset;
151         u8 reg_shift;
152         unsigned int clock;
153         unsigned int baudrate;
154 };
156 #define SERIAL_DEFAULT_ADDRESS  0xBADACCE5
157 #define SERIAL_DEFAULT_CLOCK    (16 * 115200)
159 /**
160  * struct struct dm_serial_ops - Driver model serial operations
161  *
162  * The uclass interface is implemented by all serial devices which use
163  * driver model.
164  */
165 struct dm_serial_ops {
166         /**
167          * setbrg() - Set up the baud rate generator
168          *
169          * Adjust baud rate divisors to set up a new baud rate for this
170          * device. Not all devices will support all rates. If the rate
171          * cannot be supported, the driver is free to select the nearest
172          * available rate. or return -EINVAL if this is not possible.
173          *
174          * @dev: Device pointer
175          * @baudrate: New baud rate to use
176          * @return 0 if OK, -ve on error
177          */
178         int (*setbrg)(struct udevice *dev, int baudrate);
179         /**
180          * getc() - Read a character and return it
181          *
182          * If no character is available, this should return -EAGAIN without
183          * waiting.
184          *
185          * @dev: Device pointer
186          * @return character (0..255), -ve on error
187          */
188         int (*getc)(struct udevice *dev);
189         /**
190          * putc() - Write a character
191          *
192          * @dev: Device pointer
193          * @ch: character to write
194          * @return 0 if OK, -ve on error
195          */
196         int (*putc)(struct udevice *dev, const char ch);
197         /**
198          * pending() - Check if input/output characters are waiting
199          *
200          * This can be used to return an indication of the number of waiting
201          * characters if the driver knows this (e.g. by looking at the FIFO
202          * level). It is acceptable to return 1 if an indeterminant number
203          * of characters is waiting.
204          *
205          * This method is optional.
206          *
207          * @dev: Device pointer
208          * @input: true to check input characters, false for output
209          * @return number of waiting characters, 0 for none, -ve on error
210          */
211         int (*pending)(struct udevice *dev, bool input);
212         /**
213          * clear() - Clear the serial FIFOs/holding registers
214          *
215          * This method is optional.
216          *
217          * This quickly clears any input/output characters from the UART.
218          * If this is not possible, but characters still exist, then it
219          * is acceptable to return -EAGAIN (try again) or -EINVAL (not
220          * supported).
221          *
222          * @dev: Device pointer
223          * @return 0 if OK, -ve on error
224          */
225         int (*clear)(struct udevice *dev);
226 #if CONFIG_POST & CONFIG_SYS_POST_UART
227         /**
228          * loop() - Control serial device loopback mode
229          *
230          * @dev: Device pointer
231          * @on: 1 to turn loopback on, 0 to turn if off
232          */
233         int (*loop)(struct udevice *dev, int on);
234 #endif
236         /**
237          * getconfig() - Get the uart configuration
238          * (parity, 5/6/7/8 bits word length, stop bits)
239          *
240          * Get a current config for this device.
241          *
242          * @dev: Device pointer
243          * @serial_config: Returns config information (see SERIAL_... above)
244          * @return 0 if OK, -ve on error
245          */
246         int (*getconfig)(struct udevice *dev, uint *serial_config);
247         /**
248          * setconfig() - Set up the uart configuration
249          * (parity, 5/6/7/8 bits word length, stop bits)
250          *
251          * Set up a new config for this device.
252          *
253          * @dev: Device pointer
254          * @serial_config: number of bits, parity and number of stopbits to use
255          * @return 0 if OK, -ve on error
256          */
257         int (*setconfig)(struct udevice *dev, uint serial_config);
258         /**
259          * getinfo() - Get serial device information
260          *
261          * @dev: Device pointer
262          * @info: struct serial_device_info to fill
263          * @return 0 if OK, -ve on error
264          */
265         int (*getinfo)(struct udevice *dev, struct serial_device_info *info);
266 };
268 /**
269  * struct serial_dev_priv - information about a device used by the uclass
270  *
271  * @sdev:       stdio device attached to this uart
272  *
273  * @buf:        Pointer to the RX buffer
274  * @rd_ptr:     Read pointer in the RX buffer
275  * @wr_ptr:     Write pointer in the RX buffer
276  */
277 struct serial_dev_priv {
278         struct stdio_dev *sdev;
280         char *buf;
281         int rd_ptr;
282         int wr_ptr;
283 };
285 /* Access the serial operations for a device */
286 #define serial_get_ops(dev)     ((struct dm_serial_ops *)(dev)->driver->ops)
288 /**
289  * serial_getconfig() - Get the uart configuration
290  * (parity, 5/6/7/8 bits word length, stop bits)
291  *
292  * Get a current config for this device.
293  *
294  * @dev: Device pointer
295  * @serial_config: Returns config information (see SERIAL_... above)
296  * @return 0 if OK, -ve on error
297  */
298 int serial_getconfig(struct udevice *dev, uint *config);
300 /**
301  * serial_setconfig() - Set up the uart configuration
302  * (parity, 5/6/7/8 bits word length, stop bits)
303  *
304  * Set up a new config for this device.
305  *
306  * @dev: Device pointer
307  * @serial_config: number of bits, parity and number of stopbits to use
308  * @return 0 if OK, -ve on error
309  */
310 int serial_setconfig(struct udevice *dev, uint config);
312 /**
313  * serial_getinfo() - Get serial device information
314  *
315  * @dev: Device pointer
316  * @info: struct serial_device_info to fill
317  * @return 0 if OK, -ve on error
318  */
319 int serial_getinfo(struct udevice *dev, struct serial_device_info *info);
321 void atmel_serial_initialize(void);
322 void mcf_serial_initialize(void);
323 void mpc85xx_serial_initialize(void);
324 void mxc_serial_initialize(void);
325 void ns16550_serial_initialize(void);
326 void pl01x_serial_initialize(void);
327 void pxa_serial_initialize(void);
328 void sh_serial_initialize(void);
330 /**
331  * serial_printf() - Write a formatted string to the serial console
332  *
333  * The total size of the output must be less than CONFIG_SYS_PBSIZE.
334  *
335  * @fmt: Printf format string, followed by format arguments
336  * @return number of characters written
337  */
338 int serial_printf(const char *fmt, ...)
339                 __attribute__ ((format (__printf__, 1, 2)));
341 int serial_init(void);
342 void serial_setbrg(void);
343 void serial_putc(const char ch);
344 void serial_putc_raw(const char ch);
345 void serial_puts(const char *str);
346 int serial_getc(void);
347 int serial_tstc(void);
349 #endif