]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - ti-u-boot/ti-u-boot.git/blob - include/video_osd.h
Prepare v2024.04
[ti-u-boot/ti-u-boot.git] / include / video_osd.h
1 /* SPDX-License-Identifier: GPL-2.0+ */
2 /*
3  * (C) Copyright 2017
4  * Mario Six,  Guntermann & Drunck GmbH, mario.six@gdsys.cc
5  */
7 #ifndef _VIDEO_OSD_H_
8 #define _VIDEO_OSD_H_
10 struct video_osd_info {
11         /* The width of the OSD display in columns */
12         uint width;
13         /* The height of the OSD display in rows */
14         uint height;
15         /* The major version of the OSD device */
16         uint major_version;
17         /* The minor version of the OSD device */
18         uint minor_version;
19 };
21 /**
22  * struct video_osd_ops - driver operations for OSD uclass
23  *
24  * The OSD uclass implements support for text-oriented on-screen displays,
25  * which are taken to be devices that independently display a graphical
26  * text-based overlay over the video output of an associated display.
27  *
28  * The functions defined by the uclass support writing text to the display in
29  * either a generic form (by specifying a string, a driver-specific color value
30  * for the text, and screen coordinates in rows and columns) or a
31  * driver-specific form (by specifying "raw" driver-specific data to display at
32  * a given coordinate).
33  *
34  * Functions to read device information and set the size of the virtual OSD
35  * screen (in rows and columns) are also supported.
36  *
37  * Drivers should support these operations unless otherwise noted. These
38  * operations are intended to be used by uclass code, not directly from
39  * other code.
40  */
41 struct video_osd_ops {
42         /**
43          * get_info() - Get information about a OSD instance
44          *
45          * A OSD instance may keep some internal data about itself. This
46          * function can be used to access this data.
47          *
48          * @dev:        OSD instance to query.
49          * @info:       Pointer to a structure that takes the information read
50          *              from the OSD instance.
51          * @return 0 if OK, -ve on error.
52          */
53         int (*get_info)(struct udevice *dev, struct video_osd_info *info);
55         /**
56          * set_mem() - Write driver-specific text data to OSD screen
57          *
58          * The passed data are device-specific, and it's up to the driver how
59          * to interpret them. How the count parameter is interpreted is also
60          * driver-specific; most likely the given data will be written to the
61          * OSD count times back-to-back, which is e.g. convenient for filling
62          * areas of the OSD with a single character.
63          *
64          * For example a invocation of
65          *
66          * video_osd_set_mem(dev, 0, 0, "A", 1, 10);
67          *
68          * will write the device-specific text data "A" to the positions (0, 0)
69          * to (9, 0) on the OSD.
70          *
71          * Device-specific text data may, e.g. be a special encoding of glyphs
72          * to display and color values in binary format.
73          *
74          * @dev:        OSD instance to write to.
75          * @col:        Horizontal character coordinate to write to.
76          * @row         Vertical character coordinate to write to.
77          * @buf:        Array containing device-specific data to write to the
78          *              specified coordinate on the OSD screen.
79          * @buflen:     Length of the data in the passed buffer (in byte).
80          * @count:      Write count many repetitions of the given text data
81          * @return 0 if OK, -ve on error.
82          */
83         int (*set_mem)(struct udevice *dev, uint col, uint row, u8 *buf,
84                        size_t buflen, uint count);
86         /**
87          * set_size() - Set the position and dimension of the OSD's
88          *              writeable window
89          *
90          * @dev:        OSD instance to write to.
91          * @col         The number of characters in the window's columns
92          * @row         The number of characters in the window's rows
93          * @return 0 if OK, -ve on error.
94          */
95         int (*set_size)(struct udevice *dev, uint col, uint row);
97         /**
98          * print() - Print a string in a given color to specified coordinates
99          *           on the OSD
100          *
101          * @dev:        OSD instance to write to.
102          * @col         The x-coordinate of the position the string should be
103          *              written to
104          * @row         The y-coordinate of the position the string should be
105          *              written to
106          * @color:      The color in which the specified string should be
107          *              printed; the interpretation of the value is
108          *              driver-specific, and possible values should be defined
109          *              e.g. in a driver include file.
110          * @text:       The string data that should be printed on the OSD
111          * @return 0 if OK, -ve on error.
112          */
113         int (*print)(struct udevice *dev, uint col, uint row, ulong color,
114                      char *text);
115 };
117 #define video_osd_get_ops(dev)  ((struct video_osd_ops *)(dev)->driver->ops)
119 /**
120  * video_osd_get_info() - Get information about a OSD instance
121  *
122  * A OSD instance may keep some internal data about itself. This function can
123  * be used to access this data.
124  *
125  * @dev:        OSD instance to query.
126  * @info:       Pointer to a structure that takes the information read from the
127  *              OSD instance.
128  * @return 0 if OK, -ve on error.
129  */
130 int video_osd_get_info(struct udevice *dev, struct video_osd_info *info);
132 /**
133  * video_osd_set_mem() - Write text data to OSD memory
134  *
135  * The passed data are device-specific, and it's up to the driver how to
136  * interpret them. How the count parameter is interpreted is also
137  * driver-specific; most likely the given data will be written to the OSD count
138  * times back-to-back, which is e.g. convenient for filling areas of the OSD
139  * with a single character.
140  *
141  * For example a invocation of
142  *
143  * video_osd_set_mem(dev, 0, 0, "A", 1, 10);
144  *
145  * will write the device-specific text data "A" to the positions (0, 0) to (9,
146  * 0) on the OSD.
147  *
148  * Device-specific text data may, e.g. be a special encoding of glyphs to
149  * display and color values in binary format.
150  *
151  * @dev:        OSD instance to write to.
152  * @col:        Horizontal character coordinate to write to.
153  * @row         Vertical character coordinate to write to.
154  * @buf:        Array containing device-specific data to write to the specified
155  *              coordinate on the OSD screen.
156  * @buflen:     Length of the data in the passed buffer (in byte).
157  * @count:      Write count many repetitions of the given text data
158  * @return 0 if OK, -ve on error.
159  */
160 int video_osd_set_mem(struct udevice *dev, uint col, uint row, u8 *buf,
161                       size_t buflen, uint count);
163 /**
164  * video_osd_set_size() - Set the position and dimension of the OSD's
165  *              writeable window
166  *
167  * @dev:        OSD instance to write to.
168  * @col         The number of characters in the window's columns
169  * @row         The number of characters in the window's rows
170  * @return 0 if OK, -ve on error.
171  */
172 int video_osd_set_size(struct udevice *dev, uint col, uint row);
174 /**
175  * video_osd_print() - Print a string in a given color to specified coordinates
176  *                     on the OSD
177  *
178  * @dev:        OSD instance to write to.
179  * @col         The x-coordinate of the position the string should be written
180  *              to
181  * @row         The y-coordinate of the position the string should be written
182  *              to
183  * @color:      The color in which the specified string should be printed; the
184  *              interpretation of the value is driver-specific, and possible
185  *              values should be defined e.g. in a driver include file.
186  * @text:       The string data that should be printed on the OSD
187  * @return 0 if OK, -ve on error.
188  */
189 int video_osd_print(struct udevice *dev, uint col, uint row, ulong color,
190                     char *text);
192 #endif /* !_VIDEO_OSD_H_ */