CONFIG_ARM=y CONFIG_SKIP_LOWLEVEL_INIT=y CONFIG_ARCH_CPU_INIT=y CONFIG_ARCH_AT91=y CONFIG_TEXT_BASE=0x21F00000 CONFIG_SYS_MALLOC_LEN=0x2d000 CONFIG_TARGET_AT91SAM9RLEK=y CONFIG_ATMEL_LEGACY=y CONFIG_NR_DRAM_BANKS=1 CONFIG_ENV_SIZE=0x4200 CONFIG_ENV_OFFSET=0x4200 CONFIG_ENV_SECT_SIZE=0x210 CONFIG_DM_GPIO=y CONFIG_DEFAULT_DEVICE_TREE="at91sam9rlek" CONFIG_DEBUG_UART_BASE=0xfffff200 CONFIG_DEBUG_UART_CLOCK=100000000 CONFIG_DEBUG_UART_BOARD_INIT=y CONFIG_SYS_LOAD_ADDR=0x22000000 CONFIG_DEBUG_UART=y CONFIG_BOOTDELAY=3 CONFIG_USE_BOOTARGS=y CONFIG_BOOTARGS="console=ttyS0,115200 root=/dev/mtdblock0 mtdparts=atmel_nand:-(root) rw rootfstype=jffs2" CONFIG_USE_BOOTCOMMAND=y CONFIG_BOOTCOMMAND="sf probe 0; sf read 0x22000000 0x84000 0x294000; bootm 0x22000000" CONFIG_SYS_CBSIZE=256 CONFIG_SYS_PBSIZE=281 CONFIG_SYS_CONSOLE_IS_IN_ENV=y # CONFIG_DISPLAY_BOARDINFO is not set CONFIG_HUSH_PARSER=y CONFIG_SYS_PROMPT="U-Boot> " # CONFIG_CMD_BDI is not set CONFIG_CMD_BOOTZ=y # CONFIG_CMD_IMI is not set # CONFIG_CMD_LOADS is not set CONFIG_CMD_MMC=y CONFIG_CMD_NAND=y # CONFIG_CMD_SOURCE is not set # CONFIG_CMD_SETEXPR is not set CONFIG_CMD_FAT=y CONFIG_OF_CONTROL=y CONFIG_ENV_IS_IN_SPI_FLASH=y CONFIG_ENV_SPI_MAX_HZ=15000000 CONFIG_SYS_RELOC_GD_ENV_ADDR=y # CONFIG_NET is not set CONFIG_CLK=y CONFIG_CLK_AT91=y CONFIG_AT91_GPIO=y CONFIG_GENERIC_ATMEL_MCI=y CONFIG_MTD=y CONFIG_MTD_RAW_NAND=y CONFIG_NAND_ATMEL=y CONFIG_DM_SPI_FLASH=y CONFIG_SPI_FLASH_ATMEL=y CONFIG_SPI_FLASH_DATAFLASH=y CONFIG_PINCTRL=y CONFIG_PINCTRL_AT91=y CONFIG_DM_SERIAL=y CONFIG_DEBUG_UART_ANNOUNCE=y CONFIG_ATMEL_USART=y CONFIG_SPI=y CONFIG_DM_SPI=y CONFIG_TIMER=y CONFIG_ATMEL_PIT_TIMER=y