// SPDX-License-Identifier: GPL-2.0+ /* * (C) Copyright 2001 * Erik Theisen, Wave 7 Optics, etheisen@mindspring.com. */ #ifdef USE_HOSTCC #include #endif #ifndef __ASSEMBLY__ #define __ASSEMBLY__ /* Dirty trick to get only #defines */ #endif #define __ASM_STUB_PROCESSOR_H__ /* don't include asm/processor. */ #include #undef __ASSEMBLY__ #include #include /* Handle HOSTS that have prepended crap on symbol names, not TARGETS. */ #if defined(__APPLE__) /* Leading underscore on symbols */ # define SYM_CHAR "_" #else /* No leading character on symbols */ # define SYM_CHAR #endif /* * Generate embedded environment table * inside U-Boot image, if needed. */ #if defined(ENV_IS_EMBEDDED) /* * Put the environment in the .text section when we are building * U-Boot proper. The host based program "tools/envcrc" does not need * a seperate section. */ #if defined(USE_HOSTCC) /* Native for 'tools/envcrc' */ # define __UBOOT_ENV_SECTION__(name) /*XXX DO_NOT_DEL_THIS_COMMENT*/ #else /* Environment is embedded in U-Boot's .text section */ /* XXX - This only works with GNU C */ # define __UBOOT_ENV_SECTION__(name) __attribute__ ((section(".text."#name))) #endif /* * Macros to generate global absolutes. */ #if defined(__bfin__) # define GEN_SET_VALUE(name, value) \ asm(".set " GEN_SYMNAME(name) ", " GEN_VALUE(value)) #else # define GEN_SET_VALUE(name, value) \ asm(GEN_SYMNAME(name) " = " GEN_VALUE(value)) #endif #define GEN_SYMNAME(str) SYM_CHAR #str #define GEN_VALUE(str) #str #define GEN_ABS(name, value) \ asm(".globl " GEN_SYMNAME(name)); \ GEN_SET_VALUE(name, value) /* * Check to see if we are building with a * computed CRC. Otherwise define it as ~0. */ #if !defined(ENV_CRC) # define ENV_CRC (~0) #endif #define DEFAULT_ENV_INSTANCE_EMBEDDED #include #include #ifdef CONFIG_ENV_ADDR_REDUND env_t redundand_environment __UBOOT_ENV_SECTION__(redundand_environment) = { 0, /* CRC Sum: invalid */ 0, /* Flags: invalid */ { "\0" } }; #endif /* CONFIG_ENV_ADDR_REDUND */ /* * These will end up in the .text section * if the environment strings are embedded * in the image. When this is used for * tools/envcrc, they are placed in the * .data/.sdata section. * */ unsigned long env_size __UBOOT_ENV_SECTION__(env_size) = sizeof(env_t); /* * Add in absolutes. */ GEN_ABS(env_offset, (CONFIG_ENV_ADDR - CFG_SYS_FLASH_BASE)); #endif /* ENV_IS_EMBEDDED */