/* SPDX-License-Identifier: GPL-2.0 */ #ifndef _FDT_REGION_H #define _FDT_REGION_H #ifndef SWIG /* Not available in Python */ struct fdt_region { int offset; int size; }; /* * Flags for fdt_find_regions() * * Add a region for the string table (always the last region) */ #define FDT_REG_ADD_STRING_TAB (1 << 0) /* * Add all supernodes of a matching node/property, useful for creating a * valid subset tree */ #define FDT_REG_SUPERNODES (1 << 1) /* Add the FDT_BEGIN_NODE tags of subnodes, including their names */ #define FDT_REG_DIRECT_SUBNODES (1 << 2) /* Add all subnodes of a matching node */ #define FDT_REG_ALL_SUBNODES (1 << 3) /* Add a region for the mem_rsvmap table (always the first region) */ #define FDT_REG_ADD_MEM_RSVMAP (1 << 4) /* Indicates what an fdt part is (node, property, value) */ #define FDT_IS_NODE (1 << 0) #define FDT_IS_PROP (1 << 1) #define FDT_IS_VALUE (1 << 2) /* not supported */ #define FDT_IS_COMPAT (1 << 3) /* used internally */ #define FDT_NODE_HAS_PROP (1 << 4) /* node contains prop */ #define FDT_ANY_GLOBAL (FDT_IS_NODE | FDT_IS_PROP | FDT_IS_VALUE | \ FDT_IS_COMPAT) #define FDT_IS_ANY 0x1f /* all the above */ /* We set a reasonable limit on the number of nested nodes */ #define FDT_MAX_DEPTH 32 /* Decribes what we want to include from the current tag */ enum want_t { WANT_NOTHING, WANT_NODES_ONLY, /* No properties */ WANT_NODES_AND_PROPS, /* Everything for one level */ WANT_ALL_NODES_AND_PROPS /* Everything for all levels */ }; /* Keeps track of the state at parent nodes */ struct fdt_subnode_stack { int offset; /* Offset of node */ enum want_t want; /* The 'want' value here */ int included; /* 1 if we included this node, 0 if not */ }; struct fdt_region_ptrs { int depth; /* Current tree depth */ int done; /* What we have completed scanning */ enum want_t want; /* What we are currently including */ char *end; /* Pointer to end of full node path */ int nextoffset; /* Next node offset to check */ }; /* The state of our finding algortihm */ struct fdt_region_state { struct fdt_subnode_stack stack[FDT_MAX_DEPTH]; /* node stack */ struct fdt_region *region; /* Contains list of regions found */ int count; /* Numnber of regions found */ const void *fdt; /* FDT blob */ int max_regions; /* Maximum regions to find */ int can_merge; /* 1 if we can merge with previous region */ int start; /* Start position of current region */ bool have_node; /* True if any node is included */ struct fdt_region_ptrs ptrs; /* Pointers for what we are up to */ }; /** * fdt_find_regions() - find regions in device tree * * Given a list of nodes to include and properties to exclude, find * the regions of the device tree which describe those included parts. * * The intent is to get a list of regions which will be invariant provided * those parts are invariant. For example, if you request a list of regions * for all nodes but exclude the property "data", then you will get the * same region contents regardless of any change to "data" properties. * * This function can be used to produce a byte-stream to send to a hashing * function to verify that critical parts of the FDT have not changed. * * Nodes which are given in 'inc' are included in the region list, as * are the names of the immediate subnodes nodes (but not the properties * or subnodes of those subnodes). * * For eaxample "/" means to include the root node, all root properties * and the FDT_BEGIN_NODE and FDT_END_NODE of all subnodes of /. The latter * ensures that we capture the names of the subnodes. In a hashing situation * it prevents the root node from changing at all Any change to non-excluded * properties, names of subnodes or number of subnodes would be detected. * * When used with FITs this provides the ability to hash and sign parts of * the FIT based on different configurations in the FIT. Then it is * impossible to change anything about that configuration (include images * attached to the configuration), but it may be possible to add new * configurations, new images or new signatures within the existing * framework. * * Adding new properties to a device tree may result in the string table * being extended (if the new property names are different from those * already added). This function can optionally include a region for * the string table so that this can be part of the hash too. * * The device tree header is not included in the list. * * @fdt: Device tree to check * @inc: List of node paths to included * @inc_count: Number of node paths in list * @exc_prop: List of properties names to exclude * @exc_prop_count: Number of properties in exclude list * @region: Returns list of regions * @max_region: Maximum length of region list * @path: Pointer to a temporary string for the function to use for * building path names * @path_len: Length of path, must be large enough to hold the longest * path in the tree * @add_string_tab: 1 to add a region for the string table * Return: number of regions in list. If this is >max_regions then the * region array was exhausted. You should increase max_regions and try * the call again. */ int fdt_find_regions(const void *fdt, char * const inc[], int inc_count, char * const exc_prop[], int exc_prop_count, struct fdt_region region[], int max_regions, char *path, int path_len, int add_string_tab); /** * fdt_first_region() - find regions in device tree * * Given a nodes and properties to include and properties to exclude, find * the regions of the device tree which describe those included parts. * * The use for this function is twofold. Firstly it provides a convenient * way of performing a structure-aware grep of the tree. For example it is * possible to grep for a node and get all the properties associated with * that node. Trees can be subsetted easily, by specifying the nodes that * are required, and then writing out the regions returned by this function. * This is useful for small resource-constrained systems, such as boot * loaders, which want to use an FDT but do not need to know about all of * it. * * Secondly it makes it easy to hash parts of the tree and detect changes. * The intent is to get a list of regions which will be invariant provided * those parts are invariant. For example, if you request a list of regions * for all nodes but exclude the property "data", then you will get the * same region contents regardless of any change to "data" properties. * * This function can be used to produce a byte-stream to send to a hashing * function to verify that critical parts of the FDT have not changed. * Note that semantically null changes in order could still cause false * hash misses. Such reordering might happen if the tree is regenerated * from source, and nodes are reordered (the bytes-stream will be emitted * in a different order and many hash functions will detect this). However * if an existing tree is modified using libfdt functions, such as * fdt_add_subnode() and fdt_setprop(), then this problem is avoided. * * The nodes/properties to include/exclude are defined by a function * provided by the caller. This function is called for each node and * property, and must return: * * 0 - to exclude this part * 1 - to include this part * -1 - for FDT_IS_PROP only: no information is available, so include * if its containing node is included * * The last case is only used to deal with properties. Often a property is * included if its containing node is included - this is the case where * -1 is returned.. However if the property is specifically required to be * included/excluded, then 0 or 1 can be returned. Note that including a * property when the FDT_REG_SUPERNODES flag is given will force its * containing node to be included since it is not valid to have a property * that is not in a node. * * Using the information provided, the inclusion of a node can be controlled * either by a node name or its compatible string, or any other property * that the function can determine. * * As an example, including node "/" means to include the root node and all * root properties. A flag provides a way of also including supernodes (of * which there is none for the root node), and another flag includes * immediate subnodes, so in this case we would get the FDT_BEGIN_NODE and * FDT_END_NODE of all subnodes of /. * * The subnode feature helps in a hashing situation since it prevents the * root node from changing at all. Any change to non-excluded properties, * names of subnodes or number of subnodes would be detected. * * When used with FITs this provides the ability to hash and sign parts of * the FIT based on different configurations in the FIT. Then it is * impossible to change anything about that configuration (include images * attached to the configuration), but it may be possible to add new * configurations, new images or new signatures within the existing * framework. * * Adding new properties to a device tree may result in the string table * being extended (if the new property names are different from those * already added). This function can optionally include a region for * the string table so that this can be part of the hash too. This is always * the last region. * * The FDT also has a mem_rsvmap table which can also be included, and is * always the first region if so. * * The device tree header is not included in the region list. Since the * contents of the FDT are changing (shrinking, often), the caller will need * to regenerate the header anyway. * * @fdt: Device tree to check * @h_include: Function to call to determine whether to include a part or * not: * * @priv: Private pointer as passed to fdt_find_regions() * @fdt: Pointer to FDT blob * @offset: Offset of this node / property * @type: Type of this part, FDT_IS_... * @data: Pointer to data (node name, property name, compatible * string, value (not yet supported) * @size: Size of data, or 0 if none * Return: 0 to exclude, 1 to include, -1 if no information is * available * @priv: Private pointer passed to h_include * @region: Returns list of regions, sorted by offset * @max_regions: Maximum length of region list * @path: Pointer to a temporary string for the function to use for * building path names * @path_len: Length of path, must be large enough to hold the longest * path in the tree * @flags: Various flags that control the region algortihm, see * FDT_REG_... * Return: number of regions in list. If this is >max_regions then the * region array was exhausted. You should increase max_regions and try * the call again. Only the first max_regions elements are available in the * array. * * On error a -ve value is return, which can be: * * -FDT_ERR_BADSTRUCTURE (too deep or more END tags than BEGIN tags * -FDT_ERR_BADLAYOUT * -FDT_ERR_NOSPACE (path area is too small) */ int fdt_first_region(const void *fdt, int (*h_include)(void *priv, const void *fdt, int offset, int type, const char *data, int size), void *priv, struct fdt_region *region, char *path, int path_len, int flags, struct fdt_region_state *info); /** fdt_next_region() - find next region * * See fdt_first_region() for full description. This function finds the * next region according to the provided parameters, which must be the same * as passed to fdt_first_region(). * * This function can additionally return -FDT_ERR_NOTFOUND when there are no * more regions */ int fdt_next_region(const void *fdt, int (*h_include)(void *priv, const void *fdt, int offset, int type, const char *data, int size), void *priv, struct fdt_region *region, char *path, int path_len, int flags, struct fdt_region_state *info); /** * fdt_add_alias_regions() - find aliases that point to existing regions * * Once a device tree grep is complete some of the nodes will be present * and some will have been dropped. This function checks all the alias nodes * to figure out which points point to nodes which are still present. These * aliases need to be kept, along with the nodes they reference. * * Given a list of regions function finds the aliases that still apply and * adds more regions to the list for these. This function is called after * fdt_next_region() has finished returning regions and requires the same * state. * * @fdt: Device tree file to reference * @region: List of regions that will be kept * @count: Number of regions * @max_regions: Number of entries that can fit in @region * @info: Region state as returned from fdt_next_region() * Return: new number of regions in @region (i.e. count + the number added) * or -FDT_ERR_NOSPACE if there was not enough space. */ int fdt_add_alias_regions(const void *fdt, struct fdt_region *region, int count, int max_regions, struct fdt_region_state *info); #endif /* SWIG */ #endif /* _FDT_REGION_H */