/* SPDX-License-Identifier: GPL-2.0+ */ /* * Copyright (c) 2012 The Chromium OS Authors. */ #ifndef _HASH_H #define _HASH_H #ifdef USE_HOSTCC #include #endif struct cmd_tbl; /* * Maximum digest size for all algorithms we support. Having this value * avoids a malloc() or C99 local declaration in common/cmd_hash.c. */ #if CONFIG_IS_ENABLED(SHA384) || CONFIG_IS_ENABLED(SHA512) #define HASH_MAX_DIGEST_SIZE 64 #else #define HASH_MAX_DIGEST_SIZE 32 #endif enum { HASH_FLAG_VERIFY = 1 << 0, /* Enable verify mode */ HASH_FLAG_ENV = 1 << 1, /* Allow env vars */ }; struct hash_algo { const char *name; /* Name of algorithm */ int digest_size; /* Length of digest */ /** * hash_func_ws: Generic hashing function * * This is the generic prototype for a hashing function. We only * have the watchdog version at present. * * @input: Input buffer * @ilen: Input buffer length * @output: Checksum result (length depends on algorithm) * @chunk_sz: Trigger watchdog after processing this many bytes */ void (*hash_func_ws)(const unsigned char *input, unsigned int ilen, unsigned char *output, unsigned int chunk_sz); int chunk_size; /* Watchdog chunk size */ /* * hash_init: Create the context for progressive hashing * * @algo: Pointer to the hash_algo struct * @ctxp: Pointer to the pointer of the context for hashing * @return 0 if ok, -1 on error */ int (*hash_init)(struct hash_algo *algo, void **ctxp); /* * hash_update: Perform hashing on the given buffer * * The context is freed by this function if an error occurs. * * @algo: Pointer to the hash_algo struct * @ctx: Pointer to the context for hashing * @buf: Pointer to the buffer being hashed * @size: Size of the buffer being hashed * @is_last: 1 if this is the last update; 0 otherwise * @return 0 if ok, -1 on error */ int (*hash_update)(struct hash_algo *algo, void *ctx, const void *buf, unsigned int size, int is_last); /* * hash_finish: Write the hash result to the given buffer * * The context is freed by this function. * * @algo: Pointer to the hash_algo struct * @ctx: Pointer to the context for hashing * @dest_buf: Pointer to the buffer for the result * @size: Size of the buffer for the result * @return 0 if ok, -ENOSPC if size of the result buffer is too small * or -1 on other errors */ int (*hash_finish)(struct hash_algo *algo, void *ctx, void *dest_buf, int size); }; #ifndef USE_HOSTCC /** * hash_command: Process a hash command for a particular algorithm * * This common function is used to implement specific hash commands. * * @algo_name: Hash algorithm being used (lower case!) * @flags: Flags value (HASH_FLAG_...) * @cmdtp: Pointer to command table entry * @flag: Some flags normally 0 (see CMD_FLAG_.. above) * @argc: Number of arguments (arg 0 must be the command text) * @argv: Arguments */ int hash_command(const char *algo_name, int flags, struct cmd_tbl *cmdtp, int flag, int argc, char *const argv[]); /** * hash_block() - Hash a block according to the requested algorithm * * The caller probably knows the hash length for the chosen algorithm, but * in order to provide a general interface, and output_size parameter is * provided. * * @algo_name: Hash algorithm to use * @data: Data to hash * @len: Lengh of data to hash in bytes * @output: Place to put hash value * @output_size: On entry, pointer to the number of bytes available in * output. On exit, pointer to the number of bytes used. * If NULL, then it is assumed that the caller has * allocated enough space for the hash. This is possible * since the caller is selecting the algorithm. * Return: 0 if ok, -ve on error: -EPROTONOSUPPORT for an unknown algorithm, * -ENOSPC if the output buffer is not large enough. */ int hash_block(const char *algo_name, const void *data, unsigned int len, uint8_t *output, int *output_size); #endif /* !USE_HOSTCC */ /** * hash_lookup_algo() - Look up the hash_algo struct for an algorithm * * The function returns the pointer to the struct or -EPROTONOSUPPORT if the * algorithm is not available. * * @algo_name: Hash algorithm to look up * @algop: Pointer to the hash_algo struct if found * * Return: 0 if ok, -EPROTONOSUPPORT for an unknown algorithm. */ int hash_lookup_algo(const char *algo_name, struct hash_algo **algop); /** * hash_progressive_lookup_algo() - Look up hash_algo for prog. hash support * * The function returns the pointer to the struct or -EPROTONOSUPPORT if the * algorithm is not available with progressive hash support. * * @algo_name: Hash algorithm to look up * @algop: Pointer to the hash_algo struct if found * * Return: 0 if ok, -EPROTONOSUPPORT for an unknown algorithm. */ int hash_progressive_lookup_algo(const char *algo_name, struct hash_algo **algop); /** * hash_parse_string() - Parse hash string into a binary array * * The function parses a hash string into a binary array that * can for example easily be used to compare to hash values. * * @algo_name: Hash algorithm to look up * @str: Hash string to get parsed * @result: Binary array of the parsed hash string * * Return: 0 if ok, -EPROTONOSUPPORT for an unknown algorithm. */ int hash_parse_string(const char *algo_name, const char *str, uint8_t *result); #endif