index 6d45534cf16d10ce85fdadd2ff8c7444b733a06d..5710934000f636c864f27d0e4bc5427f1cbe086e 100644 (file)
--- a/Kconfig
+++ b/Kconfig
#
mainmenu "U-Boot $(UBOOTVERSION) Configuration"
+comment "Compiler: $(CC_VERSION_TEXT)"
+
+source "scripts/Kconfig.include"
+
# Allow defaults in arch-specific code to override any given here
source "arch/Kconfig"
which is done within the script "scripts/setlocalversion".)
+config CC_IS_GCC
+ def_bool $(success,$(CC) --version | head -n 1 | grep -q gcc)
+
+config GCC_VERSION
+ int
+ default $(shell,$(srctree)/scripts/gcc-version.sh -p $(CC) | sed 's/^0*//') if CC_IS_GCC
+ default 0
+
+config CC_IS_CLANG
+ def_bool $(success,$(CC) --version | head -n 1 | grep -q clang)
+
+config CLANG_VERSION
+ int
+ default $(shell,$(srctree)/scripts/clang-version.sh $(CC))
+
+choice
+ prompt "Optimization level"
+ default CC_OPTIMIZE_FOR_SIZE
+
config CC_OPTIMIZE_FOR_SIZE
bool "Optimize for size"
- default y
help
- Enabling this option will pass "-Os" instead of "-O2" to gcc
- resulting in a smaller U-Boot image.
+ Enabling this option will pass "-Os" to gcc, resulting in a smaller
+ U-Boot image.
This option is enabled by default for U-Boot.
+config CC_OPTIMIZE_FOR_SPEED
+ bool "Optimize for speed"
+ help
+ Enabling this option will pass "-O2" to gcc, resulting in a faster
+ U-Boot image.
+
+config CC_OPTIMIZE_FOR_DEBUG
+ bool "Optimize for debugging"
+ help
+ Enabling this option will pass "-Og" to gcc, enabling optimizations
+ which don't interfere with debugging.
+
+endchoice
+
+config OPTIMIZE_INLINING
+ bool "Allow compiler to uninline functions marked 'inline' in full U-Boot"
+ help
+ This option determines if U-Boot forces gcc to inline the functions
+ developers have marked 'inline'. Doing so takes away freedom from gcc to
+ do what it thinks is best, which is desirable in some cases for size
+ reasons.
+
+config SPL_OPTIMIZE_INLINING
+ bool "Allow compiler to uninline functions marked 'inline' in SPL"
+ depends on SPL
+ help
+ This option determines if U-Boot forces gcc to inline the functions
+ developers have marked 'inline'. Doing so takes away freedom from gcc to
+ do what it thinks is best, which is desirable in some cases for size
+ reasons.
+
+config ARCH_SUPPORTS_LTO
+ bool
+
+config LTO
+ bool "Enable Link Time Optimizations"
+ depends on ARCH_SUPPORTS_LTO
+ help
+ This option enables Link Time Optimization (LTO), a mechanism which
+ allows the compiler to optimize between different compilation units.
+
+ This can optimize away dead code paths, resulting in smaller binary
+ size (if CC_OPTIMIZE_FOR_SIZE is enabled).
+
+ This option is not available for every architecture and may
+ introduce bugs.
+
+ Currently, when compiling with GCC, due to a weird bug regarding
+ jobserver, the final linking will not respect make's --jobs argument.
+ Instead all available processors will be used (as reported by the
+ nproc command).
+
+ If unsure, say n.
+
+config TPL_OPTIMIZE_INLINING
+ bool "Allow compiler to uninline functions marked 'inline' in TPL"
+ depends on TPL
+ help
+ This option determines if U-Boot forces gcc to inline the functions
+ developers have marked 'inline'. Doing so takes away freedom from gcc to
+ do what it thinks is best, which is desirable in some cases for size
+ reasons.
+
config CC_COVERAGE
bool "Enable code coverage analysis"
depends on SANDBOX
Enabling this option will pass "--coverage" to gcc to compile
and link code instrumented for coverage analysis.
-config DISTRO_DEFAULTS
- bool "Select defaults suitable for booting general purpose Linux distributions"
- select AUTO_COMPLETE
- select CMDLINE_EDITING
- select CMD_BOOTI if ARM64
- select CMD_BOOTZ if ARM && !ARM64
- select CMD_DHCP if CMD_NET
- select CMD_ENV_EXISTS
- select CMD_EXT2
- select CMD_EXT4
- select CMD_FAT
- select CMD_FS_GENERIC
- select CMD_PART if PARTITIONS
- select CMD_PING if CMD_NET
- select CMD_PXE if NET
- select CMD_SYSBOOT
- select ENV_VARS_UBOOT_CONFIG
- select HUSH_PARSER
- select SUPPORT_RAW_INITRD
- select SYS_LONGHELP
- imply CMD_MII if NET
- imply USB_STORAGE
- imply USE_BOOTCOMMAND
- help
- Select this to enable various options and commands which are suitable
- for building u-boot for booting general purpose Linux distributions.
+config ASAN
+ bool "Enable AddressSanitizer"
+ depends on SANDBOX
+ help
+ Enables AddressSanitizer to discover out-of-bounds accesses,
+ use-after-free, double-free and memory leaks.
+
+config FUZZ
+ bool "Enable fuzzing"
+ depends on CC_IS_CLANG
+ depends on DM_FUZZING_ENGINE
+ select ASAN
+ help
+ Enables the fuzzing infrastructure to generate fuzzing data and run
+ fuzz tests.
+
+config CC_HAS_ASM_INLINE
+ def_bool $(success,echo 'void foo(void) { asm inline (""); }' | $(CC) -x c - -c -o /dev/null)
+
+config XEN
+ bool "Select U-Boot be run as a bootloader for XEN Virtual Machine"
+ depends on ARM64
+ select SSCANF
+ help
+ Enabling this option will make U-Boot be run as a bootloader
+ for XEN [1] Virtual Machine.
+
+ Xen is a virtual machine monitor (VMM) or a type-1 hypervisor with support
+ for para-virtualization. Xen can organize the safe execution of several
+ virtual machines on the same physical system with performance close to
+ native. It is used as the basis for a number of different commercial and
+ open source applications, such as: server virtualization, Infrastructure
+ as a Service (IaaS), desktop virtualization, security applications,
+ embedded and hardware appliances.
+ Xen has a special VM called Domain-0 that runs the Dom0 kernel and allows
+ Xen to use the device drivers for the Domain-0 kernel by default.
+
+ [1] - https://xenproject.org/
config ENV_VARS_UBOOT_CONFIG
bool "Add arch, board, vendor and soc variables to default environment"
Enables allocating and saving kernel cmdline in space between
"bootm_low" and "bootm_low" + BOOTMAPSZ.
+config SYS_BARGSIZE
+ int "Size of kernel command line buffer in bytes"
+ depends on SYS_BOOT_GET_CMDLINE
+ default 512
+ help
+ Buffer size for Boot Arguments which are passed to the application
+ (usually a Linux kernel) when it is booted
+
config SYS_BOOT_GET_KBD
bool "Enable kernel board information setup"
help
Enables allocating and saving a kernel copy of the bd_info in
space between "bootm_low" and "bootm_low" + BOOTMAPSZ.
+config HAS_CUSTOM_SYS_INIT_SP_ADDR
+ bool "Use a custom location for the initial stack pointer address"
+ depends on ARC || (ARM && !INIT_SP_RELATIVE) || MIPS || PPC || RISCV
+ default y if TFABOOT
+ help
+ Typically, we use an initial stack pointer address that is calculated
+ by taking the statically defined CFG_SYS_INIT_RAM_ADDR, adding the
+ statically defined CFG_SYS_INIT_RAM_SIZE and then subtracting the
+ build-time constant of GENERATED_GBL_DATA_SIZE. On MIPS a different
+ but statica calculation is performed. However, some platforms will
+ take a different approach. Say Y here to define the address statically
+ instead.
+
+config CUSTOM_SYS_INIT_SP_ADDR
+ hex "Static location for the initial stack pointer"
+ depends on HAS_CUSTOM_SYS_INIT_SP_ADDR
+ default TEXT_BASE if TFABOOT
+
config SYS_MALLOC_F
bool "Enable malloc() pool before relocation"
default y if DM
config SYS_MALLOC_F_LEN
hex "Size of malloc() pool before relocation"
depends on SYS_MALLOC_F
- default 0x1000 if AM33XX
- default 0x2800 if SANDBOX
- default 0x2000 if (ARCH_IMX8 || ARCH_IMX8M || ARCH_MX7 || \
- ARCH_MX7ULP || ARCH_MX6 || ARCH_MX5 || \
- ARCH_LS1012A || ARCH_LS1021A || ARCH_LS1043A || \
- ARCH_LS1046A || ARCH_QEMU)
- default 0x400
- help
- Before relocation, memory is very limited on many platforms. Still,
- we can provide a small malloc() pool if needed. Driver model in
- particular needs this to operate, so that it can allocate the
- initial serial device and any others that are needed.
+ default 0x400 if M68K || PPC || ROCKCHIP_PX30 || ROCKCHIP_RK3036 || \
+ ROCKCHIP_RK3308 || ROCKCHIP_RV1108
+ default 0x600 if ARCH_ZYNQMP_R5 || ARCH_ZYNQMP
+ default 0x800 if ARCH_ZYNQ || ROCKCHIP_RK3128 || ROCKCHIP_RK3188 || \
+ ROCKCHIP_RK322X || X86
+ default 0x1000 if ARCH_MESON || ARCH_BMIPS || ARCH_MTMIPS
+ default 0x1800 if ARCH_TEGRA
+ default 0x4000 if SANDBOX || RISCV || ARCH_APPLE || ROCKCHIP_RK3368 || \
+ ROCKCHIP_RK3399
+ default 0x8000 if RCAR_GEN3
+ default 0x10000 if ARCH_IMX8 || ARCH_IMX8M
+ default 0x2000
+ help
+ Size of the malloc() pool for use before relocation. If
+ this is defined, then a very simple malloc() implementation
+ will become available before relocation. The address is just
+ below the global data, and the stack is moved down to make
+ space.
+
+ This feature allocates regions with increasing addresses
+ within the region. calloc() is supported, but realloc()
+ is not available. free() is supported but does nothing.
+ The memory will be freed (or in fact just forgotten) when
+ U-Boot relocates itself.
config SYS_MALLOC_LEN
hex "Define memory for Dynamic allocation"
- depends on ARCH_ZYNQ || ARCH_VERSAL || ARCH_STM32MP || ARCH_ROCKCHIP
- default 0x2000000 if ARCH_ROCKCHIP
+ default 0x4000000 if SANDBOX
+ default 0x2000000 if ARCH_ROCKCHIP || ARCH_OMAP2PLUS || ARCH_MESON
+ default 0x200000 if ARCH_BMIPS || X86
+ default 0x4020000 if SUNXI_MINIMUM_DRAM_MB >= 256
+ default 0x220000 if SUNXI_MINIMUM_DRAM_MB >= 64
+ default 0x120000 if SUNXI_MINIMUM_DRAM_MB >= 32
+ default 0x400000
help
This defines memory to be allocated for Dynamic allocation
TODO: Use for other architectures
+config SPL_SYS_MALLOC_F
+ bool "Enable malloc() pool in SPL"
+ depends on SPL_FRAMEWORK && SYS_MALLOC_F && SPL
+ default y
+ help
+ In SPL memory is very limited on many platforms. Still,
+ we can provide a small malloc() pool if needed. Driver model in
+ particular needs this to operate, so that it can allocate the
+ initial serial device and any others that are needed.
+
config SPL_SYS_MALLOC_F_LEN
- hex "Size of malloc() pool in SPL before relocation"
- depends on SYS_MALLOC_F && SPL
+ hex "Size of malloc() pool in SPL"
+ depends on SPL_SYS_MALLOC_F
default 0x2800 if RCAR_GEN3
+ default 0x2000 if IMX8MQ
default SYS_MALLOC_F_LEN
help
- Before relocation, memory is very limited on many platforms. Still,
+ Sets the size of the malloc() pool in SPL. This is used for
+ driver model and other features, which must allocate memory for
+ data structures.
+
+ It is possible to enable CFG_SPL_SYS_MALLOC_START to start a new
+ malloc() region in SDRAM once it is inited.
+
+config TPL_SYS_MALLOC_F
+ bool "Enable malloc() pool in TPL"
+ depends on SYS_MALLOC_F && TPL
+ default y if SPL_SYS_MALLOC_F
+ help
+ In TPL memory is very limited on many platforms. Still,
we can provide a small malloc() pool if needed. Driver model in
particular needs this to operate, so that it can allocate the
initial serial device and any others that are needed.
config TPL_SYS_MALLOC_F_LEN
- hex "Size of malloc() pool in TPL before relocation"
- depends on SYS_MALLOC_F && TPL
- default SYS_MALLOC_F_LEN
- help
- Before relocation, memory is very limited on many platforms. Still,
+ hex "Size of malloc() pool in TPL"
+ depends on TPL_SYS_MALLOC_F
+ default SPL_SYS_MALLOC_F_LEN
+ help
+ Sets the size of the malloc() pool in TPL. This is used for
+ driver model and other features, which must allocate memory for
+ data structures.
+
+config VALGRIND
+ bool "Inform valgrind about memory allocations"
+ depends on !RISCV
+ help
+ Valgrind is an instrumentation framework for building dynamic analysis
+ tools. In particular, it may be used to detect memory management bugs
+ in U-Boot. It relies on knowing when heap blocks are allocated in
+ order to give accurate results. This happens automatically for
+ standard allocator functions provided by the host OS. However, this
+ doesn't automatically happen for U-Boot's malloc implementation.
+
+ Enable this option to annotate U-Boot's malloc implementation so that
+ it can be handled accurately by Valgrind. If you aren't planning on
+ using valgrind to debug U-Boot, say 'n'.
+
+config VPL_SYS_MALLOC_F
+ bool "Enable malloc() pool in VPL"
+ depends on SYS_MALLOC_F && VPL
+ default y if SPL_SYS_MALLOC_F
+ help
+ In VPL memory is very limited on many platforms. Still,
we can provide a small malloc() pool if needed. Driver model in
particular needs this to operate, so that it can allocate the
initial serial device and any others that are needed.
+config VPL_SYS_MALLOC_F_LEN
+ hex "Size of malloc() pool in VPL before relocation"
+ depends on VPL_SYS_MALLOC_F
+ default SPL_SYS_MALLOC_F_LEN
+ help
+ Sets the size of the malloc() pool in VPL. This is used for
+ driver model and other features, which must allocate memory for
+ data structures.
+
menuconfig EXPERT
bool "Configure standard U-Boot features (expert users)"
default y
When disabling this, please check if malloc calls, maybe
should be replaced by calloc - if one expects zeroed memory.
+config SPL_SYS_MALLOC_CLEAR_ON_INIT
+ bool "Init with zeros the memory reserved for malloc (slow) in SPL"
+ depends on SPL
+ default SYS_MALLOC_CLEAR_ON_INIT
+ help
+ Same as SYS_MALLOC_CLEAR_ON_INIT, but for SPL. It's possible to
+ Enable it without SYS_MALLOC_CLEAR_ON_INIT. It's useful for boards
+ that must have particular memory regions zero'ed before first use.
+ If SYS_SPL_MALLOC_START is configured to be in such region, this
+ option should be enabled.
+
config SYS_MALLOC_DEFAULT_TO_INIT
bool "Default malloc to init while reserving the memory for it"
- default n
help
It may happen that one needs to move the dynamic allocation
from one to another memory range, eg. when moving the malloc
config PHYS_64BIT
bool "64bit physical address support"
+ select FDT_64BIT
help
Say Y here to support 64bit physical memory address.
This can be used not only for 64bit SoCs, but also for
large physical address extension on 32bit SoCs.
-config BUILD_ROM
- bool "Build U-Boot as BIOS replacement"
- depends on X86
+config FDT_64BIT
+ bool "64bit fdt address support"
+ help
+ Say Y here to support 64bit fdt addresses.
+ This can be used not only for 64bit SoCs, but also
+ for large address extensions on 32bit SoCs.
+
+config HAS_ROM
+ bool
+ select BINMAN
help
- This option allows to build a ROM version of U-Boot.
- The build process generally requires several binary blobs
- which are not shipped in the U-Boot source tree.
- Please, see doc/arch/x86.rst for details.
+ Enables building of a u-boot.rom target. This collects U-Boot and
+ any necessary binary blobs.
config SPL_IMAGE
string "SPL image used in the combined SPL+U-Boot image"
used to generate a combined image with SPL and main U-Boot
proper as one single image.
+config REMAKE_ELF
+ bool "Recreate an ELF image from raw U-Boot binary"
+ help
+ Enable this to recreate an ELF image (u-boot.elf) from the raw
+ U-Boot binary (u-boot.bin), which may already have been statically
+ relocated and may already have a device-tree appended to it.
+
config BUILD_TARGET
string "Build target special images"
- default "u-boot-with-spl.sfp" if TARGET_SOCFPGA_ARRIA10
- default "u-boot-with-spl.sfp" if TARGET_SOCFPGA_GEN5
- default "u-boot-spl.kwb" if ARCH_MVEBU && SPL
- default "u-boot-elf.srec" if RCAR_GEN3
- default "u-boot.itb" if SPL_LOAD_FIT && (ARCH_ROCKCHIP || \
- ARCH_SUNXI || RISCV || ARCH_ZYNQMP)
- default "u-boot.kwb" if ARCH_KIRKWOOD
+ default "u-boot-elf.srec" if RCAR_64
default "u-boot-with-spl.bin" if ARCH_AT91 && SPL_NAND_SUPPORT
+ default "u-boot-with-spl.bin" if MPC85xx && !E500MC && !E5500 && !E6500 && SPL
default "u-boot-with-spl.imx" if ARCH_MX6 && SPL
+ default "u-boot-with-spl.kwb" if ARMADA_32BIT && SPL
+ default "u-boot-with-spl.sfp" if TARGET_SOCFPGA_ARRIA10
+ default "u-boot-with-spl.sfp" if TARGET_SOCFPGA_GEN5
+ default "u-boot.itb" if !BINMAN && SPL_LOAD_FIT && (ARCH_ROCKCHIP || \
+ RISCV || ARCH_ZYNQMP)
+ default "u-boot.kwb" if (ARCH_KIRKWOOD || ARMADA_32BIT) && !SPL
help
Some SoCs need special image types (e.g. U-Boot binary
with a special header) as build targets. By defining
special image will be automatically built upon calling
make / buildman.
+config HAS_BOARD_SIZE_LIMIT
+ bool "Define a maximum size for the U-Boot image"
+ default y if RCAR_32 || RCAR_64
+ help
+ In some cases, we need to enforce a hard limit on how big the U-Boot
+ image itself can be.
+
+config BOARD_SIZE_LIMIT
+ int "Maximum size of the U-Boot image in bytes"
+ default 524288 if RCAR_32
+ default 1048576 if RCAR_64
+ depends on HAS_BOARD_SIZE_LIMIT
+ help
+ Maximum size of the U-Boot image. When defined, the build system
+ checks that the actual size does not exceed it. This does not
+ include SPL nor TPL, on platforms that use that functionality, they
+ have a separate option to restict size.
+
config SYS_CUSTOM_LDSCRIPT
bool "Use a custom location for the U-Boot linker script"
help
Path within the source tree to the linker script to use for the
main U-Boot binary.
+config SYS_LOAD_ADDR
+ hex "Address in memory to use by default"
+ default 0x01000000 if ARCH_SOCFPGA
+ default 0x02000000 if PPC || X86
+ default 0x81000000 if MACH_SUNIV
+ default 0x22000000 if MACH_SUN9I
+ default 0x42000000 if ARCH_SUNXI
+ default 0x82000000 if ARCH_KEYSTONE || ARCH_OMAP2PLUS || ARCH_K3
+ default 0x82000000 if ARCH_MX6 && (MX6SL || MX6SLL || MX6SX || MX6UL || MX6ULL)
+ default 0x12000000 if ARCH_MX6 && !(MX6SL || MX6SLL || MX6SX || MX6UL || MX6ULL)
+ default 0x80800000 if ARCH_MX7
+ default 0x90000000 if FSL_LSCH2 || FSL_LSCH3
+ help
+ Address in memory to use as the default safe load address.
+
config ERR_PTR_OFFSET
hex
default 0x0
default "__start" if MIPS
default "_start"
-endmenu # General setup
-
-menu "Boot images"
+config STACK_SIZE
+ hex "Define max stack size that can be used by U-Boot"
+ default 0x4000000 if ARCH_VERSAL_NET || ARCH_VERSAL || ARCH_ZYNQMP
+ default 0x200000 if MICROBLAZE
+ default 0x1000000
+ help
+ Define Max stack size that can be used by U-Boot. This value is used
+ by the UEFI sub-system. On some boards initrd_high is calculated as
+ base stack pointer minus this stack size.
-config ANDROID_BOOT_IMAGE
- bool "Enable support for Android Boot Images"
- default y if FASTBOOT
+config SYS_MEM_TOP_HIDE
+ hex "Exclude some memory from U-Boot / OS information"
+ default 0x0
help
- This enables support for booting images which use the Android
- image format header.
+ If set, this specified memory area will get subtracted from the top
+ (end) of RAM and won't get "touched" at all by U-Boot. By fixing up
+ gd->ram_size the OS / next stage should gets passed the now
+ "corrected" memory size and won't touch it either.
+ WARNING: Please make sure that this value is a multiple of the OS
+ page size.
-config FIT
- bool "Support Flattened Image Tree"
- select MD5
- select SHA1
+config SYS_HAS_SRAM
+ bool
+ default y if TARGET_PIC32MZDASK
+ default y if TARGET_DEVKIT8000
+ default y if TARGET_TRICORDER
help
- This option allows you to boot the new uImage structure,
- Flattened Image Tree. FIT is formally a FDT, which can include
- images of various types (kernel, FDT blob, ramdisk, etc.)
- in a single blob. To boot this new uImage structure,
- pass the address of the blob to the "bootm" command.
- FIT is very flexible, supporting compression, multiple images,
- multiple configurations, verification through hashing and also
- verified boot (secure boot using RSA).
+ Enable this to allow support for the on board SRAM.
+ SRAM base address is controlled by CONFIG_SYS_SRAM_BASE.
+ SRAM size is controlled by CONFIG_SYS_SRAM_SIZE.
-if FIT
+config SYS_SRAM_BASE
+ hex
+ default 0x80000000 if TARGET_PIC32MZDASK
+ default 0x40200000 if TARGET_DEVKIT8000
+ default 0x40200000 if TARGET_TRICORDER
+ default 0x0
-config FIT_EXTERNAL_OFFSET
- hex "FIT external data offset"
+config SYS_SRAM_SIZE
+ hex
+ default 0x00080000 if TARGET_PIC32MZDASK
+ default 0x10000 if TARGET_DEVKIT8000
+ default 0x10000 if TARGET_TRICORDER
default 0x0
+
+config SYS_MONITOR_LEN
+ int "Maximum size in bytes reserved for U-Boot in memory"
+ default 1048576 if X86
+ default 786432 if ARCH_SUNXI
+ default 0
help
- This specifies a data offset in fit image.
- The offset is from data payload offset to the beginning of
- fit image header. When specifies a offset, specific data
- could be put in the hole between data payload and fit image
- header, such as CSF data on i.MX platform.
+ Size of memory reserved for monitor code, used to determine
+ _at_compile_time_ (!) if the environment is embedded within the
+ U-Boot image, or in a separate flash sector, among other uses where
+ we need to set a maximum size of the U-Boot binary itself that will
+ be loaded.
-config FIT_ENABLE_SHA256_SUPPORT
- bool "Support SHA256 checksum of FIT image contents"
- default y
- select SHA256
- help
- Enable this to support SHA256 checksum of FIT image contents. A
- SHA256 checksum is a 256-bit (32-byte) hash value used to check that
- the image contents have not been corrupted.
-
-config FIT_ENABLE_SHA384_SUPPORT
- bool "Support SHA384 checksum of FIT image contents"
- default n
- select SHA384
- help
- Enable this to support SHA384 checksum of FIT image contents. A
- SHA384 checksum is a 384-bit (48-byte) hash value used to check that
- the image contents have not been corrupted. Use this for the highest
- security.
-
-config FIT_ENABLE_SHA512_SUPPORT
- bool "Support SHA512 checksum of FIT image contents"
- default n
- select SHA512
- help
- Enable this to support SHA512 checksum of FIT image contents. A
- SHA512 checksum is a 512-bit (64-byte) hash value used to check that
- the image contents have not been corrupted.
-
-config FIT_SIGNATURE
- bool "Enable signature verification of FIT uImages"
- depends on DM
- select HASH
- select RSA
- select RSA_VERIFY
- select IMAGE_SIGN_INFO
- help
- This option enables signature verification of FIT uImages,
- using a hash signed and verified using RSA. If
- CONFIG_SHA_PROG_HW_ACCEL is defined, i.e support for progressive
- hashing is available using hardware, then the RSA library will use
- it. See doc/uImage.FIT/signature.txt for more details.
-
- WARNING: When relying on signed FIT images with a required signature
- check the legacy image format is disabled by default, so that
- unsigned images cannot be loaded. If a board needs the legacy image
- format support in this case, enable it using
- CONFIG_LEGACY_IMAGE_FORMAT.
-
-config FIT_SIGNATURE_MAX_SIZE
- hex "Max size of signed FIT structures"
- depends on FIT_SIGNATURE
- default 0x10000000
- help
- This option sets a max size in bytes for verified FIT uImages.
- A sane value of 256MB protects corrupted DTB structures from overlapping
- device memory. Assure this size does not extend past expected storage
- space.
-
-config FIT_ENABLE_RSASSA_PSS_SUPPORT
- bool "Support rsassa-pss signature scheme of FIT image contents"
- depends on FIT_SIGNATURE
- default n
- help
- Enable this to support the pss padding algorithm as described
- in the rfc8017 (https://tools.ietf.org/html/rfc8017).
-
-config FIT_CIPHER
- bool "Enable ciphering data in a FIT uImages"
- depends on DM
- select AES
- help
- Enable the feature of data ciphering/unciphering in the tool mkimage
- and in the u-boot support of the FIT image.
-
-config FIT_VERBOSE
- bool "Show verbose messages when FIT images fail"
- help
- Generally a system will have valid FIT images so debug messages
- are a waste of code space. If you are debugging your images then
- you can enable this option to get more verbose information about
- failures.
-
-config FIT_BEST_MATCH
- bool "Select the best match for the kernel device tree"
- help
- When no configuration is explicitly selected, default to the
- one whose fdt's compatibility field best matches that of
- U-Boot itself. A match is considered "best" if it matches the
- most specific compatibility entry of U-Boot's fdt's root node.
- The order of entries in the configuration's fdt is ignored.
-
-config FIT_IMAGE_POST_PROCESS
- bool "Enable post-processing of FIT artifacts after loading by U-Boot"
- depends on TI_SECURE_DEVICE
- help
- Allows doing any sort of manipulation to blobs after they got extracted
- from FIT images like stripping off headers or modifying the size of the
- blob, verification, authentication, decryption etc. in a platform or
- board specific way. In order to use this feature a platform or board-
- specific implementation of board_fit_image_post_process() must be
- provided. Also, anything done during this post-processing step would
- need to be comprehended in how the images were prepared before being
- injected into the FIT creation (i.e. the blobs would have been pre-
- processed before being added to the FIT image).
-
-if SPL
-
-config SPL_FIT
- bool "Support Flattened Image Tree within SPL"
- depends on SPL
- select SPL_OF_LIBFDT
-
-config SPL_FIT_PRINT
- bool "Support FIT printing within SPL"
- depends on SPL_FIT
- help
- Support printing the content of the fitImage in a verbose manner in SPL.
-
-config SPL_FIT_SIGNATURE
- bool "Enable signature verification of FIT firmware within SPL"
- depends on SPL_DM
- select SPL_FIT
- select SPL_RSA
- select SPL_RSA_VERIFY
- select SPL_IMAGE_SIGN_INFO
-
-config SPL_LOAD_FIT
- bool "Enable SPL loading U-Boot as a FIT (basic fitImage features)"
- select SPL_FIT
- help
- Normally with the SPL framework a legacy image is generated as part
- of the build. This contains U-Boot along with information as to
- where it should be loaded. This option instead enables generation
- of a FIT (Flat Image Tree) which provides more flexibility. In
- particular it can handle selecting from multiple device tree
- and passing the correct one to U-Boot.
-
-config SPL_LOAD_FIT_APPLY_OVERLAY
- bool "Enable SPL applying DT overlays from FIT"
- depends on SPL_LOAD_FIT
- select OF_LIBFDT_OVERLAY
- help
- The device tree is loaded from the FIT image. Allow the SPL is to
- also load device-tree overlays from the FIT image an apply them
- over the device tree.
-
-config SPL_LOAD_FIT_APPLY_OVERLAY_BUF_SZ
- depends on SPL_LOAD_FIT_APPLY_OVERLAY
- default 0x10000
- hex "size of temporary buffer used to load the overlays"
- help
- The size of the area where the overlays will be loaded and
- uncompress. Must be at least as large as biggest overlay
- (uncompressed)
-
-config SPL_LOAD_FIT_FULL
- bool "Enable SPL loading U-Boot as a FIT (full fitImage features)"
- select SPL_FIT
- help
- Normally with the SPL framework a legacy image is generated as part
- of the build. This contains U-Boot along with information as to
- where it should be loaded. This option instead enables generation
- of a FIT (Flat Image Tree) which provides more flexibility. In
- particular it can handle selecting from multiple device tree
- and passing the correct one to U-Boot.
-
-config SPL_FIT_IMAGE_POST_PROCESS
- bool "Enable post-processing of FIT artifacts after loading by the SPL"
- depends on SPL_LOAD_FIT
- help
- Allows doing any sort of manipulation to blobs after they got extracted
- from the U-Boot FIT image like stripping off headers or modifying the
- size of the blob, verification, authentication, decryption etc. in a
- platform or board specific way. In order to use this feature a platform
- or board-specific implementation of board_fit_image_post_process() must
- be provided. Also, anything done during this post-processing step would
- need to be comprehended in how the images were prepared before being
- injected into the FIT creation (i.e. the blobs would have been pre-
- processed before being added to the FIT image).
-
-config SPL_FIT_SOURCE
- string ".its source file for U-Boot FIT image"
- depends on SPL_FIT
- help
- Specifies a (platform specific) FIT source file to generate the
- U-Boot FIT image. This could specify further image to load and/or
- execute.
-
-config SPL_FIT_GENERATOR
- string ".its file generator script for U-Boot FIT image"
- depends on SPL_FIT
- default "board/sunxi/mksunxi_fit_atf.sh" if SPL_LOAD_FIT && ARCH_SUNXI
- default "arch/arm/mach-rockchip/make_fit_atf.py" if SPL_LOAD_FIT && ARCH_ROCKCHIP
- default "arch/arm/mach-zynqmp/mkimage_fit_atf.sh" if SPL_LOAD_FIT && ARCH_ZYNQMP
- default "arch/riscv/lib/mkimage_fit_opensbi.sh" if SPL_LOAD_FIT && RISCV
- help
- Specifies a (platform specific) script file to generate the FIT
- source file used to build the U-Boot FIT image file. This gets
- passed a list of supported device tree file stub names to
- include in the generated image.
-
-endif # SPL
-
-endif # FIT
-
-config LEGACY_IMAGE_FORMAT
- bool "Enable support for the legacy image format"
- default y if !FIT_SIGNATURE
- help
- This option enables the legacy image format. It is enabled by
- default for backward compatibility, unless FIT_SIGNATURE is
- set where it is disabled so that unsigned images cannot be
- loaded. If a board needs the legacy image format support in this
- case, enable it here.
-
-config OF_BOARD_SETUP
- bool "Set up board-specific details in device tree before boot"
- depends on OF_LIBFDT
- help
- This causes U-Boot to call ft_board_setup() before booting into
- the Operating System. This function can set up various
- board-specific information in the device tree for use by the OS.
- The device tree is then passed to the OS.
-
-config OF_SYSTEM_SETUP
- bool "Set up system-specific details in device tree before boot"
- depends on OF_LIBFDT
- help
- This causes U-Boot to call ft_system_setup() before booting into
- the Operating System. This function can set up various
- system-specific information in the device tree for use by the OS.
- The device tree is then passed to the OS.
-
-config OF_STDOUT_VIA_ALIAS
- bool "Update the device-tree stdout alias from U-Boot"
- depends on OF_LIBFDT
- help
- This uses U-Boot's serial alias from the aliases node to update
- the device tree passed to the OS. The "linux,stdout-path" property
- in the chosen node is set to point to the correct serial node.
- This option currently references CONFIG_CONS_INDEX, which is
- incorrect when used with device tree as this option does not
- exist / should not be used.
-
-config SYS_EXTRA_OPTIONS
- string "Extra Options (DEPRECATED)"
- help
- The old configuration infrastructure (= mkconfig + boards.cfg)
- provided the extra options field. If you have something like
- "HAS_BAR,BAZ=64", the optional options
- #define CONFIG_HAS
- #define CONFIG_BAZ 64
- will be defined in include/config.h.
- This option was prepared for the smooth migration from the old
- configuration to Kconfig. Since this option will be removed sometime,
- new boards should not use this option.
-
-config HAVE_SYS_TEXT_BASE
+config MP
+ bool "Support for multiprocessor"
+ help
+ This provides an option to bringup different processors
+ in multiprocessor cases.
+
+config HAVE_TEXT_BASE
bool
depends on !NIOS2 && !XTENSA
depends on !EFI_APP
default y
-config SYS_TEXT_BASE
- depends on HAVE_SYS_TEXT_BASE
+config TEXT_BASE
+ depends on HAVE_TEXT_BASE
+ default 0x0 if POSITION_INDEPENDENT
default 0x80800000 if ARCH_OMAP2PLUS || ARCH_K3
- default 0x4a000000 if ARCH_SUNXI && !MACH_SUN9I && !MACH_SUN8I_V3S
- default 0x2a000000 if ARCH_SUNXI && MACH_SUN9I
- default 0x42e00000 if ARCH_SUNXI && MACH_SUN8I_V3S
+ default 0x81700000 if MACH_SUNIV
+ default 0x2a000000 if MACH_SUN9I
+ default 0x4a000000 if SUNXI_MINIMUM_DRAM_MB >= 256
+ default 0x42e00000 if SUNXI_MINIMUM_DRAM_MB >= 64
hex "Text Base"
help
- The address in memory that U-Boot will be running from, initially.
+ The address in memory that U-Boot will be copied and executed from
+ initially.
-config SYS_CLK_FREQ
- depends on ARC || ARCH_SUNXI || MPC83xx
- int "CPU clock frequency"
+config HAVE_SYS_UBOOT_START
+ bool "Use custom U-Boot Start"
+ depends on HAVE_TEXT_BASE
+ help
+ By default, the address in memory that U-Boot will be copied from
+ (TEXT_BASE) and the entry point are the same. Select this to start the
+ execution of U-Boot from a different address.
+ This may be required if a header or vector table needs to be copied
+ but not executed.
+
+config SYS_UBOOT_START
+ hex
+ depends on HAVE_TEXT_BASE
+ default TEXT_BASE
+ prompt "U-Boot entry" if HAVE_SYS_UBOOT_START
help
- TODO: Move CONFIG_SYS_CLK_FREQ for all the architecture
+ If TEXT_BASE differs from the start of execution, this sets the
+ address in memory that U-Boot will start execution from initially.
-config ARCH_FIXUP_FDT_MEMORY
- bool "Enable arch_fixup_memory_banks() call"
+config HAVE_SYS_MONITOR_BASE
+ bool
+ depends on ARC || MIPS || M68K || NIOS2 || PPC || XTENSA || X86 \
+ || ENV_IS_IN_FLASH || MTD_NOR_FLASH
+ depends on !EFI_APP
default y
+
+config SYS_MONITOR_BASE
+ depends on HAVE_SYS_MONITOR_BASE
+ hex "Physical start address of boot monitor code"
+ default TEXT_BASE
+ help
+ The physical start address of boot monitor code (which is the same as
+ CONFIG_TEXT_BASE when linking) and the same as CFG_SYS_FLASH_BASE
+ when booting from flash.
+
+config SPL_SYS_MONITOR_BASE
+ depends on MPC85xx && SPL && HAVE_SYS_MONITOR_BASE
+ hex "Physical start address of SPL monitor code"
+ default SPL_TEXT_BASE
+
+config TPL_SYS_MONITOR_BASE
+ depends on MPC85xx && TPL && HAVE_SYS_MONITOR_BASE
+ hex "Physical start address of TPL monitor code"
+
+config DYNAMIC_SYS_CLK_FREQ
+ bool "Determine CPU clock frequency at run-time"
help
- Enable FDT memory map syncup before OS boot. This feature can be
- used for booting OS with different memory setup where the part of
- the memory location should be used for different purpose.
+ Implement a get_board_sys_clk function that will determine the CPU
+ clock frequency at run time, rather than define it statically.
-endmenu # Boot images
+config SYS_CLK_FREQ
+ depends on !DYNAMIC_SYS_CLK_FREQ
+ int "CPU clock frequency"
+ default 125000000 if ARCH_LS1012A
+ default 100000000 if ARCH_P2020 || ARCH_T1024 || ARCH_T1042 || \
+ ARCH_LS1021A || FSL_LSCH2 || FSL_LSCH3
+ default 66666666 if ARCH_P1010 || ARCH_P1020 || ARCH_T4240
+ default 66660000 if ARCH_T2080
+ default 33333333 if RCAR_GEN3
+ default 24000000 if ARCH_EXYNOS
+ default 20000000 if RCAR_GEN2
+ default 0
+ help
+ A static value for the CPU frequency. Note that if not required
+ for a given SoC, this can be left at 0.
source "api/Kconfig"
+endmenu # General setup
+
+source "boot/Kconfig"
+
source "common/Kconfig"
source "cmd/Kconfig"
source "lib/Kconfig"
source "test/Kconfig"
+
+source "tools/Kconfig"