summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 84b2cd7)
raw | patch | inline | side by side (parent: 84b2cd7)
author | Andre Przywara <andre.przywara@arm.com> | |
Mon, 12 Apr 2021 00:04:51 +0000 (01:04 +0100) | ||
committer | Tom Rini <trini@konsulko.com> | |
Tue, 20 Apr 2021 11:31:12 +0000 (07:31 -0400) |
All Calxeda machines are actually a poster book example of device tree
usage: the DT is loaded from flash by the management processor into
DRAM, the memory node is populated with the detected DRAM size and this
DT is then handed over to the kernel.
So it's a shame that U-Boot didn't participate in this chain, but
fortunately this is easy to fix:
Define CONFIG_OF_CONTROL and CONFIG_OF_BOARD, and provide a trivial
function to tell U-Boot about the (fixed) location of the DTB in DRAM.
Then enable DM_SERIAL, to let the PL011 driver pick up the UART platform
data from the DT. Also define AHCI, to bring this driver into the driver
model world as well.
Signed-off-by: Andre Przywara <andre.przywara@arm.com>
usage: the DT is loaded from flash by the management processor into
DRAM, the memory node is populated with the detected DRAM size and this
DT is then handed over to the kernel.
So it's a shame that U-Boot didn't participate in this chain, but
fortunately this is easy to fix:
Define CONFIG_OF_CONTROL and CONFIG_OF_BOARD, and provide a trivial
function to tell U-Boot about the (fixed) location of the DTB in DRAM.
Then enable DM_SERIAL, to let the PL011 driver pick up the UART platform
data from the DT. Also define AHCI, to bring this driver into the driver
model world as well.
Signed-off-by: Andre Przywara <andre.przywara@arm.com>
arch/arm/Kconfig | patch | blob | history | |
board/highbank/highbank.c | patch | blob | history | |
configs/highbank_defconfig | patch | blob | history | |
include/configs/highbank.h | patch | blob | history |
diff --git a/arch/arm/Kconfig b/arch/arm/Kconfig
index 15b845449dbb05c87ba297b174ed4dde555da43c..358642669c70344bd6d4da91899e5ea3dc105232 100644 (file)
--- a/arch/arm/Kconfig
+++ b/arch/arm/Kconfig
config ARCH_HIGHBANK
bool "Calxeda Highbank"
select CPU_V7A
- select PL011_SERIAL
+ select PL01X_SERIAL
+ select DM
+ select DM_SERIAL
+ select OF_CONTROL
+ select OF_BOARD
+ select CLK
+ select CLK_CCF
+ select AHCI
config ARCH_INTEGRATOR
bool "ARM Ltd. Integrator family"
index 906bd9b6dda56ba783d92cc025a4b5c1919634ca..2e2300a307f148ae0c622535b4face80ddd27013 100644 (file)
}
#endif
+void *board_fdt_blob_setup(void)
+{
+ /*
+ * The ECME management processor loads the DTB from NOR flash
+ * into DRAM (at 4KB), where it gets patched to contain the
+ * detected memory size.
+ */
+ return (void *)0x1000;
+}
+
static int is_highbank(void)
{
uint32_t midr;
index 369b65ceee880fd461e460273eeacb623564898f..773ed7a00bf09f9cdb01ea93c8e2b25aa4ccb4e9 100644 (file)
CONFIG_SCSI=y
CONFIG_CONS_INDEX=0
CONFIG_OF_LIBFDT=y
+CONFIG_OF_BOARD=y
index 5e3cc3a1db61b82d87527328f6be26c70d59b29c..7f37c81fc9f1c3cebd27d8261f5773bf10ebb437 100644 (file)
#define CONFIG_SYS_MALLOC_LEN (512 * 1024)
#define CONFIG_PL011_CLOCK 150000000
-#define CONFIG_PL01x_PORTS { (void *)(0xFFF36000) }
#define CONFIG_SYS_BOOTCOUNT_LE /* Use little-endian accessors */