summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 035e405)
raw | patch | inline | side by side (parent: 035e405)
author | Simon Glass <sjg@chromium.org> | |
Mon, 15 Mar 2021 04:25:43 +0000 (17:25 +1300) | ||
committer | Simon Glass <sjg@chromium.org> | |
Fri, 26 Mar 2021 04:03:09 +0000 (17:03 +1300) |
Add a description of the new features, along with internal technical
documentation.
Signed-off-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Simon Glass <sjg@chromium.org>
documentation.
Signed-off-by: Simon Glass <sjg@chromium.org>
Signed-off-by: Simon Glass <sjg@chromium.org>
doc/driver-model/of-plat.rst | patch | blob | history |
index 3c9ba01b3020204c21820d4e86dfee4542737251..74f1932473ba2d3ae99afd31fcc24739abcf5bcc 100644 (file)
tree data, since then libfdt would still be needed for those drivers and
there would be no code-size benefit.
+
+Build-time instantiation
+------------------------
+
+Even with of-platdata there is a fair amount of code required in driver model.
+It is possible to have U-Boot handle the instantiation of devices at build-time,
+so avoiding the need for the `device_bind()` code and some parts of
+`device_probe()`.
+
+The feature is enabled by CONFIG_OF_PLATDATA_INST.
+
+Here is an example device, as generated by dtoc::
+
+ /*
+ * Node /serial index 6
+ * driver sandbox_serial parent root_driver
+ */
+
+ #include <asm/serial.h>
+ struct sandbox_serial_plat __attribute__ ((section (".priv_data")))
+ _sandbox_serial_plat_serial = {
+ .dtplat = {
+ .sandbox_text_colour = "cyan",
+ },
+ };
+ #include <asm/serial.h>
+ u8 _sandbox_serial_priv_serial[sizeof(struct sandbox_serial_priv)]
+ __attribute__ ((section (".priv_data")));
+ #include <serial.h>
+ u8 _sandbox_serial_uc_priv_serial[sizeof(struct serial_dev_priv)]
+ __attribute__ ((section (".priv_data")));
+
+ DM_DEVICE_INST(serial) = {
+ .driver = DM_DRIVER_REF(sandbox_serial),
+ .name = "sandbox_serial",
+ .plat_ = &_sandbox_serial_plat_serial,
+ .priv_ = _sandbox_serial_priv_serial,
+ .uclass = DM_UCLASS_REF(serial),
+ .uclass_priv_ = _sandbox_serial_uc_priv_serial,
+ .uclass_node = {
+ .prev = &DM_UCLASS_REF(serial)->dev_head,
+ .next = &DM_UCLASS_REF(serial)->dev_head,
+ },
+ .child_head = {
+ .prev = &DM_DEVICE_REF(serial)->child_head,
+ .next = &DM_DEVICE_REF(serial)->child_head,
+ },
+ .sibling_node = {
+ .prev = &DM_DEVICE_REF(i2c_at_0)->sibling_node,
+ .next = &DM_DEVICE_REF(spl_test)->sibling_node,
+ },
+ .seq_ = 0,
+ };
+
+Here is part of the driver, for reference::
+
+ static const struct udevice_id sandbox_serial_ids[] = {
+ { .compatible = "sandbox,serial" },
+ { }
+ };
+
+ U_BOOT_DRIVER(sandbox_serial) = {
+ .name = "sandbox_serial",
+ .id = UCLASS_SERIAL,
+ .of_match = sandbox_serial_ids,
+ .of_to_plat = sandbox_serial_of_to_plat,
+ .plat_auto = sizeof(struct sandbox_serial_plat),
+ .priv_auto = sizeof(struct sandbox_serial_priv),
+ .probe = sandbox_serial_probe,
+ .remove = sandbox_serial_remove,
+ .ops = &sandbox_serial_ops,
+ .flags = DM_FLAG_PRE_RELOC,
+ };
+
+
+The `DM_DEVICE_INST()` macro declares a struct udevice so you can see that the
+members are from that struct. The private data is declared immediately above,
+as `_sandbox_serial_priv_serial`, so there is no need for run-time memory
+allocation. The #include lines are generated as well, since dtoc searches the
+U-Boot source code for the definition of `struct sandbox_serial_priv` and adds
+the relevant header so that the code will compile without errors.
+
+The `plat_` member is set to the dtv data which is declared immediately above
+the device. This is similar to how it would look without of-platdata-inst, but
+node that the `dtplat` member inside is part of the wider
+`_sandbox_serial_plat_serial` struct. This is because the driver declares its
+own platform data, and the part generated by dtoc can only be a portion of it.
+The `dtplat` part is always first in the struct. If the device has no
+`.plat_auto` field, then a simple dtv struct can be used as with this example::
+
+ static struct dtd_sandbox_clk dtv_clk_sbox = {
+ .assigned_clock_rates = 0x141,
+ .assigned_clocks = {0x7, 0x3},
+ };
+
+ #include <asm/clk.h>
+ u8 _sandbox_clk_priv_clk_sbox[sizeof(struct sandbox_clk_priv)]
+ __attribute__ ((section (".priv_data")));
+
+ DM_DEVICE_INST(clk_sbox) = {
+ .driver = DM_DRIVER_REF(sandbox_clk),
+ .name = "sandbox_clk",
+ .plat_ = &dtv_clk_sbox,
+
+Here is part of the driver, for reference::
+
+ static const struct udevice_id sandbox_clk_ids[] = {
+ { .compatible = "sandbox,clk" },
+ { }
+ };
+
+ U_BOOT_DRIVER(sandbox_clk) = {
+ .name = "sandbox_clk",
+ .id = UCLASS_CLK,
+ .of_match = sandbox_clk_ids,
+ .ops = &sandbox_clk_ops,
+ .probe = sandbox_clk_probe,
+ .priv_auto = sizeof(struct sandbox_clk_priv),
+ };
+
+
+You can see that `dtv_clk_sbox` just has the devicetree contents and there is
+no need for the `dtplat` separation, since the driver has no platform data of
+its own, besides that provided by the devicetree (i.e. no `.plat_auto` field).
+
+The doubly linked lists are handled by explicitly declaring the value of each
+node, as you can see with the `.prev` and `.next` values in the example above.
+Since dtoc knows the order of devices it can link them into the appropriate
+lists correctly.
+
+One of the features of driver model is the ability for a uclass to have a
+small amount of private data for each device in that uclass. This is used to
+provide a generic data structure that the uclass can use for all devices, thus
+allowing generic features to be implemented in common code. An example is I2C,
+which stores the bus speed there.
+
+Similarly, parent devices can have data associated with each of their children.
+This is used to provide information common to all children of a particular bus.
+For an I2C bus, this is used to store the I2C address of each child on the bus.
+
+This is all handled automatically by dtoc::
+
+ #include <asm/i2c.h>
+ u8 _sandbox_i2c_priv_i2c_at_0[sizeof(struct sandbox_i2c_priv)]
+ __attribute__ ((section (".priv_data")));
+ #include <i2c.h>
+ u8 _sandbox_i2c_uc_priv_i2c_at_0[sizeof(struct dm_i2c_bus)]
+ __attribute__ ((section (".priv_data")));
+
+ DM_DEVICE_INST(i2c_at_0) = {
+ .driver = DM_DRIVER_REF(sandbox_i2c),
+ .name = "sandbox_i2c",
+ .plat_ = &dtv_i2c_at_0,
+ .priv_ = _sandbox_i2c_priv_i2c_at_0,
+ .uclass = DM_UCLASS_REF(i2c),
+ .uclass_priv_ = _sandbox_i2c_uc_priv_i2c_at_0,
+ ...
+
+Part of driver, for reference::
+
+ static const struct udevice_id sandbox_i2c_ids[] = {
+ { .compatible = "sandbox,i2c" },
+ { }
+ };
+
+ U_BOOT_DRIVER(sandbox_i2c) = {
+ .name = "sandbox_i2c",
+ .id = UCLASS_I2C,
+ .of_match = sandbox_i2c_ids,
+ .ops = &sandbox_i2c_ops,
+ .priv_auto = sizeof(struct sandbox_i2c_priv),
+ };
+
+Part of I2C uclass, for reference::
+
+ UCLASS_DRIVER(i2c) = {
+ .id = UCLASS_I2C,
+ .name = "i2c",
+ .flags = DM_UC_FLAG_SEQ_ALIAS,
+ .post_bind = i2c_post_bind,
+ .pre_probe = i2c_pre_probe,
+ .post_probe = i2c_post_probe,
+ .per_device_auto = sizeof(struct dm_i2c_bus),
+ .per_child_plat_auto = sizeof(struct dm_i2c_chip),
+ .child_post_bind = i2c_child_post_bind,
+ };
+
+Here, `_sandbox_i2c_uc_priv_i2c_at_0` is required by the uclass but is declared
+in the device, as required by driver model. The required header file is included
+so that the code will compile without errors. A similar mechanism is used for
+child devices, but is not shown by this example.
+
+It would not be that useful to avoid binding devices but still need to allocate
+uclasses at runtime. So dtoc generates uclass instances as well::
+
+ struct list_head uclass_head = {
+ .prev = &DM_UCLASS_REF(serial)->sibling_node,
+ .next = &DM_UCLASS_REF(clk)->sibling_node,
+ };
+
+ DM_UCLASS_INST(clk) = {
+ .uc_drv = DM_UCLASS_DRIVER_REF(clk),
+ .sibling_node = {
+ .prev = &uclass_head,
+ .next = &DM_UCLASS_REF(i2c)->sibling_node,
+ },
+ .dev_head = {
+ .prev = &DM_DEVICE_REF(clk_sbox)->uclass_node,
+ .next = &DM_DEVICE_REF(clk_fixed)->uclass_node,
+ },
+ };
+
+At the top is the list head. Driver model uses this on start-up, instead of
+creating its own.
+
+Below that are a set of `DM_UCLASS_INST()` macros, each declaring a
+`struct uclass`. The doubly linked lists work as for devices.
+
+All private data is placed into a `.priv_data` section so that it is contiguous
+in the resulting output binary.
+
+
+Indexes
+-------
+
+U-Boot stores drivers, devices and many other things in linker_list structures.
+These are sorted by name, so dtoc knows the order that they will appear when
+the linker runs. Each driver_info / udevice is referenced by its index in the
+linker_list array, called 'idx' in the code.
+
+When CONFIG_OF_PLATDATA_INST is enabled, idx is the udevice index, otherwise it
+is the driver_info index. In either case, indexes are used to reference devices
+using device_get_by_ofplat_idx(). This allows phandles to work as expected.
+
+
+Phases
+------
+
+U-Boot operates in several phases, typically TPL, SPL and U-Boot proper.
+The latter does not use dtoc.
+
+In some rare cases different drivers are used for two phases. For example,
+in TPL it may not be necessary to use the full PCI subsystem, so a simple
+driver can be used instead.
+
+This works in the build system simply by compiling in one driver or the
+other (e.g. PCI driver + uclass for SPL; simple_bus for TPL). But dtoc has
+no way of knowing which code is compiled in for which phase, since it does
+not inspect Makefiles or dependency graphs.
+
+So to make this work for dtoc, we need to be able to explicitly mark
+drivers with their phase. This is done by adding a macro to the driver::
+
+ /* code in tpl.c only compiled into TPL */
+ U_BOOT_DRIVER(pci_x86) = {
+ .name = "pci_x86",
+ .id = UCLASS_SIMPLE_BUS,
+ .of_match = of_match_ptr(tpl_fake_pci_ids),
+ DM_PHASE(tpl)
+ };
+
+
+ /* code in pci_x86.c compiled into SPL and U-Boot proper */
+ U_BOOT_DRIVER(pci_x86) = {
+ .name = "pci_x86",
+ .id = UCLASS_PCI,
+ .of_match = pci_x86_ids,
+ .ops = &pci_x86_ops,
+ };
+
+
+Notice that the second driver has the same name but no DM_PHASE(), so it will be
+used for SPL and U-Boot.
+
+Note also that this only affects the code generated by dtoc. You still need to
+make sure that only the required driver is build into each phase.
+
+
+Header files
+------------
+
+With OF_PLATDATA_INST, dtoc must include the correct header file in the
+generated code for any structs that are used, so that the code will compile.
+For example, if `struct ns16550_plat` is used, the code must include the
+`ns16550.h` header file.
+
+Typically dtoc can detect the header file needed for a driver by looking
+for the structs that it uses. For example, if a driver as a `.priv_auto`
+that uses `struct ns16550_plat`, then dtoc can search header files for the
+definition of that struct and use the file.
+
+In some cases, enums are used in drivers, typically with the `.data` field
+of `struct udevice_id`. Since dtoc does not support searching for these,
+you must use the `DM_HDR()` macro to tell dtoc which header to use. This works
+as a macro included in the driver definition::
+
+ static const struct udevice_id apl_syscon_ids[] = {
+ { .compatible = "intel,apl-punit", .data = X86_SYSCON_PUNIT },
+ { }
+ };
+
+ U_BOOT_DRIVER(intel_apl_punit) = {
+ .name = "intel_apl_punit",
+ .id = UCLASS_SYSCON,
+ .of_match = apl_syscon_ids,
+ .probe = apl_punit_probe,
+ DM_HEADER(<asm/cpu.h>) /* for X86_SYSCON_PUNIT */
+ };
+
+
+
+Caveats
+-------
+
+There are various complications with this feature which mean it should only
+be used when strictly necessary, i.e. in SPL with limited memory. Notable
+caveats include:
+
+ - Device tree does not describe data types. But the C code must define a
+ type for each property. These are guessed using heuristics which
+ are wrong in several fairly common cases. For example an 8-byte value
+ is considered to be a 2-item integer array, and is byte-swapped. A
+ boolean value that is not present means 'false', but cannot be
+ included in the structures since there is generally no mention of it
+ in the devicetree file.
+
+ - Naming of nodes and properties is automatic. This means that they follow
+ the naming in the devicetree, which may result in C identifiers that
+ look a bit strange.
+
+ - It is not possible to find a value given a property name. Code must use
+ the associated C member variable directly in the code. This makes
+ the code less robust in the face of devicetree changes. To avoid having
+ a second struct with similar members and names you need to explicitly
+ declare it as an alias with `DM_DRIVER_ALIAS()`.
+
+ - The platform data is provided to drivers as a C structure. The driver
+ must use the same structure to access the data. Since a driver
+ normally also supports devicetree it must use `#ifdef` to separate
+ out this code, since the structures are only available in SPL. This could
+ be fixed fairly easily by making the structs available outside SPL, so
+ that `IS_ENABLED()` could be used.
+
+ - With CONFIG_OF_PLATDATA_INST all binding happens at build-time, meaning
+ that (by default) it is not possible to call `device_bind()` from C code.
+ This means that all devices must have an associated devicetree node and
+ compatible string. For example if a GPIO device currently creates child
+ devices in its `bind()` method, it will not work with
+ CONFIG_OF_PLATDATA_INST. Arguably this is bad practice anyway and the
+ devicetree binding should be updated to declare compatible strings for
+ the child devices. It is possible to disable OF_PLATDATA_NO_BIND but this
+ is not recommended since it increases code size.
+
+
Internals
---------
+Generated files
+```````````````
+
+When enabled, dtoc generates the following five files:
+
+include/generated/dt-decl.h (OF_PLATDATA_INST only)
+ Contains declarations for all drivers, devices and uclasses. This allows
+ any `struct udevice`, `struct driver` or `struct uclass` to be located by its
+ name
+
+include/generated/dt-structs-gen.h
+ Contains the struct definitions for the devicetree nodes that are used. This
+ is the same as without OF_PLATDATA_INST
+
+spl/dts/dt-plat.c (only with !OF_PLATDATA_INST)
+ Contains the `U_BOOT_DRVINFO()` declarations that U-Boot uses to bind devices
+ at start-up. See above for an example
+
+spl/dts/dt-device.c (only with OF_PLATDATA_INST)
+ Contains `DM_DEVICE_INST()` declarations for each device that can be used at
+ run-time. These are declared in the file along with any private/platform data
+ that they use. Every device has an idx, as above. Since each device must be
+ part of a double-linked list, the nodes are declared in the code as well.
+
+spl/dts/dt-uclass.c (only with OF_PLATDATA_INST)
+ Contains `DM_UCLASS_INST()` declarations for each uclass that can be used at
+ run-time. These are declared in the file along with any private data
+ associated with the uclass itself (the `.priv_auto` member). Since each
+ uclass must be part of a double-linked list, the nodes are declared in the
+ code as well.
+
The dt-structs.h file includes the generated file
`(include/generated/dt-structs.h`) if CONFIG_SPL_OF_PLATDATA is enabled.
Otherwise (such as in U-Boot proper) these structs are not available. This
The dt-plat.c file contains the device declarations and is is built in
spl/dt-plat.c.
+
+CONFIG options
+``````````````
+
+Several CONFIG options are used to control the behaviour of of-platdata, all
+available for both SPL and TPL:
+
+OF_PLATDATA
+ This is the main option which enables the of-platdata feature
+
+OF_PLATDATA_PARENT
+ This allows `device_get_parent()` to work. Without this, all devices exist as
+ direct children of the root node. This option is highly desirable (if not
+ always absolutely essential) for buses such as I2C.
+
+OF_PLATDATA_INST
+ This controls the instantiation of devices at build time. With it disabled,
+ only `U_BOOT_DRVINFO()` records are created, with U-Boot handling the binding
+ in `device_bind()` on start-up. With it enabled, only `DM_DEVICE_INST()` and
+ `DM_UCLASS_INST()` records are created, and `device_bind()` is not needed at
+ runtime.
+
+OF_PLATDATA_NO_BIND
+ This controls whether `device_bind()` is supported. It is enabled by default
+ with OF_PLATDATA_INST since code-size reduction is really the main point of
+ the feature. It can be disabled if needed but is not likely to be supported
+ in the long term.
+
+OF_PLATDATA_DRIVER_RT
+ This controls whether the `struct driver_rt` records are used by U-Boot.
+ Normally when a device is bound, U-Boot stores the device pointer in one of
+ these records. There is one for every `struct driver_info` in the system,
+ i.e. one for every device that is bound from those records. It provides a
+ way to locate a device in the code and is used by
+ `device_get_by_ofplat_idx()`. This option is always enabled with of-platdata,
+ provided OF_PLATDATA_INST is not. In that case the records are useless since
+ we don't have any `struct driver_info` records.
+
+OF_PLATDATA_RT
+ This controls whether the `struct udevice_rt` records are used by U-Boot.
+ It moves the updatable fields from `struct udevice` (currently only `flags`)
+ into a separate structure, allowing the records to be kept in read-only
+ memory. It is generally enabled if OF_PLATDATA_INST is enabled. This option
+ also controls whether the private data is used in situ, or first copied into
+ an allocated region. Again this is to allow the private data declared by
+ dtoc-generated code to be in read-only memory. Note that access to private
+ data must be done via accessor functions, such as `dev_get_priv()`, so that
+ the relocation is handled.
+
+READ_ONLY
+ This indicates that the data generated by dtoc should not be modified. Only
+ a few fields actually do get changed in U-Boot, such as device flags. This
+ option causes those to move into an allocated space (see OF_PLATDATA_RT).
+ Also, since updating doubly linked lists is generally impossible when some of
+ the nodes cannot be updated, OF_PLATDATA_NO_BIND is enabled.
+
+Data structures
+```````````````
+
+A few extra data structures are used with of-platdata:
+
+`struct udevice_rt`
+ Run-time information for devices. When OF_PLATDATA_RT is enabled, this holds
+ the flags for each device, so that `struct udevice` can remain unchanged by
+ U-Boot, and potentially reside in read-only memory. Access to flags is then
+ via functions like `dev_get_flags()` and `dev_or_flags()`. This data
+ structure is allocated on start-up, where the private data is also copied.
+ All flags values start at 0 and any changes are handled by `dev_or_flags()`
+ and `dev_bic_flags()`. It would be more correct for the flags to be set to
+ `DM_FLAG_BOUND`, or perhaps `DM_FLAG_BOUND | DM_FLAG_ALLOC_PDATA`, but since
+ there is no code to bind/unbind devices and no code to allocate/free
+ private data / platform data, it doesn't matter.
+
+`struct driver_rt`
+ Run-time information for `struct driver_info` records. When
+ OF_PLATDATA_DRIVER_RT is enabled, this holds a pointer to the device
+ created by each record. This is needed so that is it possible to locate a
+ device from C code. Specifically, the code can use `DM_DRVINFO_GET(name)` to
+ get a reference to a particular `struct driver_info`, with `name` being the
+ name of the devicetree node. This is very convenient. It is also fast, since
+ no searching or string comparison is needed. This data structure is
+ allocated on start-up, filled out by `device_bind()` and used by
+ `device_get_by_ofplat_idx()`.
+
+Other changes
+`````````````
+
+Some other changes are made with of-platdata:
+
+Accessor functions
+ Accessing private / platform data via functions such as `dev_get_priv()` has
+ always been encouraged. With OF_PLATDATA_RT this is essential, since the
+ `priv_` and `plat_` (etc.) values point to the data generated by dtoc, not
+ the read-write copy that is sometimes made on start-up. Changing the
+ private / platform data pointers has always been discouraged (the API is
+ marked internal) but with OF_PLATDATA_RT this is not currently supported in
+ general, since it assumes that all such pointers point to the relocated data.
+ Note also that the renaming of struct members to have a trailing underscore
+ was partly done to make people aware that they should not be accessed
+ directly.
+
+`gd->uclass_root_s`
+ Normally U-Boot sets up the head of the uclass list here and makes
+ `gd->uclass_root` point to it. With OF_PLATDATA_INST, dtoc generates a
+ declaration of `uclass_head` in `dt-uclass.c` since it needs to link the
+ head node into the list. In that case, `gd->uclass_root_s` is not used and
+ U-Boot just makes `gd->uclass_root` point to `uclass_head`.
+
+`gd->dm_driver_rt`
+ This holds a pointer to a list of `struct driver_rt` records, one for each
+ `struct driver_info`. The list is in alphabetical order by the name used
+ in `U_BOOT_DRVINFO(name)` and indexed by idx, with the first record having
+ an index of 0. It is only used if OF_PLATDATA_INST is not enabled. This is
+ accessed via macros so that it can be used inside IS_ENABLED(), rather than
+ requiring #ifdefs in the C code when it is not present.
+
+`gd->dm_udevice_rt`
+ This holds a pointer to a list of `struct udevice_rt` records, one for each
+ `struct udevice`. The list is in alphabetical order by the name used
+ in `DM_DEVICE_INST(name)` (a C version of the devicetree node) and indexed by
+ idx, with the first record having an index of 0. It is only used if
+ OF_PLATDATA_INST is enabled. This is accessed via macros so that it can be
+ used inside `IS_ENABLED()`, rather than requiring #ifdefs in the C code when
+ it is not present.
+
+`gd->dm_priv_base`
+ When OF_PLATDATA_RT is enabled, the private/platform data for each device is
+ copied into an allocated region by U-Boot on start-up. This points to that
+ region. All calls to accessor functions (e.g. `dev_get_priv()`) then
+ translate from the pointer provided by the caller (assumed to lie between
+ `__priv_data_start` and `__priv_data_end`) to the new allocated region. This
+ member is accessed via macros so that it can be used inside IS_ENABLED(),
+ rather than required #ifdefs in the C code when it is not present.
+
+`struct udevice->flags_`
+ When OF_PLATDATA_RT is enabled, device flags are no-longer part of
+ `struct udevice`, but are instead kept in `struct udevice_rt`, as described
+ above. Flags are accessed via functions, such as `dev_get_flags()` and
+ `dev_or_flags()`.
+
+`struct udevice->node_`
+ When OF_PLATDATA is enabled, there is no devicetree at runtime, so no need
+ for this field. It is removed, just to save space.
+
+`DM_PHASE`
+ This macro is used to indicate which phase of U-Boot a driver is intended
+ for. See above for details.
+
+`DM_HDR`
+ This macro is used to indicate which header file dtoc should use to allow
+ a driver declaration to compile correctly. See above for details.
+
+`device_get_by_ofplat_idx()`
+ There used to be a function called `device_get_by_driver_info()` which
+ looked up a `struct driver_info` pointer and returned the `struct udevice`
+ that was created from it. It was only available for use with of-platdata.
+ This has been removed in favour of `device_get_by_ofplat_idx()` which uses
+ `idx`, the index of the `struct driver_info` or `struct udevice` in the
+ linker_list. Similarly, the `struct phandle_0_arg` (etc.) structs have been
+ updated to use this index instead of a pointer to `struct driver_info`.
+
+`DM_DRVINFO_GET`
+ This has been removed since we now use indexes to obtain a driver from
+ `struct phandle_0_arg` and the like.
+
+Two-pass binding
+ The original of-platdata tried to order `U_BOOT_DRVINFO()` in the generated
+ files so as to have parents declared ahead of children. This was convenient
+ as it avoided any special code in U-Boot. With OF_PLATDATA_INST this does
+ not work as the idx value relies on using alphabetical order for everything,
+ so that dtoc and U-Boot's linker_lists agree on the idx value. Devices are
+ then bound in order of idx, having no regard to parent/child relationships.
+ For this reason, device binding now hapens in multiple passes, with parents
+ being bound before their children. This is important so that children can
+ find their parents in the bind() method if needed.
+
+Root device
+ The root device is generally bound by U-Boot but with OF_PLATDATA_INST it
+ cannot be, since binding needs to be done at build time. So in this case
+ dtoc sets up a root device using `DM_DEVICE_INST()` in `dt-device.c` and
+ U-Boot makes use of that. When OF_PLATDATA_INST is not enabled, U-Boot
+ generally ignores the root node and does not create a `U_BOOT_DRVINFO()`
+ record for it. This means that the idx numbers used by `struct driver_info`
+ (when OF_PLATDATA_INST is disabled) and the idx numbers used by
+ `struct udevice` (when OF_PLATDATA_INST is enabled) differ, since one has a
+ root node and the other does not. This does not actually matter, since only
+ one of them is actually used for any particular build, but it is worth
+ keeping in mind if comparing index values and switching OF_PLATDATA_INST on
+ and off.
+
+`__priv_data_start` and `__priv_data_end`
+ The private/platform data declared by dtoc is all collected together in
+ a linker section and these symbols mark the start and end of it. This allows
+ U-Boot to relocate the area to a new location if needed (with
+ OF_PLATDATA_RT)
+
+`dm_priv_to_rw()`
+ This function converts a private- or platform-data pointer value generated by
+ dtoc into one that can be used by U-Boot. It is a NOP unless OF_PLATDATA_RT
+ is enabled, in which case it translates the address to the relocated
+ region. See above for more information.
+
The dm_populate_phandle_data() function that was previous needed has now been
removed, since dtoc can address the drivers directly from dt-plat.c and does
not need to fix up things at runtime.