summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: e7bae82)
raw | patch | inline | side by side (parent: e7bae82)
author | Simon Glass <sjg@chromium.org> | |
Mon, 15 Mar 2021 05:00:24 +0000 (18:00 +1300) | ||
committer | Simon Glass <sjg@chromium.org> | |
Sat, 27 Mar 2021 02:04:30 +0000 (15:04 +1300) |
This information is interesting to look at and can be important for
debugging and inspection. Add a command to display it in a helpful
format.
Signed-off-by: Simon Glass <sjg@chromium.org>
debugging and inspection. Add a command to display it in a helpful
format.
Signed-off-by: Simon Glass <sjg@chromium.org>
cmd/Kconfig | patch | blob | history | |
cmd/x86/Makefile | patch | blob | history | |
cmd/x86/cbsysinfo.c | [new file with mode: 0644] | patch | blob |
doc/usage/index.rst | patch | blob | history | |
doc/usage/x86/cbsysinfo.rst | [new file with mode: 0644] | patch | blob |
diff --git a/cmd/Kconfig b/cmd/Kconfig
index e4bb1d4c4a7655797b02eaa577bb6618f5e3dc32..8ab34f3798d07246bb5ebe406eafa2f278b4fc7f 100644 (file)
--- a/cmd/Kconfig
+++ b/cmd/Kconfig
for some PowerPC processors. For details please see the
documentation in doc/README.bedbug.
+config CMD_CBSYSINFO
+ bool "cbsysinfo"
+ depends on X86
+ default y if SYS_COREBOOT
+ help
+ This provides information about the coreboot sysinfo table stored in
+ memory by coreboot before jumping to U-Boot. It can be useful for
+ debugging the beaaviour of coreboot or U-Boot.
+
config CMD_DIAG
bool "diag - Board diagnostics"
help
diff --git a/cmd/x86/Makefile b/cmd/x86/Makefile
index 144b1cf5abeccf30b6ac44102c31a17b739546fe..5f82204c87e65868c52cbfcdbe38dae199c7bf19 100644 (file)
--- a/cmd/x86/Makefile
+++ b/cmd/x86/Makefile
# SPDX-License-Identifier: GPL-2.0+
+obj-$(CONFIG_CMD_CBSYSINFO) += cbsysinfo.o
obj-y += mtrr.o
obj-$(CONFIG_CMD_EXCEPTION) += exception.o
obj-$(CONFIG_USE_HOB) += hob.o
diff --git a/cmd/x86/cbsysinfo.c b/cmd/x86/cbsysinfo.c
--- /dev/null
+++ b/cmd/x86/cbsysinfo.c
@@ -0,0 +1,394 @@
+// SPDX-License-Identifier: GPL-2.0+
+/*
+ * Copyright 2021 Google LLC
+ * Written by Simon Glass <sjg@chromium.org>
+ */
+
+#include <common.h>
+#include <asm/cb_sysinfo.h>
+#include <command.h>
+#include <console.h>
+#include <asm/global_data.h>
+
+DECLARE_GLOBAL_DATA_PTR;
+
+static void cbprompt(const char *name)
+{
+ for (; *name == '>'; name++)
+ puts(" ");
+ printf("%-12s: ", name);
+}
+
+static void print_dec(const char *name, int value)
+{
+ cbprompt(name);
+ printf(value > 9 ? "0d%d\n" : "%d\n", value);
+}
+
+static void print_hex(const char *name, int value)
+{
+ cbprompt(name);
+ printf("%x\n", value);
+}
+
+static void print_addr(const char *name, ulong value)
+{
+ cbprompt(name);
+ printf("%08lx\n", value);
+}
+
+static void print_addr64(const char *name, u64 value)
+{
+ cbprompt(name);
+ printf("%16llx\n", value);
+}
+
+static void print_ptr(const char *name, const void *value)
+{
+ cbprompt(name);
+ printf("%p\n", value);
+}
+
+static void print_str(const char *name, const char *value)
+{
+ if (value) {
+ cbprompt(name);
+ printf("%s\n", value);
+ }
+}
+
+static void print_idx(const char *name, uint idx, const u8 *strings)
+{
+ const char *ptr;
+
+ cbprompt(name);
+ ptr = (char *)strings + idx;
+ printf("%d: %s\n", idx, ptr ? ptr : "(unknown)");
+}
+
+static const char *const cb_mem_name[] = {
+ NULL,
+ "ram",
+ "reserved",
+ "acpi",
+ "nvs",
+ "unusable",
+ "vendor",
+};
+
+static const char *get_mem_name(int tag)
+{
+ if (tag >= CB_MEM_RAM && tag <= CB_MEM_VENDOR_RSVD)
+ return cb_mem_name[tag];
+
+ if (tag == CB_MEM_TABLE)
+ return "table";
+
+ return "(unknown)";
+}
+
+static const struct timestamp_id_to_name {
+ uint id;
+ const char *name;
+} timestamp_ids[] = {
+ /* Marker to report base_time */
+ { 0, "1st timestamp" },
+ { TS_START_ROMSTAGE, "start of romstage" },
+ { TS_BEFORE_INITRAM, "before ram initialization" },
+ { TS_AFTER_INITRAM, "after ram initialization" },
+ { TS_END_ROMSTAGE, "end of romstage" },
+ { TS_START_VBOOT, "start of verified boot" },
+ { TS_END_VBOOT, "end of verified boot" },
+ { TS_START_COPYRAM, "starting to load ramstage" },
+ { TS_END_COPYRAM, "finished loading ramstage" },
+ { TS_START_RAMSTAGE, "start of ramstage" },
+ { TS_START_BOOTBLOCK, "start of bootblock" },
+ { TS_END_BOOTBLOCK, "end of bootblock" },
+ { TS_START_COPYROM, "starting to load romstage" },
+ { TS_END_COPYROM, "finished loading romstage" },
+ { TS_START_ULZMA, "starting LZMA decompress (ignore for x86)" },
+ { TS_END_ULZMA, "finished LZMA decompress (ignore for x86)" },
+ { TS_START_ULZ4F, "starting LZ4 decompress (ignore for x86)" },
+ { TS_END_ULZ4F, "finished LZ4 decompress (ignore for x86)" },
+ { TS_DEVICE_ENUMERATE, "device enumeration" },
+ { TS_DEVICE_CONFIGURE, "device configuration" },
+ { TS_DEVICE_ENABLE, "device enable" },
+ { TS_DEVICE_INITIALIZE, "device initialization" },
+ { TS_DEVICE_DONE, "device setup done" },
+ { TS_CBMEM_POST, "cbmem post" },
+ { TS_WRITE_TABLES, "write tables" },
+ { TS_FINALIZE_CHIPS, "finalize chips" },
+ { TS_LOAD_PAYLOAD, "load payload" },
+ { TS_ACPI_WAKE_JUMP, "ACPI wake jump" },
+ { TS_SELFBOOT_JUMP, "selfboot jump" },
+
+ { TS_START_COPYVER, "starting to load verstage" },
+ { TS_END_COPYVER, "finished loading verstage" },
+ { TS_START_TPMINIT, "starting to initialize TPM" },
+ { TS_END_TPMINIT, "finished TPM initialization" },
+ { TS_START_VERIFY_SLOT, "starting to verify keyblock/preamble (RSA)" },
+ { TS_END_VERIFY_SLOT, "finished verifying keyblock/preamble (RSA)" },
+ { TS_START_HASH_BODY, "starting to verify body (load+SHA2+RSA) " },
+ { TS_DONE_LOADING, "finished loading body (ignore for x86)" },
+ { TS_DONE_HASHING, "finished calculating body hash (SHA2)" },
+ { TS_END_HASH_BODY, "finished verifying body signature (RSA)" },
+
+ { TS_START_COPYVPD, "starting to load Chrome OS VPD" },
+ { TS_END_COPYVPD_RO, "finished loading Chrome OS VPD (RO)" },
+ { TS_END_COPYVPD_RW, "finished loading Chrome OS VPD (RW)" },
+
+ { TS_U_BOOT_INITTED, "U-Boot start" },
+ { TS_RO_PARAMS_INIT, "RO parameter init" },
+ { TS_RO_VB_INIT, "RO vboot init" },
+ { TS_RO_VB_SELECT_FIRMWARE, "RO vboot select firmware" },
+ { TS_RO_VB_SELECT_AND_LOAD_KERNEL, "RO vboot select&load kernel" },
+ { TS_RW_VB_SELECT_AND_LOAD_KERNEL, "RW vboot select&load kernel" },
+ { TS_VB_SELECT_AND_LOAD_KERNEL, "vboot select&load kernel" },
+ { TS_VB_EC_VBOOT_DONE, "finished EC verification" },
+ { TS_VB_STORAGE_INIT_DONE, "finished storage device initialization" },
+ { TS_VB_READ_KERNEL_DONE, "finished reading kernel from disk" },
+ { TS_VB_VBOOT_DONE, "finished vboot kernel verification" },
+ { TS_KERNEL_DECOMPRESSION, "starting kernel decompression/relocation" },
+ { TS_START_KERNEL, "jumping to kernel" },
+ { TS_U_BOOT_START_KERNEL, "just before jump to kernel" },
+
+ /* Intel ME-related timestamps */
+ { TS_ME_INFORM_DRAM_WAIT, "waiting for ME acknowledgment of raminit"},
+ { TS_ME_INFORM_DRAM_DONE, "finished waiting for ME response"},
+
+ /* FSP-related timestamps */
+ { TS_FSP_MEMORY_INIT_START, "calling FspMemoryInit" },
+ { TS_FSP_MEMORY_INIT_END, "returning from FspMemoryInit" },
+ { TS_FSP_TEMP_RAM_EXIT_START, "calling FspTempRamExit" },
+ { TS_FSP_TEMP_RAM_EXIT_END, "returning from FspTempRamExit" },
+ { TS_FSP_SILICON_INIT_START, "calling FspSiliconInit" },
+ { TS_FSP_SILICON_INIT_END, "returning from FspSiliconInit" },
+ { TS_FSP_BEFORE_ENUMERATE, "calling FspNotify(AfterPciEnumeration)" },
+ { TS_FSP_AFTER_ENUMERATE,
+ "returning from FspNotify(AfterPciEnumeration)" },
+ { TS_FSP_BEFORE_FINALIZE, "calling FspNotify(ReadyToBoot)" },
+ { TS_FSP_AFTER_FINALIZE, "returning from FspNotify(ReadyToBoot)" },
+ { TS_FSP_BEFORE_END_OF_FIRMWARE, "calling FspNotify(EndOfFirmware)" },
+ { TS_FSP_AFTER_END_OF_FIRMWARE,
+ "returning from FspNotify(EndOfFirmware)" },
+};
+
+static const char *timestamp_name(uint32_t id)
+{
+ int i;
+
+ for (i = 0; i < ARRAY_SIZE(timestamp_ids); i++) {
+ if (timestamp_ids[i].id == id)
+ return timestamp_ids[i].name;
+ }
+
+ return "<unknown>";
+}
+
+static void show_table(struct sysinfo_t *info, bool verbose)
+{
+ struct cb_serial *ser = info->serial;
+ int i;
+
+ printf("Coreboot table at %lx, decoded to %p",
+ gd->arch.coreboot_table, info);
+ if (info->header)
+ printf(", forwarded to %p\n", info->header);
+ printf("\n");
+
+ print_dec("CPU KHz", info->cpu_khz);
+
+ print_addr("Serial I/O port", info->ser_ioport);
+ print_addr(">base", info->ser_base);
+ print_ptr(">pointer", ser);
+ if (ser) {
+ print_hex(">type", ser->type);
+ print_addr(">base", ser->baseaddr);
+ print_dec(">baud", ser->baud);
+ print_hex(">baud", ser->regwidth);
+ print_dec(">input_hz", ser->input_hertz);
+ print_addr(">PCI addr", ser->uart_pci_addr);
+ }
+
+ print_dec("Mem ranges", info->n_memranges);
+ printf("%12s: %-11s || base || size\n", "id", "type");
+ for (i = 0; i < info->n_memranges; i++) {
+ const struct memrange *mr = &info->memrange[i];
+
+ printf("%12d: %02x:%-8s %016llx %016llx\n", i, mr->type,
+ get_mem_name(mr->type), mr->base, mr->size);
+ }
+ print_ptr("option_table", info->option_table);
+
+ print_hex("CMOS start", info->cmos_range_start);
+ if (info->cmos_range_start) {
+ print_hex(">CMOS end", info->cmos_range_end);
+ print_hex(">CMOS csum loc", info->cmos_checksum_location);
+ }
+
+ print_hex("VBNV start", info->vbnv_start);
+ print_hex("VBNV size", info->vbnv_size);
+
+ print_str("CB version", info->cb_version);
+ print_str(">Extra", info->extra_version);
+ print_str(">Build", info->build);
+ print_str(">Time", info->compile_time);
+ print_str(">By", info->compile_by);
+ print_str(">Host", info->compile_host);
+ print_str(">Domain", info->compile_domain);
+ print_str(">Compiler", info->compiler);
+ print_str(">Linker", info->linker);
+ print_str(">Assembler", info->assembler);
+
+ print_ptr("Framebuffer", info->framebuffer);
+ if (info->framebuffer) {
+ struct cb_framebuffer *fb = info->framebuffer;
+
+ print_addr64(">Phys addr", fb->physical_address);
+ print_dec(">X res", fb->x_resolution);
+ print_dec(">X res", fb->y_resolution);
+ print_hex(">Bytes / line", fb->bytes_per_line);
+ print_dec(">Bpp", fb->bits_per_pixel);
+ printf(" %-12s red %d/%d, green %d/%d, blue %d/%d, reserved %d/%d\n",
+ "pos/size", fb->red_mask_pos, fb->red_mask_size,
+ fb->green_mask_pos, fb->green_mask_size,
+ fb->blue_mask_pos, fb->blue_mask_size,
+ fb->reserved_mask_pos, fb->reserved_mask_size);
+ }
+
+ print_dec("GPIOs", info->num_gpios);
+ printf("%12s: %4s %12s %3s %s\n", "id", "port", "polarity", "val",
+ "name");
+ for (i = 0; i < info->num_gpios; i++) {
+ const struct cb_gpio *gpio = &info->gpios[i];
+ char portstr[4];
+
+ if (gpio->port == 0xffffffff)
+ strcpy(portstr, "-");
+ else
+ sprintf(portstr, "%x", gpio->port);
+ printf("%12d: %4s %12s %3d %s\n", i, portstr,
+ gpio->polarity == CB_GPIO_ACTIVE_LOW ? "active-low" :
+ "active-high", gpio->value, gpio->name);
+ }
+ print_dec("MACs", info->num_macs);
+ for (i = 0; i < info->num_macs; i++) {
+ const struct mac_address *mac = &info->macs[i];
+ int j;
+
+ printf("%12d: ", i);
+ for (j = 0; j < sizeof(mac->mac_addr); j++)
+ printf("%s%02x", j ? ":" : "", mac->mac_addr[j]);
+ printf("\n");
+ }
+ print_str(">Serial #", info->serialno);
+ print_ptr("Multiboot tab", info->mbtable);
+ print_ptr("CB header", info->header);
+ print_ptr("CB mainboard", info->mainboard);
+ if (info->mainboard) {
+ struct cb_mainboard *mb = info->mainboard;
+
+ print_idx(">vendor", mb->vendor_idx, mb->strings);
+ print_idx(">part_number", mb->part_number_idx, mb->strings);
+ }
+ print_ptr("vboot handoff", info->vboot_handoff);
+ print_hex(">size", info->vboot_handoff_size);
+ print_ptr(">vdat addr", info->vdat_addr);
+ print_hex(">size", info->vdat_size);
+
+ print_addr64("SMBIOS", info->smbios_start);
+ print_hex(">size", info->smbios_size);
+ print_hex("ROM MTRR", info->x86_rom_var_mtrr_index);
+
+ print_ptr("Tstamp table", info->tstamp_table);
+ if (verbose && info->tstamp_table) {
+ struct timestamp_table *ts = info->tstamp_table;
+
+ printf("%-12s", "Base_time");
+ print_grouped_ull(ts->base_time, 12);
+ printf("\n");
+ print_dec("Tick MHz", ts->tick_freq_mhz);
+ for (i = 0; i < ts->num_entries; i++) {
+ const struct timestamp_entry *tse;
+
+ tse = &ts->entries[i];
+ printf(" ");
+ print_grouped_ull(tse->entry_stamp, 12);
+ printf(" %s\n", timestamp_name(tse->entry_id));
+ }
+ }
+
+ print_ptr("CBmem cons", info->cbmem_cons);
+ if (info->cbmem_cons) {
+ struct cbmem_console *cons = info->cbmem_cons;
+ int i;
+
+ print_hex("Size", cons->size);
+ print_hex("Cursor", cons->cursor);
+ if (verbose) {
+ for (i = 0; i < cons->cursor; i++) {
+ int ch = cons->body[i];
+
+ putc(ch);
+
+ if (ch == '\n') {
+ /* check for ctrl-c to abort... */
+ if (ctrlc()) {
+ puts("Abort\n");
+ return;
+ }
+ printf(" ");
+ }
+ }
+ printf("\n");
+ }
+ }
+
+ print_ptr("MRC cache", info->mrc_cache);
+ print_ptr("ACPI GNVS", info->acpi_gnvs);
+ print_hex("Board ID", info->board_id);
+ print_hex("RAM code", info->ram_code);
+ print_ptr("WiFi calib", info->wifi_calibration);
+ print_addr64("Ramoops buff", info->ramoops_buffer);
+ print_hex(">size", info->ramoops_buffer_size);
+ print_hex("SF size", info->spi_flash.size);
+ print_hex("SF sector", info->spi_flash.sector_size);
+ print_hex("SF erase cmd", info->spi_flash.erase_cmd);
+
+ print_addr64("FMAP offset", info->fmap_offset);
+ print_addr64("CBFS offset", info->cbfs_offset);
+ print_addr64("CBFS size", info->cbfs_size);
+ print_addr64("Boot media size", info->boot_media_size);
+ print_addr64("MTC start", info->mtc_start);
+ print_hex("MTC size", info->mtc_size);
+
+ print_ptr("Chrome OS VPD", info->chromeos_vpd);
+}
+
+static int do_cbsysinfo(struct cmd_tbl *cmdtp, int flag, int argc,
+ char *const argv[])
+{
+ bool verbose = false;
+
+ if (argc > 1) {
+ if (!strcmp("-v", argv[1]))
+ verbose = true;
+ else
+ return CMD_RET_USAGE;
+ }
+
+ if (!gd->arch.coreboot_table) {
+ printf("No coreboot sysinfo table found\n");
+ return CMD_RET_FAILURE;
+ }
+ show_table(&lib_sysinfo, verbose);
+
+ return 0;
+}
+
+U_BOOT_CMD(
+ cbsysinfo, 2, 1, do_cbsysinfo,
+ "Show coreboot sysinfo table",
+ "[-v] Dumps out the contents of the sysinfo table. This only\n"
+ "works if U-Boot is booted from coreboot"
+);
diff --git a/doc/usage/index.rst b/doc/usage/index.rst
index 35c515f8b590cdc9111effd1d04cf7b964197f2f..fb834349ca3d5fd1ca75879e5ddef64aacb46ce4 100644 (file)
--- a/doc/usage/index.rst
+++ b/doc/usage/index.rst
booti
bootmenu
button
+ x86/cbsysinfo
conitrace
echo
exception
diff --git a/doc/usage/x86/cbsysinfo.rst b/doc/usage/x86/cbsysinfo.rst
--- /dev/null
@@ -0,0 +1,25 @@
+.. SPDX-License-Identifier: GPL-2.0+
+
+cbsysinfo
+=========
+
+Synopis
+-------
+
+::
+
+ cbsysinfo
+
+
+Description
+-----------
+
+This displays information obtained from the coreboot sysinfo table. It is only
+useful when booting U-Boot from coreboot.
+
+Example
+-------
+
+::
+
+ => cbsysinfo