summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 018aad8)
raw | patch | inline | side by side (parent: 018aad8)
author | Sean Anderson <seanga2@gmail.com> | |
Tue, 27 Oct 2020 23:55:36 +0000 (19:55 -0400) | ||
committer | Tom Rini <trini@konsulko.com> | |
Fri, 30 Oct 2020 14:56:11 +0000 (10:56 -0400) |
Some commands can get very unweildy if they have too many positional
arguments. Adding options makes them easier to read, remember, and
understand.
This implementation of getopt has been taken from barebox, which has had
option support for quite a while. I have made a few modifications to their
version, such as the removal of opterr in favor of a separate getopt_silent
function. In addition, I have moved all global variables into struct
getopt_context.
The getopt from barebox also re-orders the arguments passed to it so that
non-options are placed last. This allows users to specify options anywhere.
For example, `ls -l foo/ -R` would be re-ordered to `ls -l -R foo/` as
getopt parsed the options. However, this feature conflicts with the const
argv in cmd_tbl->cmd. This was originally added in 54841ab50c ("Make sure
that argv[] argument pointers are not modified."). The reason stated in
that commit is that hush requires argv to stay unmodified. Has this
situation changed? Barebox also uses hush, and does not have this problem.
Perhaps we could use their fix?
I have assigned maintenance of getopt to Simon Glass, as it is currently
only used by the log command. I would also be fine maintaining it.
Signed-off-by: Sean Anderson <seanga2@gmail.com>
arguments. Adding options makes them easier to read, remember, and
understand.
This implementation of getopt has been taken from barebox, which has had
option support for quite a while. I have made a few modifications to their
version, such as the removal of opterr in favor of a separate getopt_silent
function. In addition, I have moved all global variables into struct
getopt_context.
The getopt from barebox also re-orders the arguments passed to it so that
non-options are placed last. This allows users to specify options anywhere.
For example, `ls -l foo/ -R` would be re-ordered to `ls -l -R foo/` as
getopt parsed the options. However, this feature conflicts with the const
argv in cmd_tbl->cmd. This was originally added in 54841ab50c ("Make sure
that argv[] argument pointers are not modified."). The reason stated in
that commit is that hush requires argv to stay unmodified. Has this
situation changed? Barebox also uses hush, and does not have this problem.
Perhaps we could use their fix?
I have assigned maintenance of getopt to Simon Glass, as it is currently
only used by the log command. I would also be fine maintaining it.
Signed-off-by: Sean Anderson <seanga2@gmail.com>
MAINTAINERS | patch | blob | history | |
doc/api/getopt.rst | [new file with mode: 0644] | patch | blob |
doc/api/index.rst | patch | blob | history | |
include/getopt.h | [new file with mode: 0644] | patch | blob |
lib/Kconfig | patch | blob | history | |
lib/Makefile | patch | blob | history | |
lib/getopt.c | [new file with mode: 0644] | patch | blob |
diff --git a/MAINTAINERS b/MAINTAINERS
index 1505e745590796f380550c6294606d85107d92d5..874cf2c0e576645df13058381c79af7884433e5d 100644 (file)
--- a/MAINTAINERS
+++ b/MAINTAINERS
F: common/log*
F: cmd/log.c
F: doc/develop/logging.rst
+F: lib/getopt.c
F: test/log/
F: test/py/tests/test_log.py
diff --git a/doc/api/getopt.rst b/doc/api/getopt.rst
--- /dev/null
+++ b/doc/api/getopt.rst
@@ -0,0 +1,8 @@
+.. SPDX-License-Identifier: GPL-2.0+
+.. Copyright (C) 2020 Sean Anderson <seanga2@gmail.com>
+
+Option Parsing
+==============
+
+.. kernel-doc:: include/getopt.h
+ :internal:
diff --git a/doc/api/index.rst b/doc/api/index.rst
index 787b6778e591594b1d783adb9ababc1e9869c0f4..ae4a1b6c634019cfefa4186677356af6c27d95c4 100644 (file)
--- a/doc/api/index.rst
+++ b/doc/api/index.rst
dfu
efi
+ getopt
linker_lists
pinctrl
rng
diff --git a/include/getopt.h b/include/getopt.h
--- /dev/null
+++ b/include/getopt.h
@@ -0,0 +1,130 @@
+/* SPDX-License-Identifier: GPL-2.0-only */
+/*
+ * getopt.h - a simple getopt(3) implementation.
+ *
+ * Copyright (C) 2020 Sean Anderson <seanga2@gmail.com>
+ * Copyright (c) 2007 Sascha Hauer <s.hauer@pengutronix.de>, Pengutronix
+ */
+
+#ifndef __GETOPT_H
+#define __GETOPT_H
+
+/**
+ * struct getopt_state - Saved state across getopt() calls
+ */
+struct getopt_state {
+ /**
+ * @index: Index of the next unparsed argument of @argv. If getopt() has
+ * parsed all of @argv, then @index will equal @argc.
+ */
+ int index;
+ /* private: */
+ /** @arg_index: Index within the current argument */
+ int arg_index;
+ union {
+ /* public: */
+ /**
+ * @opt: Option being parsed when an error occurs. @opt is only
+ * valid when getopt() returns ``?`` or ``:``.
+ */
+ int opt;
+ /**
+ * @arg: The argument to an option, NULL if there is none. @arg
+ * is only valid when getopt() returns an option character.
+ */
+ char *arg;
+ /* private: */
+ };
+};
+
+/**
+ * getopt_init_state() - Initialize a &struct getopt_state
+ * @gs: The state to initialize
+ *
+ * This must be called before using @gs with getopt().
+ */
+void getopt_init_state(struct getopt_state *gs);
+
+int __getopt(struct getopt_state *gs, int argc, char *const argv[],
+ const char *optstring, bool silent);
+
+/**
+ * getopt() - Parse short command-line options
+ * @gs: Internal state and out-of-band return arguments. This must be
+ * initialized with getopt_init_context() beforehand.
+ * @argc: Number of arguments, not including the %NULL terminator
+ * @argv: Argument list, terminated by %NULL
+ * @optstring: Option specification, as described below
+ *
+ * getopt() parses short options. Short options are single characters. They may
+ * be followed by a required argument or an optional argument. Arguments to
+ * options may occur in the same argument as an option (like ``-larg``), or
+ * in the following argument (like ``-l arg``). An argument containing
+ * options begins with a ``-``. If an option expects no arguments, then it may
+ * be immediately followed by another option (like ``ls -alR``).
+ *
+ * @optstring is a list of accepted options. If an option is followed by ``:``
+ * in @optstring, then it expects a mandatory argument. If an option is followed
+ * by ``::`` in @optstring, it expects an optional argument. @gs.arg points
+ * to the argument, if one is parsed.
+ *
+ * getopt() stops parsing options when it encounters the first non-option
+ * argument, when it encounters the argument ``--``, or when it runs out of
+ * arguments. For example, in ``ls -l foo -R``, option parsing will stop when
+ * getopt() encounters ``foo``, if ``l`` does not expect an argument. However,
+ * the whole list of arguments would be parsed if ``l`` expects an argument.
+ *
+ * An example invocation of getopt() might look like::
+ *
+ * char *argv[] = { "program", "-cbx", "-a", "foo", "bar", 0 };
+ * int opt, argc = ARRAY_SIZE(argv) - 1;
+ * struct getopt_state gs;
+ *
+ * getopt_init_state(&gs);
+ * while ((opt = getopt(&gs, argc, argv, "a::b:c")) != -1)
+ * printf("opt = %c, index = %d, arg = \"%s\"\n", opt, gs.index, gs.arg);
+ * printf("%d argument(s) left\n", argc - gs.index);
+ *
+ * and would produce an output of::
+ *
+ * opt = c, index = 1, arg = "<NULL>"
+ * opt = b, index = 2, arg = "x"
+ * opt = a, index = 4, arg = "foo"
+ * 1 argument(s) left
+ *
+ * For further information, refer to the getopt(3) man page.
+ *
+ * Return:
+ * * An option character if an option is found. @gs.arg is set to the
+ * argument if there is one, otherwise it is set to ``NULL``.
+ * * ``-1`` if there are no more options, if a non-option argument is
+ * encountered, or if an ``--`` argument is encountered.
+ * * ``'?'`` if we encounter an option not in @optstring. @gs.opt is set to
+ * the unknown option.
+ * * ``':'`` if an argument is required, but no argument follows the
+ * option. @gs.opt is set to the option missing its argument.
+ *
+ * @gs.index is always set to the index of the next unparsed argument in @argv.
+ */
+static inline int getopt(struct getopt_state *gs, int argc,
+ char *const argv[], const char *optstring)
+{
+ return __getopt(gs, argc, argv, optstring, false);
+}
+
+/**
+ * getopt_silent() - Parse short command-line options silently
+ * @gs: State
+ * @argc: Argument count
+ * @argv: Argument list
+ * @optstring: Option specification
+ *
+ * Same as getopt(), except no error messages are printed.
+ */
+static inline int getopt_silent(struct getopt_state *gs, int argc,
+ char *const argv[], const char *optstring)
+{
+ return __getopt(gs, argc, argv, optstring, true);
+}
+
+#endif /* __GETOPT_H */
diff --git a/lib/Kconfig b/lib/Kconfig
index 37aae73a266403e06b95e5f425d19959a26512d4..79651eaad199fcc4526466653f4e7f3ef53c881b 100644 (file)
--- a/lib/Kconfig
+++ b/lib/Kconfig
This enables functions for printing dumps of binary data in
SPL.
+config GETOPT
+ bool "Enable getopt"
+ help
+ This enables functions for parsing command-line options.
+
config OF_LIBFDT
bool "Enable the FDT library"
default y if OF_CONTROL
diff --git a/lib/Makefile b/lib/Makefile
index 0cd7bea282366eff6314772344b6a77d326f9f5b..7c7fb9aae78c2573caa1670445d07386fad1a63c 100644 (file)
--- a/lib/Makefile
+++ b/lib/Makefile
obj-y += tables_csum.o
obj-y += time.o
obj-y += hexdump.o
+obj-$(CONFIG_GETOPT) += getopt.o
obj-$(CONFIG_TRACE) += trace.o
obj-$(CONFIG_LIB_UUID) += uuid.o
obj-$(CONFIG_LIB_RAND) += rand.o
diff --git a/lib/getopt.c b/lib/getopt.c
--- /dev/null
+++ b/lib/getopt.c
@@ -0,0 +1,125 @@
+// SPDX-License-Identifier: GPL-2.0-only
+/*
+ * getopt.c - a simple getopt(3) implementation. See getopt.h for explanation.
+ *
+ * Copyright (C) 2020 Sean Anderson <seanga2@gmail.com>
+ * Copyright (c) 2007 Sascha Hauer <s.hauer@pengutronix.de>, Pengutronix
+ */
+
+#define LOG_CATEGORY LOGC_CORE
+
+#include <common.h>
+#include <getopt.h>
+#include <log.h>
+
+void getopt_init_state(struct getopt_state *gs)
+{
+ gs->index = 1;
+ gs->arg_index = 1;
+}
+
+int __getopt(struct getopt_state *gs, int argc, char *const argv[],
+ const char *optstring, bool silent)
+{
+ char curopt; /* current option character */
+ const char *curoptp; /* pointer to the current option in optstring */
+
+ while (1) {
+ log_debug("arg_index: %d index: %d\n", gs->arg_index,
+ gs->index);
+
+ /* `--` indicates the end of options */
+ if (gs->arg_index == 1 && argv[gs->index] &&
+ !strcmp(argv[gs->index], "--")) {
+ gs->index++;
+ return -1;
+ }
+
+ /* Out of arguments */
+ if (gs->index >= argc)
+ return -1;
+
+ /* Can't parse non-options */
+ if (*argv[gs->index] != '-')
+ return -1;
+
+ /* We have found an option */
+ curopt = argv[gs->index][gs->arg_index];
+ if (curopt)
+ break;
+ /*
+ * no more options in current argv[] element; try the next one
+ */
+ gs->index++;
+ gs->arg_index = 1;
+ }
+
+ /* look up current option in optstring */
+ curoptp = strchr(optstring, curopt);
+
+ if (!curoptp) {
+ if (!silent)
+ printf("%s: invalid option -- %c\n", argv[0], curopt);
+ gs->opt = curopt;
+ gs->arg_index++;
+ return '?';
+ }
+
+ if (*(curoptp + 1) != ':') {
+ /* option with no argument. Just return it */
+ gs->arg = NULL;
+ gs->arg_index++;
+ return curopt;
+ }
+
+ if (*(curoptp + 1) && *(curoptp + 2) == ':') {
+ /* optional argument */
+ if (argv[gs->index][gs->arg_index + 1]) {
+ /* optional argument with directly following arg */
+ gs->arg = argv[gs->index++] + gs->arg_index + 1;
+ gs->arg_index = 1;
+ return curopt;
+ }
+ if (gs->index + 1 == argc) {
+ /* We are at the last argv[] element */
+ gs->arg = NULL;
+ gs->index++;
+ return curopt;
+ }
+ if (*argv[gs->index + 1] != '-') {
+ /*
+ * optional argument with arg in next argv[] element
+ */
+ gs->index++;
+ gs->arg = argv[gs->index++];
+ gs->arg_index = 1;
+ return curopt;
+ }
+
+ /* no optional argument found */
+ gs->arg = NULL;
+ gs->arg_index = 1;
+ gs->index++;
+ return curopt;
+ }
+
+ if (argv[gs->index][gs->arg_index + 1]) {
+ /* required argument with directly following arg */
+ gs->arg = argv[gs->index++] + gs->arg_index + 1;
+ gs->arg_index = 1;
+ return curopt;
+ }
+
+ gs->index++;
+ gs->arg_index = 1;
+
+ if (gs->index >= argc || argv[gs->index][0] == '-') {
+ if (!silent)
+ printf("option requires an argument -- %c\n", curopt);
+ gs->opt = curopt;
+ return ':';
+ }
+
+ gs->arg = argv[gs->index++];
+ return curopt;
+}