summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: f191f3a)
raw | patch | inline | side by side (parent: f191f3a)
author | Reuben Dowle <reubendowle0@gmail.com> | |
Thu, 16 Apr 2020 05:36:52 +0000 (17:36 +1200) | ||
committer | Tom Rini <trini@konsulko.com> | |
Fri, 12 Jun 2020 17:14:07 +0000 (13:14 -0400) |
The current recommendation for best security practice from the US government
is to use SHA384 for TOP SECRET [1].
This patch adds support for SHA384 and SHA512 in the hash command, and also
allows FIT images to be hashed with these algorithms, and signed with
sha384,rsaXXXX and sha512,rsaXXXX
The SHA implementation is adapted from the linux kernel implementation.
[1] Commercial National Security Algorithm Suite
http://www.iad.gov/iad/programs/iad-initiatives/cnsa-suite.cfm
Signed-off-by: Reuben Dowle <reuben.dowle@4rf.com>
is to use SHA384 for TOP SECRET [1].
This patch adds support for SHA384 and SHA512 in the hash command, and also
allows FIT images to be hashed with these algorithms, and signed with
sha384,rsaXXXX and sha512,rsaXXXX
The SHA implementation is adapted from the linux kernel implementation.
[1] Commercial National Security Algorithm Suite
http://www.iad.gov/iad/programs/iad-initiatives/cnsa-suite.cfm
Signed-off-by: Reuben Dowle <reuben.dowle@4rf.com>
13 files changed:
Kconfig | patch | blob | history | |
common/hash.c | patch | blob | history | |
common/image-fit.c | patch | blob | history | |
common/image-sig.c | patch | blob | history | |
common/spl/Kconfig | patch | blob | history | |
include/hash.h | patch | blob | history | |
include/image.h | patch | blob | history | |
include/u-boot/rsa-checksum.h | patch | blob | history | |
include/u-boot/sha512.h | [new file with mode: 0644] | patch | blob |
lib/Kconfig | patch | blob | history | |
lib/Makefile | patch | blob | history | |
lib/sha512.c | [new file with mode: 0644] | patch | blob |
tools/Makefile | patch | blob | history |
index 0e7ccc0b074cb0300d1e12018b2606d208e0851d..34a88ebe34896ed5f66e11dcc8086776302012fb 100644 (file)
--- a/Kconfig
+++ b/Kconfig
help
Enable this to support SHA256 checksum of FIT image contents. A
SHA256 checksum is a 256-bit (32-byte) hash value used to check that
- the image contents have not been corrupted. SHA256 is recommended
- for use in secure applications since (as at 2016) there is no known
- feasible attack that could produce a 'collision' with differing
- input data. Use this for the highest security. Note that only the
- SHA256 variant is supported: SHA512 and others are not currently
- supported in U-Boot.
+ the image contents have not been corrupted.
+
+config FIT_ENABLE_SHA384_SUPPORT
+ bool "Support SHA384 checksum of FIT image contents"
+ default n
+ select SHA384
+ help
+ Enable this to support SHA384 checksum of FIT image contents. A
+ SHA384 checksum is a 384-bit (48-byte) hash value used to check that
+ the image contents have not been corrupted. Use this for the highest
+ security.
+
+config FIT_ENABLE_SHA512_SUPPORT
+ bool "Support SHA512 checksum of FIT image contents"
+ default n
+ select SHA512
+ help
+ Enable this to support SHA512 checksum of FIT image contents. A
+ SHA512 checksum is a 512-bit (64-byte) hash value used to check that
+ the image contents have not been corrupted.
config FIT_SIGNATURE
bool "Enable signature verification of FIT uImages"
diff --git a/common/hash.c b/common/hash.c
index 8c00659d252891b631f6299bdae9c789a72cab5d..5c75848b7d92e0a05b1eaebb04a52cd88a45f46d 100644 (file)
--- a/common/hash.c
+++ b/common/hash.c
#include <u-boot/crc.h>
#include <u-boot/sha1.h>
#include <u-boot/sha256.h>
+#include <u-boot/sha512.h>
#include <u-boot/md5.h>
#if !defined(USE_HOSTCC) && defined(CONFIG_NEEDS_MANUAL_RELOC)
}
#endif
+#if defined(CONFIG_SHA384)
+static int hash_init_sha384(struct hash_algo *algo, void **ctxp)
+{
+ sha512_context *ctx = malloc(sizeof(sha512_context));
+ sha384_starts(ctx);
+ *ctxp = ctx;
+ return 0;
+}
+
+static int hash_update_sha384(struct hash_algo *algo, void *ctx,
+ const void *buf, unsigned int size, int is_last)
+{
+ sha384_update((sha512_context *)ctx, buf, size);
+ return 0;
+}
+
+static int hash_finish_sha384(struct hash_algo *algo, void *ctx, void
+ *dest_buf, int size)
+{
+ if (size < algo->digest_size)
+ return -1;
+
+ sha384_finish((sha512_context *)ctx, dest_buf);
+ free(ctx);
+ return 0;
+}
+#endif
+
+#if defined(CONFIG_SHA512)
+static int hash_init_sha512(struct hash_algo *algo, void **ctxp)
+{
+ sha512_context *ctx = malloc(sizeof(sha512_context));
+ sha512_starts(ctx);
+ *ctxp = ctx;
+ return 0;
+}
+
+static int hash_update_sha512(struct hash_algo *algo, void *ctx,
+ const void *buf, unsigned int size, int is_last)
+{
+ sha512_update((sha512_context *)ctx, buf, size);
+ return 0;
+}
+
+static int hash_finish_sha512(struct hash_algo *algo, void *ctx, void
+ *dest_buf, int size)
+{
+ if (size < algo->digest_size)
+ return -1;
+
+ printf("hello world\n");
+
+ sha512_finish((sha512_context *)ctx, dest_buf);
+ free(ctx);
+ return 0;
+}
+#endif
+
+
static int hash_init_crc16_ccitt(struct hash_algo *algo, void **ctxp)
{
uint16_t *ctx = malloc(sizeof(uint16_t));
.hash_finish = hash_finish_sha256,
#endif
},
+#endif
+#ifdef CONFIG_SHA384
+ {
+ .name = "sha384",
+ .digest_size = SHA384_SUM_LEN,
+ .chunk_size = CHUNKSZ_SHA384,
+ .hash_func_ws = sha384_csum_wd,
+ .hash_init = hash_init_sha384,
+ .hash_update = hash_update_sha384,
+ .hash_finish = hash_finish_sha384,
+ },
+#endif
+#ifdef CONFIG_SHA512
+ {
+ .name = "sha512",
+ .digest_size = SHA512_SUM_LEN,
+ .chunk_size = CHUNKSZ_SHA512,
+ .hash_func_ws = sha512_csum_wd,
+ .hash_init = hash_init_sha512,
+ .hash_update = hash_update_sha512,
+ .hash_finish = hash_finish_sha512,
+ },
#endif
{
.name = "crc16-ccitt",
/* Try to minimize code size for boards that don't want much hashing */
#if defined(CONFIG_SHA256) || defined(CONFIG_CMD_SHA1SUM) || \
- defined(CONFIG_CRC32_VERIFY) || defined(CONFIG_CMD_HASH)
+ defined(CONFIG_CRC32_VERIFY) || defined(CONFIG_CMD_HASH) || \
+ defined(CONFIG_SHA384) || defined(CONFIG_SHA512)
#define multi_hash() 1
#else
#define multi_hash() 0
diff --git a/common/image-fit.c b/common/image-fit.c
index 1ece100a21455bc0f699c1dacd562ee619e1966a..d54eff9033cc25ebf07bfa72d182645c9aa60fca 100644 (file)
--- a/common/image-fit.c
+++ b/common/image-fit.c
#include <u-boot/md5.h>
#include <u-boot/sha1.h>
#include <u-boot/sha256.h>
+#include <u-boot/sha512.h>
/*****************************************************************************/
/* New uImage format routines */
sha256_csum_wd((unsigned char *)data, data_len,
(unsigned char *)value, CHUNKSZ_SHA256);
*value_len = SHA256_SUM_LEN;
+ } else if (IMAGE_ENABLE_SHA384 && strcmp(algo, "sha384") == 0) {
+ sha384_csum_wd((unsigned char *)data, data_len,
+ (unsigned char *)value, CHUNKSZ_SHA384);
+ *value_len = SHA384_SUM_LEN;
+ } else if (IMAGE_ENABLE_SHA512 && strcmp(algo, "sha512") == 0) {
+ sha512_csum_wd((unsigned char *)data, data_len,
+ (unsigned char *)value, CHUNKSZ_SHA512);
+ *value_len = SHA512_SUM_LEN;
} else if (IMAGE_ENABLE_MD5 && strcmp(algo, "md5") == 0) {
md5_wd((unsigned char *)data, data_len, value, CHUNKSZ_MD5);
*value_len = 16;
diff --git a/common/image-sig.c b/common/image-sig.c
index 498969d64141d5e55c593627c66835cec7d3aa66..f3c209ae8b72a8564a4ca610af138689b712205e 100644 (file)
--- a/common/image-sig.c
+++ b/common/image-sig.c
.calculate_sign = EVP_sha256,
#endif
.calculate = hash_calculate,
- }
+ },
+#ifdef CONFIG_SHA384
+ {
+ .name = "sha384",
+ .checksum_len = SHA384_SUM_LEN,
+ .der_len = SHA384_DER_LEN,
+ .der_prefix = sha384_der_prefix,
+#if IMAGE_ENABLE_SIGN
+ .calculate_sign = EVP_sha384,
+#endif
+ .calculate = hash_calculate,
+ },
+#endif
+#ifdef CONFIG_SHA512
+ {
+ .name = "sha512",
+ .checksum_len = SHA512_SUM_LEN,
+ .der_len = SHA512_DER_LEN,
+ .der_prefix = sha512_der_prefix,
+#if IMAGE_ENABLE_SIGN
+ .calculate_sign = EVP_sha512,
+#endif
+ .calculate = hash_calculate,
+ },
+#endif
};
diff --git a/common/spl/Kconfig b/common/spl/Kconfig
index 8ece9057b1e64d87f925ff6b9a35db7ca8c10610..3eae65ebc1997b7ec929154ebf24e9d85f9c5d12 100644 (file)
--- a/common/spl/Kconfig
+++ b/common/spl/Kconfig
secure as it is possible (with a brute-force attack) to adjust the
image while still retaining the same MD5 hash value. For secure
applications where images may be changed maliciously, you should
- consider SHA1 or SHA256.
+ consider SHA256 or SHA384.
config SPL_SHA1_SUPPORT
bool "Support SHA1"
image contents have not been corrupted or maliciously altered.
While SHA1 is fairly secure it is coming to the end of its life
due to the expanding computing power available to brute-force
- attacks. For more security, consider SHA256.
+ attacks. For more security, consider SHA256 or SHA384.
config SPL_SHA256_SUPPORT
bool "Support SHA256"
help
Enable this to support SHA256 in FIT images within SPL. A SHA256
checksum is a 256-bit (32-byte) hash value used to check that the
- image contents have not been corrupted. SHA256 is recommended for
- use in secure applications since (as at 2016) there is no known
- feasible attack that could produce a 'collision' with differing
- input data. Use this for the highest security. Note that only the
- SHA256 variant is supported: SHA512 and others are not currently
- supported in U-Boot.
+ image contents have not been corrupted.
+
+config SPL_SHA384_SUPPORT
+ bool "Support SHA384"
+ depends on SPL_FIT
+ select SHA384
+ select SHA512_ALGO
+ help
+ Enable this to support SHA384 in FIT images within SPL. A SHA384
+ checksum is a 384-bit (48-byte) hash value used to check that the
+ image contents have not been corrupted. Use this for the highest
+ security.
+
+config SPL_SHA512_SUPPORT
+ bool "Support SHA512"
+ depends on SPL_FIT
+ select SHA512
+ select SHA512_ALGO
+ help
+ Enable this to support SHA512 in FIT images within SPL. A SHA512
+ checksum is a 512-bit (64-byte) hash value used to check that the
+ image contents have not been corrupted.
config SPL_FIT_IMAGE_TINY
bool "Remove functionality from SPL FIT loading to reduce size"
diff --git a/include/hash.h b/include/hash.h
index 835962e7f661dae9356f4ae4258a6f44f6ff39b9..97bb3ed5d9ac0b74704e841a1750b8c687e85471 100644 (file)
--- a/include/hash.h
+++ b/include/hash.h
* Maximum digest size for all algorithms we support. Having this value
* avoids a malloc() or C99 local declaration in common/cmd_hash.c.
*/
+#if defined(CONFIG_SHA384) || defined(CONFIG_SHA512)
+#define HASH_MAX_DIGEST_SIZE 64
+#else
#define HASH_MAX_DIGEST_SIZE 32
+#endif
enum {
HASH_FLAG_VERIFY = 1 << 0, /* Enable verify mode */
diff --git a/include/image.h b/include/image.h
index ad81dad44429da7ab1b77fb8686ceb2fd2ce3ebb..ebd581a594444757a609af59d5fda30e8fc6eef9 100644 (file)
--- a/include/image.h
+++ b/include/image.h
#define CONFIG_FIT_VERBOSE 1 /* enable fit_format_{error,warning}() */
#define CONFIG_FIT_ENABLE_RSASSA_PSS_SUPPORT 1
#define CONFIG_FIT_ENABLE_SHA256_SUPPORT
+#define CONFIG_FIT_ENABLE_SHA384_SUPPORT
+#define CONFIG_FIT_ENABLE_SHA512_SUPPORT
#define CONFIG_SHA1
#define CONFIG_SHA256
+#define CONFIG_SHA384
+#define CONFIG_SHA512
#define IMAGE_ENABLE_IGNORE 0
#define IMAGE_INDENT_STRING ""
#define IMAGE_ENABLE_SHA256 0
#endif
+#if defined(CONFIG_FIT_ENABLE_SHA384_SUPPORT) || \
+ defined(CONFIG_SPL_SHA384_SUPPORT)
+#define IMAGE_ENABLE_SHA384 1
+#else
+#define IMAGE_ENABLE_SHA384 0
+#endif
+
+#if defined(CONFIG_FIT_ENABLE_SHA512_SUPPORT) || \
+ defined(CONFIG_SPL_SHA512_SUPPORT)
+#define IMAGE_ENABLE_SHA512 1
+#else
+#define IMAGE_ENABLE_SHA512 0
+#endif
+
#endif /* IMAGE_ENABLE_FIT */
#ifdef CONFIG_SYS_BOOT_GET_CMDLINE
index 02b814d34e32e9a805af6ec3e449b3187c0fb961..54e6a73744e1fe3861abb464c31164ff4537e593 100644 (file)
#include <image.h>
#include <u-boot/sha1.h>
#include <u-boot/sha256.h>
+#include <u-boot/sha512.h>
/**
* hash_calculate() - Calculate hash over the data
diff --git a/include/u-boot/sha512.h b/include/u-boot/sha512.h
--- /dev/null
+++ b/include/u-boot/sha512.h
@@ -0,0 +1,38 @@
+#ifndef _SHA512_H
+#define _SHA512_H
+
+#define SHA384_SUM_LEN 48
+#define SHA384_DER_LEN 19
+#define SHA512_SUM_LEN 64
+#define SHA512_DER_LEN 19
+#define SHA512_BLOCK_SIZE 128
+
+#define CHUNKSZ_SHA384 (16 * 1024)
+#define CHUNKSZ_SHA512 (16 * 1024)
+
+typedef struct {
+ uint64_t state[SHA512_SUM_LEN / 8];
+ uint64_t count[2];
+ uint8_t buf[SHA512_BLOCK_SIZE];
+} sha512_context;
+
+extern const uint8_t sha512_der_prefix[];
+
+void sha512_starts(sha512_context * ctx);
+void sha512_update(sha512_context *ctx, const uint8_t *input, uint32_t length);
+void sha512_finish(sha512_context * ctx, uint8_t digest[SHA512_SUM_LEN]);
+
+void sha512_csum_wd(const unsigned char *input, unsigned int ilen,
+ unsigned char *output, unsigned int chunk_sz);
+
+extern const uint8_t sha384_der_prefix[];
+
+void sha384_starts(sha512_context * ctx);
+void sha384_update(sha512_context *ctx, const uint8_t *input, uint32_t length);
+void sha384_finish(sha512_context * ctx, uint8_t digest[SHA384_SUM_LEN]);
+
+void sha384_csum_wd(const unsigned char *input, unsigned int ilen,
+ unsigned char *output, unsigned int chunk_sz);
+
+
+#endif /* _SHA512_H */
diff --git a/lib/Kconfig b/lib/Kconfig
index af5c38afd98b29a05024a7108369fcc1f27ce362..fc7d68487b21abd4170422785b233262c7845b1c 100644 (file)
--- a/lib/Kconfig
+++ b/lib/Kconfig
The SHA256 algorithm produces a 256-bit (32-byte) hash value
(digest).
+config SHA512_ALGO
+ bool "Enable SHA512 algorithm"
+ help
+ This option enables support of internal SHA512 algorithm.
+
+config SHA512
+ bool "Enable SHA512 support"
+ depends on SHA512_ALGO
+ help
+ This option enables support of hashing using SHA512 algorithm.
+ The hash is calculated in software.
+ The SHA512 algorithm produces a 512-bit (64-byte) hash value
+ (digest).
+
+config SHA384
+ bool "Enable SHA384 support"
+ depends on SHA512_ALGO
+ help
+ This option enables support of hashing using SHA384 algorithm.
+ The hash is calculated in software.
+ The SHA384 algorithm produces a 384-bit (48-byte) hash value
+ (digest).
+
config SHA_HW_ACCEL
bool "Enable hashing using hardware"
help
diff --git a/lib/Makefile b/lib/Makefile
index dc5761966c4373eed9f23aee1191faef41591d2b..1dc06c57d5fda4a76bff08b36ecc7be1b6f99f33 100644 (file)
--- a/lib/Makefile
+++ b/lib/Makefile
obj-$(CONFIG_$(SPL_)RSA) += rsa/
obj-$(CONFIG_SHA1) += sha1.o
obj-$(CONFIG_SHA256) += sha256.o
+obj-$(CONFIG_SHA512_ALGO) += sha512.o
obj-$(CONFIG_$(SPL_)ZLIB) += zlib/
obj-$(CONFIG_$(SPL_)ZSTD) += zstd/
diff --git a/lib/sha512.c b/lib/sha512.c
--- /dev/null
+++ b/lib/sha512.c
@@ -0,0 +1,383 @@
+// SPDX-License-Identifier: GPL-2.0+
+/*
+ * FIPS-180-2 compliant SHA-512 and SHA-384 implementation
+ *
+ * SHA-512 code by Jean-Luc Cooke <jlcooke@certainkey.com>
+ *
+ * Copyright (c) Jean-Luc Cooke <jlcooke@certainkey.com>
+ * Copyright (c) Andrew McDonald <andrew@mcdonald.org.uk>
+ * Copyright (c) 2003 Kyle McMartin <kyle@debian.org>
+ * Copyright (c) 2020 Reuben Dowle <reuben.dowle@4rf.com>
+ */
+
+#ifndef USE_HOSTCC
+#include <common.h>
+#include <linux/string.h>
+#else
+#include <string.h>
+#endif /* USE_HOSTCC */
+#include <watchdog.h>
+#include <u-boot/sha512.h>
+
+const uint8_t sha384_der_prefix[SHA384_DER_LEN] = {
+ 0x30, 0x41, 0x30, 0x0d, 0x06, 0x09, 0x60, 0x86,
+ 0x48, 0x01, 0x65, 0x03, 0x04, 0x02, 0x02, 0x05,
+ 0x00, 0x04, 0x30
+};
+
+const uint8_t sha512_der_prefix[SHA512_DER_LEN] = {
+ 0x30, 0x51, 0x30, 0x0d, 0x06, 0x09, 0x60, 0x86,
+ 0x48, 0x01, 0x65, 0x03, 0x04, 0x02, 0x03, 0x05,
+ 0x00, 0x04, 0x40
+};
+
+#define SHA384_H0 0xcbbb9d5dc1059ed8ULL
+#define SHA384_H1 0x629a292a367cd507ULL
+#define SHA384_H2 0x9159015a3070dd17ULL
+#define SHA384_H3 0x152fecd8f70e5939ULL
+#define SHA384_H4 0x67332667ffc00b31ULL
+#define SHA384_H5 0x8eb44a8768581511ULL
+#define SHA384_H6 0xdb0c2e0d64f98fa7ULL
+#define SHA384_H7 0x47b5481dbefa4fa4ULL
+
+#define SHA512_H0 0x6a09e667f3bcc908ULL
+#define SHA512_H1 0xbb67ae8584caa73bULL
+#define SHA512_H2 0x3c6ef372fe94f82bULL
+#define SHA512_H3 0xa54ff53a5f1d36f1ULL
+#define SHA512_H4 0x510e527fade682d1ULL
+#define SHA512_H5 0x9b05688c2b3e6c1fULL
+#define SHA512_H6 0x1f83d9abfb41bd6bULL
+#define SHA512_H7 0x5be0cd19137e2179ULL
+
+static inline uint64_t Ch(uint64_t x, uint64_t y, uint64_t z)
+{
+ return z ^ (x & (y ^ z));
+}
+
+static inline uint64_t Maj(uint64_t x, uint64_t y, uint64_t z)
+{
+ return (x & y) | (z & (x | y));
+}
+
+static const uint64_t sha512_K[80] = {
+ 0x428a2f98d728ae22ULL, 0x7137449123ef65cdULL, 0xb5c0fbcfec4d3b2fULL,
+ 0xe9b5dba58189dbbcULL, 0x3956c25bf348b538ULL, 0x59f111f1b605d019ULL,
+ 0x923f82a4af194f9bULL, 0xab1c5ed5da6d8118ULL, 0xd807aa98a3030242ULL,
+ 0x12835b0145706fbeULL, 0x243185be4ee4b28cULL, 0x550c7dc3d5ffb4e2ULL,
+ 0x72be5d74f27b896fULL, 0x80deb1fe3b1696b1ULL, 0x9bdc06a725c71235ULL,
+ 0xc19bf174cf692694ULL, 0xe49b69c19ef14ad2ULL, 0xefbe4786384f25e3ULL,
+ 0x0fc19dc68b8cd5b5ULL, 0x240ca1cc77ac9c65ULL, 0x2de92c6f592b0275ULL,
+ 0x4a7484aa6ea6e483ULL, 0x5cb0a9dcbd41fbd4ULL, 0x76f988da831153b5ULL,
+ 0x983e5152ee66dfabULL, 0xa831c66d2db43210ULL, 0xb00327c898fb213fULL,
+ 0xbf597fc7beef0ee4ULL, 0xc6e00bf33da88fc2ULL, 0xd5a79147930aa725ULL,
+ 0x06ca6351e003826fULL, 0x142929670a0e6e70ULL, 0x27b70a8546d22ffcULL,
+ 0x2e1b21385c26c926ULL, 0x4d2c6dfc5ac42aedULL, 0x53380d139d95b3dfULL,
+ 0x650a73548baf63deULL, 0x766a0abb3c77b2a8ULL, 0x81c2c92e47edaee6ULL,
+ 0x92722c851482353bULL, 0xa2bfe8a14cf10364ULL, 0xa81a664bbc423001ULL,
+ 0xc24b8b70d0f89791ULL, 0xc76c51a30654be30ULL, 0xd192e819d6ef5218ULL,
+ 0xd69906245565a910ULL, 0xf40e35855771202aULL, 0x106aa07032bbd1b8ULL,
+ 0x19a4c116b8d2d0c8ULL, 0x1e376c085141ab53ULL, 0x2748774cdf8eeb99ULL,
+ 0x34b0bcb5e19b48a8ULL, 0x391c0cb3c5c95a63ULL, 0x4ed8aa4ae3418acbULL,
+ 0x5b9cca4f7763e373ULL, 0x682e6ff3d6b2b8a3ULL, 0x748f82ee5defb2fcULL,
+ 0x78a5636f43172f60ULL, 0x84c87814a1f0ab72ULL, 0x8cc702081a6439ecULL,
+ 0x90befffa23631e28ULL, 0xa4506cebde82bde9ULL, 0xbef9a3f7b2c67915ULL,
+ 0xc67178f2e372532bULL, 0xca273eceea26619cULL, 0xd186b8c721c0c207ULL,
+ 0xeada7dd6cde0eb1eULL, 0xf57d4f7fee6ed178ULL, 0x06f067aa72176fbaULL,
+ 0x0a637dc5a2c898a6ULL, 0x113f9804bef90daeULL, 0x1b710b35131c471bULL,
+ 0x28db77f523047d84ULL, 0x32caab7b40c72493ULL, 0x3c9ebe0a15c9bebcULL,
+ 0x431d67c49c100d4cULL, 0x4cc5d4becb3e42b6ULL, 0x597f299cfc657e2aULL,
+ 0x5fcb6fab3ad6faecULL, 0x6c44198c4a475817ULL,
+};
+
+static inline uint64_t ror64(uint64_t word, unsigned int shift)
+{
+ return (word >> (shift & 63)) | (word << ((-shift) & 63));
+}
+
+#define e0(x) (ror64(x,28) ^ ror64(x,34) ^ ror64(x,39))
+#define e1(x) (ror64(x,14) ^ ror64(x,18) ^ ror64(x,41))
+#define s0(x) (ror64(x, 1) ^ ror64(x, 8) ^ (x >> 7))
+#define s1(x) (ror64(x,19) ^ ror64(x,61) ^ (x >> 6))
+
+/*
+ * 64-bit integer manipulation macros (big endian)
+ */
+#ifndef GET_UINT64_BE
+#define GET_UINT64_BE(n,b,i) { \
+ (n) = ( (unsigned long long) (b)[(i) ] << 56 ) \
+ | ( (unsigned long long) (b)[(i) + 1] << 48 ) \
+ | ( (unsigned long long) (b)[(i) + 2] << 40 ) \
+ | ( (unsigned long long) (b)[(i) + 3] << 32 ) \
+ | ( (unsigned long long) (b)[(i) + 4] << 24 ) \
+ | ( (unsigned long long) (b)[(i) + 5] << 16 ) \
+ | ( (unsigned long long) (b)[(i) + 6] << 8 ) \
+ | ( (unsigned long long) (b)[(i) + 7] ); \
+}
+#endif
+#ifndef PUT_UINT64_BE
+#define PUT_UINT64_BE(n,b,i) { \
+ (b)[(i) ] = (unsigned char) ( (n) >> 56 ); \
+ (b)[(i) + 1] = (unsigned char) ( (n) >> 48 ); \
+ (b)[(i) + 2] = (unsigned char) ( (n) >> 40 ); \
+ (b)[(i) + 3] = (unsigned char) ( (n) >> 32 ); \
+ (b)[(i) + 4] = (unsigned char) ( (n) >> 24 ); \
+ (b)[(i) + 5] = (unsigned char) ( (n) >> 16 ); \
+ (b)[(i) + 6] = (unsigned char) ( (n) >> 8 ); \
+ (b)[(i) + 7] = (unsigned char) ( (n) ); \
+}
+#endif
+
+static inline void LOAD_OP(int I, uint64_t *W, const uint8_t *input)
+{
+ GET_UINT64_BE(W[I], input, I*8);
+}
+
+static inline void BLEND_OP(int I, uint64_t *W)
+{
+ W[I & 15] += s1(W[(I-2) & 15]) + W[(I-7) & 15] + s0(W[(I-15) & 15]);
+}
+
+static void
+sha512_transform(uint64_t *state, const uint8_t *input)
+{
+ uint64_t a, b, c, d, e, f, g, h, t1, t2;
+
+ int i;
+ uint64_t W[16];
+
+ /* load the state into our registers */
+ a=state[0]; b=state[1]; c=state[2]; d=state[3];
+ e=state[4]; f=state[5]; g=state[6]; h=state[7];
+
+ /* now iterate */
+ for (i=0; i<80; i+=8) {
+ if (!(i & 8)) {
+ int j;
+
+ if (i < 16) {
+ /* load the input */
+ for (j = 0; j < 16; j++)
+ LOAD_OP(i + j, W, input);
+ } else {
+ for (j = 0; j < 16; j++) {
+ BLEND_OP(i + j, W);
+ }
+ }
+ }
+
+ t1 = h + e1(e) + Ch(e,f,g) + sha512_K[i ] + W[(i & 15)];
+ t2 = e0(a) + Maj(a,b,c); d+=t1; h=t1+t2;
+ t1 = g + e1(d) + Ch(d,e,f) + sha512_K[i+1] + W[(i & 15) + 1];
+ t2 = e0(h) + Maj(h,a,b); c+=t1; g=t1+t2;
+ t1 = f + e1(c) + Ch(c,d,e) + sha512_K[i+2] + W[(i & 15) + 2];
+ t2 = e0(g) + Maj(g,h,a); b+=t1; f=t1+t2;
+ t1 = e + e1(b) + Ch(b,c,d) + sha512_K[i+3] + W[(i & 15) + 3];
+ t2 = e0(f) + Maj(f,g,h); a+=t1; e=t1+t2;
+ t1 = d + e1(a) + Ch(a,b,c) + sha512_K[i+4] + W[(i & 15) + 4];
+ t2 = e0(e) + Maj(e,f,g); h+=t1; d=t1+t2;
+ t1 = c + e1(h) + Ch(h,a,b) + sha512_K[i+5] + W[(i & 15) + 5];
+ t2 = e0(d) + Maj(d,e,f); g+=t1; c=t1+t2;
+ t1 = b + e1(g) + Ch(g,h,a) + sha512_K[i+6] + W[(i & 15) + 6];
+ t2 = e0(c) + Maj(c,d,e); f+=t1; b=t1+t2;
+ t1 = a + e1(f) + Ch(f,g,h) + sha512_K[i+7] + W[(i & 15) + 7];
+ t2 = e0(b) + Maj(b,c,d); e+=t1; a=t1+t2;
+ }
+
+ state[0] += a; state[1] += b; state[2] += c; state[3] += d;
+ state[4] += e; state[5] += f; state[6] += g; state[7] += h;
+
+ /* erase our data */
+ a = b = c = d = e = f = g = h = t1 = t2 = 0;
+}
+
+static void sha512_block_fn(sha512_context *sst, const uint8_t *src,
+ int blocks)
+{
+ while (blocks--) {
+ sha512_transform(sst->state, src);
+ src += SHA512_BLOCK_SIZE;
+ }
+}
+
+static void sha512_base_do_update(sha512_context *sctx,
+ const uint8_t *data,
+ unsigned int len)
+{
+ unsigned int partial = sctx->count[0] % SHA512_BLOCK_SIZE;
+
+ sctx->count[0] += len;
+ if (sctx->count[0] < len)
+ sctx->count[1]++;
+
+ if (unlikely((partial + len) >= SHA512_BLOCK_SIZE)) {
+ int blocks;
+
+ if (partial) {
+ int p = SHA512_BLOCK_SIZE - partial;
+
+ memcpy(sctx->buf + partial, data, p);
+ data += p;
+ len -= p;
+
+ sha512_block_fn(sctx, sctx->buf, 1);
+ }
+
+ blocks = len / SHA512_BLOCK_SIZE;
+ len %= SHA512_BLOCK_SIZE;
+
+ if (blocks) {
+ sha512_block_fn(sctx, data, blocks);
+ data += blocks * SHA512_BLOCK_SIZE;
+ }
+ partial = 0;
+ }
+ if (len)
+ memcpy(sctx->buf + partial, data, len);
+}
+
+static void sha512_base_do_finalize(sha512_context *sctx)
+{
+ const int bit_offset = SHA512_BLOCK_SIZE - sizeof(uint64_t[2]);
+ uint64_t *bits = (uint64_t *)(sctx->buf + bit_offset);
+ unsigned int partial = sctx->count[0] % SHA512_BLOCK_SIZE;
+
+ sctx->buf[partial++] = 0x80;
+ if (partial > bit_offset) {
+ memset(sctx->buf + partial, 0x0, SHA512_BLOCK_SIZE - partial);
+ partial = 0;
+
+ sha512_block_fn(sctx, sctx->buf, 1);
+ }
+
+ memset(sctx->buf + partial, 0x0, bit_offset - partial);
+ bits[0] = cpu_to_be64(sctx->count[1] << 3 | sctx->count[0] >> 61);
+ bits[1] = cpu_to_be64(sctx->count[0] << 3);
+ sha512_block_fn(sctx, sctx->buf, 1);
+}
+
+#if defined(CONFIG_SHA384)
+void sha384_starts(sha512_context * ctx)
+{
+ ctx->state[0] = SHA384_H0;
+ ctx->state[1] = SHA384_H1;
+ ctx->state[2] = SHA384_H2;
+ ctx->state[3] = SHA384_H3;
+ ctx->state[4] = SHA384_H4;
+ ctx->state[5] = SHA384_H5;
+ ctx->state[6] = SHA384_H6;
+ ctx->state[7] = SHA384_H7;
+ ctx->count[0] = ctx->count[1] = 0;
+}
+
+void sha384_update(sha512_context *ctx, const uint8_t *input, uint32_t length)
+{
+ sha512_base_do_update(ctx, input, length);
+}
+
+void sha384_finish(sha512_context * ctx, uint8_t digest[SHA384_SUM_LEN])
+{
+ int i;
+
+ sha512_base_do_finalize(ctx);
+ for(i=0; i<SHA384_SUM_LEN / sizeof(uint64_t); i++)
+ PUT_UINT64_BE(ctx->state[i], digest, i * 8);
+}
+
+/*
+ * Output = SHA-512( input buffer ). Trigger the watchdog every 'chunk_sz'
+ * bytes of input processed.
+ */
+void sha384_csum_wd(const unsigned char *input, unsigned int ilen,
+ unsigned char *output, unsigned int chunk_sz)
+{
+ sha512_context ctx;
+#if defined(CONFIG_HW_WATCHDOG) || defined(CONFIG_WATCHDOG)
+ const unsigned char *end;
+ unsigned char *curr;
+ int chunk;
+#endif
+
+ sha384_starts(&ctx);
+
+#if defined(CONFIG_HW_WATCHDOG) || defined(CONFIG_WATCHDOG)
+ curr = (unsigned char *)input;
+ end = input + ilen;
+ while (curr < end) {
+ chunk = end - curr;
+ if (chunk > chunk_sz)
+ chunk = chunk_sz;
+ sha384_update(&ctx, curr, chunk);
+ curr += chunk;
+ WATCHDOG_RESET();
+ }
+#else
+ sha384_update(&ctx, input, ilen);
+#endif
+
+ sha384_finish(&ctx, output);
+}
+
+#endif
+
+#if defined(CONFIG_SHA512)
+void sha512_starts(sha512_context * ctx)
+{
+ ctx->state[0] = SHA512_H0;
+ ctx->state[1] = SHA512_H1;
+ ctx->state[2] = SHA512_H2;
+ ctx->state[3] = SHA512_H3;
+ ctx->state[4] = SHA512_H4;
+ ctx->state[5] = SHA512_H5;
+ ctx->state[6] = SHA512_H6;
+ ctx->state[7] = SHA512_H7;
+ ctx->count[0] = ctx->count[1] = 0;
+}
+
+void sha512_update(sha512_context *ctx, const uint8_t *input, uint32_t length)
+{
+ sha512_base_do_update(ctx, input, length);
+}
+
+void sha512_finish(sha512_context * ctx, uint8_t digest[SHA512_SUM_LEN])
+{
+ int i;
+
+ sha512_base_do_finalize(ctx);
+ for(i=0; i<SHA512_SUM_LEN / sizeof(uint64_t); i++)
+ PUT_UINT64_BE(ctx->state[i], digest, i * 8);
+}
+
+/*
+ * Output = SHA-512( input buffer ). Trigger the watchdog every 'chunk_sz'
+ * bytes of input processed.
+ */
+void sha512_csum_wd(const unsigned char *input, unsigned int ilen,
+ unsigned char *output, unsigned int chunk_sz)
+{
+ sha512_context ctx;
+#if defined(CONFIG_HW_WATCHDOG) || defined(CONFIG_WATCHDOG)
+ const unsigned char *end;
+ unsigned char *curr;
+ int chunk;
+#endif
+
+ sha512_starts(&ctx);
+
+#if defined(CONFIG_HW_WATCHDOG) || defined(CONFIG_WATCHDOG)
+ curr = (unsigned char *)input;
+ end = input + ilen;
+ while (curr < end) {
+ chunk = end - curr;
+ if (chunk > chunk_sz)
+ chunk = chunk_sz;
+ sha512_update(&ctx, curr, chunk);
+ curr += chunk;
+ WATCHDOG_RESET();
+ }
+#else
+ sha512_update(&ctx, input, ilen);
+#endif
+
+ sha512_finish(&ctx, output);
+}
+#endif
diff --git a/tools/Makefile b/tools/Makefile
index 879c3fd4a7485e1797b1f0d87bb0bdf6c9f45f0a..51123fd929839896a663e1bc3ab7894951b86d47 100644 (file)
--- a/tools/Makefile
+++ b/tools/Makefile
lib/crc16.o \
lib/sha1.o \
lib/sha256.o \
+ lib/sha512.o \
common/hash.o \
ublimage.o \
zynqimage.o \
HOSTCFLAGS_md5.o := -pedantic
HOSTCFLAGS_sha1.o := -pedantic
HOSTCFLAGS_sha256.o := -pedantic
+HOSTCFLAGS_sha512.o := -pedantic -DCONFIG_SHA512 -DCONFIG_SHA384
quiet_cmd_wrap = WRAP $@
cmd_wrap = echo "\#include <../$(patsubst $(obj)/%,%,$@)>" >$@