Merge tag 'dm-pull-29apr21' of https://source.denx.de/u-boot/custodians/u-boot-dm
[ti-u-boot/ti-u-boot.git] / tools /
7 days ago Tom RiniMerge tag 'dm-pull-29apr21' of https://source.denx... master
7 days ago Simon Glassbuildman: Use bytes for the environment
7 days ago Simon Glassbuildman: Handle exceptions in threads gracefully
7 days ago Simon Glassbuildman: Use common code to send an result
7 days ago Simon Glassbuildman: Tidy up a few comments
7 days ago Simon Glassbinman: Support adding sections to FMAPs
7 days ago Simon Glassbinman: Tweak implementation of fmap
7 days ago Evan Bennpatman: Parse checkpatch by message instead of by line
7 days ago Tom Rinipatman: Assume we always have pygit2 for tests
7 days ago Simon Glassdtoc: Correct dtoc output when testing
7 days ago Simon Glassbinman: Correct testSplNoDtb() and Tpl also
2021-04-18 Tom RiniMerge tag 'ti-v2021.07-rc1' of https://source.denx...
2021-04-16 Tom RiniMerge https://gitlab.denx.de/u-boot/custodians/u-boot...
2021-04-15 Tom RiniMerge branch '2021-04-14-assorted-vboot-improvements'
2021-04-14 Alexandru Gagniucmkimage: Add a 'keyfile' argument for image signing
2021-04-14 Alexandru Gagniuclib: Add support for ECDSA image signing
2021-04-14 Alexandru Gagniuclib/rsa: Make fdt_add_bignum() available outside of...
2021-04-14 Alexandru Gagniuclib: Rename rsa-checksum.c to hash-checksum.c
2021-04-13 Tom RiniMerge branch '2021-04-13-assorted-improvements'
2021-04-12 Trevor Woernermoveconfig.py: add to the "do not process" list
2021-04-12 Sean Andersoncheckpatch: Add warnings for using strn(cat|cpy)
2021-04-11 Tom RiniMerge branch '2021-04-11-remove-non-migrated-boards'
2021-04-11 Tom RiniMerge tag 'video-2021-07-rc1' of https://source.denx...
2021-04-10 Tom RiniMerge tag 'efi-2021-07-rc1' of https://source.denx...
2021-04-10 Heinrich Schuchardttools/mkeficapsule: improve online help
2021-04-09 Tom RiniMerge tag 'u-boot-stm32-20210409' of https://source...
2021-04-09 Tom RiniMerge branch 'v2021.07-rc1' of https://github.com/lftan...
2021-04-09 Tom RiniMerge tag 'u-boot-imx-20210409' of https://gitlab.denx...
2021-04-08 Heinrich Schuchardtimx6: icorem6: chmod 644 enigcam.bmp
2021-04-08 Peng Fantools: imx image: fix write warning
2021-04-07 Tom RiniMerge branch '2021-04-07-CI-improvements'
2021-04-07 Tom Rinitools: Integrate the Dockerfile used for CI
2021-04-07 Tom RiniMerge tag 'mmc-2021-4-6' of https://source.denx.de...
2021-04-06 Tom RiniMerge https://source.denx.de/u-boot/custodians/u-boot-usb
2021-04-06 Tom RiniMerge tag 'u-boot-amlogic-20210406' of https://source...
2021-04-06 Tom RiniMerge https://source.denx.de/u-boot/custodians/u-boot...
2021-04-06 Tom RiniMerge https://source.denx.de/u-boot/custodians/u-boot...
2021-04-06 Tom RiniMerge tag 'dm-pull-6apr21' of https://source.denx.de...
2021-04-06 Simon Glassmoveconfig: Handle binary files cleanly
2021-04-06 Simon Glassdtoc: Improve handling of reg properties
2021-04-06 Simon Glassdtoc: Adjust detection of 64-bit properties
2021-04-06 Simon Glassdtoc: Show driver warnings once at the end
2021-04-06 Simon Glassbuildman: Add an encoding to the out-env file
2021-04-06 Simon Glasspatman: Continue on if warnings are found outside a...
2021-04-06 Tom RiniMerge tag 'rockchip-for-v2021.07' of https://source...
2021-04-05 Tom RiniMerge branch 'next'
2021-03-31 Tom RiniMerge tag 'xilinx-for-v2021.07' of https://source.denx...
2021-03-30 Tom RiniMerge tag 'u-boot-atmel-2021.07-a' of https://source...
2021-03-29 Tom RiniMerge tag 'v2021.04-rc5' into next
2021-03-29 Tom RiniMerge tag 'dm-pull-28mar21' of git://git.denx.de/u...
2021-03-29 Tom RiniMerge branch '2021-03-28-assorted-bugfixes'
2021-03-28 Jessica ClarkeSupport building on macOS/arm64
2021-03-27 Simon Glassdtoc: Add new check that offsets are correct
2021-03-27 Simon Glassdtoc: Support adding subnodes alongside existing ones
2021-03-27 Simon Glassdtoc: Add a subnode test for multiple nodes
2021-03-27 Simon Glassdtoc: Tweak ordering of fdt-offsets refreshing
2021-03-27 Simon Glassdtoc: Tidy up property-offset handling
2021-03-27 Simon Glassdtoc: Improve internal error for Refresh()
2021-03-27 Simon Glassbinman: Support default alignment for sections
2021-03-27 Simon Glassbinman: Support obtaining section contents immediately
2021-03-27 Simon Glassbinman: Add support for a collection of entries
2021-03-27 Simon Glassbinman: Allow disabling expanding an entry
2021-03-27 Simon Glassbinman: Use a unique number for the symbols test file
2021-03-26 Tom RiniMerge tag 'dm-pull-26mar21-take2' of git://git.denx...
2021-03-26 Simon Glassbinman: Update various pieces of the documentation
2021-03-26 Simon Glassbinman: Drop repetitive heading for each entry
2021-03-26 Simon Glassbinman: Incorporate entry documentation
2021-03-26 Simon Glassbinman: Rearrange documentation into headings
2021-03-26 Simon Glassbinman: doc: Add documentation to htmldocs
2021-03-26 Simon Glassbinman: Automatically expand phase binaries into sections
2021-03-26 Simon Glassbinman: Plumb expanded entries through fully
2021-03-26 Simon Glassbinman: Allow a way to select expanded entries
2021-03-26 Simon Glassbinman: Allow using an an 'expanded' entry type
2021-03-26 Simon Glassbinman: Use standard filenames for SPL/TPL devicetree
2021-03-26 Simon Glassbinman: Move the comment for GetFdts() to the base...
2021-03-26 Simon Glassbinman: Drop unnecessary field in output_fdt_info
2021-03-26 Simon Glassbinman: Use the fake SPL/TPL only if requested
2021-03-26 Simon Glassbinman: Drop unnecessary 'type' property in tests
2021-03-26 Simon Glassbinman: Add support for u-boot-tpl-bss-bad
2021-03-26 Simon Glassbinman: Add support for u-boot-tpl-nodtb
2021-03-26 Simon Glassbinman: Support symbols in u-boot-spl-nodtb
2021-03-26 Simon Glassbinman: Correct the documentation for u-boot-spl-bss-pad
2021-03-26 Simon Glassbinman: Tidy up underscores in entry documentation
2021-03-26 Simon Glassbinman: Update entry help for files-align
2021-03-26 Simon Glassbinman: Document ExpandEntries() in the base class
2021-03-26 Simon Glassbinman: Allow extracting to current directory
2021-03-26 Simon Glassdtoc: Only generate the required files
2021-03-22 Simon Glassdtoc: Drop use of DECL() macros
2021-03-22 Simon Glassdtoc: Generate device instances
2021-03-22 Simon Glassdtoc: Generate uclass devices
2021-03-22 Simon Glassdtoc: Generate a summary in the dt-plat.c file
2021-03-22 Simon Glassdtoc: Tidy up the list of supported phandle properties
2021-03-22 Simon Glassdtoc: Don't generate platform data with instantiation
2021-03-22 Simon Glassdtoc: Add support for decl file
2021-03-22 Simon Glassdtoc: Add an option for device instantiation
2021-03-22 Simon Glassdtoc: Support processing the root node
2021-03-22 Simon Glassdtoc: Set up the uclasses that are used
2021-03-22 Simon Glassdtoc: Assign a sequence number to each node
2021-03-22 Simon Glassdtoc: Detect drivers only at the start of start of...
2021-03-22 Simon Glassdtoc: Read aliases for uclasses
next