added readme
[tida-00561-firmware-files/tida-00561-firmware-files.git] / readme.txt
1 The files in this repository should be added to the standard Sensortag project from the CC2650-ble_sdk_2_02_01_18. 
2 There will be some duplicates, some new, and some existing that will need to be replaced in the standard STK project.
4 Build the project with the FLASHROM project Build config. 
5 Tools used are as defined for this stack release - 
7 TI ARM Compiler version 5.2.6
8 XDC Tools 3.32.00.06 
9 TI-RTOS version 2.20.01.08
10 CCS6.2.0 or later (CCSv7.2 was used)
11 No IAR project at the moment.