028b747b0133c073e94980532d74189c73d82adb
[tidl/tidl-api.git] / docs / Makefile
1 # Makefile for Sphinx documentation
2 #
4 default: html
6 # You can set these variables from the command line.
7 SPHINXOPTS    =
8 SPHINXBUILD   = sphinx-build
9 PAPER         =
10 #BUILDDIR      = /var/www/mctools/opencl
11 BUILDDIR      = build
13 # User-friendly check for sphinx-build
14 ifeq ($(shell which $(SPHINXBUILD) >/dev/null 2>&1; echo $$?), 1)
15 $(error The '$(SPHINXBUILD)' command was not found. Make sure you have Sphinx installed, then set the SPHINXBUILD environment variable to point to the full path of the '$(SPHINXBUILD)' executable. Alternatively you can add the directory with the executable to your PATH. If you don't have Sphinx installed, grab it from http://sphinx-doc.org/)
16 endif
18 # Internal variables.
19 PAPEROPT_a4     = -D latex_paper_size=a4
20 PAPEROPT_letter = -D latex_paper_size=letter
21 ALLSPHINXOPTS   = -d $(BUILDDIR)/doctrees $(PAPEROPT_$(PAPER)) $(SPHINXOPTS) source
22 # the i18n builder cannot share the environment and doctrees with the others
23 I18NSPHINXOPTS  = $(PAPEROPT_$(PAPER)) $(SPHINXOPTS) source
25 .PHONY: help clean html dirhtml singlehtml pickle json htmlhelp qthelp devhelp epub latex latexpdf text man changes linkcheck doctest coverage gettext
27 help:
28         @echo "Please use \`make <target>' where <target> is one of"
29         @echo "  html       to make standalone HTML files"
30         @echo "  dirhtml    to make HTML files named index.html in directories"
31         @echo "  singlehtml to make a single large HTML file"
32         @echo "  pickle     to make pickle files"
33         @echo "  json       to make JSON files"
34         @echo "  htmlhelp   to make HTML files and a HTML help project"
35         @echo "  qthelp     to make HTML files and a qthelp project"
36         @echo "  applehelp  to make an Apple Help Book"
37         @echo "  devhelp    to make HTML files and a Devhelp project"
38         @echo "  epub       to make an epub"
39         @echo "  latex      to make LaTeX files, you can set PAPER=a4 or PAPER=letter"
40         @echo "  latexpdf   to make LaTeX files and run them through pdflatex"
41         @echo "  latexpdfja to make LaTeX files and run them through platex/dvipdfmx"
42         @echo "  text       to make text files"
43         @echo "  man        to make manual pages"
44         @echo "  texinfo    to make Texinfo files"
45         @echo "  info       to make Texinfo files and run them through makeinfo"
46         @echo "  gettext    to make PO message catalogs"
47         @echo "  changes    to make an overview of all changed/added/deprecated items"
48         @echo "  xml        to make Docutils-native XML files"
49         @echo "  pseudoxml  to make pseudoxml-XML files for display purposes"
50         @echo "  linkcheck  to check all external links for integrity"
51         @echo "  doctest    to run all doctests embedded in the documentation (if enabled)"
52         @echo "  coverage   to run coverage check of the documentation (if enabled)"
54 clean:
55         rm -rf $(BUILDDIR)/*
57 html: api-xml 
58         $(SPHINXBUILD) -b html $(ALLSPHINXOPTS) $(BUILDDIR)
59         @echo
60         @echo "Build finished. The HTML pages are in $(BUILDDIR)."
62 dirhtml:
63         $(SPHINXBUILD) -b dirhtml $(ALLSPHINXOPTS) $(BUILDDIR)/dirhtml
64         @echo
65         @echo "Build finished. The HTML pages are in $(BUILDDIR)/dirhtml."
67 singlehtml:
68         $(SPHINXBUILD) -b singlehtml $(ALLSPHINXOPTS) $(BUILDDIR)/singlehtml
69         @echo
70         @echo "Build finished. The HTML page is in $(BUILDDIR)/singlehtml."
72 pickle:
73         $(SPHINXBUILD) -b pickle $(ALLSPHINXOPTS) $(BUILDDIR)/pickle
74         @echo
75         @echo "Build finished; now you can process the pickle files."
77 json:
78         $(SPHINXBUILD) -b json $(ALLSPHINXOPTS) $(BUILDDIR)/json
79         @echo
80         @echo "Build finished; now you can process the JSON files."
82 htmlhelp:
83         $(SPHINXBUILD) -b htmlhelp $(ALLSPHINXOPTS) $(BUILDDIR)/htmlhelp
84         @echo
85         @echo "Build finished; now you can run HTML Help Workshop with the" \
86               ".hhp project file in $(BUILDDIR)/htmlhelp."
88 qthelp:
89         $(SPHINXBUILD) -b qthelp $(ALLSPHINXOPTS) $(BUILDDIR)/qthelp
90         @echo
91         @echo "Build finished; now you can run "qcollectiongenerator" with the" \
92               ".qhcp project file in $(BUILDDIR)/qthelp, like this:"
93         @echo "# qcollectiongenerator $(BUILDDIR)/qthelp/TIOpenCL.qhcp"
94         @echo "To view the help file:"
95         @echo "# assistant -collectionFile $(BUILDDIR)/qthelp/TIOpenCL.qhc"
97 applehelp:
98         $(SPHINXBUILD) -b applehelp $(ALLSPHINXOPTS) $(BUILDDIR)/applehelp
99         @echo
100         @echo "Build finished. The help book is in $(BUILDDIR)/applehelp."
101         @echo "N.B. You won't be able to view it unless you put it in" \
102               "~/Library/Documentation/Help or install it in your application" \
103               "bundle."
105 devhelp:
106         $(SPHINXBUILD) -b devhelp $(ALLSPHINXOPTS) $(BUILDDIR)/devhelp
107         @echo
108         @echo "Build finished."
109         @echo "To view the help file:"
110         @echo "# mkdir -p $$HOME/.local/share/devhelp/TIOpenCL"
111         @echo "# ln -s $(BUILDDIR)/devhelp $$HOME/.local/share/devhelp/TIOpenCL"
112         @echo "# devhelp"
114 epub:
115         $(SPHINXBUILD) -b epub $(ALLSPHINXOPTS) $(BUILDDIR)/epub
116         @echo
117         @echo "Build finished. The epub file is in $(BUILDDIR)/epub."
119 latex:
120         $(SPHINXBUILD) -b latex $(ALLSPHINXOPTS) $(BUILDDIR)/latex
121         @echo
122         @echo "Build finished; the LaTeX files are in $(BUILDDIR)/latex."
123         @echo "Run \`make' in that directory to run these through (pdf)latex" \
124               "(use \`make latexpdf' here to do that automatically)."
126 latexpdf:
127         $(SPHINXBUILD) -b latex $(ALLSPHINXOPTS) $(BUILDDIR)/latex
128         @echo "Running LaTeX files through pdflatex..."
129         $(MAKE) -C $(BUILDDIR)/latex all-pdf
130         @echo "pdflatex finished; the PDF files are in $(BUILDDIR)/latex."
132 latexpdfja:
133         $(SPHINXBUILD) -b latex $(ALLSPHINXOPTS) $(BUILDDIR)/latex
134         @echo "Running LaTeX files through platex and dvipdfmx..."
135         $(MAKE) -C $(BUILDDIR)/latex all-pdf-ja
136         @echo "pdflatex finished; the PDF files are in $(BUILDDIR)/latex."
138 text:
139         $(SPHINXBUILD) -b text $(ALLSPHINXOPTS) $(BUILDDIR)/text
140         @echo
141         @echo "Build finished. The text files are in $(BUILDDIR)/text."
143 man:
144         $(SPHINXBUILD) -b man $(ALLSPHINXOPTS) $(BUILDDIR)/man
145         @echo
146         @echo "Build finished. The manual pages are in $(BUILDDIR)/man."
148 texinfo:
149         $(SPHINXBUILD) -b texinfo $(ALLSPHINXOPTS) $(BUILDDIR)/texinfo
150         @echo
151         @echo "Build finished. The Texinfo files are in $(BUILDDIR)/texinfo."
152         @echo "Run \`make' in that directory to run these through makeinfo" \
153               "(use \`make info' here to do that automatically)."
155 info:
156         $(SPHINXBUILD) -b texinfo $(ALLSPHINXOPTS) $(BUILDDIR)/texinfo
157         @echo "Running Texinfo files through makeinfo..."
158         make -C $(BUILDDIR)/texinfo info
159         @echo "makeinfo finished; the Info files are in $(BUILDDIR)/texinfo."
161 gettext:
162         $(SPHINXBUILD) -b gettext $(I18NSPHINXOPTS) $(BUILDDIR)/locale
163         @echo
164         @echo "Build finished. The message catalogs are in $(BUILDDIR)/locale."
166 changes:
167         $(SPHINXBUILD) -b changes $(ALLSPHINXOPTS) $(BUILDDIR)/changes
168         @echo
169         @echo "The overview file is in $(BUILDDIR)/changes."
171 linkcheck:
172         $(SPHINXBUILD) -b linkcheck $(ALLSPHINXOPTS) $(BUILDDIR)/linkcheck
173         @echo
174         @echo "Link check complete; look for any errors in the above output " \
175               "or in $(BUILDDIR)/linkcheck/output.txt."
177 doctest:
178         $(SPHINXBUILD) -b doctest $(ALLSPHINXOPTS) $(BUILDDIR)/doctest
179         @echo "Testing of doctests in the sources finished, look at the " \
180               "results in $(BUILDDIR)/doctest/output.txt."
182 coverage:
183         $(SPHINXBUILD) -b coverage $(ALLSPHINXOPTS) $(BUILDDIR)/coverage
184         @echo "Testing of coverage in the sources finished, look at the " \
185               "results in $(BUILDDIR)/coverage/python.txt."
187 xml:
188         $(SPHINXBUILD) -b xml $(ALLSPHINXOPTS) $(BUILDDIR)/xml
189         @echo
190         @echo "Build finished. The XML files are in $(BUILDDIR)/xml."
192 pseudoxml:
193         $(SPHINXBUILD) -b pseudoxml $(ALLSPHINXOPTS) $(BUILDDIR)/pseudoxml
194         @echo
195         @echo "Build finished. The pseudo-XML files are in $(BUILDDIR)/pseudoxml."
197 artifacts:
198         $(MAKE) -c artifacts
200 api-xml:
201         (cd ../tinn_api/doxygen; doxygen)