]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - tidl/tidl-api.git/blob - docs/make.bat
Use malloc for user application buffer allocation
[tidl/tidl-api.git] / docs / make.bat
1 @ECHO OFF
3 REM Command file for Sphinx documentation
5 if "%SPHINXBUILD%" == "" (
6         set SPHINXBUILD=sphinx-build
7 )
8 set BUILDDIR=build
9 set ALLSPHINXOPTS=-d %BUILDDIR%/doctrees %SPHINXOPTS% source
10 set I18NSPHINXOPTS=%SPHINXOPTS% source
11 if NOT "%PAPER%" == "" (
12         set ALLSPHINXOPTS=-D latex_paper_size=%PAPER% %ALLSPHINXOPTS%
13         set I18NSPHINXOPTS=-D latex_paper_size=%PAPER% %I18NSPHINXOPTS%
14 )
16 if "%1" == "" goto help
18 if "%1" == "help" (
19         :help
20         echo.Please use `make ^<target^>` where ^<target^> is one of
21         echo.  html       to make standalone HTML files
22         echo.  dirhtml    to make HTML files named index.html in directories
23         echo.  singlehtml to make a single large HTML file
24         echo.  pickle     to make pickle files
25         echo.  json       to make JSON files
26         echo.  htmlhelp   to make HTML files and a HTML help project
27         echo.  qthelp     to make HTML files and a qthelp project
28         echo.  devhelp    to make HTML files and a Devhelp project
29         echo.  epub       to make an epub
30         echo.  latex      to make LaTeX files, you can set PAPER=a4 or PAPER=letter
31         echo.  text       to make text files
32         echo.  man        to make manual pages
33         echo.  texinfo    to make Texinfo files
34         echo.  gettext    to make PO message catalogs
35         echo.  changes    to make an overview over all changed/added/deprecated items
36         echo.  xml        to make Docutils-native XML files
37         echo.  pseudoxml  to make pseudoxml-XML files for display purposes
38         echo.  linkcheck  to check all external links for integrity
39         echo.  doctest    to run all doctests embedded in the documentation if enabled
40         echo.  coverage   to run coverage check of the documentation if enabled
41         goto end
42 )
44 if "%1" == "clean" (
45         for /d %%i in (%BUILDDIR%\*) do rmdir /q /s %%i
46         del /q /s %BUILDDIR%\*
47         goto end
48 )
51 REM Check if sphinx-build is available and fallback to Python version if any
52 %SPHINXBUILD% 2> nul
53 if errorlevel 9009 goto sphinx_python
54 goto sphinx_ok
56 :sphinx_python
58 set SPHINXBUILD=python -m sphinx.__init__
59 %SPHINXBUILD% 2> nul
60 if errorlevel 9009 (
61         echo.
62         echo.The 'sphinx-build' command was not found. Make sure you have Sphinx
63         echo.installed, then set the SPHINXBUILD environment variable to point
64         echo.to the full path of the 'sphinx-build' executable. Alternatively you
65         echo.may add the Sphinx directory to PATH.
66         echo.
67         echo.If you don't have Sphinx installed, grab it from
68         echo.http://sphinx-doc.org/
69         exit /b 1
70 )
72 :sphinx_ok
75 if "%1" == "html" (
76         %SPHINXBUILD% -b html %ALLSPHINXOPTS% %BUILDDIR%/html
77         if errorlevel 1 exit /b 1
78         echo.
79         echo.Build finished. The HTML pages are in %BUILDDIR%/html.
80         goto end
81 )
83 if "%1" == "dirhtml" (
84         %SPHINXBUILD% -b dirhtml %ALLSPHINXOPTS% %BUILDDIR%/dirhtml
85         if errorlevel 1 exit /b 1
86         echo.
87         echo.Build finished. The HTML pages are in %BUILDDIR%/dirhtml.
88         goto end
89 )
91 if "%1" == "singlehtml" (
92         %SPHINXBUILD% -b singlehtml %ALLSPHINXOPTS% %BUILDDIR%/singlehtml
93         if errorlevel 1 exit /b 1
94         echo.
95         echo.Build finished. The HTML pages are in %BUILDDIR%/singlehtml.
96         goto end
97 )
99 if "%1" == "pickle" (
100         %SPHINXBUILD% -b pickle %ALLSPHINXOPTS% %BUILDDIR%/pickle
101         if errorlevel 1 exit /b 1
102         echo.
103         echo.Build finished; now you can process the pickle files.
104         goto end
107 if "%1" == "json" (
108         %SPHINXBUILD% -b json %ALLSPHINXOPTS% %BUILDDIR%/json
109         if errorlevel 1 exit /b 1
110         echo.
111         echo.Build finished; now you can process the JSON files.
112         goto end
115 if "%1" == "htmlhelp" (
116         %SPHINXBUILD% -b htmlhelp %ALLSPHINXOPTS% %BUILDDIR%/htmlhelp
117         if errorlevel 1 exit /b 1
118         echo.
119         echo.Build finished; now you can run HTML Help Workshop with the ^
120 .hhp project file in %BUILDDIR%/htmlhelp.
121         goto end
124 if "%1" == "qthelp" (
125         %SPHINXBUILD% -b qthelp %ALLSPHINXOPTS% %BUILDDIR%/qthelp
126         if errorlevel 1 exit /b 1
127         echo.
128         echo.Build finished; now you can run "qcollectiongenerator" with the ^
129 .qhcp project file in %BUILDDIR%/qthelp, like this:
130         echo.^> qcollectiongenerator %BUILDDIR%\qthelp\TIOpenCL.qhcp
131         echo.To view the help file:
132         echo.^> assistant -collectionFile %BUILDDIR%\qthelp\TIOpenCL.ghc
133         goto end
136 if "%1" == "devhelp" (
137         %SPHINXBUILD% -b devhelp %ALLSPHINXOPTS% %BUILDDIR%/devhelp
138         if errorlevel 1 exit /b 1
139         echo.
140         echo.Build finished.
141         goto end
144 if "%1" == "epub" (
145         %SPHINXBUILD% -b epub %ALLSPHINXOPTS% %BUILDDIR%/epub
146         if errorlevel 1 exit /b 1
147         echo.
148         echo.Build finished. The epub file is in %BUILDDIR%/epub.
149         goto end
152 if "%1" == "latex" (
153         %SPHINXBUILD% -b latex %ALLSPHINXOPTS% %BUILDDIR%/latex
154         if errorlevel 1 exit /b 1
155         echo.
156         echo.Build finished; the LaTeX files are in %BUILDDIR%/latex.
157         goto end
160 if "%1" == "latexpdf" (
161         %SPHINXBUILD% -b latex %ALLSPHINXOPTS% %BUILDDIR%/latex
162         cd %BUILDDIR%/latex
163         make all-pdf
164         cd %~dp0
165         echo.
166         echo.Build finished; the PDF files are in %BUILDDIR%/latex.
167         goto end
170 if "%1" == "latexpdfja" (
171         %SPHINXBUILD% -b latex %ALLSPHINXOPTS% %BUILDDIR%/latex
172         cd %BUILDDIR%/latex
173         make all-pdf-ja
174         cd %~dp0
175         echo.
176         echo.Build finished; the PDF files are in %BUILDDIR%/latex.
177         goto end
180 if "%1" == "text" (
181         %SPHINXBUILD% -b text %ALLSPHINXOPTS% %BUILDDIR%/text
182         if errorlevel 1 exit /b 1
183         echo.
184         echo.Build finished. The text files are in %BUILDDIR%/text.
185         goto end
188 if "%1" == "man" (
189         %SPHINXBUILD% -b man %ALLSPHINXOPTS% %BUILDDIR%/man
190         if errorlevel 1 exit /b 1
191         echo.
192         echo.Build finished. The manual pages are in %BUILDDIR%/man.
193         goto end
196 if "%1" == "texinfo" (
197         %SPHINXBUILD% -b texinfo %ALLSPHINXOPTS% %BUILDDIR%/texinfo
198         if errorlevel 1 exit /b 1
199         echo.
200         echo.Build finished. The Texinfo files are in %BUILDDIR%/texinfo.
201         goto end
204 if "%1" == "gettext" (
205         %SPHINXBUILD% -b gettext %I18NSPHINXOPTS% %BUILDDIR%/locale
206         if errorlevel 1 exit /b 1
207         echo.
208         echo.Build finished. The message catalogs are in %BUILDDIR%/locale.
209         goto end
212 if "%1" == "changes" (
213         %SPHINXBUILD% -b changes %ALLSPHINXOPTS% %BUILDDIR%/changes
214         if errorlevel 1 exit /b 1
215         echo.
216         echo.The overview file is in %BUILDDIR%/changes.
217         goto end
220 if "%1" == "linkcheck" (
221         %SPHINXBUILD% -b linkcheck %ALLSPHINXOPTS% %BUILDDIR%/linkcheck
222         if errorlevel 1 exit /b 1
223         echo.
224         echo.Link check complete; look for any errors in the above output ^
225 or in %BUILDDIR%/linkcheck/output.txt.
226         goto end
229 if "%1" == "doctest" (
230         %SPHINXBUILD% -b doctest %ALLSPHINXOPTS% %BUILDDIR%/doctest
231         if errorlevel 1 exit /b 1
232         echo.
233         echo.Testing of doctests in the sources finished, look at the ^
234 results in %BUILDDIR%/doctest/output.txt.
235         goto end
238 if "%1" == "coverage" (
239         %SPHINXBUILD% -b coverage %ALLSPHINXOPTS% %BUILDDIR%/coverage
240         if errorlevel 1 exit /b 1
241         echo.
242         echo.Testing of coverage in the sources finished, look at the ^
243 results in %BUILDDIR%/coverage/python.txt.
244         goto end
247 if "%1" == "xml" (
248         %SPHINXBUILD% -b xml %ALLSPHINXOPTS% %BUILDDIR%/xml
249         if errorlevel 1 exit /b 1
250         echo.
251         echo.Build finished. The XML files are in %BUILDDIR%/xml.
252         goto end
255 if "%1" == "pseudoxml" (
256         %SPHINXBUILD% -b pseudoxml %ALLSPHINXOPTS% %BUILDDIR%/pseudoxml
257         if errorlevel 1 exit /b 1
258         echo.
259         echo.Build finished. The pseudo-XML files are in %BUILDDIR%/pseudoxml.
260         goto end
263 :end