961e830b4968b9171b9132f68851af1c253cef85
1 ********
2 Examples
3 ********
5 We ship three end-to-end examples within the tidl-api packge
6 to demonstrate three categories of deep learning networks. The first
7 two examples can run on AM57x SoCs with either DLA or DSP. The last
8 example requires AM57x SoCs with both DLA and DSP. The performance
9 numbers that we present here were obtained on an AM5729 EVM, which
10 includes 2 ARM A15 cores running at 1.5GHz, 4 DLA cores at 535MHz, and
11 2 DSP cores at 750MHz.
13 Imagenet
14 --------
16 The imagenet example takes an image as input and outputs 1000 probabilities.
17 Each probability corresponds to one object in the 1000 objects that the
18 network is pre-trained with. Our example outputs top 5 probabilities
19 as the most likely objects that the input image can be.
21 The following figure and tables shows an input image, top 5 predicted
22 objects as output, and the processing time on either DLA or DSP.
24 .. image:: ../../examples/test/testvecs/input/objects/cat-pet-animal-domestic-104827.jpeg
25 :width: 600
27 .. table::
29 ==== ============== ============
30 Rank Object Classes Probability
31 ==== ============== ============
32 1 tabby 0.996
33 2 Egyptian_cat 0.977
34 3 tiger_cat 0.973
35 4 lynx 0.941
36 5 Persian_cat 0.922
37 ==== ============== ============
39 .. table::
41 ====================== ==================== ============
42 Device Processing Time Host Processing Time API Overhead
43 ====================== ==================== ============
44 DLA: 123.1 ms 124.7 ms 1.34 %
45 **OR**
46 DSP: 117.9 ms 119.3 ms 1.14 %
47 ====================== ==================== ============
49 The particular network that we ran in this category, jacintonet11v2,
50 has 14 layers. User can specify whether to run the network on DLA or DSP
51 for acceleration. We can see that DLA time is slightly higher than DSP time.
52 Host time includes the OpenCL runtime overhead and the time to copy user
53 input data into padded TIDL buffers. We can see that the overall overhead
54 is less than 1.5%.
56 Segmentation
57 ------------
59 The segmentation example takes an image as input and performs pixel-level
60 classification according to pre-trained categories. The following figures
61 show a street scene as input and the scene overlaid with pixel-level
62 classifications as output: road in green, pedestrians in red, vehicles
63 in blue and background in gray.
65 .. image:: ../../examples/test/testvecs/input/roads/pexels-photo-972355.jpeg
66 :width: 600
68 .. image:: images/pexels-photo-972355-seg.jpg
69 :width: 600
71 The network we ran in this category is jsegnet21v2, which has 26 layers.
72 From the reported time in the following table, we can see that this network
73 runs significantly faster on DLA than on DSP.
75 .. table::
77 ====================== ==================== ============
78 Device Processing Time Host Processing Time API Overhead
79 ====================== ==================== ============
80 DLA: 296.5 ms 303.3 ms 2.26 %
81 **OR**
82 DSP: 812.0 ms 818.4 ms 0.79 %
83 ====================== ==================== ============
85 SSD
86 ---
88 SSD is the abbreviation for Single Shot multi-box Detector.
89 The ssd_multibox example takes an image as input and detects multiple
90 objects with bounding boxes according to pre-trained categories.
91 The following figures show another street scene as input and the scene
92 with recognized objects boxed as output: pedestrians in red,
93 vehicles in blue and road signs in yellow.
95 .. image:: ../../examples/test/testvecs/input/roads/pexels-photo-378570.jpeg
96 :width: 600
98 .. image:: images/pexels-photo-378570-ssd.jpg
99 :width: 600
101 The network can be run entirely on either DLA or DSP. But the best
102 performance comes with running the first 30 layers on DLA and the
103 next 13 layers on DSP, for this particular jdetnet_ssd network.
104 Note the **AND** in the following table for the reported time.
105 Our end-to-end example shows how easy it is to assign a layers group id
106 to an *Executor* and how easy it is to connect the output from one
107 *ExecutionObject* to the input to another *ExecutionObject*.
109 .. table::
111 ====================== ==================== ============
112 Device Processing Time Host Processing Time API Overhead
113 ====================== ==================== ============
114 DLA: 175.2 ms 179.1 ms 2.14 %
115 **AND**
116 DSP: 21.1 ms 22.3 ms 5.62 %
117 ====================== ==================== ============
119 Running Examples
120 ----------------
122 The examples are located in ``/usr/share/ti/tidl-api/examples`` on
123 the EVM filesystem. Each example needs to be run its own directory.
124 Running an example with ``-h`` will show help message with option set.
125 The following code section shows how to run the examples, and
126 the test program that tests all supported TIDL network configs.
128 .. code:: shell
130 root@am57xx-evm:~# cd /usr/share/ti/tidl-api/examples/imagenet/
131 root@am57xx-evm:/usr/share/ti/tidl-api/examples/imagenet# make -j4
132 root@am57xx-evm:/usr/share/ti/tidl-api/examples/imagenet# ./imagenet -t d
133 Input: ../test/testvecs/input/objects/cat-pet-animal-domestic-104827.jpeg
134 frame[0]: Time on device: 117.9ms, host: 119.3ms API overhead: 1.17 %
135 1: tabby, prob = 0.996
136 2: Egyptian_cat, prob = 0.977
137 3: tiger_cat, prob = 0.973
138 4: lynx, prob = 0.941
139 5: Persian_cat, prob = 0.922
140 imagenet PASSED
142 root@am57xx-evm:/usr/share/ti/tidl-api/examples/imagenet# cd ../segmentation/; make -j4
143 root@am57xx-evm:/usr/share/ti/tidl-api/examples/segmentation# ./segmentation -i ../test/testvecs/input/roads/pexels-photo-972355.jpeg
144 Input: ../test/testvecs/input/roads/pexels-photo-972355.jpeg
145 frame[0]: Time on device: 296.5ms, host: 303.2ms API overhead: 2.21 %
146 Saving frame 0 overlayed with segmentation to: overlay_0.png
147 segmentation PASSED
149 root@am57xx-evm:/usr/share/ti/tidl-api/examples/segmentation# cd ../ssd_multibox/; make -j4
150 root@am57xx-evm:/usr/share/ti/tidl-api/examples/ssd_multibox# ./ssd_multibox -i ../test/testvecs/input/roads/pexels-photo-378570.jpeg
151 Input: ../test/testvecs/input/roads/pexels-photo-378570.jpeg
152 frame[0]: Time on DLA: 175.2ms, host: 179ms API overhead: 2.1 %
153 frame[0]: Time on DSP: 21.06ms, host: 22.43ms API overhead: 6.08 %
154 Saving frame 0 with SSD multiboxes to: multibox_0.png
155 Loop total time (including read/write/print/etc): 423.8ms
156 ssd_multibox PASSED
158 root@am57xx-evm:/usr/share/ti/tidl-api/examples/ssd_multibox# cd ../test; make -j4
159 root@am57xx-evm:/usr/share/ti/tidl-api/examples/test# ./test_tidl
160 API Version: 01.00.00.d91e442
161 Running dense_1x1 on 2 devices, type EVE
162 frame[0]: Time on device: 134.3ms, host: 135.6ms API overhead: 0.994 %
163 dense_1x1 : PASSED
164 Running j11_bn on 2 devices, type EVE
165 frame[0]: Time on device: 176.2ms, host: 177.7ms API overhead: 0.835 %
166 j11_bn : PASSED
167 Running j11_cifar on 2 devices, type EVE
168 frame[0]: Time on device: 53.86ms, host: 54.88ms API overhead: 1.85 %
169 j11_cifar : PASSED
170 Running j11_controlLayers on 2 devices, type EVE
171 frame[0]: Time on device: 122.9ms, host: 123.9ms API overhead: 0.821 %
172 j11_controlLayers : PASSED
173 Running j11_prelu on 2 devices, type EVE
174 frame[0]: Time on device: 300.8ms, host: 302.1ms API overhead: 0.437 %
175 j11_prelu : PASSED
176 Running j11_v2 on 2 devices, type EVE
177 frame[0]: Time on device: 124.1ms, host: 125.6ms API overhead: 1.18 %
178 j11_v2 : PASSED
179 Running jseg21 on 2 devices, type EVE
180 frame[0]: Time on device: 367ms, host: 374ms API overhead: 1.88 %
181 jseg21 : PASSED
182 Running jseg21_tiscapes on 2 devices, type EVE
183 frame[0]: Time on device: 302.2ms, host: 308.5ms API overhead: 2.02 %
184 frame[1]: Time on device: 301.9ms, host: 312.5ms API overhead: 3.38 %
185 frame[2]: Time on device: 302.7ms, host: 305.9ms API overhead: 1.04 %
186 frame[3]: Time on device: 301.9ms, host: 305ms API overhead: 1.01 %
187 frame[4]: Time on device: 302.7ms, host: 305.9ms API overhead: 1.05 %
188 frame[5]: Time on device: 301.9ms, host: 305.5ms API overhead: 1.17 %
189 frame[6]: Time on device: 302.7ms, host: 305.9ms API overhead: 1.06 %
190 frame[7]: Time on device: 301.9ms, host: 305ms API overhead: 1.02 %
191 frame[8]: Time on device: 297ms, host: 300.3ms API overhead: 1.09 %
192 Comparing frame: 0
193 jseg21_tiscapes : PASSED
194 Running smallRoi on 2 devices, type EVE
195 frame[0]: Time on device: 2.548ms, host: 3.637ms API overhead: 29.9 %
196 smallRoi : PASSED
197 Running squeeze1_1 on 2 devices, type EVE
198 frame[0]: Time on device: 292.9ms, host: 294.6ms API overhead: 0.552 %
199 squeeze1_1 : PASSED
201 Multiple Executor...
202 Running network tidl_config_j11_v2.txt on EVEs: 1 in thread 0
203 Running network tidl_config_j11_cifar.txt on EVEs: 0 in thread 1
204 Multiple executors: PASSED
205 Running j11_bn on 2 devices, type DSP
206 frame[0]: Time on device: 170.5ms, host: 171.5ms API overhead: 0.568 %
207 j11_bn : PASSED
208 Running j11_controlLayers on 2 devices, type DSP
209 frame[0]: Time on device: 416.4ms, host: 417.1ms API overhead: 0.176 %
210 j11_controlLayers : PASSED
211 Running j11_v2 on 2 devices, type DSP
212 frame[0]: Time on device: 118ms, host: 119.2ms API overhead: 1.01 %
213 j11_v2 : PASSED
214 Running jseg21 on 2 devices, type DSP
215 frame[0]: Time on device: 1123ms, host: 1128ms API overhead: 0.443 %
216 jseg21 : PASSED
217 Running jseg21_tiscapes on 2 devices, type DSP
218 frame[0]: Time on device: 812.3ms, host: 817.3ms API overhead: 0.614 %
219 frame[1]: Time on device: 812.6ms, host: 818.6ms API overhead: 0.738 %
220 frame[2]: Time on device: 812.3ms, host: 815.1ms API overhead: 0.343 %
221 frame[3]: Time on device: 812.7ms, host: 815.2ms API overhead: 0.312 %
222 frame[4]: Time on device: 812.3ms, host: 815.1ms API overhead: 0.353 %
223 frame[5]: Time on device: 812.6ms, host: 815.1ms API overhead: 0.302 %
224 frame[6]: Time on device: 812.2ms, host: 815.1ms API overhead: 0.357 %
225 frame[7]: Time on device: 812.6ms, host: 815.2ms API overhead: 0.315 %
226 frame[8]: Time on device: 812ms, host: 815ms API overhead: 0.367 %
227 Comparing frame: 0
228 jseg21_tiscapes : PASSED
229 Running smallRoi on 2 devices, type DSP
230 frame[0]: Time on device: 14.21ms, host: 14.94ms API overhead: 4.89 %
231 smallRoi : PASSED
232 Running squeeze1_1 on 2 devices, type DSP
233 frame[0]: Time on device: 960ms, host: 961.1ms API overhead: 0.116 %
234 squeeze1_1 : PASSED
235 tidl PASSED
237 Possible runtime errors: out of memory
238 """"""""""""""""""""""""""""""""""""""
240 .. code:: shell
242 tidl: device_alloc.h:31: T* tidl::malloc_ddr(size_t) [with T = char; size_t = unsigned int]: Assertion `val != nullptr' failed
244 One possible reason is that previous aborted runs didn't properly release
245 allocation. Use ti-mct-heap-check with "-c" option to clean up.
247 .. code:: shell
249 root@am57xx-evm:~# ti-mct-heap-check -c
250 -- ddr_heap1 ------------------------------
251 Addr : 0xa2000000
252 Size : 0xa000000
253 Avail: 0xa000000
254 Align: 0x80
255 -----------------------------------------
257 Another possible reason is that total memory requirement exceeds default
258 memory allocated for OpenCL. See below how to patch device tree to
259 increase OpenCL memory.
261 .. code:: shell
263 $ sudo apt-get install device-tree-compiler # In case dtc is not already installed
264 $ scp root@am57:/boot/am57xx-evm-reva3.dtb .
265 $ dtc -I dtb -O dts am57xx-evm-reva3.dtb -o am57xx-evm-reva3.dts
266 $ cp am57xx-evm-reva3.dts am57xx-evm-reva3.dts.orig
267 $ # increase cmem block size
268 $ diff -u am57xx-evm-reva3.dts.orig am57xx-evm-reva3.dts
269 --- am57xx-evm-reva3.dts.orig 2018-01-11 14:47:51.491572739 -0600
270 +++ am57xx-evm-reva3.dts 2018-01-16 15:43:33.981431971 -0600
271 @@ -5657,7 +5657,7 @@
272 };
274 cmem_block_mem@a0000000 {
275 - reg = <0x0 0xa0000000 0x0 0xc000000>;
276 + reg = <0x0 0xa0000000 0x0 0x18000000>;
277 no-map;
278 status = "okay";
279 linux,phandle = <0x13c>;
280 @@ -5823,7 +5823,7 @@
281 cmem_block@0 {
282 reg = <0x0>;
283 memory-region = <0x13c>;
284 - cmem-buf-pools = <0x1 0x0 0xc000000>;
285 + cmem-buf-pools = <0x1 0x0 0x18000000>;
286 };
288 cmem_block@1 {
289 $ dtc -I dts -O dtb am57xx-evm-reva3.dts -o am57xx-evm-reva3.dtb
290 $ scp am57xx-evm-reva3.dtb root@am57:/boot/
291 # reboot to make memory changes effective (run "cat /proc/iomem" to check)