ff70804267e5179aab6316088b66020e00a8a4a5
[tidl/tidl-api.git] / docs / source / example.rst
1 .. _examples:
3 ********
4 Examples
5 ********
7 .. list-table:: TIDL API Examples
8    :header-rows: 1
9    :widths: 12 43 20 25
11    * - Example
12      - Description
13      - Compute cores
14      - Input image
15    * - one_eo_per_frame
16      - Processes a single frame with one :term:`EO` using the j11_v2 network. Throughput is increased by distributing frame processing across EOs. Refer :ref:`use-case-1`.
17      - EVE or C66x
18      - Pre-processed image read from file.
19    * - two_eo_per_frame
20      - Processes a single frame with an :term:`EOP` using the j11_v2 network to reduce per-frame processing latency. Also increases throughput by distributing frame processing across EOPs. The EOP consists of two EOs. Refer :ref:`use-case-2`.
21      - EVE and C66x (network is split across both EVE and C66x)
22      - Pre-processed image read from file.
23    * - two_eo_per_frame_opt
24      - Builds on ``two_eo_per_frame``. Adds double buffering to improve performance. Refer :ref:`use-case-3`.
25      - EVE and C66x (network is split across both EVE and C66x)
26      - Pre-processed image read from file.
28    * - imagenet
29      - Classification example
30      - EVE or C66x
31      - OpenCV used to read input image from file or capture from camera.
32    * - segmentation
33      - Pixel level segmentation example
34      - EVE or C66x
35      - OpenCV used to read input image from file or capture from camera.
36    * - ssd_multibox
37      - Object detection
38      - EVE and C66x (network is split across both EVE and C66x)
39      - OpenCV used to read input image from file or capture from camera.
40    * - mnist
41      - handwritten digits recognition (MNIST).  This example illustrates
42        low TIDL API overhead (~1.8%) for small networks with low compute
43        requirements (<5ms).
44      - EVE
45      - Pre-processed white-on-black images read from file, with or without
46        MNIST database file headers.
47    * - classification
48      - Classification example, called from the Matrix GUI.
49      - EVE or C66x
50      - OpenCV used to read input image from file or capture from camera.
51    * - mcbench
52      - Used to benchmark supported networks. Refer ``mcbench/scripts`` for command line options.
53      - EVE or C66x
54      - Pre-processed image read from file.
55    * - layer_output
56      - Illustrates using TIDL APIs to access output buffers of intermediate :term:`layers<Layer>` in the network.
57      - EVE or C66x
58      - Pre-processed image read from file.
59    * - test
60      - This example is used to test pre-converted networks included in the TIDL API package (``test/testvecs/config/tidl_models``). When run without any arguments, the program ``test_tidl`` will run all available networks on the C66x DSPs and EVEs available on the SoC. Use the ``-c`` option to specify a single network. Run ``test_tidl -h``  for details.
61      - C66x and EVEs (if available)
62      - Pre-processed image read from file.
64 The included examples demonstrate three categories of deep learning networks: classification, segmentation and object detection.  ``imagenet`` and ``segmentation`` can run on AM57x processors with either EVE or C66x cores.  ``ssd_multibox`` requires AM57x processors with both EVE and C66x. The examples are available at ``/usr/share/ti/tidl/examples`` on the EVM file system and in the linux devkit.
66 The performance numbers were obtained using:
68 * `AM574x IDK EVM`_ with the Sitara `AM5749`_ Processor - 2 Arm Cortex-A15 cores running at 1.0GHz, 2 EVE cores at 650MHz, and 2 C66x cores at 750MHz.
69 * `Processor SDK Linux`_ v5.1 with TIDL API v1.1
71 For each example, device processing time, host processing time,
72 and TIDL API overhead is reported.
74 * **Device processing time** is measured on the device, from the moment processing starts for a frame till processing finishes.
75 * **Host processing time** is measured on the host, from the moment ``ProcessFrameStartAsync()`` is called till ``ProcessFrameWait()`` returns in user application.  It includes the TIDL API overhead, the OpenCL runtime overhead, and the time to copy user input data into padded TIDL internal buffers. ``Host processing time = Device processing time + TIDL API overhead``.
78 Imagenet
79 --------
81 The imagenet example takes an image as input and outputs 1000 probabilities.
82 Each probability corresponds to one object in the 1000 objects that the
83 network is pre-trained with.  The example outputs top 5 (up to) predictions
84 with probabilities of 5% or higher for a given input image.
86 The following figure and tables shows an input image, top 5 predicted
87 objects as output, and the processing time on either EVE or C66x.
89 .. image:: ../../examples/test/testvecs/input/objects/cat-pet-animal-domestic-104827.jpeg
90    :width: 600
93 ==== ============== ===========
94 Rank Object Classes Probability
95 ==== ============== ===========
96 1    tabby          52.55%
97 2    Egyptian_cat   21.18%
98 3    tiger_cat      17.65%
99 ==== ============== ===========
101 =======   ====================== ==================== ============
102 Device    Device Processing Time Host Processing Time API Overhead
103 =======   ====================== ==================== ============
104 EVE       106.5 ms               107.9 ms             1.37 %
105 C66x      117.9 ms               118.7 ms             0.93 %
106 =======   ====================== ==================== ============
108 The :term:`network<Network>` used in the example is jacintonet11v2. It has
109 14 layers. Input to the network is RGB image of 224x224. Users can specify whether to run the network on EVE or C66x.
111 The example code sets ``buffer_factor`` to 2 to create duplicated
112 ExecutionObjectPipelines with identical ExecutionObjects to
113 perform double buffering, so that host pre/post-processing can be overlapped
114 with device processing (see comments in the code for details).
115 The following table shows the loop overall time over 10 frames
116 with single buffering and double buffering,
117 ``./imagenet -f 10 -d <num> -e <num>``.
119 .. list-table:: Loop overall time over 10 frames
120    :header-rows: 1
122    * - Device(s)
123      - Single Buffering (buffer_factor=1)
124      - Double Buffering (buffer_factor=2)
125    * - 1 EVE
126      - 1744 ms
127      - 1167 ms
128    * - 2 EVEs
129      - 966 ms
130      - 795 ms
131    * - 1 C66x
132      - 1879 ms
133      - 1281 ms
134    * - 2 C66xs
135      - 1021 ms
136      - 814 ms
138 Segmentation
139 ------------
141 The segmentation example takes an image as input and performs pixel-level
142 classification according to pre-trained categories.  The following figures
143 show a street scene as input and the scene overlaid with pixel-level
144 classifications as output: road in green, pedestrians in red, vehicles
145 in blue and background in gray.
147 .. image:: ../../examples/test/testvecs/input/roads/pexels-photo-972355.jpeg
148    :width: 600
150 .. image:: images/pexels-photo-972355-seg.jpg
151    :width: 600
153 The :term:`network<Network>` used in the example is jsegnet21v2. It has
154 26 layers.  Users can specify whether to run the network on EVE or C66x.
155 Input to the network is RGB image of size 1024x512.  The output is 1024x512
156 values, each value indicates which pre-trained category the current pixel
157 belongs to.  The example will take the network output, create an overlay,
158 and blend the overlay onto the original input image to create an output image.
159 From the reported time in the following table, we can see that this network
160 runs significantly faster on EVE than on C66x.
162 =======     ====================== ==================== ============
163 Device      Device Processing Time Host Processing Time API Overhead
164 =======     ====================== ==================== ============
165 EVE         251.8 ms               254.2 ms             0.96 %
166 C66x        812.7 ms               815.0 ms             0.27 %
167 =======     ====================== ==================== ============
169 The example code sets ``buffer_factor`` to 2 to create duplicated
170 ExecutionObjectPipelines with identical ExecutionObjects to
171 perform double buffering, so that host pre/post-processing can be overlapped
172 with device processing (see comments in the code for details).
173 The following table shows the loop overall time over 10 frames
174 with single buffering and double buffering,
175 ``./segmentation -f 10 -d <num> -e <num>``.
177 .. list-table:: Loop overall time over 10 frames
178    :header-rows: 1
180    * - Device(s)
181      - Single Buffering (buffer_factor=1)
182      - Double Buffering (buffer_factor=2)
183    * - 1 EVE
184      - 5233 ms
185      - 3017 ms
186    * - 2 EVEs
187      - 3032 ms
188      - 3015 ms
189    * - 1 C66x
190      - 10890 ms
191      - 8416 ms
192    * - 2 C66xs
193      - 5742 ms
194      - 4638 ms
196 .. _ssd-example:
198 SSD
199 ---
201 SSD is the abbreviation for Single Shot multi-box Detector.
202 The ssd_multibox example takes an image as input and detects multiple
203 objects with bounding boxes according to pre-trained categories.
204 The example supports the ssd network with two sets of pretrained categories:
205 ``jdetnet_voc`` and ``jdetnet``.
207 The following figures show an image as input and the image with recognized
208 objects boxed as output from ``jdetnet_voc``: person in red and horse in green.
210 .. figure:: images/horse.png
211    :width: 600
213 .. figure:: images/horse_multibox.png
214    :width: 600
216 The following figures show another street scene as input and the scene
217 with recognized objects boxed as output from ``jdetnet``: pedestrians in red,
218 vehicles in blue and road signs in yellow.
220 .. image:: ../../examples/test/testvecs/input/roads/pexels-photo-378570.jpeg
221    :width: 600
223 .. image:: images/pexels-photo-378570-ssd.jpg
224    :width: 600
226 Please use command line options to switch between these two sets of pre-trained
227 categoris, e.g.
229 .. code-block:: shell
231    ./ssd_multibox # default is jdetnet_voc 
232    ./ssd_multibox -c jdetnet -l jdetnet_objects.json -p 16 -i ../test/testvecs/input/preproc_0_768x320.y
234 The ssd network used in both categories has 43 layers.
235 Input to the network is RGB image of size 768x320.  Output is a list of
236 boxes (up to 20), each box has information about the box coordinates, and
237 which pre-trained category that the object inside the box belongs to.
238 The example will take the network output, draw boxes accordingly,
239 and create an output image.
240 The network can be run entirely on either EVE or C66x.  However, the best
241 performance comes with running the first 30 layers as a group on EVE
242 and the next 13 layers as another group on C66x.
243 Our end-to-end example shows how easy it is to assign a :term:`Layer Group` id
244 to an :term:`Executor` and how easy it is to construct an :term:`ExecutionObjectPipeline` to connect the output of one *Executor*'s :term:`ExecutionObject`
245 to the input of another *Executor*'s *ExecutionObject*.
247 ========      ====================== ==================== ============
248 Device        Device Processing Time Host Processing Time API Overhead
249 ========      ====================== ==================== ============
250 EVE+C66x      169.5ms                172.0ms              1.68 %
251 ========      ====================== ==================== ============
253 The example code sets ``pipeline_depth`` to 2 to create duplicated
254 ExecutionObjectPipelines with identical ExecutionObjects to
255 perform pipelined execution at the ExecutionObject level.
256 The side effect is that it also overlaps host pre/post-processing
257 with device processing (see comments in the code for details).
258 The following table shows the loop overall time over 10 frames
259 with pipelining at ExecutionObjectPipeline level
260 versus ExecutionObject level.
261 ``./ssd_multibox -f 10 -d <num> -e <num>``.
263 .. list-table:: Loop overall time over 10 frames
264    :header-rows: 1
266    * - Device(s)
267      - pipeline_depth=1
268      - pipeline_depth=2
269    * - 1 EVE + 1 C66x
270      - 2900 ms
271      - 1735 ms
272    * - 2 EVEs + 2 C66xs
273      - 1630 ms
274      - 1408 ms
276 .. _mnist-example:
278 MNIST
279 -----
281 The MNIST example takes a pre-processed 28x28 white-on-black frame from
282 a file as input and predicts the hand-written digit in the frame.
283 For example, the example will predict 0 for the following frame.
285 .. code-block:: none
287     root@am57xx-evm:~/tidl/examples/mnist# hexdump -v -e '28/1 "%2x" "\n"' -n 784 ../test/testvecs/input/digits10_images_28x28.y
288      0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0
289      0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0
290      0 0 0 0 0 0 0 0 0 0 0 0 0 0 3 314 8 0 0 0 0 0 0 0 0 0 0
291      0 0 0 0 0 0 0 0 0 0 0 0319bdfeec1671b 0 0 0 0 0 0 0 0 0
292      0 0 0 0 0 0 0 0 0 0 01ed5ffd2a4e4ec89 0 0 0 0 0 0 0 0 0
293      0 0 0 0 0 0 0 0 0 0 1bcffee2a 031e6e225 0 0 0 0 0 0 0 0
294      0 0 0 0 0 0 0 0 0 05ff7ffbf 2 0 078ffa1 0 0 0 0 0 0 0 0
295      0 0 0 0 0 0 0 0 0 0b2f2f34e 0 0 015e0d8 0 0 0 0 0 0 0 0
296      0 0 0 0 0 0 0 0 0148deab2 0 0 0 0 0bdec 2 0 0 0 0 0 0 0
297      0 0 0 0 0 0 0 0 0 084f845 0 0 0 0 0a4f222 0 0 0 0 0 0 0
298      0 0 0 0 0 0 0 0 0 0c4d3 5 0 0 0 0 096f21c 0 0 0 0 0 0 0
299      0 0 0 0 0 0 0 0 052f695 0 0 0 0 0 0a7ed 8 0 0 0 0 0 0 0
300      0 0 0 0 0 0 0 0 09af329 0 0 0 0 0 0d1cf 0 0 0 0 0 0 0 0
301      0 0 0 0 0 0 0 0 2d4c8 0 0 0 0 0 01ae9a2 0 0 0 0 0 0 0 0
302      0 0 0 0 0 0 0 038fa9a 0 0 0 0 0 062ff76 0 0 0 0 0 0 0 0
303      0 0 0 0 0 0 0 07afe5d 0 0 0 0 0 0a9e215 0 0 0 0 0 0 0 0
304      0 0 0 0 0 0 0 0bdec1d 0 0 0 0 017e7aa 0 0 0 0 0 0 0 0 0
305      0 0 0 0 0 0 0 1e7d6 0 0 0 0 0 096f85a 0 0 0 0 0 0 0 0 0
306      0 0 0 0 0 0 01df2bf 0 0 0 0 015e1ca 0 0 0 0 0 0 0 0 0 0
307      0 0 0 0 0 0 061fc95 0 0 0 0 084f767 0 0 0 0 0 0 0 0 0 0
308      0 0 0 0 0 0 06eff8b 0 0 0 033e8ca 4 0 0 0 0 0 0 0 0 0 0
309      0 0 0 0 0 0 060fc9e 0 0 0 092d63e 0 0 0 0 0 0 0 0 0 0 0
310      0 0 0 0 0 0 01bf1da 6 0 019b656 0 0 0 0 0 0 0 0 0 0 0 0
311      0 0 0 0 0 0 0 0c3fb8e a613e7b 5 0 0 0 0 0 0 0 0 0 0 0 0
312      0 0 0 0 0 0 0 049f1fcf5f696 9 0 0 0 0 0 0 0 0 0 0 0 0 0
313      0 0 0 0 0 0 0 0 04ca0b872 1 0 0 0 0 0 0 0 0 0 0 0 0 0 0
314      0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0
315      0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0
317 The file can contain multiple frames.  If an optional label file is also
318 given, the example will compare predicted result against pre-determined
319 label for accuracy.  The input files may or may not have `MNIST dataset
320 file headers <http://yann.lecun.com/exdb/mnist/>`_.  If using headers,
321 input filenames must end with idx3-ubyte or idx1-ubyte.
323 The MNIST example also illustrates low overhead of TIDL API for small
324 networks with low compute requirements (<5ms).  The network runs about 3ms
325 on EVE for a single frame.  As shown in the following table, when running
326 over 1000 frames, the overhead is about 1.8%.
328 .. list-table:: Loop overall time over 1000 frames
329    :header-rows: 1
331    * - Device(s)
332      - Device Processing Time
333      - Host Processing Time
334      - API Overhead
335    * - 1 EVE
336      - 3091 ms
337      - 3146 ms
338      - 1.78%
340 Running Examples
341 ----------------
343 The examples are located in ``/usr/share/ti/tidl/examples`` on
344 the EVM file system.  **Each example needs to be run in its own directory** due to relative paths to configuration files.
345 Running an example with ``-h`` will show help message with option set.
346 The following listing illustrates how to build and run the examples.
348 .. code-block:: shell
350    root@am57xx-evm:~/tidl/examples/imagenet# ./imagenet
351    Input: ../test/testvecs/input/objects/cat-pet-animal-domestic-104827.jpeg
352    1: tabby,   prob = 52.55%
353    2: Egyptian_cat,   prob = 21.18%
354    3: tiger_cat,   prob = 17.65%
355    Loop total time (including read/write/opencv/print/etc):  183.3ms
356    imagenet PASSED
358    root@am57xx-evm:~/tidl-api/examples/segmentation# ./segmentation
359    Input: ../test/testvecs/input/000100_1024x512_bgr.y
360    frame[  0]: Time on EVE0: 251.74 ms, host: 258.02 ms API overhead: 2.43 %
361    Saving frame 0 to: frame_0.png
362    Saving frame 0 overlayed with segmentation to: overlay_0.png
363    frame[  1]: Time on EVE0: 251.76 ms, host: 255.79 ms API overhead: 1.58 %
364    Saving frame 1 to: frame_1.png
365    Saving frame 1 overlayed with segmentation to: overlay_1.png
366    ...
367    frame[  8]: Time on EVE0: 251.75 ms, host: 254.21 ms API overhead: 0.97 %
368    Saving frame 8 to: frame_8.png
369    Saving frame 8 overlayed with segmentation to: overlay_8.png
370    Loop total time (including read/write/opencv/print/etc):   4809ms
371    segmentation PASSED
373    root@am57xx-evm:~/tidl-api/examples/ssd_multibox# ./ssd_multibox
374    Input: ../test/testvecs/input/preproc_0_768x320.y
375    frame[  0]: Time on EVE0+DSP0: 169.44 ms, host: 173.56 ms API overhead: 2.37 %
376    Saving frame 0 to: frame_0.png
377    Saving frame 0 with SSD multiboxes to: multibox_0.png
378    Loop total time (including read/write/opencv/print/etc):  320.2ms
379    ssd_multibox PASSED
381    root@am57xx-evm:~/tidl/examples/mnist# ./mnist
382    Input images: ../test/testvecs/input/digits10_images_28x28.y
383    Input labels: ../test/testvecs/input/digits10_labels_10x1.y
384    0
385    1
386    2
387    3
388    4
389    5
390    6
391    7
392    8
393    9
394    Device total time:  31.02ms
395    Loop total time (including read/write/print/etc):  32.49ms
396    Accuracy:    100%
397    mnist PASSED
400 Image input
401 ^^^^^^^^^^^
403 The image input option, ``-i <image>``, takes an image file as input.
404 You can supply an image file with format that OpenCV can read, since
405 we use OpenCV for image pre/post-processing.  When ``-f <number>`` option
406 is used, the same image will be processed repeatedly.
408 Camera (live video) input
409 ^^^^^^^^^^^^^^^^^^^^^^^^^
411 The input option, ``-i camera<number>``, enables live frame inputs
412 from camera.  ``<number>`` is the video input port number
413 of your camera in Linux.  Use the following command to check video
414 input ports.  The number defaults to ``1`` for TMDSCM572X camera module
415 used on AM57x EVMs.  You can use ``-f <number>`` to specify the number
416 of frames you want to process.
418 .. code-block:: shell
420   root@am57xx-evm:~# v4l2-ctl --list-devices
421   omapwb-cap (platform:omapwb-cap):
422         /dev/video11
424   omapwb-m2m (platform:omapwb-m2m):
425         /dev/video10
427   vip (platform:vip):
428         /dev/video1
430   vpe (platform:vpe):
431         /dev/video0
434 Pre-recorded video (mp4/mov/avi) input
435 ^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^
437 The input option, ``-i <name>.{mp4,mov,avi}``, enables frame inputs from
438 pre-recorded video file in mp4, mov or avi format.  If you have a video in
439 a different OpenCV-supported format/suffix, you can simply create a softlink
440 with one of the mp4, mov or avi suffixes and feed it into the example.
441 Again, use ``-f <number>`` to specify the number of frames you want to process.
443 Displaying video output
444 ^^^^^^^^^^^^^^^^^^^^^^^
446 When using video input, live or pre-recorded, the example will display
447 the output in a window using OpenCV.  If you have a LCD screen attached
448 to the EVM, you will need to kill the ``matrix-gui`` first in order to
449 see the example display window, as shown in the following example.
451 .. code-block:: shell
453   root@am57xx-evm:/usr/share/ti/tidl/examples/ssd_multibox# /etc/init.d/matrix-gui-2.0 stop
454   Stopping Matrix GUI application.
455   root@am57xx-evm:/usr/share/ti/tidl/examples/ssd_multibox# ./ssd_multibox -i camera -f 100
456   Input: camera
457   init done
458   Using Wayland-EGL
459   wlpvr: PVR Services Initialised
460   Using the 'xdg-shell-v5' shell integration
461   ... ...
462   root@am57xx-evm:/usr/share/ti/tidl/examples/ssd_multibox# /etc/init.d/matrix-gui-2.0 start
463   /usr/share/ti/tidl/examples/ssd_multibox
464   Removing stale PID file /var/run/matrix-gui-2.0.pid.
465   Starting Matrix GUI application.
468 .. _AM574x IDK EVM:  http://www.ti.com/tool/tmdsidk574
469 .. _AM5749: http://www.ti.com/product/AM5749/
470 .. _Processor SDK Linux: http://software-dl.ti.com/processor-sdk-linux/esd/AM57X/latest/index_FDS.html