1 ********
2 Examples
3 ********
5 We ship three end-to-end examples within the tidl-api package
6 to demonstrate three categories of deep learning networks. The first
7 two examples can run on AM57x SoCs with either EVE or DSP. The last
8 example requires AM57x SoCs with both EVE and DSP. The performance
9 numbers that we present here were obtained on an AM5729 EVM, which
10 includes 2 ARM A15 cores running at 1.5GHz, 4 EVE cores at 535MHz, and
11 2 DSP cores at 750MHz.
13 Imagenet
14 --------
16 The imagenet example takes an image as input and outputs 1000 probabilities.
17 Each probability corresponds to one object in the 1000 objects that the
18 network is pre-trained with. Our example outputs top 5 probabilities
19 as the most likely objects that the input image can be.
21 The following figure and tables shows an input image, top 5 predicted
22 objects as output, and the processing time on either EVE or DSP.
24 .. image:: ../../examples/test/testvecs/input/objects/cat-pet-animal-domestic-104827.jpeg
25 :width: 600
27 .. table::
29 ==== ============== ============
30 Rank Object Classes Probability
31 ==== ============== ============
32 1 tabby 0.996
33 2 Egyptian_cat 0.977
34 3 tiger_cat 0.973
35 4 lynx 0.941
36 5 Persian_cat 0.922
37 ==== ============== ============
39 .. table::
41 ====================== ==================== ============
42 Device Processing Time Host Processing Time API Overhead
43 ====================== ==================== ============
44 EVE: 123.1 ms 124.7 ms 1.34 %
45 **OR**
46 DSP: 117.9 ms 119.3 ms 1.14 %
47 ====================== ==================== ============
49 The particular network that we ran in this category, jacintonet11v2,
50 has 14 layers. User can specify whether to run the network on EVE or DSP
51 for acceleration. We can see that EVE time is slightly higher than DSP time.
52 Host time includes the OpenCL runtime overhead and the time to copy user
53 input data into padded TIDL buffers. We can see that the overall overhead
54 is less than 1.5%.
56 Segmentation
57 ------------
59 The segmentation example takes an image as input and performs pixel-level
60 classification according to pre-trained categories. The following figures
61 show a street scene as input and the scene overlaid with pixel-level
62 classifications as output: road in green, pedestrians in red, vehicles
63 in blue and background in gray.
65 .. image:: ../../examples/test/testvecs/input/roads/pexels-photo-972355.jpeg
66 :width: 600
68 .. image:: images/pexels-photo-972355-seg.jpg
69 :width: 600
71 The network we ran in this category is jsegnet21v2, which has 26 layers.
72 From the reported time in the following table, we can see that this network
73 runs significantly faster on EVE than on DSP.
75 .. table::
77 ====================== ==================== ============
78 Device Processing Time Host Processing Time API Overhead
79 ====================== ==================== ============
80 EVE: 296.5 ms 303.3 ms 2.26 %
81 **OR**
82 DSP: 812.0 ms 818.4 ms 0.79 %
83 ====================== ==================== ============
85 .. _ssd-example:
87 SSD
88 ---
90 SSD is the abbreviation for Single Shot multi-box Detector.
91 The ssd_multibox example takes an image as input and detects multiple
92 objects with bounding boxes according to pre-trained categories.
93 The following figures show another street scene as input and the scene
94 with recognized objects boxed as output: pedestrians in red,
95 vehicles in blue and road signs in yellow.
97 .. image:: ../../examples/test/testvecs/input/roads/pexels-photo-378570.jpeg
98 :width: 600
100 .. image:: images/pexels-photo-378570-ssd.jpg
101 :width: 600
103 The network can be run entirely on either EVE or DSP. But the best
104 performance comes with running the first 30 layers on EVE and the
105 next 13 layers on DSP, for this particular jdetnet_ssd network.
106 Note the **AND** in the following table for the reported time.
107 Our end-to-end example shows how easy it is to assign a layers group id
108 to an *Executor* and how easy it is to connect the output from one
109 *ExecutionObject* to the input to another *ExecutionObject*.
111 .. table::
113 ====================== ==================== ============
114 Device Processing Time Host Processing Time API Overhead
115 ====================== ==================== ============
116 EVE: 175.2 ms 179.1 ms 2.14 %
117 **AND**
118 DSP: 21.1 ms 22.3 ms 5.62 %
119 ====================== ==================== ============
121 Running Examples
122 ----------------
124 The examples are located in ``/usr/share/ti/tidl-api/examples`` on
125 the EVM file system. Each example needs to be run its own directory.
126 Running an example with ``-h`` will show help message with option set.
127 The following code section shows how to run the examples, and
128 the test program that tests all supported TIDL network configs.
130 .. code:: shell
132 root@am57xx-evm:~# cd /usr/share/ti/tidl-api/examples/imagenet/
133 root@am57xx-evm:/usr/share/ti/tidl-api/examples/imagenet# make -j4
134 root@am57xx-evm:/usr/share/ti/tidl-api/examples/imagenet# ./imagenet -t d
135 Input: ../test/testvecs/input/objects/cat-pet-animal-domestic-104827.jpeg
136 frame[0]: Time on device: 117.9ms, host: 119.3ms API overhead: 1.17 %
137 1: tabby, prob = 0.996
138 2: Egyptian_cat, prob = 0.977
139 3: tiger_cat, prob = 0.973
140 4: lynx, prob = 0.941
141 5: Persian_cat, prob = 0.922
142 imagenet PASSED
144 root@am57xx-evm:/usr/share/ti/tidl-api/examples/imagenet# cd ../segmentation/; make -j4
145 root@am57xx-evm:/usr/share/ti/tidl-api/examples/segmentation# ./segmentation -i ../test/testvecs/input/roads/pexels-photo-972355.jpeg
146 Input: ../test/testvecs/input/roads/pexels-photo-972355.jpeg
147 frame[0]: Time on device: 296.5ms, host: 303.2ms API overhead: 2.21 %
148 Saving frame 0 overlayed with segmentation to: overlay_0.png
149 segmentation PASSED
151 root@am57xx-evm:/usr/share/ti/tidl-api/examples/segmentation# cd ../ssd_multibox/; make -j4
152 root@am57xx-evm:/usr/share/ti/tidl-api/examples/ssd_multibox# ./ssd_multibox -i ../test/testvecs/input/roads/pexels-photo-378570.jpeg
153 Input: ../test/testvecs/input/roads/pexels-photo-378570.jpeg
154 frame[0]: Time on EVE: 175.2ms, host: 179ms API overhead: 2.1 %
155 frame[0]: Time on DSP: 21.06ms, host: 22.43ms API overhead: 6.08 %
156 Saving frame 0 with SSD multiboxes to: multibox_0.png
157 Loop total time (including read/write/print/etc): 423.8ms
158 ssd_multibox PASSED
160 root@am57xx-evm:/usr/share/ti/tidl-api/examples/ssd_multibox# cd ../test; make -j4
161 root@am57xx-evm:/usr/share/ti/tidl-api/examples/test# ./test_tidl
162 API Version: 01.00.00.d91e442
163 Running dense_1x1 on 2 devices, type EVE
164 frame[0]: Time on device: 134.3ms, host: 135.6ms API overhead: 0.994 %
165 dense_1x1 : PASSED
166 Running j11_bn on 2 devices, type EVE
167 frame[0]: Time on device: 176.2ms, host: 177.7ms API overhead: 0.835 %
168 j11_bn : PASSED
169 Running j11_cifar on 2 devices, type EVE
170 frame[0]: Time on device: 53.86ms, host: 54.88ms API overhead: 1.85 %
171 j11_cifar : PASSED
172 Running j11_controlLayers on 2 devices, type EVE
173 frame[0]: Time on device: 122.9ms, host: 123.9ms API overhead: 0.821 %
174 j11_controlLayers : PASSED
175 Running j11_prelu on 2 devices, type EVE
176 frame[0]: Time on device: 300.8ms, host: 302.1ms API overhead: 0.437 %
177 j11_prelu : PASSED
178 Running j11_v2 on 2 devices, type EVE
179 frame[0]: Time on device: 124.1ms, host: 125.6ms API overhead: 1.18 %
180 j11_v2 : PASSED
181 Running jseg21 on 2 devices, type EVE
182 frame[0]: Time on device: 367ms, host: 374ms API overhead: 1.88 %
183 jseg21 : PASSED
184 Running jseg21_tiscapes on 2 devices, type EVE
185 frame[0]: Time on device: 302.2ms, host: 308.5ms API overhead: 2.02 %
186 frame[1]: Time on device: 301.9ms, host: 312.5ms API overhead: 3.38 %
187 frame[2]: Time on device: 302.7ms, host: 305.9ms API overhead: 1.04 %
188 frame[3]: Time on device: 301.9ms, host: 305ms API overhead: 1.01 %
189 frame[4]: Time on device: 302.7ms, host: 305.9ms API overhead: 1.05 %
190 frame[5]: Time on device: 301.9ms, host: 305.5ms API overhead: 1.17 %
191 frame[6]: Time on device: 302.7ms, host: 305.9ms API overhead: 1.06 %
192 frame[7]: Time on device: 301.9ms, host: 305ms API overhead: 1.02 %
193 frame[8]: Time on device: 297ms, host: 300.3ms API overhead: 1.09 %
194 Comparing frame: 0
195 jseg21_tiscapes : PASSED
196 Running smallRoi on 2 devices, type EVE
197 frame[0]: Time on device: 2.548ms, host: 3.637ms API overhead: 29.9 %
198 smallRoi : PASSED
199 Running squeeze1_1 on 2 devices, type EVE
200 frame[0]: Time on device: 292.9ms, host: 294.6ms API overhead: 0.552 %
201 squeeze1_1 : PASSED
203 Multiple Executor...
204 Running network tidl_config_j11_v2.txt on EVEs: 1 in thread 0
205 Running network tidl_config_j11_cifar.txt on EVEs: 0 in thread 1
206 Multiple executors: PASSED
207 Running j11_bn on 2 devices, type DSP
208 frame[0]: Time on device: 170.5ms, host: 171.5ms API overhead: 0.568 %
209 j11_bn : PASSED
210 Running j11_controlLayers on 2 devices, type DSP
211 frame[0]: Time on device: 416.4ms, host: 417.1ms API overhead: 0.176 %
212 j11_controlLayers : PASSED
213 Running j11_v2 on 2 devices, type DSP
214 frame[0]: Time on device: 118ms, host: 119.2ms API overhead: 1.01 %
215 j11_v2 : PASSED
216 Running jseg21 on 2 devices, type DSP
217 frame[0]: Time on device: 1123ms, host: 1128ms API overhead: 0.443 %
218 jseg21 : PASSED
219 Running jseg21_tiscapes on 2 devices, type DSP
220 frame[0]: Time on device: 812.3ms, host: 817.3ms API overhead: 0.614 %
221 frame[1]: Time on device: 812.6ms, host: 818.6ms API overhead: 0.738 %
222 frame[2]: Time on device: 812.3ms, host: 815.1ms API overhead: 0.343 %
223 frame[3]: Time on device: 812.7ms, host: 815.2ms API overhead: 0.312 %
224 frame[4]: Time on device: 812.3ms, host: 815.1ms API overhead: 0.353 %
225 frame[5]: Time on device: 812.6ms, host: 815.1ms API overhead: 0.302 %
226 frame[6]: Time on device: 812.2ms, host: 815.1ms API overhead: 0.357 %
227 frame[7]: Time on device: 812.6ms, host: 815.2ms API overhead: 0.315 %
228 frame[8]: Time on device: 812ms, host: 815ms API overhead: 0.367 %
229 Comparing frame: 0
230 jseg21_tiscapes : PASSED
231 Running smallRoi on 2 devices, type DSP
232 frame[0]: Time on device: 14.21ms, host: 14.94ms API overhead: 4.89 %
233 smallRoi : PASSED
234 Running squeeze1_1 on 2 devices, type DSP
235 frame[0]: Time on device: 960ms, host: 961.1ms API overhead: 0.116 %
236 squeeze1_1 : PASSED
237 tidl PASSED