]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - tidl/tidl-api.git/blob - docs/source/example.rst
Renamed namespace (tidl -> tinn), updated documentation
[tidl/tidl-api.git] / docs / source / example.rst
1 ******************
2 Using the TINN API
3 ******************
5 This example illustrates using the TI Neural Network (TINN) API to offload deep learning network processing from a Linux application to the C66x DSPs or DLAs on AM57x devices.
7 Step 1
8 ======
10 Determine if there are any TINN capable devices on the AM57x SoC:
12 .. code-block:: c++
14     uint32_t num_dla = Executor::GetNumDevices(DeviceType::DLA);
15     uint32_t num_dsp = Executor::GetNumDevices(DeviceType::DSP);
17 Step 2
18 ======
19 Create a Configuration object by reading it from a file or by initializing it directly. The example below parses a configuration file and initializes the Configuration object. See ``tidl/testvecs/config/infer`` for examples of configuration files.
21 .. code::
23     Configuration configuration;
24     bool status = configuration.ReadFromFile(config_file);
26 .. note::
27     Refer TINN Translation Tool documentation for creating TINN network and parameter binary files from TensorFlow and Caffe.
29 Step 3
30 ======
31 Create an Executor with the approriate device type, set of devices and a configuration. In the snippet below, an Executor is created on 2 DLAs.
33 .. code-block:: c++
35         DeviceIds ids = {DeviceId::ID0, DeviceId::ID1};
36         Executor executor(DeviceType::DLA, ids, configuration);
38 Step 4
39 ======
40 Get the set of available ExecutionObjects and allocate input and output buffers for each ExecutionObject.
42 .. code-block:: c++
44         const ExecutionObjects& execution_objects = executor.GetExecutionObjects();
45         int num_eos = execution_objects.size();
47         // Allocate input and output buffers for each execution object
48         std::vector<void *> buffers;
49         for (auto &eo : execution_objects)
50         {
51             ArgInfo in  = { ArgInfo(malloc(frame_sz), frame_sz)};
52             ArgInfo out = { ArgInfo(malloc(frame_sz), frame_sz)};
53             eo->SetInputOutputBuffer(in, out);
55             buffers.push_back(in.ptr());
56             buffers.push_back(out.ptr());
57         }
61 Step 5
62 ======
63 Run the network on each input frame.  The frames are processed with available execution objects in a pipelined manner with additional num_eos iterations to flush the pipeline (epilogue).
65 .. code-block:: c++
67         for (int frame_idx = 0; frame_idx < configuration.numFrames + num_eos; frame_idx++)
68         {
69             ExecutionObject* eo = execution_objects[frame_idx % num_eos].get();
71             // Wait for previous frame on the same eo to finish processing
72             if (eo->ProcessFrameWait())
73                 WriteFrame(*eo, output_data_file);
75             // Read a frame and start processing it with current eo
76             if (ReadFrame(*eo, frame_idx, configuration, input_data_file))
77                 eo->ProcessFrameStartAsync();
78         }
82 Putting it together
83 ===================
84 The code snippet :ref:`tidl_main` illustrates using the API to offload a network.
86 .. literalinclude:: ../../examples/test/main.cpp
87     :name: tidl_main
88     :caption: examples/test/main.cpp
89     :lines: 161-195,213-218,220-225
90     :linenos:
92 For a complete example of using the API, refer ``tinn/examples/opencl/tidl/main.cpp`` on the EVM filesystem.