]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - tidl/tidl-api.git/blob - docs/source/example.rst
Merge branch 'release/v01.00.00'
[tidl/tidl-api.git] / docs / source / example.rst
1 ********
2 Examples
3 ********
5 We ship three end-to-end examples within the tidl-api package
6 to demonstrate three categories of deep learning networks.  The first
7 two examples can run on AM57x SoCs with either DLA or DSP.  The last
8 example requires AM57x SoCs with both DLA and DSP.  The performance
9 numbers that we present here were obtained on an AM5729 EVM, which
10 includes 2 ARM A15 cores running at 1.5GHz, 4 DLA cores at 535MHz, and
11 2 DSP cores at 750MHz.
13 Imagenet
14 --------
16 The imagenet example takes an image as input and outputs 1000 probabilities.
17 Each probability corresponds to one object in the 1000 objects that the
18 network is pre-trained with.  Our example outputs top 5 probabilities
19 as the most likely objects that the input image can be.
21 The following figure and tables shows an input image, top 5 predicted
22 objects as output, and the processing time on either DLA or DSP.
24 .. image:: ../../examples/test/testvecs/input/objects/cat-pet-animal-domestic-104827.jpeg
25    :width: 600
27 .. table::
29     ==== ============== ============
30     Rank Object Classes Probability
31     ==== ============== ============
32     1    tabby          0.996
33     2    Egyptian_cat   0.977
34     3    tiger_cat      0.973
35     4    lynx           0.941
36     5    Persian_cat    0.922
37     ==== ============== ============
39 .. table::
41    ====================== ==================== ============
42    Device Processing Time Host Processing Time API Overhead
43    ====================== ==================== ============
44    DLA: 123.1 ms          124.7 ms             1.34 %
45    **OR**
46    DSP: 117.9 ms          119.3 ms             1.14 %
47    ====================== ==================== ============
49 The particular network that we ran in this category, jacintonet11v2,
50 has 14 layers.  User can specify whether to run the network on DLA or DSP
51 for acceleration.  We can see that DLA time is slightly higher than DSP time.
52 Host time includes the OpenCL runtime overhead and the time to copy user
53 input data into padded TIDL buffers.  We can see that the overall overhead
54 is less than 1.5%.
56 Segmentation
57 ------------
59 The segmentation example takes an image as input and performs pixel-level
60 classification according to pre-trained categories.  The following figures
61 show a street scene as input and the scene overlaid with pixel-level
62 classifications as output: road in green, pedestrians in red, vehicles
63 in blue and background in gray.
65 .. image:: ../../examples/test/testvecs/input/roads/pexels-photo-972355.jpeg
66    :width: 600
68 .. image:: images/pexels-photo-972355-seg.jpg
69    :width: 600
71 The network we ran in this category is jsegnet21v2, which has 26 layers.
72 From the reported time in the following table, we can see that this network
73 runs significantly faster on DLA than on DSP.
75 .. table::
77    ====================== ==================== ============
78    Device Processing Time Host Processing Time API Overhead
79    ====================== ==================== ============
80    DLA: 296.5 ms          303.3 ms             2.26 %
81    **OR**
82    DSP: 812.0 ms          818.4 ms             0.79 %
83    ====================== ==================== ============
85 .. _ssd-example:
87 SSD
88 ---
90 SSD is the abbreviation for Single Shot multi-box Detector.
91 The ssd_multibox example takes an image as input and detects multiple
92 objects with bounding boxes according to pre-trained categories.
93 The following figures show another street scene as input and the scene
94 with recognized objects boxed as output: pedestrians in red,
95 vehicles in blue and road signs in yellow.
97 .. image:: ../../examples/test/testvecs/input/roads/pexels-photo-378570.jpeg
98    :width: 600
100 .. image:: images/pexels-photo-378570-ssd.jpg
101    :width: 600
103 The network can be run entirely on either DLA or DSP.  But the best
104 performance comes with running the first 30 layers on DLA and the
105 next 13 layers on DSP, for this particular jdetnet_ssd network.
106 Note the **AND** in the following table for the reported time.
107 Our end-to-end example shows how easy it is to assign a layers group id
108 to an *Executor* and how easy it is to connect the output from one
109 *ExecutionObject* to the input to another *ExecutionObject*.
111 .. table::
113    ====================== ==================== ============
114    Device Processing Time Host Processing Time API Overhead
115    ====================== ==================== ============
116    DLA: 175.2 ms          179.1 ms             2.14 %
117    **AND**
118    DSP:  21.1 ms           22.3 ms             5.62 %
119    ====================== ==================== ============
121 Running Examples
122 ----------------
124 The examples are located in ``/usr/share/ti/tidl-api/examples`` on
125 the EVM file system.  Each example needs to be run its own directory.
126 Running an example with ``-h`` will show help message with option set.
127 The following code section shows how to run the examples, and
128 the test program that tests all supported TIDL network configs.
130 .. code:: shell
132    root@am57xx-evm:~# cd /usr/share/ti/tidl-api/examples/imagenet/
133    root@am57xx-evm:/usr/share/ti/tidl-api/examples/imagenet# make -j4
134    root@am57xx-evm:/usr/share/ti/tidl-api/examples/imagenet# ./imagenet -t d
135    Input: ../test/testvecs/input/objects/cat-pet-animal-domestic-104827.jpeg
136    frame[0]: Time on device:  117.9ms, host:  119.3ms API overhead:   1.17 %
137    1: tabby, prob = 0.996
138    2: Egyptian_cat, prob = 0.977
139    3: tiger_cat, prob = 0.973
140    4: lynx, prob = 0.941
141    5: Persian_cat, prob = 0.922
142    imagenet PASSED
144    root@am57xx-evm:/usr/share/ti/tidl-api/examples/imagenet# cd ../segmentation/; make -j4
145    root@am57xx-evm:/usr/share/ti/tidl-api/examples/segmentation# ./segmentation -i ../test/testvecs/input/roads/pexels-photo-972355.jpeg
146    Input: ../test/testvecs/input/roads/pexels-photo-972355.jpeg
147    frame[0]: Time on device:  296.5ms, host:  303.2ms API overhead:   2.21 %
148    Saving frame 0 overlayed with segmentation to: overlay_0.png
149    segmentation PASSED
151    root@am57xx-evm:/usr/share/ti/tidl-api/examples/segmentation# cd ../ssd_multibox/; make -j4
152    root@am57xx-evm:/usr/share/ti/tidl-api/examples/ssd_multibox# ./ssd_multibox -i ../test/testvecs/input/roads/pexels-photo-378570.jpeg
153    Input: ../test/testvecs/input/roads/pexels-photo-378570.jpeg
154    frame[0]: Time on DLA:  175.2ms, host:    179ms API overhead:    2.1 %
155    frame[0]: Time on DSP:  21.06ms, host:  22.43ms API overhead:   6.08 %
156    Saving frame 0 with SSD multiboxes to: multibox_0.png
157    Loop total time (including read/write/print/etc):  423.8ms
158    ssd_multibox PASSED
160    root@am57xx-evm:/usr/share/ti/tidl-api/examples/ssd_multibox# cd ../test; make -j4
161    root@am57xx-evm:/usr/share/ti/tidl-api/examples/test# ./test_tidl
162    API Version: 01.00.00.d91e442
163    Running dense_1x1 on 2 devices, type EVE
164    frame[0]: Time on device:  134.3ms, host:  135.6ms API overhead:  0.994 %
165    dense_1x1 : PASSED
166    Running j11_bn on 2 devices, type EVE
167    frame[0]: Time on device:  176.2ms, host:  177.7ms API overhead:  0.835 %
168    j11_bn : PASSED
169    Running j11_cifar on 2 devices, type EVE
170    frame[0]: Time on device:  53.86ms, host:  54.88ms API overhead:   1.85 %
171    j11_cifar : PASSED
172    Running j11_controlLayers on 2 devices, type EVE
173    frame[0]: Time on device:  122.9ms, host:  123.9ms API overhead:  0.821 %
174    j11_controlLayers : PASSED
175    Running j11_prelu on 2 devices, type EVE
176    frame[0]: Time on device:  300.8ms, host:  302.1ms API overhead:  0.437 %
177    j11_prelu : PASSED
178    Running j11_v2 on 2 devices, type EVE
179    frame[0]: Time on device:  124.1ms, host:  125.6ms API overhead:   1.18 %
180    j11_v2 : PASSED
181    Running jseg21 on 2 devices, type EVE
182    frame[0]: Time on device:    367ms, host:    374ms API overhead:   1.88 %
183    jseg21 : PASSED
184    Running jseg21_tiscapes on 2 devices, type EVE
185    frame[0]: Time on device:  302.2ms, host:  308.5ms API overhead:   2.02 %
186    frame[1]: Time on device:  301.9ms, host:  312.5ms API overhead:   3.38 %
187    frame[2]: Time on device:  302.7ms, host:  305.9ms API overhead:   1.04 %
188    frame[3]: Time on device:  301.9ms, host:    305ms API overhead:   1.01 %
189    frame[4]: Time on device:  302.7ms, host:  305.9ms API overhead:   1.05 %
190    frame[5]: Time on device:  301.9ms, host:  305.5ms API overhead:   1.17 %
191    frame[6]: Time on device:  302.7ms, host:  305.9ms API overhead:   1.06 %
192    frame[7]: Time on device:  301.9ms, host:    305ms API overhead:   1.02 %
193    frame[8]: Time on device:    297ms, host:  300.3ms API overhead:   1.09 %
194    Comparing frame: 0
195    jseg21_tiscapes : PASSED
196    Running smallRoi on 2 devices, type EVE
197    frame[0]: Time on device:  2.548ms, host:  3.637ms API overhead:   29.9 %
198    smallRoi : PASSED
199    Running squeeze1_1 on 2 devices, type EVE
200    frame[0]: Time on device:  292.9ms, host:  294.6ms API overhead:  0.552 %
201    squeeze1_1 : PASSED
203    Multiple Executor...
204    Running network tidl_config_j11_v2.txt on EVEs: 1  in thread 0
205    Running network tidl_config_j11_cifar.txt on EVEs: 0  in thread 1
206    Multiple executors: PASSED
207    Running j11_bn on 2 devices, type DSP
208    frame[0]: Time on device:  170.5ms, host:  171.5ms API overhead:  0.568 %
209    j11_bn : PASSED
210    Running j11_controlLayers on 2 devices, type DSP
211    frame[0]: Time on device:  416.4ms, host:  417.1ms API overhead:  0.176 %
212    j11_controlLayers : PASSED
213    Running j11_v2 on 2 devices, type DSP
214    frame[0]: Time on device:    118ms, host:  119.2ms API overhead:   1.01 %
215    j11_v2 : PASSED
216    Running jseg21 on 2 devices, type DSP
217    frame[0]: Time on device:   1123ms, host:   1128ms API overhead:  0.443 %
218    jseg21 : PASSED
219    Running jseg21_tiscapes on 2 devices, type DSP
220    frame[0]: Time on device:  812.3ms, host:  817.3ms API overhead:  0.614 %
221    frame[1]: Time on device:  812.6ms, host:  818.6ms API overhead:  0.738 %
222    frame[2]: Time on device:  812.3ms, host:  815.1ms API overhead:  0.343 %
223    frame[3]: Time on device:  812.7ms, host:  815.2ms API overhead:  0.312 %
224    frame[4]: Time on device:  812.3ms, host:  815.1ms API overhead:  0.353 %
225    frame[5]: Time on device:  812.6ms, host:  815.1ms API overhead:  0.302 %
226    frame[6]: Time on device:  812.2ms, host:  815.1ms API overhead:  0.357 %
227    frame[7]: Time on device:  812.6ms, host:  815.2ms API overhead:  0.315 %
228    frame[8]: Time on device:    812ms, host:    815ms API overhead:  0.367 %
229    Comparing frame: 0
230    jseg21_tiscapes : PASSED
231    Running smallRoi on 2 devices, type DSP
232    frame[0]: Time on device:  14.21ms, host:  14.94ms API overhead:   4.89 %
233    smallRoi : PASSED
234    Running squeeze1_1 on 2 devices, type DSP
235    frame[0]: Time on device:    960ms, host:  961.1ms API overhead:  0.116 %
236    squeeze1_1 : PASSED
237    tidl PASSED