1 ************
2 Introduction
3 ************
5 TI Deep Learning (TIDL) API brings deep learning to the edge by enabling applications to leverage TI's proprietary, highly optimized CNN/DNN implementation on the EVE and C66x DSP compute engines. TIDL will initially target Vision/2D use cases on AM57x Sitara Processors.
7 The TIDL API leverages TI's `OpenCL`_ product to offload deep learning applications to both EVE(s) and DSP(s). The TIDL API significantly improves the out-of-box deep learning experience for users and enables them to focus on their overall use case. They do not have to spend time on the mechanics of ARM ↔ DSP/EVE communication or implementing optimized network layers on EVE(s) and/or DSP(s). The API allows customers to easily integrate frameworks such as OpenCV and rapidly prototype deep learning applications.
9 .. note::
11 This User's Guide focuses on the TIDL API. For information on TIDL such as the overall development flow, techniques to optimize performance of CNN/DNN on TI's processors, performance/benchmarking data and list of supported layers, see the TIDL section in the `Processor SDK Linux Software Developer's Guide (TIDL chapter)`_.
13 Key Features
14 ------------
15 **Ease of use**
17 * Easily integrate TIDL APIs into other frameworks such as `OpenCV`_
18 * Provides a common host abstraction for user applications across multiple compute engines (EVEs and C66x DSPs)
20 **Low overhead**
22 The execution time of TIDL APIs on the host is a fairly small percentage of the overall per-frame execution time. For example, with jseg21 network, 1024x512 frame with 3 channels, the APIs account for ~1.5% of overall per-frame processing time.
24 Development Flow
25 ----------------
27 .. _`TIDL Development flow`:
29 .. figure:: images/tidl-development-flow.png
30 :align: center
31 :scale: 50
33 Development flow with TIDL APIs
35 :numref:`TIDL Development flow` shows the overall development process. Deep learning consists to two stages: training at development stage and inference at deployment stage. Training involves designing neural network model, running training data through the network to tune the model parameters. Inference takes the pre-trained model including parameters, applies to new input and produces output. Training is computationally intensive and is done using frameworks such as Caffe/TensorFlow. Once the network is trained, the TIDL converter tool can be used to translate the network and parameters to TIDL. The `Processor SDK Linux Software Developer's Guide (TIDL chapter)`_ provides details on the development flow and and the converter tool.
37 .. _Processor SDK Linux Software Developer's Guide: http://software-dl.ti.com/processor-sdk-linux/esd/docs/latest/linux/index.html
38 .. _Processor SDK Linux Software Developer's Guide (TIDL chapter): http://software-dl.ti.com/processor-sdk-linux/esd/docs/latest/linux/Foundational_Components_TIDL.html
39 .. _OpenCV: http://software-dl.ti.com/processor-sdk-linux/esd/docs/latest/linux/Foundational_Components.html#opencv
40 .. _OpenCL: http://software-dl.ti.com/mctools/esd/docs/opencl/index.html