]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - tidl/tidl-api.git/blob - docs/source/using_api.rst
Documentation - additions and cleanup
[tidl/tidl-api.git] / docs / source / using_api.rst
1 .. _using-tidl-api:
3 ******************
4 Using the TIDL API
5 ******************
7 This example illustrates using the TIDL API to offload deep learning network processing from a Linux application to the C66x DSPs or DLAs on AM57x devices. The API consists of three classes: ``Configuration``, ``Executor`` and ``ExecutionObject``.
9 Step 1
10 ======
12 Determine if there are any TIDL capable devices on the AM57x SoC:
14 .. code-block:: c++
16     uint32_t num_dla = Executor::GetNumDevices(DeviceType::DLA);
17     uint32_t num_dsp = Executor::GetNumDevices(DeviceType::DSP);
19 Step 2
20 ======
21 Create a Configuration object by reading it from a file or by initializing it directly. The example below parses a configuration file and initializes the Configuration object. See ``examples/test/testvecs/config/infer`` for examples of configuration files.
23 .. code::
25     Configuration configuration;
26     bool status = configuration.ReadFromFile(config_file);
28 .. note::
29     Refer `Processor SDK Linux Software Developer's Guide`_ for creating TIDL network and parameter binary files from TensorFlow and Caffe.
31 Step 3
32 ======
33 Create an Executor with the appropriate device type, set of devices and a configuration. In the snippet below, an Executor is created on 2 DLAs.
35 .. code-block:: c++
37         DeviceIds ids = {DeviceId::ID0, DeviceId::ID1};
38         Executor executor(DeviceType::DLA, ids, configuration);
40 Step 4
41 ======
42 Get the set of available ExecutionObjects and allocate input and output buffers for each ExecutionObject.
44 .. code-block:: c++
46         const ExecutionObjects& execution_objects = executor.GetExecutionObjects();
47         int num_eos = execution_objects.size();
49         // Allocate input and output buffers for each execution object
50         std::vector<void *> buffers;
51         for (auto &eo : execution_objects)
52         {
53             ArgInfo in  = { ArgInfo(malloc(frame_sz), frame_sz)};
54             ArgInfo out = { ArgInfo(malloc(frame_sz), frame_sz)};
55             eo->SetInputOutputBuffer(in, out);
57             buffers.push_back(in.ptr());
58             buffers.push_back(out.ptr());
59         }
61 Step 5
62 ======
63 Run the network on each input frame.  The frames are processed with available execution objects in a pipelined manner with additional num_eos iterations to flush the pipeline (epilogue).
65 .. code-block:: c++
67         for (int frame_idx = 0; frame_idx < configuration.numFrames + num_eos; frame_idx++)
68         {
69             ExecutionObject* eo = execution_objects[frame_idx % num_eos].get();
71             // Wait for previous frame on the same eo to finish processing
72             if (eo->ProcessFrameWait())
73                 WriteFrame(*eo, output_data_file);
75             // Read a frame and start processing it with current eo
76             if (ReadFrame(*eo, frame_idx, configuration, input_data_file))
77                 eo->ProcessFrameStartAsync();
78         }
80 For a complete example of using the API, refer any of the examples available at ``/usr/share/ti/tidl-api/examples`` on the EVM file system.
82 .. _Processor SDK Linux Software Developer's Guide: http://software-dl.ti.com/processor-sdk-linux/esd/docs/latest/linux/index.html