1 .. _using-tidl-api:
3 *************
4 Using the API
5 *************
7 This section illustrates using TIDL APIs to leverage deep learning in user applications. The overall flow is as follows:
9 * Create a :term:`Configuration` object to specify the set of parameters required for network exectution.
10 * Create :term:`Executor` objects - one to manage overall execution on the EVEs, the other for C66x DSPs.
11 * Use the :term:`Execution Objects<EO>` (EO) created by the Executor to process :term:`frames<Frame>`. There are two approaches to processing frames using Execution Objects:
13 #. Each EO processes a single frame.
14 #. Split processing frame across multiple EOs using an :term:`ExecutionObjectPipeline`.
16 Refer Section :ref:`api-documentation` for API documentation.
18 Use Cases
19 +++++++++
21 .. _use-case-1:
23 Each EO processes a single frame
24 ================================
26 In this approach, the :term:`network<Network>` is set up as a single :term:`Layer Group`. An :term:`EO` runs the entire layer group on a single frame. To increase throughput, frame processing can be pipelined across available EOs. For example, on AM5749, frames can be processed by 4 EOs: one each on EVE1, EVE2, DSP1, and DSP2.
29 .. figure:: images/tidl-one-eo-per-frame.png
30 :align: center
31 :scale: 80
33 Processing a frame with one EO. Not to scale. Fn: Frame n, LG: Layer Group.
35 #. Determine if there are any TIDL capable :term:`compute cores<Compute core>` on the AM57x Processor:
37 .. literalinclude:: ../../examples/one_eo_per_frame/main.cpp
38 :language: c++
39 :lines: 64-65
40 :linenos:
42 #. Create a Configuration object by reading it from a file or by initializing it directly. The example below parses a configuration file and initializes the Configuration object. See ``examples/test/testvecs/config/infer`` for examples of configuration files.
44 .. literalinclude:: ../../examples/one_eo_per_frame/main.cpp
45 :language: c++
46 :lines: 92-94
47 :linenos:
49 #. Create Executor on C66x and EVE. In this example, all available C66x and EVE cores are used (lines 1-2 and :ref:`CreateExecutor`).
50 #. Create a vector of available ExecutionObjects from both Executors (lines 7-8 and :ref:`CollectEOs`).
51 #. Allocate input and output buffers for each ExecutionObject (:ref:`AllocateMemory`)
52 #. Run the network on each input frame. The frames are processed with available execution objects in a pipelined manner. The additional num_eos iterations are required to flush the pipeline (lines 15-26).
54 * Wait for the EO to finish processing. If the EO is not processing a frame (the first iteration on each EO), the call to ``ProcessFrameWait`` returns false. ``ReportTime`` is used to report host and device execution times.
55 * Read a frame and start running the network. ``ProcessFrameStartAsync`` is asynchronous and returns before processing is complete. ``ReadFrame`` is application specific and used to read an input frame for processing. For example, with OpenCV, ``ReadFrame`` is implemented using OpenCV APIs to capture a frame from the camera.
57 .. literalinclude:: ../../examples/one_eo_per_frame/main.cpp
58 :language: c++
59 :lines: 108-127,129,133-139
60 :linenos:
62 .. literalinclude:: ../../examples/one_eo_per_frame/main.cpp
63 :language: c++
64 :lines: 154-163
65 :linenos:
66 :caption: CreateExecutor
67 :name: CreateExecutor
69 .. literalinclude:: ../../examples/one_eo_per_frame/main.cpp
70 :language: c++
71 :lines: 166-172
72 :linenos:
73 :caption: CollectEOs
74 :name: CollectEOs
76 .. literalinclude:: ../../examples/common/utils.cpp
77 :language: c++
78 :lines: 197-212
79 :linenos:
80 :caption: AllocateMemory
81 :name: AllocateMemory
83 The complete example is available at ``/usr/share/ti/tidl/examples/one_eo_per_frame/main.cpp``.
85 .. note::
86 The double buffering technique described in :ref:`use-case-3` can be used with a single :term:`ExecutionObject` to overlap reading a frame with the processing of the previous frame.
88 .. _use-case-2:
90 Frame split across EOs
91 ======================
92 This approach is typically used to reduce the latency of processing a single frame. Certain network layers such as Softmax and Pooling run faster on the C66x vs. EVE. Running these layers on C66x can lower the per-frame latency.
94 Time to process a single frame 224x224x3 frame on AM574x IDK EVM (Arm @ 1GHz, C66x @ 0.75GHz, EVE @ 0.65GHz) with JacintoNet11 (tidl_net_imagenet_jacintonet11v2.bin), TIDL API v1.1:
96 ====== ======= ===================
97 EVE C66x EVE + C66x
98 ====== ======= ===================
99 ~112ms ~120ms ~64ms :sup:`1`
100 ====== ======= ===================
102 :sup:`1` BatchNorm and Convolution layers run on EVE are placed in a :term:`Layer Group` and run on EVE. Pooling, InnerProduct, SoftMax layers are placed in a second :term:`Layer Group` and run on C66x. The EVE layer group takes ~57.5ms, C66x layer group takes ~6.5ms.
104 .. _frame-across-eos:
105 .. figure:: images/tidl-frame-across-eos.png
106 :align: center
107 :scale: 80
109 Processing a frame across EOs. Not to scale. Fn: Frame n, LG: Layer Group.
111 The network consists of 2 :term:`Layer Groups<Layer Group>`. :term:`Execution Objects<EO>` are organized into :term:`Execution Object Pipelines<EOP>` (EOP). Each :term:`EOP` processes a frame. The API manages inter-EO synchronization.
113 #. Determine if there are any TIDL capable :term:`compute cores<Compute core>` on the AM57x Processor:
115 .. literalinclude:: ../../examples/one_eo_per_frame/main.cpp
116 :language: c++
117 :lines: 64-65
118 :linenos:
120 #. Create a Configuration object by reading it from a file or by initializing it directly. The example below parses a configuration file and initializes the Configuration object. See ``examples/test/testvecs/config/infer`` for examples of configuration files.
122 .. literalinclude:: ../../examples/one_eo_per_frame/main.cpp
123 :language: c++
124 :lines: 92-94
125 :linenos:
127 #. Update the default layer group index assignment. Pooling (layer 12), InnerProduct (layer 13) and SoftMax (layer 14) are added to a second layer group. Refer :ref:`layer-group-override` for details.
129 .. literalinclude:: ../../examples/two_eo_per_frame/main.cpp
130 :language: c++
131 :lines: 101-102
132 :linenos:
134 #. Create :term:`Executors<Executor>` on C66x and EVE. The EVE Executor runs layer group 1, the C66x executor runs layer group 2.
136 #. Create two :term:`Execution Object Pipelines<EOP>`. Each EOP contains one EVE and one C66x :term:`Execution Object<EO>` respectively.
137 #. Allocate input and output buffers for each ExecutionObject in the EOP. (:ref:`AllocateMemory2`)
138 #. Run the network on each input frame. The frames are processed with available EOPs in a pipelined manner. For ease of use, EOP and EO present the same interface to the user.
140 * Wait for the EOP to finish processing. If the EOP is not processing a frame (the first iteration on each EOP), the call to ``ProcessFrameWait`` returns false. ``ReportTime`` is used to report host and device execution times.
141 * Read a frame and start running the network. ``ProcessFrameStartAsync`` is asynchronous and returns before processing is complete. ``ReadFrame`` is application specific and used to read an input frame for processing. For example, with OpenCV, ``ReadFrame`` is implemented using OpenCV APIs to capture a frame from the camera.
144 .. literalinclude:: ../../examples/two_eo_per_frame/main.cpp
145 :language: c++
146 :lines: 110-138,140,147-153
147 :linenos:
149 .. literalinclude:: ../../examples/common/utils.cpp
150 :language: c++
151 :lines: 225-240
152 :linenos:
153 :caption: AllocateMemory
154 :name: AllocateMemory2
157 The complete example is available at ``/usr/share/ti/tidl/examples/two_eo_per_frame/main.cpp``. Another example of using the EOP is :ref:`ssd-example`.
159 .. _use-case-3:
161 Using EOPs for double buffering
162 ===============================
164 The timeline shown in :numref:`frame-across-eos` indicates that EO-EVE1 waits for processing on E0-DSP1 to complete before it starts processing its next frame. It is possible to optimize the example further and overlap processing F :sub:`n-2` on EO-DSP1 and F :sub:`n` on E0-EVE1. This is illustrated in :numref:`frame-across-eos-opt`.
166 .. _frame-across-eos-opt:
167 .. figure:: images/tidl-frame-across-eos-opt.png
168 :align: center
169 :scale: 80
171 Optimizing using double buffered EOPs. Not to scale. Fn: Frame n, LG: Layer Group.
173 EOP1 and EOP2 use the same :term:`EOs<EO>`: E0-EVE1 and E0-DSP1. Each :term:`EOP` has it's own input and output buffer. This enables EOP2 to read an input frame when EOP1 is processing its input frame. This in turn enables EOP2 to start processing on EO-EVE1 as soon as EOP1 completes processing on E0-EVE1.
175 The only change in the code compared to :ref:`use-case-2` is to create an additional set of EOPs for double buffering:
177 .. literalinclude:: ../../examples/two_eo_per_frame_opt/main.cpp
178 :language: c++
179 :lines: 117-129
180 :linenos:
181 :caption: Setting up EOPs for double buffering
182 :name: test-code
184 .. note::
185 EOP1 in :numref:`frame-across-eos-opt` -> EOPs[0] in :numref:`test-code`.
186 EOP2 in :numref:`frame-across-eos-opt` -> EOPs[1] in :numref:`test-code`.
187 EOP3 in :numref:`frame-across-eos-opt` -> EOPs[2] in :numref:`test-code`.
188 EOP4 in :numref:`frame-across-eos-opt` -> EOPs[3] in :numref:`test-code`.
190 The complete example is available at ``/usr/share/ti/tidl/examples/two_eo_per_frame_opt/main.cpp``.
192 .. _sizing_device_heaps:
194 Sizing device side heaps
195 ++++++++++++++++++++++++
197 TIDL API allocates 2 heaps for device size allocations during network setup/initialization:
199 +-----------+-----------------------------------+-----------------------------+
200 | Heap Name | Configuration parameter | Default size |
201 +-----------+-----------------------------------+-----------------------------+
202 | Parameter | Configuration::PARAM_HEAP_SIZE | 9MB, 1 per Executor |
203 +-----------+-----------------------------------+-----------------------------+
204 | Network | Configuration::NETWORK_HEAP_SIZE | 64MB, 1 per ExecutionObject |
205 +-----------+-----------------------------------+-----------------------------+
207 Depending on the network being deployed, these defaults may be smaller or larger than required. In order to determine the exact sizes for the heaps, the following approach can be used:
209 Start with the default heap sizes. The API displays heap usage statistics when Configuration::showHeapStats is set to true.
211 .. code-block:: c++
213 Configuration configuration;
214 bool status = configuration.ReadFromFile(config_file);
215 configuration.showHeapStats = true;
217 If the heap size is larger than required by device side allocations, the API displays usage statistics. When ``Free`` > 0, the heaps are larger than required.
219 .. code-block:: bash
221 # ./test_tidl -n 1 -t e -c testvecs/config/infer/tidl_config_j11_v2.txt
222 API Version: 01.01.00.00.e4e45c8
223 [eve 0] TIDL Device Trace: PARAM heap: Size 9437184, Free 6556180, Total requested 2881004
224 [eve 0] TIDL Device Trace: NETWORK heap: Size 67108864, Free 47047680, Total requested 20061184
227 Update the application to set the heap sizes to the "Total requested size" displayed:
229 .. code-block:: c++
231 configuration.PARAM_HEAP_SIZE = 2881004;
232 configuration.NETWORK_HEAP_SIZE = 20061184;
234 .. code-block:: bash
236 # ./test_tidl -n 1 -t e -c testvecs/config/infer/tidl_config_j11_v2.txt
237 API Version: 01.01.00.00.e4e45c8
238 [eve 0] TIDL Device Trace: PARAM heap: Size 2881004, Free 0, Total requested 2881004
239 [eve 0] TIDL Device Trace: NETWORK heap: Size 20061184, Free 0, Total requested 20061184
241 Now, the heaps are sized as required by network execution (i.e. ``Free`` is 0)
242 and the ``configuration.showHeapStats = true`` line can be removed.
244 .. note::
246 If the default heap sizes are smaller than required, the device will report an allocation failure and indicate the required minimum size. E.g.
247 .. code-block:: bash
249 # ./test_tidl -n 1 -t e -c testvecs/config/infer/tidl_config_j11_v2.txt
250 API Version: 01.01.00.00.0ba86d4
251 [eve 0] TIDL Device Error: Allocation failure with NETWORK heap, request size 161472, avail 102512
252 [eve 0] TIDL Device Error: Network heap must be >= 20061184 bytes, 19960944 not sufficient. Update Configuration::NETWORK_HEAP_SIZE
253 TIDL Error: [src/execution_object.cpp, Wait, 548]: Allocation failed on device
255 .. note::
257 The memory for parameter and network heaps is itself allocated from OpenCL global memory (CMEM). Refer :ref:`opencl-global-memory` for details.
261 .. _network_layer_output:
263 Accessing outputs of network layers
264 +++++++++++++++++++++++++++++++++++
266 TIDL API v1.1 and higher provides the following APIs to access the output buffers associated with network layers:
268 * :cpp:`ExecutionObject::WriteLayerOutputsToFile` - write outputs from each layer into individual files. Files are named ``<filename_prefix>_<layer_index>.bin``.
269 * :cpp:`ExecutionObject::GetOutputsFromAllLayers` - Get output buffers from all layers.
270 * :cpp:`ExecutionObject::GetOutputFromLayer` - Get a single output buffer from a layer.
272 See ``examples/layer_output/main.cpp, ProcessTrace()`` for examples of using these tracing APIs.
274 .. note::
275 The :cpp:`ExecutionObject::GetOutputsFromAllLayers` method can be memory intensive if the network has a large number of layers. This method allocates sufficient host memory to hold all output buffers from all layers.
277 .. _Processor SDK Linux Software Developer's Guide: http://software-dl.ti.com/processor-sdk-linux/esd/docs/latest/linux/index.html
278 .. _Processor SDK Linux Software Developer's Guide (TIDL chapter): http://software-dl.ti.com/processor-sdk-linux/esd/docs/latest/linux/Foundational_Components_TIDL.html