1 .. _using-tidl-api:
3 ******************
4 Using the TIDL API
5 ******************
7 This example illustrates using the TIDL API to offload deep learning network processing from a Linux application to the C66x DSPs or EVEs on AM57x devices. The API consists of three classes: ``Configuration``, ``Executor`` and ``ExecutionObject``.
9 Step 1
10 ======
12 Determine if there are any TIDL capable devices on the AM57x SoC:
14 .. code-block:: c++
16 uint32_t num_eve = Executor::GetNumDevices(DeviceType::EVE);
17 uint32_t num_dsp = Executor::GetNumDevices(DeviceType::DSP);
19 .. note::
20 By default, the OpenCL runtime is configured with sufficient global memory
21 (via CMEM) to offload TIDL networks to 2 OpenCL devices. On devices where
22 ``Executor::GetNumDevices`` returns 4 (E.g. AM5729 with 4 EVE OpenCL
23 devices) the amount of memory available to the runtime must be increased.
24 Refer :ref:`opencl-global-memory` for details
26 Step 2
27 ======
28 Create a Configuration object by reading it from a file or by initializing it directly. The example below parses a configuration file and initializes the Configuration object. See ``examples/test/testvecs/config/infer`` for examples of configuration files.
30 .. code::
32 Configuration configuration;
33 bool status = configuration.ReadFromFile(config_file);
35 .. note::
36 Refer `Processor SDK Linux Software Developer's Guide`_ for creating TIDL network and parameter binary files from TensorFlow and Caffe.
38 Step 3
39 ======
40 Create an Executor with the appropriate device type, set of devices and a configuration. In the snippet below, an Executor is created on 2 EVEs.
42 .. code-block:: c++
44 DeviceIds ids = {DeviceId::ID0, DeviceId::ID1};
45 Executor executor(DeviceType::EVE, ids, configuration);
47 Step 4
48 ======
49 Get the set of available ExecutionObjects and allocate input and output buffers for each ExecutionObject.
51 .. code-block:: c++
53 const ExecutionObjects& execution_objects = executor.GetExecutionObjects();
54 int num_eos = execution_objects.size();
56 // Allocate input and output buffers for each execution object
57 std::vector<void *> buffers;
58 for (auto &eo : execution_objects)
59 {
60 ArgInfo in = { ArgInfo(malloc(frame_sz), frame_sz)};
61 ArgInfo out = { ArgInfo(malloc(frame_sz), frame_sz)};
62 eo->SetInputOutputBuffer(in, out);
64 buffers.push_back(in.ptr());
65 buffers.push_back(out.ptr());
66 }
68 Step 5
69 ======
70 Run the network on each input frame. The frames are processed with available execution objects in a pipelined manner with additional num_eos iterations to flush the pipeline (epilogue).
72 .. code-block:: c++
74 for (int frame_idx = 0; frame_idx < configuration.numFrames + num_eos; frame_idx++)
75 {
76 ExecutionObject* eo = execution_objects[frame_idx % num_eos].get();
78 // Wait for previous frame on the same eo to finish processing
79 if (eo->ProcessFrameWait())
80 WriteFrame(*eo, output_data_file);
82 // Read a frame and start processing it with current eo
83 if (ReadFrame(*eo, frame_idx, configuration, input_data_file))
84 eo->ProcessFrameStartAsync();
85 }
87 For a complete example of using the API, refer any of the examples available at ``/usr/share/ti/tidl/examples`` on the EVM file system.
89 .. _Processor SDK Linux Software Developer's Guide: http://software-dl.ti.com/processor-sdk-linux/esd/docs/latest/linux/index.html