5d54c66c36acbd77d4b6d6cf5ce04090f0632ce8
[tidl/tidl-api.git] / examples / imagenet / main.cpp
1 /******************************************************************************
2  * Copyright (c) 2018, Texas Instruments Incorporated - http://www.ti.com/
3  *   All rights reserved.
4  *
5  *   Redistribution and use in source and binary forms, with or without
6  *   modification, are permitted provided that the following conditions are met:
7  *       * Redistributions of source code must retain the above copyright
8  *         notice, this list of conditions and the following disclaimer.
9  *       * Redistributions in binary form must reproduce the above copyright
10  *         notice, this list of conditions and the following disclaimer in the
11  *         documentation and/or other materials provided with the distribution.
12  *       * Neither the name of Texas Instruments Incorporated nor the
13  *         names of its contributors may be used to endorse or promote products
14  *         derived from this software without specific prior written permission.
15  *
16  *   THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
17  *   AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
18  *   IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
19  *   ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE
20  *   LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
21  *   CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
22  *   SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
23  *   INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
24  *   CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
25  *   ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF
26  *   THE POSSIBILITY OF SUCH DAMAGE.
27  *****************************************************************************/
28 #include <signal.h>
29 #include <getopt.h>
30 #include <iostream>
31 #include <iomanip>
32 #include <fstream>
33 #include <cassert>
34 #include <string>
35 #include <functional>
36 #include <algorithm>
37 #include <time.h>
38 #include <unistd.h>
40 #include <queue>
41 #include <vector>
43 #include "executor.h"
44 #include "execution_object.h"
45 #include "configuration.h"
46 #include "imagenet_classes.h"
47 #include "imgutil.h"
49 #include "opencv2/core.hpp"
50 #include "opencv2/imgproc.hpp"
51 #include "opencv2/highgui.hpp"
52 #include "opencv2/videoio.hpp"
55 bool __TI_show_debug_ = false;
57 using namespace tidl;
58 using namespace tidl::imgutil;
59 using namespace cv;
61 #define NUM_VIDEO_FRAMES  100
63 bool RunConfiguration(const std::string& config_file, int num_devices,
64                       DeviceType device_type, std::string& input_file);
65 bool RunAllConfigurations(int32_t num_devices, DeviceType device_type);
67 bool ReadFrame(ExecutionObject& eo, int frame_idx,
68                const Configuration& configuration, int num_frames,
69                std::string& image_file, VideoCapture &cap);
71 bool WriteFrameOutput(const ExecutionObject &eo);
73 static void ProcessArgs(int argc, char *argv[],
74                         std::string& config,
75                         int& num_devices,
76                         DeviceType& device_type,
77                         std::string& input_file);
79 static void DisplayHelp();
81 static double ms_diff(struct timespec &t0, struct timespec &t1)
82 { return (t1.tv_sec - t0.tv_sec) * 1e3 + (t1.tv_nsec - t0.tv_nsec) / 1e6; }
85 int main(int argc, char *argv[])
86 {
87     // Catch ctrl-c to ensure a clean exit
88     signal(SIGABRT, exit);
89     signal(SIGTERM, exit);
91     // If there are no devices capable of offloading TIDL on the SoC, exit
92     uint32_t num_eve = Executor::GetNumDevices(DeviceType::EVE);
93     uint32_t num_dsp = Executor::GetNumDevices(DeviceType::DSP);
94     if (num_eve == 0 && num_dsp == 0)
95     {
96         std::cout << "TI DL not supported on this SoC." << std::endl;
97         return EXIT_SUCCESS;
98     }
100     // Process arguments
101     std::string config      = "j11_v2";
102     std::string input_file  = "../test/testvecs/input/objects/cat-pet-animal-domestic-104827.jpeg";
103     int         num_devices = 1;
104     DeviceType  device_type = (num_eve > 0 ? DeviceType::EVE:DeviceType::DSP);
105     ProcessArgs(argc, argv, config, num_devices, device_type, input_file);
107     std::cout << "Input: " << input_file << std::endl;
108     std::string config_file = "../test/testvecs/config/infer/tidl_config_"
109                               + config + ".txt";
110     bool status = RunConfiguration(config_file, num_devices, device_type,
111                                    input_file);
113     if (!status)
114     {
115         std::cout << "imagenet FAILED" << std::endl;
116         return EXIT_FAILURE;
117     }
119     std::cout << "imagenet PASSED" << std::endl;
120     return EXIT_SUCCESS;
123 bool RunConfiguration(const std::string& config_file, int num_devices,
124                       DeviceType device_type, std::string& input_file)
126     DeviceIds ids;
127     for (int i = 0; i < num_devices; i++)
128         ids.insert(static_cast<DeviceId>(i));
130     // Read the TI DL configuration file
131     Configuration configuration;
132     bool status = configuration.ReadFromFile(config_file);
133     if (!status)
134     {
135         std::cerr << "Error in configuration file: " << config_file
136                   << std::endl;
137         return false;
138     }
140     // setup input
141     int num_frames = 1;
142     VideoCapture cap;
143     std::string image_file;
144     if (input_file == "camera")
145     {
146         cap = VideoCapture(1);  // cap = VideoCapture("test.mp4");
147         if (! cap.isOpened())
148         {
149             std::cerr << "Cannot open camera input." << std::endl;
150             return false;
151         }
152         num_frames = NUM_VIDEO_FRAMES;
153         namedWindow("ImageNet", WINDOW_AUTOSIZE | CV_GUI_NORMAL);
154     }
155     else
156     {
157         image_file = input_file;
158     }
160     try
161     {
162         // Create a executor with the approriate core type, number of cores
163         // and configuration specified
164         Executor executor(device_type, ids, configuration);
166         // Query Executor for set of ExecutionObjects created
167         const ExecutionObjects& execution_objects =
168                                                 executor.GetExecutionObjects();
169         int num_eos = execution_objects.size();
171         // Allocate input and output buffers for each execution object
172         std::vector<void *> buffers;
173         for (auto &eo : execution_objects)
174         {
175             size_t in_size  = eo->GetInputBufferSizeInBytes();
176             size_t out_size = eo->GetOutputBufferSizeInBytes();
177             ArgInfo in  = { ArgInfo(malloc(in_size),  in_size)};
178             ArgInfo out = { ArgInfo(malloc(out_size), out_size)};
179             eo->SetInputOutputBuffer(in, out);
181             buffers.push_back(in.ptr());
182             buffers.push_back(out.ptr());
183         }
185         #define MAX_NUM_EOS  4
186         struct timespec t0[MAX_NUM_EOS], t1;
188         // Process frames with available execution objects in a pipelined manner
189         // additional num_eos iterations to flush the pipeline (epilogue)
190         for (int frame_idx = 0;
191              frame_idx < num_frames + num_eos; frame_idx++)
192         {
193             ExecutionObject* eo = execution_objects[frame_idx % num_eos].get();
195             // Wait for previous frame on the same eo to finish processing
196             if (eo->ProcessFrameWait())
197             {
198                 clock_gettime(CLOCK_MONOTONIC, &t1);
199                 double elapsed_host =
200                                 ms_diff(t0[eo->GetFrameIndex() % num_eos], t1);
201                 double elapsed_device = eo->GetProcessTimeInMilliSeconds();
202                 double overhead = 100 - (elapsed_device/elapsed_host*100);
204                 std::cout << "frame[" << eo->GetFrameIndex() << "]: "
205                           << "Time on device: "
206                           << std::setw(6) << std::setprecision(4)
207                           << elapsed_device << "ms, "
208                           << "host: "
209                           << std::setw(6) << std::setprecision(4)
210                           << elapsed_host << "ms ";
211                 std::cout << "API overhead: "
212                           << std::setw(6) << std::setprecision(3)
213                           << overhead << " %" << std::endl;
215                 WriteFrameOutput(*eo);
216             }
218             // Read a frame and start processing it with current eo
219             if (ReadFrame(*eo, frame_idx, configuration, num_frames,
220                           image_file, cap))
221             {
222                 clock_gettime(CLOCK_MONOTONIC, &t0[frame_idx % num_eos]);
223                 eo->ProcessFrameStartAsync();
224             }
225         }
227         for (auto b : buffers)
228             free(b);
230     }
231     catch (tidl::Exception &e)
232     {
233         std::cerr << e.what() << std::endl;
234         status = false;
235     }
237     return status;
241 bool ReadFrame(ExecutionObject &eo, int frame_idx,
242                const Configuration& configuration, int num_frames,
243                std::string& image_file, VideoCapture &cap)
245     if (frame_idx >= num_frames)
246         return false;
247     eo.SetFrameIndex(frame_idx);
249     char*  frame_buffer = eo.GetInputBufferPtr();
250     assert (frame_buffer != nullptr);
252     Mat image;
253     if (! image_file.empty())
254     {
255         image = cv::imread(image_file, CV_LOAD_IMAGE_COLOR);
256         if (image.empty())
257         {
258             std::cerr << "Unable to read from: " << image_file << std::endl;
259             return false;
260         }
261     }
262     else
263     {
264         Mat v_image;
265         if (! cap.grab())  return false;
266         if (! cap.retrieve(v_image)) return false;
267         // Crop 640x480 camera input to center 256x256 input
268         image = Mat(v_image, Rect(192, 112, 256, 256));
269         cv::imshow("ImageNet", image);
270         waitKey(2);
271     }
273     // TI DL image preprocessing, into frame_buffer
274     return PreProcImage(image, frame_buffer, 1, 3,
275                         configuration.inWidth, configuration.inHeight,
276                         configuration.inWidth,
277                         configuration.inWidth * configuration.inHeight,
278                         1, configuration.preProcType);
281 // Display top 5 classified imagenet classes with probabilities
282 bool WriteFrameOutput(const ExecutionObject &eo)
284     const int k = 5;
285     unsigned char *out = (unsigned char *) eo.GetOutputBufferPtr();
286     int out_size = eo.GetOutputBufferSizeInBytes();
288     // sort and get k largest values and corresponding indices
289     typedef std::pair<unsigned char, int> val_index;
290     auto constexpr cmp = [](val_index &left, val_index &right)
291                          { return left.first > right.first; };
292     std::priority_queue<val_index, std::vector<val_index>, decltype(cmp)>
293             queue(cmp);
294     // initialize priority queue with smallest value on top
295     for (int i = 0; i < k; i++)
296         queue.push(val_index(out[i], i));
298     // for rest output, if larger than current min, pop min, push new val
299     for (int i = k; i < out_size; i++)
300     {
301         if (out[i] > queue.top().first)
302         {
303           queue.pop();
304           queue.push(val_index(out[i], i));
305         }
306     }
308     // output top k values in reverse order: largest val first
309     std::vector<val_index> sorted;
310     while (! queue.empty())
311     {
312       sorted.push_back(queue.top());
313       queue.pop();
314     }
316     for (int i = k - 1; i >= 0; i--)
317     {
318         std::cout << k-i << ": " << imagenet_classes[sorted[i].second]
319                   << std::endl;
320     }
322     return true;
326 void ProcessArgs(int argc, char *argv[], std::string& config,
327                  int& num_devices, DeviceType& device_type,
328                  std::string& input_file)
330     const struct option long_options[] =
331     {
332         {"config",      required_argument, 0, 'c'},
333         {"num_devices", required_argument, 0, 'n'},
334         {"device_type", required_argument, 0, 't'},
335         {"image_file",  required_argument, 0, 'i'},
336         {"help",        no_argument,       0, 'h'},
337         {"verbose",     no_argument,       0, 'v'},
338         {0, 0, 0, 0}
339     };
341     int option_index = 0;
343     while (true)
344     {
345         int c = getopt_long(argc, argv, "c:n:t:i:hv", long_options, &option_index);
347         if (c == -1)
348             break;
350         switch (c)
351         {
352             case 'c': config = optarg;
353                       break;
355             case 'n': num_devices = atoi(optarg);
356                       assert (num_devices > 0 && num_devices <= 4);
357                       break;
359             case 't': if (*optarg == 'e')
360                           device_type = DeviceType::EVE;
361                       else if (*optarg == 'd')
362                           device_type = DeviceType::DSP;
363                       else
364                       {
365                           std::cerr << "Invalid argument to -t, only e or d"
366                                        " allowed" << std::endl;
367                           exit(EXIT_FAILURE);
368                       }
369                       break;
371             case 'i': input_file = optarg;
372                       break;
374             case 'v': __TI_show_debug_ = true;
375                       break;
377             case 'h': DisplayHelp();
378                       exit(EXIT_SUCCESS);
379                       break;
381             case '?': // Error in getopt_long
382                       exit(EXIT_FAILURE);
383                       break;
385             default:
386                       std::cerr << "Unsupported option: " << c << std::endl;
387                       break;
388         }
389     }
392 void DisplayHelp()
394     std::cout << "Usage: imagenet\n"
395                  "  Will run imagenet network to predict top 5 object"
396                  " classes for the input.\n  Use -c to run a"
397                  "  different imagenet network. Default is j11_v2.\n"
398                  "Optional arguments:\n"
399                  " -c <config>          Valid configs: j11_bn, j11_prelu, j11_v2\n"
400                  " -n <number of cores> Number of cores to use (1 - 4)\n"
401                  " -t <d|e>             Type of core. d -> DSP, e -> EVE\n"
402                  " -i <image>           Path to the image file\n"
403                  " -i camera            Use camera as input\n"
404                  " -v                   Verbose output during execution\n"
405                  " -h                   Help\n";