]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - tidl/tidl-api.git/blob - examples/imagenet/main.cpp
74e926057e34989096c0eaca16e6fdf899ece3a7
[tidl/tidl-api.git] / examples / imagenet / main.cpp
1 /******************************************************************************
2  * Copyright (c) 2018, Texas Instruments Incorporated - http://www.ti.com/
3  *   All rights reserved.
4  *
5  *   Redistribution and use in source and binary forms, with or without
6  *   modification, are permitted provided that the following conditions are met:
7  *       * Redistributions of source code must retain the above copyright
8  *         notice, this list of conditions and the following disclaimer.
9  *       * Redistributions in binary form must reproduce the above copyright
10  *         notice, this list of conditions and the following disclaimer in the
11  *         documentation and/or other materials provided with the distribution.
12  *       * Neither the name of Texas Instruments Incorporated nor the
13  *         names of its contributors may be used to endorse or promote products
14  *         derived from this software without specific prior written permission.
15  *
16  *   THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
17  *   AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
18  *   IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
19  *   ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE
20  *   LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
21  *   CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
22  *   SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
23  *   INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
24  *   CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
25  *   ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF
26  *   THE POSSIBILITY OF SUCH DAMAGE.
27  *****************************************************************************/
28 #include <signal.h>
29 #include <getopt.h>
30 #include <iostream>
31 #include <iomanip>
32 #include <fstream>
33 #include <cassert>
34 #include <string>
35 #include <functional>
36 #include <algorithm>
37 #include <time.h>
38 #include <unistd.h>
40 #include <queue>
41 #include <vector>
43 #include "executor.h"
44 #include "execution_object.h"
45 #include "configuration.h"
46 #include "imagenet_classes.h"
47 #include "imgutil.h"
49 #include "opencv2/core.hpp"
50 #include "opencv2/imgproc.hpp"
51 #include "opencv2/highgui.hpp"
52 #include "opencv2/videoio.hpp"
55 bool __TI_show_debug_ = false;
57 using namespace tinn;
58 using namespace tinn::imgutil;
59 using namespace cv;
61 #define NUM_VIDEO_FRAMES  100
63 bool RunConfiguration(const std::string& config_file, int num_devices,
64                       DeviceType device_type, std::string& input_file);
65 bool RunAllConfigurations(int32_t num_devices, DeviceType device_type);
67 bool ReadFrame(ExecutionObject& eo, int frame_idx,
68                const Configuration& configuration, int num_frames,
69                std::string& image_file, VideoCapture &cap);
71 bool WriteFrameOutput(const ExecutionObject &eo);
73 static void ProcessArgs(int argc, char *argv[],
74                         std::string& config,
75                         int& num_devices,
76                         DeviceType& device_type,
77                         std::string& input_file);
79 static void DisplayHelp();
81 static double ms_diff(struct timespec &t0, struct timespec &t1)
82 { return (t1.tv_sec - t0.tv_sec) * 1e3 + (t1.tv_nsec - t0.tv_nsec) / 1e6; }
85 int main(int argc, char *argv[])
86 {
87     // Catch ctrl-c to ensure a clean exit
88     signal(SIGABRT, exit);
89     signal(SIGTERM, exit);
91     // If there are no devices capable of offloading TIDL on the SoC, exit
92     uint32_t num_dla = Executor::GetNumDevices(DeviceType::DLA);
93     uint32_t num_dsp = Executor::GetNumDevices(DeviceType::DSP);
94     if (num_dla == 0 && num_dsp == 0)
95     {
96         std::cout << "TI DL not supported on this SoC." << std::endl;
97         return EXIT_SUCCESS;
98     }
100     // Process arguments
101     std::string config      = "j11_v2";
102     std::string input_file  = "../test/testvecs/input/airshow.jpg";
103     int         num_devices = 1;
104     DeviceType  device_type = DeviceType::DLA;
105     ProcessArgs(argc, argv, config, num_devices, device_type, input_file);
107     std::cout << "Input: " << input_file << std::endl;
108     std::string config_file = "../test/testvecs/config/infer/tidl_config_"
109                               + config + ".txt";
110     bool status = RunConfiguration(config_file, num_devices, device_type,
111                                    input_file);
113     if (!status)
114     {
115         std::cout << "imagenet FAILED" << std::endl;
116         return EXIT_FAILURE;
117     }
119     std::cout << "imagenet PASSED" << std::endl;
120     return EXIT_SUCCESS;
123 bool RunConfiguration(const std::string& config_file, int num_devices,
124                       DeviceType device_type, std::string& input_file)
126     DeviceIds ids;
127     for (int i = 0; i < num_devices; i++)
128         ids.insert(static_cast<DeviceId>(i));
130     // Read the TI DL configuration file
131     Configuration configuration;
132     bool status = configuration.ReadFromFile(config_file);
133     if (!status)
134     {
135         std::cerr << "Error in configuration file: " << config_file
136                   << std::endl;
137         return false;
138     }
140     // setup input
141     int num_frames = 1;
142     VideoCapture cap;
143     std::string image_file;
144     if (input_file == "camera")
145     {
146         cap = VideoCapture(1);  // cap = VideoCapture("test.mp4");
147         if (! cap.isOpened())
148         {
149             std::cerr << "Cannot open camera input." << std::endl;
150             return false;
151         }
152         num_frames = NUM_VIDEO_FRAMES;
153         namedWindow("ImageNet", WINDOW_AUTOSIZE | CV_GUI_NORMAL);
154     }
155     else
156     {
157         image_file = input_file;
158     }
160     // Determine input frame size from configuration
161     size_t frame_sz = configuration.inWidth * configuration.inHeight *
162                       configuration.inNumChannels;
164     try
165     {
166         // Create a executor with the approriate core type, number of cores
167         // and configuration specified
168         Executor executor(device_type, ids, configuration);
170         // Query Executor for set of ExecutionObjects created
171         const ExecutionObjects& execution_objects =
172                                                 executor.GetExecutionObjects();
173         int num_eos = execution_objects.size();
175         // Allocate input and output buffers for each execution object
176         std::vector<void *> buffers;
177         for (auto &eo : execution_objects)
178         {
179             ArgInfo in  = { ArgInfo(malloc(frame_sz), frame_sz)};
180             ArgInfo out = { ArgInfo(malloc(frame_sz), frame_sz)};
181             eo->SetInputOutputBuffer(in, out);
183             buffers.push_back(in.ptr());
184             buffers.push_back(out.ptr());
185         }
187         #define MAX_NUM_EOS  4
188         struct timespec t0[MAX_NUM_EOS], t1;
190         // Process frames with available execution objects in a pipelined manner
191         // additional num_eos iterations to flush the pipeline (epilogue)
192         for (int frame_idx = 0;
193              frame_idx < num_frames + num_eos; frame_idx++)
194         {
195             ExecutionObject* eo = execution_objects[frame_idx % num_eos].get();
197             // Wait for previous frame on the same eo to finish processing
198             if (eo->ProcessFrameWait())
199             {
200                 clock_gettime(CLOCK_MONOTONIC, &t1);
201                 double elapsed_host =
202                                 ms_diff(t0[eo->GetFrameIndex() % num_eos], t1);
203                 double elapsed_device = eo->GetProcessTimeInMilliSeconds();
204                 double overhead = 100 - (elapsed_device/elapsed_host*100);
206                 std::cout << "frame[" << eo->GetFrameIndex() << "]: "
207                           << "Time on device: "
208                           << std::setw(6) << std::setprecision(4)
209                           << elapsed_device << "ms, "
210                           << "host: "
211                           << std::setw(6) << std::setprecision(4)
212                           << elapsed_host << "ms ";
213                 std::cout << "API overhead: "
214                           << std::setw(6) << std::setprecision(3)
215                           << overhead << " %" << std::endl;
217                 WriteFrameOutput(*eo);
218             }
220             // Read a frame and start processing it with current eo
221             if (ReadFrame(*eo, frame_idx, configuration, num_frames,
222                           image_file, cap))
223             {
224                 clock_gettime(CLOCK_MONOTONIC, &t0[frame_idx % num_eos]);
225                 eo->ProcessFrameStartAsync();
226             }
227         }
229         for (auto b : buffers)
230             free(b);
232     }
233     catch (tinn::Exception &e)
234     {
235         std::cerr << e.what() << std::endl;
236         status = false;
237     }
239     return status;
243 bool ReadFrame(ExecutionObject &eo, int frame_idx,
244                const Configuration& configuration, int num_frames,
245                std::string& image_file, VideoCapture &cap)
247     if (frame_idx >= num_frames)
248         return false;
249     eo.SetFrameIndex(frame_idx);
251     char*  frame_buffer = eo.GetInputBufferPtr();
252     assert (frame_buffer != nullptr);
254     Mat image;
255     if (! image_file.empty())
256     {
257         image = cv::imread(image_file, CV_LOAD_IMAGE_COLOR);
258         if (image.empty())
259         {
260             std::cerr << "Unable to read from: " << image_file << std::endl;
261             return false;
262         }
263     }
264     else
265     {
266         Mat v_image;
267         if (! cap.grab())  return false;
268         if (! cap.retrieve(v_image)) return false;
269         // Crop 640x480 camera input to center 256x256 input
270         image = Mat(v_image, Rect(192, 112, 256, 256));
271         cv::imshow("ImageNet", image);
272         waitKey(2);
273     }
275     // TI DL image preprocessing, into frame_buffer
276     return PreProcImage(image, frame_buffer, 1, 3,
277                         configuration.inWidth, configuration.inHeight,
278                         configuration.inWidth,
279                         configuration.inWidth * configuration.inHeight,
280                         1, configuration.preProcType);
283 // Display top 5 classified imagenet classes with probabilities
284 bool WriteFrameOutput(const ExecutionObject &eo)
286     const int k = 5;
287     unsigned char *out = (unsigned char *) eo.GetOutputBufferPtr();
288     int out_size = eo.GetOutputBufferSizeInBytes();
290     // sort and get k largest values and corresponding indices
291     typedef std::pair<unsigned char, int> val_index;
292     auto constexpr cmp = [](val_index &left, val_index &right)
293                          { return left.first > right.first; };
294     std::priority_queue<val_index, std::vector<val_index>, decltype(cmp)>
295             queue(cmp);
296     // initialize priority queue with smallest value on top
297     for (int i = 0; i < k; i++)
298         queue.push(val_index(out[i], i));
300     // for rest output, if larger than current min, pop min, push new val
301     for (int i = k; i < out_size; i++)
302     {
303         if (out[i] > queue.top().first)
304         {
305           queue.pop();
306           queue.push(val_index(out[i], i));
307         }
308     }
310     // output top k values in reverse order: largest val first
311     std::vector<val_index> sorted;
312     while (! queue.empty())
313     {
314       sorted.push_back(queue.top());
315       queue.pop();
316     }
318     for (int i = k - 1; i >= 0; i--)
319     {
320         std::cout << k-i << ": " << imagenet_classes[sorted[i].second]
321                   << ", prob = " << (float) sorted[i].first / 256 << std::endl;
322     }
324     return true;
328 void ProcessArgs(int argc, char *argv[], std::string& config,
329                  int& num_devices, DeviceType& device_type,
330                  std::string& input_file)
332     const struct option long_options[] =
333     {
334         {"config",      required_argument, 0, 'c'},
335         {"num_devices", required_argument, 0, 'n'},
336         {"device_type", required_argument, 0, 't'},
337         {"image_file",  required_argument, 0, 'i'},
338         {"help",        no_argument,       0, 'h'},
339         {"verbose",     no_argument,       0, 'v'},
340         {0, 0, 0, 0}
341     };
343     int option_index = 0;
345     while (true)
346     {
347         int c = getopt_long(argc, argv, "c:n:t:i:hv", long_options, &option_index);
349         if (c == -1)
350             break;
352         switch (c)
353         {
354             case 'c': config = optarg;
355                       break;
357             case 'n': num_devices = atoi(optarg);
358                       assert (num_devices > 0 && num_devices <= 4);
359                       break;
361             case 't': if (*optarg == 'e')
362                           device_type = DeviceType::DLA;
363                       else if (*optarg == 'd')
364                           device_type = DeviceType::DSP;
365                       else
366                       {
367                           std::cerr << "Invalid argument to -t, only e or d"
368                                        " allowed" << std::endl;
369                           exit(EXIT_FAILURE);
370                       }
371                       break;
373             case 'i': input_file = optarg;
374                       break;
376             case 'v': __TI_show_debug_ = true;
377                       break;
379             case 'h': DisplayHelp();
380                       exit(EXIT_SUCCESS);
381                       break;
383             case '?': // Error in getopt_long
384                       exit(EXIT_FAILURE);
385                       break;
387             default:
388                       std::cerr << "Unsupported option: " << c << std::endl;
389                       break;
390         }
391     }
394 void DisplayHelp()
396     std::cout << "Usage: imagenet\n"
397                  "  Will run imagenet network to predict top 5 object"
398                  " classes for the input.\n  Use -c to run a"
399                  "  different imagenet network. Default is j11_v2.\n"
400                  "Optional arguments:\n"
401                  " -c <config>          Valid configs: j11_bn, j11_prelu, j11_v2\n"
402                  " -n <number of cores> Number of cores to use (1 - 4)\n"
403                  " -t <d|e>             Type of core. d -> DSP, e -> DLA\n"
404                  " -i <image>           Path to the image file\n"
405                  " -i camera            Use camera as input\n"
406                  " -v                   Verbose output during execution\n"
407                  " -h                   Help\n";