89c203ee93f37f2588cd492c4a7f3c6fa4a720cc
[tidl/tidl-api.git] / examples / imagenet / main.cpp
1 /******************************************************************************
2  * Copyright (c) 2018, Texas Instruments Incorporated - http://www.ti.com/
3  *   All rights reserved.
4  *
5  *   Redistribution and use in source and binary forms, with or without
6  *   modification, are permitted provided that the following conditions are met:
7  *       * Redistributions of source code must retain the above copyright
8  *         notice, this list of conditions and the following disclaimer.
9  *       * Redistributions in binary form must reproduce the above copyright
10  *         notice, this list of conditions and the following disclaimer in the
11  *         documentation and/or other materials provided with the distribution.
12  *       * Neither the name of Texas Instruments Incorporated nor the
13  *         names of its contributors may be used to endorse or promote products
14  *         derived from this software without specific prior written permission.
15  *
16  *   THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
17  *   AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
18  *   IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
19  *   ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE
20  *   LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
21  *   CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
22  *   SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
23  *   INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
24  *   CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
25  *   ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF
26  *   THE POSSIBILITY OF SUCH DAMAGE.
27  *****************************************************************************/
28 #include <signal.h>
29 #include <iostream>
30 #include <iomanip>
31 #include <fstream>
32 #include <cassert>
33 #include <string>
34 #include <functional>
35 #include <algorithm>
36 #include <time.h>
37 #include <unistd.h>
39 #include <queue>
40 #include <vector>
41 #include <chrono>
43 #include "executor.h"
44 #include "execution_object.h"
45 #include "execution_object_pipeline.h"
46 #include "configuration.h"
47 #include "../common/object_classes.h"
48 #include "imgutil.h"
49 #include "../common/video_utils.h"
51 #include "opencv2/core.hpp"
52 #include "opencv2/imgproc.hpp"
53 #include "opencv2/highgui.hpp"
54 #include "opencv2/videoio.hpp"
56 using namespace std;
57 using namespace tidl;
58 using namespace cv;
60 #define NUM_VIDEO_FRAMES  300
61 #define DEFAULT_CONFIG    "j11_v2"
62 #define NUM_DEFAULT_INPUTS  1
63 #define DEFAULT_OBJECT_CLASSES_LIST_FILE "imagenet_objects.json"
64 const char *default_inputs[NUM_DEFAULT_INPUTS] =
65 {
66     "../test/testvecs/input/objects/cat-pet-animal-domestic-104827.jpeg"
67 };
68 std::unique_ptr<ObjectClasses> object_classes;
71 Executor* CreateExecutor(DeviceType dt, uint32_t num, const Configuration& c);
72 bool RunConfiguration(cmdline_opts_t& opts);
73 bool ReadFrame(ExecutionObjectPipeline& eop,
74                uint32_t frame_idx, const Configuration& c,
75                const cmdline_opts_t& opts, VideoCapture &cap);
76 bool WriteFrameOutput(const ExecutionObjectPipeline &eop);
77 void DisplayHelp();
80 int main(int argc, char *argv[])
81 {
82     // Catch ctrl-c to ensure a clean exit
83     signal(SIGABRT, exit);
84     signal(SIGTERM, exit);
86     // If there are no devices capable of offloading TIDL on the SoC, exit
87     uint32_t num_eves = Executor::GetNumDevices(DeviceType::EVE);
88     uint32_t num_dsps = Executor::GetNumDevices(DeviceType::DSP);
89     if (num_eves == 0 && num_dsps == 0)
90     {
91         cout << "TI DL not supported on this SoC." << endl;
92         return EXIT_SUCCESS;
93     }
95     // Process arguments
96     cmdline_opts_t opts;
97     opts.config = DEFAULT_CONFIG;
98     opts.object_classes_list_file = DEFAULT_OBJECT_CLASSES_LIST_FILE;
99     if (num_eves != 0) { opts.num_eves = 1;  opts.num_dsps = 0; }
100     else               { opts.num_eves = 0;  opts.num_dsps = 1; }
101     if (! ProcessArgs(argc, argv, opts))
102     {
103         DisplayHelp();
104         exit(EXIT_SUCCESS);
105     }
106     assert(opts.num_dsps != 0 || opts.num_eves != 0);
107     if (opts.num_frames == 0)
108         opts.num_frames = (opts.is_camera_input || opts.is_video_input) ?
109                           NUM_VIDEO_FRAMES : 1;
110     if (opts.input_file.empty())
111         cout << "Input: " << default_inputs[0] << endl;
112     else
113         cout << "Input: " << opts.input_file << endl;
115     // Get object classes list
116     object_classes = std::unique_ptr<ObjectClasses>(
117                              new ObjectClasses(opts.object_classes_list_file));
118     if (object_classes->GetNumClasses() == 0)
119     {
120         cout << "No object classes defined for this config." << endl;
121         return EXIT_FAILURE;
122     }
124     // Run network
125     bool status = RunConfiguration(opts);
126     if (!status)
127     {
128         cout << "imagenet FAILED" << endl;
129         return EXIT_FAILURE;
130     }
132     cout << "imagenet PASSED" << endl;
133     return EXIT_SUCCESS;
136 bool RunConfiguration(cmdline_opts_t& opts)
138     // Read the TI DL configuration file
139     Configuration c;
140     string config_file = "../test/testvecs/config/infer/tidl_config_"
141                               + opts.config + ".txt";
142     bool status = c.ReadFromFile(config_file);
143     if (!status)
144     {
145         cerr << "Error in configuration file: " << config_file << endl;
146         return false;
147     }
148     c.enableApiTrace = opts.verbose;
150     // setup camera/video input/output
151     VideoCapture cap;
152     if (! SetVideoInputOutput(cap, opts, "ImageNet"))  return false;
154     try
155     {
156         // Create Executors with the approriate core type, number of cores
157         // and configuration specified
158         Executor* e_eve = CreateExecutor(DeviceType::EVE, opts.num_eves, c);
159         Executor* e_dsp = CreateExecutor(DeviceType::DSP, opts.num_dsps, c);
161         // Get ExecutionObjects from Executors
162         vector<ExecutionObject*> eos;
163         for (uint32_t i = 0; i < opts.num_eves; i++) eos.push_back((*e_eve)[i]);
164         for (uint32_t i = 0; i < opts.num_dsps; i++) eos.push_back((*e_dsp)[i]);
165         uint32_t num_eos = eos.size();
167         // Use duplicate EOPs to do double buffering on frame input/output
168         //    because each EOP has its own set of input/output buffers,
169         //    so that host ReadFrame() can be overlapped with device processing
170         // Use one EO as an example, with different buffer_factor,
171         //    we have different execution behavior:
172         // If buffer_factor is set to 1 -> single buffering
173         //    we create one EOP: eop0 (eo0)
174         //    pipeline execution of multiple frames over time is as follows:
175         //    --------------------- time ------------------->
176         //    eop0: [RF][eo0.....][WF]
177         //    eop0:                   [RF][eo0.....][WF]
178         //    eop0:                                     [RF][eo0.....][WF]
179         // If buffer_factor is set to 2 -> double buffering
180         //    we create two EOPs: eop0 (eo0), eop1(eo0)
181         //    pipeline execution of multiple frames over time is as follows:
182         //    --------------------- time ------------------->
183         //    eop0: [RF][eo0.....][WF]
184         //    eop1:     [RF]      [eo0.....][WF]
185         //    eop0:                   [RF]  [eo0.....][WF]
186         //    eop1:                             [RF]  [eo0.....][WF]
187         vector<ExecutionObjectPipeline *> eops;
188         uint32_t buffer_factor = 2;  // set to 1 for single buffering
189         for (uint32_t j = 0; j < buffer_factor; j++)
190             for (uint32_t i = 0; i < num_eos; i++)
191                 eops.push_back(new ExecutionObjectPipeline({eos[i]}));
192         uint32_t num_eops = eops.size();
194         // Allocate input and output buffers for each EOP
195         AllocateMemory(eops);
197         chrono::time_point<chrono::steady_clock> tloop0, tloop1;
198         tloop0 = chrono::steady_clock::now();
200         // Process frames with available eops in a pipelined manner
201         // additional num_eos iterations to flush the pipeline (epilogue)
202         for (uint32_t frame_idx = 0;
203              frame_idx < opts.num_frames + num_eops; frame_idx++)
204         {
205             ExecutionObjectPipeline* eop = eops[frame_idx % num_eops];
207             // Wait for previous frame on the same eop to finish processing
208             if (eop->ProcessFrameWait())
209             {
210                 WriteFrameOutput(*eop);
211             }
213             // Read a frame and start processing it with current eop
214             if (ReadFrame(*eop, frame_idx, c, opts, cap))
215                 eop->ProcessFrameStartAsync();
216         }
218         tloop1 = chrono::steady_clock::now();
219         chrono::duration<float> elapsed = tloop1 - tloop0;
220         cout << "Loop total time (including read/write/opencv/print/etc): "
221                   << setw(6) << setprecision(4)
222                   << (elapsed.count() * 1000) << "ms" << endl;
224         FreeMemory(eops);
225         for (auto eop : eops)  delete eop;
226         delete e_eve;
227         delete e_dsp;
228     }
229     catch (tidl::Exception &e)
230     {
231         cerr << e.what() << endl;
232         status = false;
233     }
235     return status;
238 // Create an Executor with the specified type and number of EOs
239 Executor* CreateExecutor(DeviceType dt, uint32_t num, const Configuration& c)
241     if (num == 0) return nullptr;
243     DeviceIds ids;
244     for (uint32_t i = 0; i < num; i++)
245         ids.insert(static_cast<DeviceId>(i));
247     return new Executor(dt, ids, c);
250 bool ReadFrame(ExecutionObjectPipeline &eop,
251                uint32_t frame_idx, const Configuration& c,
252                const cmdline_opts_t& opts, VideoCapture &cap)
254     if (frame_idx >= opts.num_frames)
255         return false;
257     eop.SetFrameIndex(frame_idx);
259     char*  frame_buffer = eop.GetInputBufferPtr();
260     assert (frame_buffer != nullptr);
262     Mat image;
263     if (! opts.is_camera_input && ! opts.is_video_input)
264     {
265         if (opts.input_file.empty())
266             image = cv::imread(default_inputs[frame_idx % NUM_DEFAULT_INPUTS],
267                                CV_LOAD_IMAGE_COLOR);
268         else
269             image = cv::imread(opts.input_file, CV_LOAD_IMAGE_COLOR);
270         if (image.empty())
271         {
272             cerr << "Unable to read input image" << endl;
273             return false;
274         }
275     }
276     else
277     {
278         Mat v_image;
279         if (! cap.grab())  return false;
280         if (! cap.retrieve(v_image)) return false;
281         int orig_width  = v_image.cols;
282         int orig_height = v_image.rows;
283         // Crop camera/video input to center 256x256 input
284         if (orig_width > 256 && orig_height > 256)
285         {
286             image = Mat(v_image, Rect((orig_width-256)/2, (orig_height-256)/2,
287                                        256, 256));
288         }
289         else
290             image = v_image;
291         cv::imshow("ImageNet", image);
292         waitKey(2);
293     }
295     // TI DL image preprocessing, into frame_buffer
296     return imgutil::PreprocessImage(image, frame_buffer, c);
299 // Display top 5 classified imagenet classes with probabilities
300 bool WriteFrameOutput(const ExecutionObjectPipeline &eop)
302     const int k = 5;
303     unsigned char *out = (unsigned char *) eop.GetOutputBufferPtr();
304     int out_size = eop.GetOutputBufferSizeInBytes();
306     // sort and get k largest values and corresponding indices
307     typedef pair<unsigned char, int> val_index;
308     auto constexpr cmp = [](val_index &left, val_index &right)
309                          { return left.first > right.first; };
310     priority_queue<val_index, vector<val_index>, decltype(cmp)> queue(cmp);
311     // initialize priority queue with smallest value on top
312     for (int i = 0; i < k; i++)
313         queue.push(val_index(out[i], i));
315     // for rest output, if larger than current min, pop min, push new val
316     for (int i = k; i < out_size; i++)
317     {
318         if (out[i] > queue.top().first)
319         {
320           queue.pop();
321           queue.push(val_index(out[i], i));
322         }
323     }
325     // output top k values in reverse order: largest val first
326     vector<val_index> sorted;
327     while (! queue.empty())
328     {
329       sorted.push_back(queue.top());
330       queue.pop();
331     }
333     for (int i = k - 1; i >= 0; i--)
334         cout << k-i << ": "
335              << object_classes->At(sorted[i].second).label << endl;
337     return true;
340 void DisplayHelp()
342     cout <<
343     "Usage: imagenet\n"
344     "  Will run imagenet network to predict top 5 object"
345     " classes for the input.\n  Use -c to run a"
346     "  different imagenet network. Default is j11_v2.\n"
347     "Optional arguments:\n"
348     " -c <config>          Valid configs: j11_bn, j11_prelu, j11_v2\n"
349     " -d <number>          Number of dsp cores to use\n"
350     " -e <number>          Number of eve cores to use\n"
351     " -i <image>           Path to the image file as input\n"
352     " -i camera<number>    Use camera as input\n"
353     "                      video input port: /dev/video<number>\n"
354     " -i <name>.{mp4,mov,avi}  Use video file as input\n"
355     " -l <objects_list>    Path to the object classes list file\n"
356     " -f <number>          Number of frames to process\n"
357     " -v                   Verbose output during execution\n"
358     " -h                   Help\n";