Add option to specify object classes list file
[tidl/tidl-api.git] / examples / mcbench / main.cpp
1 /******************************************************************************
2  * Copyright (c) 2018, Texas Instruments Incorporated - http://www.ti.com/
3  *   All rights reserved.
4  *
5  *   Redistribution and use in source and binary forms, with or without
6  *   modification, are permitted provided that the following conditions are met:
7  *       * Redistributions of source code must retain the above copyright
8  *         notice, this list of conditions and the following disclaimer.
9  *       * Redistributions in binary form must reproduce the above copyright
10  *         notice, this list of conditions and the following disclaimer in the
11  *         documentation and/or other materials provided with the distribution.
12  *       * Neither the name of Texas Instruments Incorporated nor the
13  *         names of its contributors may be used to endorse or promote products
14  *         derived from this software without specific prior written permission.
15  *
16  *   THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
17  *   AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
18  *   IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
19  *   ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE
20  *   LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
21  *   CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
22  *   SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
23  *   INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
24  *   CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
25  *   ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF
26  *   THE POSSIBILITY OF SUCH DAMAGE.
27  *****************************************************************************/
28 #include <signal.h>
29 #include <iostream>
30 #include <iomanip>
31 #include <fstream>
32 #include <cassert>
33 #include <string>
34 #include <functional>
35 #include <algorithm>
36 #include <time.h>
37 #include <unistd.h>
39 #include <queue>
40 #include <vector>
41 #include <cstdio>
42 #include <chrono>
44 #include "executor.h"
45 #include "execution_object.h"
46 #include "execution_object_pipeline.h"
47 #include "configuration.h"
48 #include "../common/utils.h"
49 #include "../common/video_utils.h"
51 using namespace std;
52 using namespace tidl;
53 using namespace cv;
56 #define NUM_VIDEO_FRAMES  100
57 #define DEFAULT_CONFIG    "../test/testvecs/config/infer/tidl_config_j11_v2.txt"
59 bool RunConfiguration(const cmdline_opts_t& opts);
60 Executor* CreateExecutor(DeviceType dt, uint32_t num, const Configuration& c,
61                          int layers_group_id);
62 bool CreateExecutionObjectPipelines(uint32_t num_eves, uint32_t num_dsps,
63                                     Configuration& configuration,
64                                     uint32_t num_layers_groups,
65                                     Executor*& e_eve, Executor*& e_dsp,
66                                   std::vector<ExecutionObjectPipeline*>& eops);
68 void AllocateMemory(const std::vector<ExecutionObjectPipeline*>& eops);
70 bool ReadFrame(ExecutionObjectPipeline& eop, uint32_t frame_idx,
71                const Configuration& c, const cmdline_opts_t& opts, char *input_frames_buffer);
72 static void DisplayHelp();
75 int main(int argc, char *argv[])
76 {
77     // Catch ctrl-c to ensure a clean exit
78     signal(SIGABRT, exit);
79     signal(SIGTERM, exit);
81     // If there are no devices capable of offloading TIDL on the SoC, exit
82     uint32_t num_eves = Executor::GetNumDevices(DeviceType::EVE);
83     uint32_t num_dsps = Executor::GetNumDevices(DeviceType::DSP);
84     if ((num_eves == 0) || (num_dsps == 0))
85     {
86         cout << "mcbench requires EVE and/or DSP for execution." << endl;
87         return EXIT_SUCCESS;
88     }
90     cout << "CMDLINE: ";
91     for(int i = 0; i < argc; ++i) cout << argv[i] << " ";
92     cout << endl;
94     // Process arguments
95     cmdline_opts_t opts;
96     opts.config = DEFAULT_CONFIG;
97     opts.num_eves = 0;
98     opts.num_dsps = 2;
99     if (! ProcessArgs(argc, argv, opts))
100     {
101         DisplayHelp();
102         exit(EXIT_SUCCESS);
103     }
104     assert((opts.num_dsps + opts.num_eves) != 0);
106     if (opts.num_frames == 0)
107         opts.num_frames = NUM_VIDEO_FRAMES;
109     // Run network
110     bool status = RunConfiguration(opts);
112     if (!status)
113     {
114         cout << "mcbench FAILED" << endl;
115         return EXIT_FAILURE;
116     }
118     cout << "mcbench PASSED" << endl;
119     return EXIT_SUCCESS;
122 bool RunConfiguration(const cmdline_opts_t& opts)
124     // Read the TI DL configuration file
125     Configuration c;
126     if (!c.ReadFromFile(opts.config))
127         return false;
129     c.enableApiTrace = opts.verbose;
130     if(opts.num_layers_groups == 1)
131        c.runFullNet = true; //Force all layers to be in the same group
133     std::string inputFile;
134     if (opts.input_file.empty())
135         inputFile   = c.inData;
136     else
137         inputFile = opts.input_file;
139     int frame_size = c.inNumChannels * c.inWidth * c.inHeight;
141     c.numFrames = GetBinaryFileSize (inputFile) / frame_size;
143     cout << "Input: " << inputFile << " frames:" << c.numFrames << endl;
145     // Read input file into memory buffer
146     char *input_frame_buffer = new char[c.numFrames * frame_size]();
147     ifstream ifs(inputFile, ios::binary);
148     ifs.read(input_frame_buffer, c.numFrames * frame_size);
149     if(!ifs.good()) {
150        std::cout << "Invalid File input:" << inputFile << std::endl;
151        return false;
152     }
154     bool status = true;
155     try
156     {
157         Executor *e_eve = NULL;
158         Executor *e_dsp = NULL;
159         std::vector<ExecutionObjectPipeline *> eops;
160         if (! CreateExecutionObjectPipelines(opts.num_eves, opts.num_dsps, c,
161                                              opts.num_layers_groups,
162                                              e_eve, e_dsp, eops))
163             return false;
165         // Allocate input/output memory for each EOP
166         AllocateMemory(eops);
168         chrono::time_point<chrono::steady_clock> tloop0, tloop1;
169         tloop0 = chrono::steady_clock::now();
171         // Process frames with available eops in a pipelined manner
172         // additional num_eops iterations to flush pipeline (epilogue)
173         uint32_t num_eops = eops.size();
174         for (uint32_t frame_idx = 0;
175              frame_idx < opts.num_frames + num_eops; frame_idx++)
176         {
177             ExecutionObjectPipeline* eop = eops[frame_idx % num_eops];
179             // Wait for previous frame on the same eop to finish processing
180             if (eop->ProcessFrameWait())
181                 ;
183             // Read a frame and start processing it with current eo
184             if (ReadFrame(*eop, frame_idx, c, opts, input_frame_buffer))
185                 eop->ProcessFrameStartAsync();
186         }
188         tloop1 = chrono::steady_clock::now();
189         chrono::duration<float> elapsed = tloop1 - tloop0;
190         cout << "Loop total time: "
191                   << setw(6) << setprecision(4)
192                   << (elapsed.count() * 1000) << "ms" << endl;
193         cout << "FPS:" << opts.num_frames / elapsed.count() << endl;
195         FreeMemory(eops);
197         for (auto eop : eops)
198             delete eop;
200         delete e_eve;
201         delete e_dsp;
202     }
203     catch (tidl::Exception &e)
204     {
205         cerr << e.what() << endl;
206         status = false;
207     }
209     delete [] input_frame_buffer;
210     return status;
213 // Create an Executor with the specified type and number of EOs
214 Executor* CreateExecutor(DeviceType dt, uint32_t num, const Configuration& c,
215                          int layers_group_id)
217     if (num == 0) return nullptr;
219     DeviceIds ids;
220     for (uint32_t i = 0; i < num; i++)
221         ids.insert(static_cast<DeviceId>(i));
223     return new Executor(dt, ids, c, layers_group_id);
226 bool CreateExecutionObjectPipelines(uint32_t num_eves, uint32_t num_dsps,
227                                     Configuration& configuration,
228                                     uint32_t num_layers_groups,
229                                     Executor*& e_eve, Executor*& e_dsp,
230                                     std::vector<ExecutionObjectPipeline*>& eops)
232     DeviceIds ids_eve, ids_dsp;
233     for (uint32_t i = 0; i < num_eves; i++)
234         ids_eve.insert(static_cast<DeviceId>(i));
235     for (uint32_t i = 0; i < num_dsps; i++)
236         ids_dsp.insert(static_cast<DeviceId>(i));
238     // Construct ExecutionObjectPipeline that utilizes multiple
239     // ExecutionObjects to process a single frame, each ExecutionObject
240     // processes one layerGroup of the network
241     //
242     // Pipeline depth can enable more optimized pipeline execution:
243     // Given one EVE and one DSP as an example, with different
244     //     buffer_factor, we have different execution behavior:
245     // If buffer_factor is set to 1,
246     //    we create one EOP: eop0 (eve0, dsp0)
247     //    pipeline execution of multiple frames over time is as follows:
248     //    --------------------- time ------------------->
249     //    eop0: [eve0...][dsp0]
250     //    eop0:                [eve0...][dsp0]
251     //    eop0:                               [eve0...][dsp0]
252     //    eop0:                                              [eve0...][dsp0]
253     // If buffer_factor is set to 2,
254     //    we create two EOPs: eop0 (eve0, dsp0), eop1(eve0, dsp0)
255     //    pipeline execution of multiple frames over time is as follows:
256     //    --------------------- time ------------------->
257     //    eop0: [eve0...][dsp0]
258     //    eop1:          [eve0...][dsp0]
259     //    eop0:                   [eve0...][dsp0]
260     //    eop1:                            [eve0...][dsp0]
261     // Additional benefit of setting buffer_factor to 2 is that
262     //    it can also overlap host ReadFrame() with device processing:
263     //    --------------------- time ------------------->
264     //    eop0: [RF][eve0...][dsp0]
265     //    eop1:     [RF]     [eve0...][dsp0]
266     //    eop0:                    [RF][eve0...][dsp0]
267     //    eop1:                             [RF][eve0...][dsp0]
268     const uint32_t buffer_factor = 2;
270     switch(num_layers_groups)
271     {
272     case 1: // Single layers group
273         e_eve = num_eves == 0 ? nullptr :
274                 new Executor(DeviceType::EVE, ids_eve, configuration);
275         e_dsp = num_dsps == 0 ? nullptr :
276                 new Executor(DeviceType::DSP, ids_dsp, configuration);
278         // Construct ExecutionObjectPipeline with single Execution Object to
279         // process each frame. This is parallel processing of frames with
280         // as many DSP and EVE cores that we have on hand.
281         // If buffer_factor == 2, duplicating EOPs for double buffering
282         // and overlapping host pre/post-processing with device processing
283         for (uint32_t j = 0; j < buffer_factor; j++)
284         {
285             for (uint32_t i = 0; i < num_eves; i++)
286                 eops.push_back(new ExecutionObjectPipeline({(*e_eve)[i]}));
287             for (uint32_t i = 0; i < num_dsps; i++)
288                 eops.push_back(new ExecutionObjectPipeline({(*e_dsp)[i]}));
289         }
290         break;
292     case 2: // Two layers group
293         // Create Executors with the approriate core type, number of cores
294         // and configuration specified
295         // EVE will run layersGroupId 1 in the network, while
296         // DSP will run layersGroupId 2 in the network
297         e_eve = num_eves == 0 ? nullptr :
298                 new Executor(DeviceType::EVE, ids_eve, configuration, 1);
299         e_dsp = num_dsps == 0 ? nullptr :
300                 new Executor(DeviceType::DSP, ids_dsp, configuration, 2);
302         // Construct ExecutionObjectPipeline that utilizes multiple
303         // ExecutionObjects to process a single frame, each ExecutionObject
304         // processes one layerGroup of the network
305         // If buffer_factor == 2, duplicating EOPs for pipelining at
306         // EO level rather than at EOP level, in addition to double buffering
307         // and overlapping host pre/post-processing with device processing
308         for (uint32_t j = 0; j < buffer_factor; j++)
309             for (uint32_t i = 0; i < std::max(num_eves, num_dsps); i++)
310                 eops.push_back(new ExecutionObjectPipeline(
311                                 {(*e_eve)[i%num_eves], (*e_dsp)[i%num_dsps]}));
312         break;
314     default:
315         std::cout << "Layers groups must be either 1 or 2!" << std::endl;
316         return false;
317         break;
318     }
320     return true;
323 static void subtractMeanValue(unsigned char *frame_buffer, int channel_size,
324                               int32_t mean_value)
326     int32_t one_pixel;
328     for (int i = 0; i < channel_size; i ++)
329     {
330         one_pixel  = (int32_t)frame_buffer[i];
331         one_pixel -= mean_value;
332         if(one_pixel > 127)  one_pixel = 127;
333         if(one_pixel < -128) one_pixel = -128;
334         frame_buffer[i] = (unsigned char)one_pixel;
335     }
338 bool ReadFrame(ExecutionObjectPipeline& eop, uint32_t frame_idx,
339                const Configuration& c, const cmdline_opts_t& opts,
340                char *input_frames_buffer)
342     if (frame_idx >= opts.num_frames)
343         return false;
345     eop.SetFrameIndex(frame_idx);
347     unsigned char* frame_buffer = (unsigned char *)eop.GetInputBufferPtr();
348     assert (frame_buffer != nullptr);
349     //Current implementation of this function assumes 3 channels on input
350     assert (c.inNumChannels == 3);
352     int channel_size = c.inWidth * c.inHeight;
353     char *bgr_frames_input = input_frames_buffer + (frame_idx % c.numFrames) *
354                              channel_size * c.inNumChannels;
356     memcpy(frame_buffer,                bgr_frames_input + 0, channel_size);
357     if(c.preProcType == 1)
358        subtractMeanValue(frame_buffer, channel_size, 104);
359     else if(c.preProcType == 2)
360        subtractMeanValue(frame_buffer, channel_size, 128);
361     frame_buffer += channel_size;
363     memcpy(frame_buffer, bgr_frames_input + 1 * channel_size, channel_size);
364     if(c.preProcType == 1)
365        subtractMeanValue(frame_buffer, channel_size, 117);
366     else if(c.preProcType == 2)
367        subtractMeanValue(frame_buffer, channel_size, 128);
368     frame_buffer += channel_size;
370     memcpy(frame_buffer, bgr_frames_input + 2 * channel_size, channel_size);
371     if(c.preProcType == 1)
372        subtractMeanValue(frame_buffer, channel_size, 123);
373     else if(c.preProcType == 2)
374        subtractMeanValue(frame_buffer, channel_size, 128);
376     return true;
379 void DisplayHelp()
381     std::cout <<
382     "Usage: mcbench\n"
383     "  Runs partitioned network to perform multi-object detection\n"
384     "  and classification. First part of network (layersGroupId 1) runs on\n"
385     "  EVE, second part (layersGroupId 2) runs on DSP.\n"
386     "  Use -c to run a different segmentation network.  Default is jdetnet.\n"
387     "Optional arguments:\n"
388     " -c <config>          Valid configs: ../test/testvecs/config/infer/... \n"
389     " -d <number>          Number of DSP cores to use\n"
390     " -e <number>          Number of EVE cores to use\n"
391     " -g <1|2>             Number of layer groups\n"
392     " -f <number>          Number of frames to process\n"
393     " -i <image>           Path to the input image file\n"
394     " -v                   Verbose output during execution\n"
395     " -h                   Help\n";