Added example to illustrate pipelining across EOs
[tidl/tidl-api.git] / examples / one_eo_per_frame / main.cpp
1 /******************************************************************************
2  * Copyright (c) 2017-2018  Texas Instruments Incorporated - http://www.ti.com/
3  *  All rights reserved.
4  *
5  *  Redistribution and use in source and binary forms, with or without
6  *  modification, are permitted provided that the following conditions are met:
7  *      * Redistributions of source code must retain the above copyright
8  *        notice, this list of conditions and the following disclaimer.
9  *      * Redistributions in binary form must reproduce the above copyright
10  *        notice, this list of conditions and the following disclaimer in the
11  *        documentation and/or other materials provided with the distribution.
12  *      * Neither the name of Texas Instruments Incorporated nor the
13  *        names of its contributors may be used to endorse or promote products
14  *        derived from this software without specific prior written permission.
15  *
16  *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
17  *  AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
18  *  IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
19  *  ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE
20  *  LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
21  *  CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
22  *  SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
23  *  INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
24  *  CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
25  *  ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF
26  *  THE POSSIBILITY OF SUCH DAMAGE.
27  *****************************************************************************/
29 //
30 // This example illustrates using a single EO to process a frame. To increase
31 // throughput, multiple EOs are used.
32 // For details, refer http://downloads.ti.com/mctools/esd/docs/tidl-api/
33 //
34 #include <signal.h>
35 #include <iostream>
36 #include <fstream>
37 #include <cassert>
38 #include <string>
40 #include "executor.h"
41 #include "execution_object.h"
42 #include "configuration.h"
43 #include "utils.h"
45 using namespace tidl;
46 using std::string;
47 using std::unique_ptr;
48 using std::vector;
50 bool Run(const string& config_file, int num_eve,int num_dsp,
51          const char* ref_output);
53 Executor* CreateExecutor(DeviceType dt, int num, const Configuration& c);
54 void      CollectEOs(const Executor *e, vector<ExecutionObject *>& EOs);
56 void AllocateMemory(const vector<ExecutionObject *>& EOs);
57 void FreeMemory    (const vector<ExecutionObject *>& EOs);
60 int main(int argc, char *argv[])
61 {
62     // Catch ctrl-c to ensure a clean exit
63     signal(SIGABRT, exit);
64     signal(SIGTERM, exit);
66     // If there are no devices capable of offloading TIDL on the SoC, exit
67     uint32_t num_eve = Executor::GetNumDevices(DeviceType::EVE);
68     uint32_t num_dsp = Executor::GetNumDevices(DeviceType::DSP);
69     if (num_eve == 0 && num_dsp == 0)
70     {
71         std::cout << "TI DL not supported on this SoC." << std::endl;
72         return EXIT_SUCCESS;
73     }
75     string config_file ="../test/testvecs/config/infer/tidl_config_j11_v2.txt";
76     string ref_file    ="../test/testvecs/reference/j11_v2_ref.bin";
78     unique_ptr<const char> reference_output(ReadReferenceOutput(ref_file));
80     bool status = Run(config_file, num_eve, num_dsp, reference_output.get());
82     if (!status)
83     {
84         std::cout << "FAILED" << std::endl;
85         return EXIT_FAILURE;
86     }
88     std::cout << "PASSED" << std::endl;
89     return EXIT_SUCCESS;
90 }
92 bool Run(const string& config_file, int num_eve, int num_dsp,
93          const char* ref_output)
94 {
95     Configuration c;
96     if (!c.ReadFromFile(config_file))
97         return false;
99     // Heap sizes for this network determined using Configuration::showHeapStats
100     c.PARAM_HEAP_SIZE   = (3 << 20); // 3MB
101     c.NETWORK_HEAP_SIZE = (20 << 20); // 20MB
103     c.numFrames = 16;
105     // Open input file for reading
106     std::ifstream input_data_file(c.inData, std::ios::binary);
108     bool status = true;
109     try
110     {
111         // Create Executors - use all the DSP and EVE cores available
112         unique_ptr<Executor> e_dsp(CreateExecutor(DeviceType::DSP, num_dsp, c));
113         unique_ptr<Executor> e_eve(CreateExecutor(DeviceType::EVE, num_eve, c));
115         // Accumulate all the EOs from across the Executors
116         vector<ExecutionObject *> EOs;
117         CollectEOs(e_eve.get(), EOs);
118         CollectEOs(e_dsp.get(), EOs);
120         AllocateMemory(EOs);
122         // Process frames with EOs in a pipelined manner
123         // additional num_eos iterations to flush the pipeline (epilogue)
124         int num_eos = EOs.size();
125         for (int frame_idx = 0; frame_idx < c.numFrames + num_eos; frame_idx++)
126         {
127             ExecutionObject* eo = EOs[frame_idx % num_eos];
129             // Wait for previous frame on the same eo to finish processing
130             if (eo->ProcessFrameWait())
131             {
132                 ReportTime(eo);
133                 if (frame_idx < num_eos && !CheckFrame(eo, ref_output))
134                     status = false;
135             }
137             // Read a frame and start processing it with current eo
138             if (ReadFrame(eo, frame_idx, c, input_data_file))
139                 eo->ProcessFrameStartAsync();
140         }
142         FreeMemory(EOs);
144     }
145     catch (tidl::Exception &e)
146     {
147         std::cerr << e.what() << std::endl;
148         status = false;
149     }
151     input_data_file.close();
153     return status;
156 // Create an Executor with the specified type and number of EOs
157 Executor* CreateExecutor(DeviceType dt, int num, const Configuration& c)
159     if (num == 0) return nullptr;
161     DeviceIds ids;
162     for (int i = 0; i < num; i++)
163         ids.insert(static_cast<DeviceId>(i));
165     return new Executor(dt, ids, c);
168 // Accumulate EOs from an Executor into a vector of EOs
169 void CollectEOs(const Executor *e, vector<ExecutionObject *>& EOs)
171     if (!e) return;
173     for (unsigned int i = 0; i < e->GetNumExecutionObjects(); i++)
174         EOs.push_back((*e)[i]);
177 // Allocate input and output memory for each EO
178 void AllocateMemory(const vector<ExecutionObject *>& EOs)
180     // Allocate input and output buffers for each execution object
181     for (auto eo : EOs)
182     {
183         size_t in_size  = eo->GetInputBufferSizeInBytes();
184         size_t out_size = eo->GetOutputBufferSizeInBytes();
185         ArgInfo in  = { ArgInfo(malloc(in_size),  in_size)};
186         ArgInfo out = { ArgInfo(malloc(out_size), out_size)};
187         eo->SetInputOutputBuffer(in, out);
188     }
191 // Free the input and output memory associated with each EO
192 void FreeMemory(const vector<ExecutionObject *>& EOs)
194     for (auto eo : EOs)
195     {
196         free(eo->GetInputBufferPtr());
197         free(eo->GetOutputBufferPtr());
198     }