Merge branch 'hotfix/v01.05.01'
[tidl/tidl-api.git] / examples / segmentation / main.cpp
1 /******************************************************************************
2  * Copyright (c) 2018, Texas Instruments Incorporated - http://www.ti.com/
3  *   All rights reserved.
4  *
5  *   Redistribution and use in source and binary forms, with or without
6  *   modification, are permitted provided that the following conditions are met:
7  *       * Redistributions of source code must retain the above copyright
8  *         notice, this list of conditions and the following disclaimer.
9  *       * Redistributions in binary form must reproduce the above copyright
10  *         notice, this list of conditions and the following disclaimer in the
11  *         documentation and/or other materials provided with the distribution.
12  *       * Neither the name of Texas Instruments Incorporated nor the
13  *         names of its contributors may be used to endorse or promote products
14  *         derived from this software without specific prior written permission.
15  *
16  *   THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
17  *   AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
18  *   IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
19  *   ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE
20  *   LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
21  *   CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
22  *   SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
23  *   INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
24  *   CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
25  *   ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF
26  *   THE POSSIBILITY OF SUCH DAMAGE.
27  *****************************************************************************/
28 #include <signal.h>
29 #include <iostream>
30 #include <iomanip>
31 #include <fstream>
32 #include <cassert>
33 #include <string>
34 #include <functional>
35 #include <algorithm>
36 #include <time.h>
37 #include <unistd.h>
39 #include <queue>
40 #include <vector>
41 #include <cstdio>
42 #include <chrono>
44 #include "executor.h"
45 #include "execution_object.h"
46 #include "configuration.h"
47 #include "../common/object_classes.h"
48 #include "../common/utils.h"
49 #include "../common/video_utils.h"
51 using namespace std;
52 using namespace tidl;
53 using namespace cv;
56 #define NUM_VIDEO_FRAMES  300
57 #define DEFAULT_CONFIG    "jseg21_tiscapes"
58 #define DEFAULT_INPUT     "../test/testvecs/input/000100_1024x512_bgr.y"
59 #define DEFAULT_INPUT_FRAMES  (9)
60 #define DEFAULT_OBJECT_CLASSES_LIST_FILE "jseg21_objects.json"
62 std::unique_ptr<ObjectClasses> object_classes;
63 uint32_t orig_width;
64 uint32_t orig_height;
67 bool RunConfiguration(const cmdline_opts_t& opts);
68 Executor* CreateExecutor(DeviceType dt, uint32_t num, const Configuration& c);
69 bool ReadFrame(ExecutionObjectPipeline& eop,
70                uint32_t frame_idx, const Configuration& c,
71                const cmdline_opts_t& opts, VideoCapture &cap);
72 bool WriteFrameOutput(const ExecutionObjectPipeline &eop,
73                       const Configuration& c, const cmdline_opts_t& opts);
74 void DisplayHelp();
77 int main(int argc, char *argv[])
78 {
79     // Catch ctrl-c to ensure a clean exit
80     signal(SIGABRT, exit);
81     signal(SIGTERM, exit);
83     // If there are no devices capable of offloading TIDL on the SoC, exit
84     uint32_t num_eves = Executor::GetNumDevices(DeviceType::EVE);
85     uint32_t num_dsps = Executor::GetNumDevices(DeviceType::DSP);
86     if (num_eves == 0 && num_dsps == 0)
87     {
88         cout << "TI DL not supported on this SoC." << endl;
89         return EXIT_SUCCESS;
90     }
92     // Process arguments
93     cmdline_opts_t opts;
94     opts.config = DEFAULT_CONFIG;
95     opts.object_classes_list_file = DEFAULT_OBJECT_CLASSES_LIST_FILE;
96     if (num_eves != 0) { opts.num_eves = 1;  opts.num_dsps = 0; }
97     else               { opts.num_eves = 0;  opts.num_dsps = 1; }
98     if (! ProcessArgs(argc, argv, opts))
99     {
100         DisplayHelp();
101         exit(EXIT_SUCCESS);
102     }
103     assert(opts.num_dsps != 0 || opts.num_eves != 0);
104     if (opts.num_frames == 0)
105         opts.num_frames = (opts.is_camera_input || opts.is_video_input) ?
106                           NUM_VIDEO_FRAMES :
107                           (opts.input_file.empty() ? DEFAULT_INPUT_FRAMES : 1);
108     if (opts.input_file.empty())
109         cout << "Input: " << DEFAULT_INPUT << endl;
110     else
111         cout << "Input: " << opts.input_file << endl;
113     // Get object classes list
114     object_classes = std::unique_ptr<ObjectClasses>(
115                              new ObjectClasses(opts.object_classes_list_file));
116     if (object_classes->GetNumClasses() == 0)
117     {
118         cout << "No object classes defined for this config." << endl;
119         return EXIT_FAILURE;
120     }
122     // Run network
123     bool status = RunConfiguration(opts);
124     if (!status)
125     {
126         cout << "segmentation FAILED" << endl;
127         return EXIT_FAILURE;
128     }
130     cout << "segmentation PASSED" << endl;
131     return EXIT_SUCCESS;
134 bool RunConfiguration(const cmdline_opts_t& opts)
136     // Read the TI DL configuration file
137     Configuration c;
138     std::string config_file = "../test/testvecs/config/infer/tidl_config_"
139                               + opts.config + ".txt";
140     bool status = c.ReadFromFile(config_file);
141     if (!status)
142     {
143         cerr << "Error in configuration file: " << config_file << endl;
144         return false;
145     }
146     c.enableApiTrace = opts.verbose;
148     // setup camera/video input/output
149     VideoCapture cap;
150     if (! SetVideoInputOutput(cap, opts, "Segmentation"))  return false;
152     try
153     {
154         // Create Executors with the approriate core type, number of cores
155         // and configuration specified
156         Executor* e_eve = CreateExecutor(DeviceType::EVE, opts.num_eves, c);
157         Executor* e_dsp = CreateExecutor(DeviceType::DSP, opts.num_dsps, c);
159         // Get ExecutionObjects from Executors
160         vector<ExecutionObject*> eos;
161         for (uint32_t i = 0; i < opts.num_eves; i++) eos.push_back((*e_eve)[i]);
162         for (uint32_t i = 0; i < opts.num_dsps; i++) eos.push_back((*e_dsp)[i]);
163         uint32_t num_eos = eos.size();
165         // Use duplicate EOPs to do double buffering on frame input/output
166         //    because each EOP has its own set of input/output buffers,
167         //    so that host ReadFrame() can be overlapped with device processing
168         // Use one EO as an example, with different buffer_factor,
169         //    we have different execution behavior:
170         // If buffer_factor is set to 1 -> single buffering
171         //    we create one EOP: eop0 (eo0)
172         //    pipeline execution of multiple frames over time is as follows:
173         //    --------------------- time ------------------->
174         //    eop0: [RF][eo0.....][WF]
175         //    eop0:                   [RF][eo0.....][WF]
176         //    eop0:                                     [RF][eo0.....][WF]
177         // If buffer_factor is set to 2 -> double buffering
178         //    we create two EOPs: eop0 (eo0), eop1(eo0)
179         //    pipeline execution of multiple frames over time is as follows:
180         //    --------------------- time ------------------->
181         //    eop0: [RF][eo0.....][WF]
182         //    eop1:     [RF]      [eo0.....][WF]
183         //    eop0:                   [RF]  [eo0.....][WF]
184         //    eop1:                             [RF]  [eo0.....][WF]
185         vector<ExecutionObjectPipeline *> eops;
186         uint32_t buffer_factor = 2;  // set to 1 for single buffering
187         for (uint32_t j = 0; j < buffer_factor; j++)
188             for (uint32_t i = 0; i < num_eos; i++)
189                 eops.push_back(new ExecutionObjectPipeline({eos[i]}));
190         uint32_t num_eops = eops.size();
192         // Allocate input and output buffers for each EOP
193         AllocateMemory(eops);
195         chrono::time_point<chrono::steady_clock> tloop0, tloop1;
196         tloop0 = chrono::steady_clock::now();
198         // Process frames with available eops in a pipelined manner
199         // additional num_eos iterations to flush the pipeline (epilogue)
200         for (uint32_t frame_idx = 0;
201              frame_idx < opts.num_frames + num_eops; frame_idx++)
202         {
203             ExecutionObjectPipeline* eop = eops[frame_idx % num_eops];
205             // Wait for previous frame on the same eop to finish processing
206             if (eop->ProcessFrameWait())
207             {
208                 WriteFrameOutput(*eop, c, opts);
209             }
211             // Read a frame and start processing it with current eop
212             if (ReadFrame(*eop, frame_idx, c, opts, cap))
213                 eop->ProcessFrameStartAsync();
214         }
216         tloop1 = chrono::steady_clock::now();
217         chrono::duration<float> elapsed = tloop1 - tloop0;
218         cout << "Loop total time (including read/write/opencv/print/etc): "
219                   << setw(6) << setprecision(4)
220                   << (elapsed.count() * 1000) << "ms" << endl;
222         FreeMemory(eops);
223         for (auto eop : eops)  delete eop;
224         delete e_eve;
225         delete e_dsp;
226     }
227     catch (tidl::Exception &e)
228     {
229         cerr << e.what() << endl;
230         status = false;
231     }
233     return status;
236 // Create an Executor with the specified type and number of EOs
237 Executor* CreateExecutor(DeviceType dt, uint32_t num, const Configuration& c)
239     if (num == 0) return nullptr;
241     DeviceIds ids;
242     for (uint32_t i = 0; i < num; i++)
243         ids.insert(static_cast<DeviceId>(i));
245     return new Executor(dt, ids, c);
248 bool ReadFrame(ExecutionObjectPipeline &eop,
249                uint32_t frame_idx, const Configuration& c,
250                const cmdline_opts_t& opts, VideoCapture &cap)
252     if (frame_idx >= opts.num_frames)
253         return false;
254     eop.SetFrameIndex(frame_idx);
256     char*  frame_buffer = eop.GetInputBufferPtr();
257     assert (frame_buffer != nullptr);
258     int channel_size = c.inWidth * c.inHeight;
260     Mat image;
261     if (! opts.is_camera_input && ! opts.is_video_input)
262     {
263         if (opts.input_file.empty())
264         {
265             ifstream ifs(DEFAULT_INPUT, ios::binary);
266             ifs.seekg((frame_idx % DEFAULT_INPUT_FRAMES) * channel_size * 3);
267             ifs.read(frame_buffer, channel_size * 3);
268             bool ifs_status = ifs.good();
269             ifs.close();
270             orig_width  = c.inWidth;
271             orig_height = c.inHeight;
272             return ifs_status;  // already PreProc-ed
273         }
274         else
275         {
276             image = cv::imread(opts.input_file, CV_LOAD_IMAGE_COLOR);
277             if (image.empty())
278             {
279                 cerr << "Unable to read from: " << opts.input_file << endl;
280                 return false;
281             }
282         }
283     }
284     else
285     {
286       if(opts.is_camera_input)
287       {
288          if (! cap.grab()) return false;
289          if (! cap.retrieve(image)) return false;
290       }
291       else
292       { //Video clip
293         if (cap.grab())
294         {
295           if (! cap.retrieve(image)) return false;
296         } else {
297           //Rewind!
298           std::cout << "Video clip rewinded!" << std::endl;
299           cap.set(CAP_PROP_POS_FRAMES, 0);
300           if (! cap.grab()) return false;
301             if (! cap.retrieve(image)) return false;
302         }
303       }
304     }
306     // scale to network input size 1024 x 512
307     Mat s_image, bgr_frames[3];
308     orig_width  = image.cols;
309     orig_height = image.rows;
310     cv::resize(image, s_image, Size(c.inWidth, c.inHeight),
311                0, 0, cv::INTER_AREA);
312     cv::split(s_image, bgr_frames);
313     memcpy(frame_buffer,                bgr_frames[0].ptr(), channel_size);
314     memcpy(frame_buffer+1*channel_size, bgr_frames[1].ptr(), channel_size);
315     memcpy(frame_buffer+2*channel_size, bgr_frames[2].ptr(), channel_size);
316     return true;
319 // Create Overlay mask for pixel-level segmentation
320 void CreateMask(uchar *classes, uchar *mb, uchar *mg, uchar* mr,
321                 int channel_size)
323     for (int i = 0; i < channel_size; i++)
324     {
325         const ObjectClass& object_class = object_classes->At(classes[i]);
326         mb[i] = object_class.color.blue;
327         mg[i] = object_class.color.green;
328         mr[i] = object_class.color.red;
329     }
332 // Create frame overlayed with pixel-level segmentation
333 bool WriteFrameOutput(const ExecutionObjectPipeline &eop,
334                       const Configuration& c,
335                       const cmdline_opts_t& opts)
337     unsigned char *out = (unsigned char *) eop.GetOutputBufferPtr();
338     int width          = c.inWidth;
339     int height         = c.inHeight;
340     int channel_size   = width * height;
342     Mat mask, frame, blend, r_blend, bgr[3];
343     // Create overlay mask
344     bgr[0] = Mat(height, width, CV_8UC(1));
345     bgr[1] = Mat(height, width, CV_8UC(1));
346     bgr[2] = Mat(height, width, CV_8UC(1));
347     CreateMask(out, bgr[0].ptr(), bgr[1].ptr(), bgr[2].ptr(), channel_size);
348     cv::merge(bgr, 3, mask);
350     // Asseembly original frame
351     unsigned char *in = (unsigned char *) eop.GetInputBufferPtr();
352     bgr[0] = Mat(height, width, CV_8UC(1), in);
353     bgr[1] = Mat(height, width, CV_8UC(1), in + channel_size);
354     bgr[2] = Mat(height, width, CV_8UC(1), in + channel_size*2);
355     cv::merge(bgr, 3, frame);
357     // Create overlayed frame
358     cv::addWeighted(frame, 0.7, mask, 0.3, 0.0, blend);
360     // Resize to output width/height, keep aspect ratio
361     uint32_t output_width = opts.output_width;
362     if (output_width == 0)  output_width = orig_width;
363     uint32_t output_height = (output_width*1.0f) / orig_width * orig_height;
364     cv::resize(blend, r_blend, Size(output_width, output_height));
366     if (opts.is_camera_input || opts.is_video_input)
367     {
368         cv::imshow("Segmentation", r_blend);
369         waitKey(1);
370     }
371     else
372     {
373         int frame_index = eop.GetFrameIndex();
374         char outfile_name[64];
375         if (opts.input_file.empty())
376         {
377             snprintf(outfile_name, 64, "frame_%d.png", frame_index);
378             cv::imwrite(outfile_name, frame);
379             printf("Saving frame %d to: %s\n", frame_index, outfile_name);
380         }
382         snprintf(outfile_name, 64, "overlay_%d.png", frame_index);
383         cv::imwrite(outfile_name, r_blend);
384         printf("Saving frame %d overlayed with segmentation to: %s\n",
385                frame_index, outfile_name);
386     }
388     return true;
391 void DisplayHelp()
393     std::cout <<
394     "Usage: segmentation\n"
395     "  Will run segmentation network to perform pixel-level"
396     " classification.\n  Use -c to run a different"
397     "  segmentation network. Default is jseg21_tiscapes.\n"
398     "Optional arguments:\n"
399     " -c <config>          Valid configs: jseg21_tiscapes, jseg21\n"
400     " -d <number>          Number of dsp cores to use\n"
401     " -e <number>          Number of eve cores to use\n"
402     " -i <image>           Path to the image file as input\n"
403     "                      Default are 9 frames in testvecs\n"
404     " -i camera<number>    Use camera as input\n"
405     "                      video input port: /dev/video<number>\n"
406     " -i <name>.{mp4,mov,avi}  Use video file as input\n"
407     " -l <objects_list>    Path to the object classes list file\n"
408     " -f <number>          Number of frames to process\n"
409     " -w <number>          Output image/video width\n"
410     " -v                   Verbose output during execution\n"
411     " -h                   Help\n";