tidl-viewer: fixes for yocto nativesdk build failures
[tidl/tidl-api.git] / examples / segmentation / main.cpp
1 /******************************************************************************
2  * Copyright (c) 2018, Texas Instruments Incorporated - http://www.ti.com/
3  *   All rights reserved.
4  *
5  *   Redistribution and use in source and binary forms, with or without
6  *   modification, are permitted provided that the following conditions are met:
7  *       * Redistributions of source code must retain the above copyright
8  *         notice, this list of conditions and the following disclaimer.
9  *       * Redistributions in binary form must reproduce the above copyright
10  *         notice, this list of conditions and the following disclaimer in the
11  *         documentation and/or other materials provided with the distribution.
12  *       * Neither the name of Texas Instruments Incorporated nor the
13  *         names of its contributors may be used to endorse or promote products
14  *         derived from this software without specific prior written permission.
15  *
16  *   THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
17  *   AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
18  *   IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
19  *   ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE
20  *   LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
21  *   CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
22  *   SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
23  *   INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
24  *   CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
25  *   ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF
26  *   THE POSSIBILITY OF SUCH DAMAGE.
27  *****************************************************************************/
28 #include <signal.h>
29 #include <getopt.h>
30 #include <iostream>
31 #include <iomanip>
32 #include <fstream>
33 #include <cassert>
34 #include <string>
35 #include <functional>
36 #include <algorithm>
37 #include <time.h>
38 #include <unistd.h>
40 #include <queue>
41 #include <vector>
42 #include <cstdio>
44 #include "executor.h"
45 #include "execution_object.h"
46 #include "configuration.h"
47 #include "object_classes.h"
49 #include "opencv2/core.hpp"
50 #include "opencv2/imgproc.hpp"
51 #include "opencv2/highgui.hpp"
52 #include "opencv2/videoio.hpp"
54 #define NUM_VIDEO_FRAMES  100
55 #define DEFAULT_CONFIG    "jseg21_tiscapes"
56 #define DEFAULT_INPUT     "../test/testvecs/input/000100_1024x512_bgr.y"
58 bool __TI_show_debug_ = false;
59 bool is_default_input = false;
60 bool is_preprocessed_input = false;
61 bool is_camera_input       = false;
62 int  orig_width;
63 int  orig_height;
64 object_class_table_t *object_class_table;
66 using namespace tidl;
67 using namespace cv;
70 bool RunConfiguration(const std::string& config_file, int num_devices,
71                       DeviceType device_type, std::string& input_file);
72 bool RunAllConfigurations(int32_t num_devices, DeviceType device_type);
74 bool ReadFrame(ExecutionObject& eo, int frame_idx,
75                const Configuration& configuration, int num_frames,
76                std::string& image_file, VideoCapture &cap);
78 bool WriteFrameOutput(const ExecutionObject &eo,
79                       const Configuration& configuration);
81 static void ProcessArgs(int argc, char *argv[],
82                         std::string& config,
83                         int& num_devices,
84                         DeviceType& device_type,
85                         std::string& input_file);
87 static void DisplayHelp();
89 static double ms_diff(struct timespec &t0, struct timespec &t1)
90 { return (t1.tv_sec - t0.tv_sec) * 1e3 + (t1.tv_nsec - t0.tv_nsec) / 1e6; }
93 int main(int argc, char *argv[])
94 {
95     // Catch ctrl-c to ensure a clean exit
96     signal(SIGABRT, exit);
97     signal(SIGTERM, exit);
99     // If there are no devices capable of offloading TIDL on the SoC, exit
100     uint32_t num_dla = Executor::GetNumDevices(DeviceType::DLA);
101     uint32_t num_dsp = Executor::GetNumDevices(DeviceType::DSP);
102     if (num_dla == 0 && num_dsp == 0)
103     {
104         std::cout << "TI DL not supported on this SoC." << std::endl;
105         return EXIT_SUCCESS;
106     }
108     // Process arguments
109     std::string config      = DEFAULT_CONFIG;
110     std::string input_file  = DEFAULT_INPUT;
111     int         num_devices = 1;
112     DeviceType  device_type = (num_dla > 0 ? DeviceType::DLA:DeviceType::DSP);
113     ProcessArgs(argc, argv, config, num_devices, device_type, input_file);
115     if ((object_class_table = GetObjectClassTable(config)) == nullptr)
116     {
117         std::cout << "No object classes defined for this config." << std::endl;
118         return EXIT_FAILURE;
119     }
121     if (input_file == DEFAULT_INPUT)  is_default_input = true;
122     if (input_file == "camera")       is_camera_input = true;
123     if (input_file.length() > 2 &&
124         input_file.compare(input_file.length() - 2, 2, ".y") == 0)
125         is_preprocessed_input = true;
126     std::cout << "Input: " << input_file << std::endl;
127     std::string config_file = "../test/testvecs/config/infer/tidl_config_"
128                               + config + ".txt";
129     bool status = RunConfiguration(config_file, num_devices, device_type,
130                                    input_file);
132     if (!status)
133     {
134         std::cout << "segmentation FAILED" << std::endl;
135         return EXIT_FAILURE;
136     }
138     std::cout << "segmentation PASSED" << std::endl;
139     return EXIT_SUCCESS;
142 bool RunConfiguration(const std::string& config_file, int num_devices,
143                       DeviceType device_type, std::string& input_file)
145     DeviceIds ids;
146     for (int i = 0; i < num_devices; i++)
147         ids.insert(static_cast<DeviceId>(i));
149     // Read the TI DL configuration file
150     Configuration configuration;
151     bool status = configuration.ReadFromFile(config_file);
152     if (!status)
153     {
154         std::cerr << "Error in configuration file: " << config_file
155                   << std::endl;
156         return false;
157     }
159     // setup input
160     int num_frames = is_default_input ? 3 : 1;
161     VideoCapture cap;
162     std::string image_file;
163     if (is_camera_input)
164     {
165         cap = VideoCapture(1);  // cap = VideoCapture("test.mp4");
166         if (! cap.isOpened())
167         {
168             std::cerr << "Cannot open camera input." << std::endl;
169             return false;
170         }
171         num_frames = NUM_VIDEO_FRAMES;
172         namedWindow("Segmentation", WINDOW_AUTOSIZE | CV_GUI_NORMAL);
173     }
174     else
175     {
176         image_file = input_file;
177     }
179     try
180     {
181         // Create a executor with the approriate core type, number of cores
182         // and configuration specified
183         Executor executor(device_type, ids, configuration);
185         // Query Executor for set of ExecutionObjects created
186         const ExecutionObjects& execution_objects =
187                                                 executor.GetExecutionObjects();
188         int num_eos = execution_objects.size();
190         // Allocate input and output buffers for each execution object
191         std::vector<void *> buffers;
192         for (auto &eo : execution_objects)
193         {
194             size_t in_size  = eo->GetInputBufferSizeInBytes();
195             size_t out_size = eo->GetOutputBufferSizeInBytes();
196             ArgInfo in  = { ArgInfo(malloc(in_size),  in_size)};
197             ArgInfo out = { ArgInfo(malloc(out_size), out_size)};
198             eo->SetInputOutputBuffer(in, out);
200             buffers.push_back(in.ptr());
201             buffers.push_back(out.ptr());
202         }
204         #define MAX_NUM_EOS  4
205         struct timespec t0[MAX_NUM_EOS], t1;
207         // Process frames with available execution objects in a pipelined manner
208         // additional num_eos iterations to flush the pipeline (epilogue)
209         for (int frame_idx = 0;
210              frame_idx < num_frames + num_eos; frame_idx++)
211         {
212             ExecutionObject* eo = execution_objects[frame_idx % num_eos].get();
214             // Wait for previous frame on the same eo to finish processing
215             if (eo->ProcessFrameWait())
216             {
217                 clock_gettime(CLOCK_MONOTONIC, &t1);
218                 double elapsed_host =
219                                 ms_diff(t0[eo->GetFrameIndex() % num_eos], t1);
220                 double elapsed_device = eo->GetProcessTimeInMilliSeconds();
221                 double overhead = 100 - (elapsed_device/elapsed_host*100);
223                 std::cout << "frame[" << eo->GetFrameIndex() << "]: "
224                           << "Time on device: "
225                           << std::setw(6) << std::setprecision(4)
226                           << elapsed_device << "ms, "
227                           << "host: "
228                           << std::setw(6) << std::setprecision(4)
229                           << elapsed_host << "ms ";
230                 std::cout << "API overhead: "
231                           << std::setw(6) << std::setprecision(3)
232                           << overhead << " %" << std::endl;
234                 WriteFrameOutput(*eo, configuration);
235             }
237             // Read a frame and start processing it with current eo
238             if (ReadFrame(*eo, frame_idx, configuration, num_frames,
239                           image_file, cap))
240             {
241                 clock_gettime(CLOCK_MONOTONIC, &t0[frame_idx % num_eos]);
242                 eo->ProcessFrameStartAsync();
243             }
244         }
246         for (auto b : buffers)
247             free(b);
249     }
250     catch (tidl::Exception &e)
251     {
252         std::cerr << e.what() << std::endl;
253         status = false;
254     }
256     return status;
260 bool ReadFrame(ExecutionObject &eo, int frame_idx,
261                const Configuration& configuration, int num_frames,
262                std::string& image_file, VideoCapture &cap)
264     if (frame_idx >= num_frames)
265         return false;
266     eo.SetFrameIndex(frame_idx);
268     char*  frame_buffer = eo.GetInputBufferPtr();
269     assert (frame_buffer != nullptr);
270     int channel_size = configuration.inWidth * configuration.inHeight;
272     Mat image;
273     if (! image_file.empty())
274     {
275         if (is_preprocessed_input)
276         {
277             std::ifstream ifs(image_file, std::ios::binary);
278             ifs.seekg(frame_idx * channel_size * 3);
279             ifs.read(frame_buffer, channel_size * 3);
280             bool ifs_status = ifs.good();
281             ifs.close();
282             orig_width  = configuration.inWidth;
283             orig_height = configuration.inHeight;
284             return ifs_status;  // already PreProc-ed
285         }
286         else
287         {
288             image = cv::imread(image_file, CV_LOAD_IMAGE_COLOR);
289             if (image.empty())
290             {
291                 std::cerr << "Unable to read from: " << image_file << std::endl;
292                 return false;
293             }
294         }
295     }
296     else
297     {
298         // 640x480 camera input, process one in every 5 frames,
299         // can adjust number of skipped frames to match real time processing
300         if (! cap.grab())  return false;
301         if (! cap.grab())  return false;
302         if (! cap.grab())  return false;
303         if (! cap.grab())  return false;
304         if (! cap.grab())  return false;
305         if (! cap.retrieve(image)) return false;
306     }
308     // scale to network input size 1024 x 512
309     Mat s_image, bgr_frames[3];
310     orig_width  = image.cols;
311     orig_height = image.rows;
312     cv::resize(image, s_image,
313                Size(configuration.inWidth, configuration.inHeight),
314                0, 0, cv::INTER_AREA);
315     cv::split(s_image, bgr_frames);
316     memcpy(frame_buffer,                bgr_frames[0].ptr(), channel_size);
317     memcpy(frame_buffer+1*channel_size, bgr_frames[1].ptr(), channel_size);
318     memcpy(frame_buffer+2*channel_size, bgr_frames[2].ptr(), channel_size);
319     return true;
322 // Create Overlay mask for pixel-level segmentation
323 void CreateMask(uchar *classes, uchar *mb, uchar *mg, uchar* mr,
324                 int channel_size)
326     for (int i = 0; i < channel_size; i++)
327     {
328         object_class_t *object_class = GetObjectClass(object_class_table,
329                                                       classes[i]);
330         mb[i] = object_class->color.blue;
331         mg[i] = object_class->color.green;
332         mr[i] = object_class->color.red;
333     }
336 // Create frame overlayed with pixel-level segmentation
337 bool WriteFrameOutput(const ExecutionObject &eo,
338                       const Configuration& configuration)
340     unsigned char *out = (unsigned char *) eo.GetOutputBufferPtr();
341     int out_size       = eo.GetOutputBufferSizeInBytes();
342     int width          = configuration.inWidth;
343     int height         = configuration.inHeight;
344     int channel_size   = width * height;
346     Mat mask, frame, blend, r_blend, bgr[3];
347     // Create overlay mask
348     bgr[0] = Mat(height, width, CV_8UC(1));
349     bgr[1] = Mat(height, width, CV_8UC(1));
350     bgr[2] = Mat(height, width, CV_8UC(1));
351     CreateMask(out, bgr[0].ptr(), bgr[1].ptr(), bgr[2].ptr(), channel_size);
352     cv::merge(bgr, 3, mask);
354     // Asseembly original frame
355     unsigned char *in = (unsigned char *) eo.GetInputBufferPtr();
356     bgr[0] = Mat(height, width, CV_8UC(1), in);
357     bgr[1] = Mat(height, width, CV_8UC(1), in + channel_size);
358     bgr[2] = Mat(height, width, CV_8UC(1), in + channel_size*2);
359     cv::merge(bgr, 3, frame);
361     // Create overlayed frame
362     cv::addWeighted(frame, 0.7, mask, 0.3, 0.0, blend);
364     cv::resize(blend, r_blend, Size(orig_width, orig_height));
365     if (is_camera_input)
366     {
367         cv::imshow("Segmentation", r_blend);
368         waitKey(1);
369     }
370     else
371     {
372         int frame_index = eo.GetFrameIndex();
373         char outfile_name[64];
374         if (is_preprocessed_input)
375         {
376             snprintf(outfile_name, 64, "frame_%d.png", frame_index);
377             cv::imwrite(outfile_name, frame);
378             printf("Saving frame %d to: %s\n", frame_index, outfile_name);
379         }
381         snprintf(outfile_name, 64, "overlay_%d.png", frame_index);
382         cv::imwrite(outfile_name, r_blend);
383         printf("Saving frame %d overlayed with segmentation to: %s\n",
384                frame_index, outfile_name);
385     }
387     return true;
391 void ProcessArgs(int argc, char *argv[], std::string& config,
392                  int& num_devices, DeviceType& device_type,
393                  std::string& input_file)
395     const struct option long_options[] =
396     {
397         {"config",      required_argument, 0, 'c'},
398         {"num_devices", required_argument, 0, 'n'},
399         {"device_type", required_argument, 0, 't'},
400         {"image_file",  required_argument, 0, 'i'},
401         {"help",        no_argument,       0, 'h'},
402         {"verbose",     no_argument,       0, 'v'},
403         {0, 0, 0, 0}
404     };
406     int option_index = 0;
408     while (true)
409     {
410         int c = getopt_long(argc, argv, "c:n:t:i:hv", long_options, &option_index);
412         if (c == -1)
413             break;
415         switch (c)
416         {
417             case 'c': config = optarg;
418                       break;
420             case 'n': num_devices = atoi(optarg);
421                       assert (num_devices > 0 && num_devices <= 4);
422                       break;
424             case 't': if (*optarg == 'e')
425                           device_type = DeviceType::DLA;
426                       else if (*optarg == 'd')
427                           device_type = DeviceType::DSP;
428                       else
429                       {
430                           std::cerr << "Invalid argument to -t, only e or d"
431                                        " allowed" << std::endl;
432                           exit(EXIT_FAILURE);
433                       }
434                       break;
436             case 'i': input_file = optarg;
437                       break;
439             case 'v': __TI_show_debug_ = true;
440                       break;
442             case 'h': DisplayHelp();
443                       exit(EXIT_SUCCESS);
444                       break;
446             case '?': // Error in getopt_long
447                       exit(EXIT_FAILURE);
448                       break;
450             default:
451                       std::cerr << "Unsupported option: " << c << std::endl;
452                       break;
453         }
454     }
457 void DisplayHelp()
459     std::cout << "Usage: segmentation\n"
460                  "  Will run segmentation network to perform pixel-level"
461                  " classification.\n  Use -c to run a different"
462                  "  segmentation network. Default is jseg21_tiscapes.\n"
463                  "Optional arguments:\n"
464                  " -c <config>          Valid configs: jseg21_tiscapes, jseg21\n"
465                  " -n <number of cores> Number of cores to use (1 - 4)\n"
466                  " -t <d|e>             Type of core. d -> DSP, e -> DLA\n"
467                  " -i <image>           Path to the image file\n"
468                  "                      Default are 3 frames in testvecs\n"
469                  " -i camera            Use camera as input\n"
470                  " -v                   Verbose output during execution\n"
471                  " -h                   Help\n";