Merge branch 'release/v01.03.00'
[tidl/tidl-api.git] / examples / ssd_multibox / main.cpp
1 /******************************************************************************
2  * Copyright (c) 2018, Texas Instruments Incorporated - http://www.ti.com/
3  *   All rights reserved.
4  *
5  *   Redistribution and use in source and binary forms, with or without
6  *   modification, are permitted provided that the following conditions are met:
7  *       * Redistributions of source code must retain the above copyright
8  *         notice, this list of conditions and the following disclaimer.
9  *       * Redistributions in binary form must reproduce the above copyright
10  *         notice, this list of conditions and the following disclaimer in the
11  *         documentation and/or other materials provided with the distribution.
12  *       * Neither the name of Texas Instruments Incorporated nor the
13  *         names of its contributors may be used to endorse or promote products
14  *         derived from this software without specific prior written permission.
15  *
16  *   THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
17  *   AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
18  *   IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
19  *   ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE
20  *   LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
21  *   CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
22  *   SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
23  *   INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
24  *   CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
25  *   ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF
26  *   THE POSSIBILITY OF SUCH DAMAGE.
27  *****************************************************************************/
28 #include <signal.h>
29 #include <iostream>
30 #include <iomanip>
31 #include <fstream>
32 #include <cassert>
33 #include <string>
34 #include <functional>
35 #include <algorithm>
36 #include <time.h>
37 #include <unistd.h>
39 #include <queue>
40 #include <vector>
41 #include <cstdio>
42 #include <string>
43 #include <chrono>
45 #include "executor.h"
46 #include "execution_object.h"
47 #include "execution_object_pipeline.h"
48 #include "configuration.h"
49 #include "../common/object_classes.h"
50 #include "../common/utils.h"
51 #include "../common/video_utils.h"
53 using namespace std;
54 using namespace tidl;
55 using namespace cv;
58 #define NUM_VIDEO_FRAMES  100
59 #define DEFAULT_CONFIG    "jdetnet_voc"
60 #define DEFAULT_INPUT     "../test/testvecs/input/horse_768x320.y"
61 #define DEFAULT_INPUT_FRAMES (1)
62 #define DEFAULT_OBJECT_CLASSES_LIST_FILE "./jdetnet_voc_objects.json"
63 #define DEFAULT_OUTPUT_PROB_THRESHOLD  25
65 /* Enable this macro to record individual output files and */
66 /* resized, cropped network input files                    */
67 //#define DEBUG_FILES
69 std::unique_ptr<ObjectClasses> object_classes;
70 uint32_t orig_width;
71 uint32_t orig_height;
72 uint32_t num_frames_file;
74 bool RunConfiguration(const cmdline_opts_t& opts);
75 Executor* CreateExecutor(DeviceType dt, uint32_t num, const Configuration& c,
76                          int layers_group_id);
77 bool ReadFrame(ExecutionObjectPipeline& eop, uint32_t frame_idx,
78                const Configuration& c, const cmdline_opts_t& opts,
79                VideoCapture &cap, ifstream &ifs);
80 bool WriteFrameOutput(const ExecutionObjectPipeline& eop,
81                       const Configuration& c, const cmdline_opts_t& opts,
82                       float confidence_value);
83 static void DisplayHelp();
85 /***************************************************************/
86 /* Slider to control detection confidence level                */
87 /***************************************************************/
88 static void on_trackbar( int slider_id, void *inst )
89 {
90   //This function is invoked on every slider move.
91   //No action required, since prob_slider is automatically updated.
92   //But, for any additional operation on slider move, this is the place to insert code.
93 }
96 int main(int argc, char *argv[])
97 {
98     // Catch ctrl-c to ensure a clean exit
99     signal(SIGABRT, exit);
100     signal(SIGTERM, exit);
102     // If there are no devices capable of offloading TIDL on the SoC, exit
103     uint32_t num_eves = Executor::GetNumDevices(DeviceType::EVE);
104     uint32_t num_dsps = Executor::GetNumDevices(DeviceType::DSP);
105     if (num_eves == 0 || num_dsps == 0)
106     {
107         cout << "ssd_multibox requires both EVE and DSP for execution." << endl;
108         return EXIT_SUCCESS;
109     }
111     // Process arguments
112     cmdline_opts_t opts;
113     opts.config = DEFAULT_CONFIG;
114     opts.object_classes_list_file = DEFAULT_OBJECT_CLASSES_LIST_FILE;
115     opts.num_eves = 1;
116     opts.num_dsps = 1;
117     opts.input_file = DEFAULT_INPUT;
118     opts.output_prob_threshold = DEFAULT_OUTPUT_PROB_THRESHOLD;
119     if (! ProcessArgs(argc, argv, opts))
120     {
121         DisplayHelp();
122         exit(EXIT_SUCCESS);
123     }
124     assert(opts.num_dsps != 0 && opts.num_eves != 0);
125     if (opts.num_frames == 0)
126         opts.num_frames = (opts.is_camera_input || opts.is_video_input) ?
127                           NUM_VIDEO_FRAMES :
128                           ((opts.input_file == DEFAULT_INPUT) ?
129                            DEFAULT_INPUT_FRAMES : 1);
130     cout << "Input: " << opts.input_file << endl;
132     // Get object classes list
133     object_classes = std::unique_ptr<ObjectClasses>(
134                              new ObjectClasses(opts.object_classes_list_file));
135     if (object_classes->GetNumClasses() == 0)
136     {
137         cout << "No object classes defined for this config." << endl;
138         return EXIT_FAILURE;
139     }
141     // Run network
142     bool status = RunConfiguration(opts);
143     if (!status)
144     {
145         cout << "ssd_multibox FAILED" << endl;
146         return EXIT_FAILURE;
147     }
149     cout << "ssd_multibox PASSED" << endl;
150     return EXIT_SUCCESS;
153 bool RunConfiguration(const cmdline_opts_t& opts)
155     int prob_slider     = opts.output_prob_threshold;
156     // Read the TI DL configuration file
157     Configuration c;
158     std::string config_file = "../test/testvecs/config/infer/tidl_config_"
159                               + opts.config + ".txt";
160     bool status = c.ReadFromFile(config_file);
161     if (!status)
162     {
163         cerr << "Error in configuration file: " << config_file << endl;
164         return false;
165     }
166     c.enableApiTrace = opts.verbose;
167     // setup camera/video input
168     VideoCapture cap;
169     if (! SetVideoInputOutput(cap, opts, "SSD_Multibox"))  return false;
171     if (opts.is_camera_input || opts.is_video_input)
172     {
173         std::string TrackbarName("Confidence(%):");
174         createTrackbar( TrackbarName.c_str(), "SSD_Multibox",
175                         &prob_slider, 100, on_trackbar );
176         std::cout << TrackbarName << std::endl;
177     }
179     // setup preprocessed input
180     ifstream ifs;
181     if (opts.is_preprocessed_input)
182     {
183         ifs.open(opts.input_file, ios::binary | ios::ate);
184         if (! ifs.good())
185         {
186             cerr << "Cannot open " << opts.input_file << endl;
187             return false;
188         }
189         num_frames_file = ((int) ifs.tellg()) /
190                           (c.inWidth * c.inHeight * c.inNumChannels);
191     }
193     try
194     {
195         // Create Executors with the approriate core type, number of cores
196         // and configuration specified
197         // EVE will run layersGroupId 1 in the network, while
198         // DSP will run layersGroupId 2 in the network
199         Executor* e_eve = CreateExecutor(DeviceType::EVE, opts.num_eves, c, 1);
200         Executor* e_dsp = CreateExecutor(DeviceType::DSP, opts.num_dsps, c, 2);
202         // Construct ExecutionObjectPipeline that utilizes multiple
203         // ExecutionObjects to process a single frame, each ExecutionObject
204         // processes one layerGroup of the network
205         //
206         // Pipeline depth can enable more optimized pipeline execution:
207         // Given one EVE and one DSP as an example, with different
208         //     pipeline_depth, we have different execution behavior:
209         // If pipeline_depth is set to 1,
210         //    we create one EOP: eop0 (eve0, dsp0)
211         //    pipeline execution of multiple frames over time is as follows:
212         //    --------------------- time ------------------->
213         //    eop0: [eve0...][dsp0]
214         //    eop0:                [eve0...][dsp0]
215         //    eop0:                               [eve0...][dsp0]
216         //    eop0:                                              [eve0...][dsp0]
217         // If pipeline_depth is set to 2,
218         //    we create two EOPs: eop0 (eve0, dsp0), eop1(eve0, dsp0)
219         //    pipeline execution of multiple frames over time is as follows:
220         //    --------------------- time ------------------->
221         //    eop0: [eve0...][dsp0]
222         //    eop1:          [eve0...][dsp0]
223         //    eop0:                   [eve0...][dsp0]
224         //    eop1:                            [eve0...][dsp0]
225         // Additional benefit of setting pipeline_depth to 2 is that
226         //    it can also overlap host ReadFrame() with device processing:
227         //    --------------------- time ------------------->
228         //    eop0: [RF][eve0...][dsp0]
229         //    eop1:     [RF]     [eve0...][dsp0]
230         //    eop0:                    [RF][eve0...][dsp0]
231         //    eop1:                             [RF][eve0...][dsp0]
232         vector<ExecutionObjectPipeline *> eops;
233         uint32_t pipeline_depth = 2;  // 2 EOs in EOP -> depth 2
234         for (uint32_t j = 0; j < pipeline_depth; j++)
235             for (uint32_t i = 0; i < max(opts.num_eves, opts.num_dsps); i++)
236                 eops.push_back(new ExecutionObjectPipeline(
237                       {(*e_eve)[i%opts.num_eves], (*e_dsp)[i%opts.num_dsps]}));
238         uint32_t num_eops = eops.size();
240         // Allocate input/output memory for each EOP
241         AllocateMemory(eops);
243         chrono::time_point<chrono::steady_clock> tloop0, tloop1;
244         tloop0 = chrono::steady_clock::now();
246         // Process frames with available eops in a pipelined manner
247         // additional num_eops iterations to flush pipeline (epilogue)
248         for (uint32_t frame_idx = 0;
249              frame_idx < opts.num_frames + num_eops; frame_idx++)
250         {
251             ExecutionObjectPipeline* eop = eops[frame_idx % num_eops];
253             // Wait for previous frame on the same eop to finish processing
254             if (eop->ProcessFrameWait())
255             {
256                 WriteFrameOutput(*eop, c, opts, (float)prob_slider);
257             }
259             // Read a frame and start processing it with current eo
260             if (ReadFrame(*eop, frame_idx, c, opts, cap, ifs))
261                 eop->ProcessFrameStartAsync();
262         }
264         tloop1 = chrono::steady_clock::now();
265         chrono::duration<float> elapsed = tloop1 - tloop0;
266         cout << "Loop total time (including read/write/opencv/print/etc): "
267                   << setw(6) << setprecision(4)
268                   << (elapsed.count() * 1000) << "ms" << endl;
270         FreeMemory(eops);
271         for (auto eop : eops)  delete eop;
272         delete e_eve;
273         delete e_dsp;
274     }
275     catch (tidl::Exception &e)
276     {
277         cerr << e.what() << endl;
278         status = false;
279     }
281     return status;
284 // Create an Executor with the specified type and number of EOs
285 Executor* CreateExecutor(DeviceType dt, uint32_t num, const Configuration& c,
286                          int layers_group_id)
288     if (num == 0) return nullptr;
290     DeviceIds ids;
291     for (uint32_t i = 0; i < num; i++)
292         ids.insert(static_cast<DeviceId>(i));
294     return new Executor(dt, ids, c, layers_group_id);
297 bool ReadFrame(ExecutionObjectPipeline& eop, uint32_t frame_idx,
298                const Configuration& c, const cmdline_opts_t& opts,
299                VideoCapture &cap, ifstream &ifs)
301     if ((uint32_t)frame_idx >= opts.num_frames)
302         return false;
304     eop.SetFrameIndex(frame_idx);
306     char*  frame_buffer = eop.GetInputBufferPtr();
307     assert (frame_buffer != nullptr);
308     int channel_size = c.inWidth * c.inHeight;
309     int frame_size   = channel_size * c.inNumChannels;
311     Mat image;
312     if (!opts.is_camera_input && !opts.is_video_input)
313     {
314         if (opts.is_preprocessed_input)
315         {
316             orig_width  = c.inWidth;
317             orig_height = c.inHeight;
318             ifs.seekg((frame_idx % num_frames_file) * frame_size);
319             ifs.read(frame_buffer, frame_size);
320             return ifs.good();
321         }
322         else
323         {
324             image = cv::imread(opts.input_file, CV_LOAD_IMAGE_COLOR);
325             if (image.empty())
326             {
327                 cerr << "Unable to read from: " << opts.input_file << endl;
328                 return false;
329             }
330         }
331     }
332     else
333     {
334         if(opts.is_camera_input)
335         {
336            if (! cap.grab()) return false;
337            if (! cap.retrieve(image)) return false;
338         }
339         else
340         { // Video clip
341            if (cap.grab())
342            {
343              if (! cap.retrieve(image)) return false;
344            } else {
345              //Rewind!
346              std::cout << "Video clip rewinded!" << std::endl;
347              cap.set(CAP_PROP_POS_FRAMES, 0);
348              if (! cap.grab()) return false;
349              if (! cap.retrieve(image)) return false;
350            }
351         }
352     }
354     // Scale to network input size:
355     Mat s_image, bgr_frames[3];
356     orig_width  = image.cols;
357     orig_height = image.rows;
358     if (!opts.is_camera_input && !opts.is_video_input)
359     {
360         cv::resize(image, s_image, Size(c.inWidth, c.inHeight),
361                    0, 0, cv::INTER_AREA);
362     }
363     else
364     {
365         // Preserve aspect ratio, by doing central cropping
366         // Choose vertical or horizontal central cropping
367         // based on dimension reduction
368         if(orig_width > orig_height)
369         {
370             float change_width  = (float)c.inWidth / (float)orig_width;
371             float change_height = (float)c.inHeight / (float)orig_height;
372             if(change_width < change_height)
373             {
374                 // E.g. for 1920x1080->512x512, we first crop central part
375                 // roi(420, 0, 1080, 1080), then resize to (512x512)
376                 int offset_x = (int)round(0.5 * ((float)orig_width -
377                   ((float)orig_height * (float)c.inWidth / (float)c.inHeight)));
378                 cv::resize(image(Rect(offset_x, 0, orig_width - 2 * offset_x,
379                                       orig_height)), s_image,
380                            Size(c.inWidth, c.inHeight), 0, 0, cv::INTER_AREA);
381             } else {
382                 // E.g. for 1920x1080->768x320, we first crop central part
383                 // roi(0, 140, 1920, 800), then resize to (768x320)
384                 int offset_y = (int)round(0.5 * ((float)orig_height -
385                   ((float)orig_width * (float)c.inHeight / (float)c.inWidth)));
386                 cv::resize(image(Rect(0, offset_y, orig_width,
387                                       orig_height - 2 * offset_y)), s_image,
388                            Size(c.inWidth, c.inHeight), 0, 0, cv::INTER_AREA);
389             }
390         } else {
391           // E.g. for 540x960->512x512, we first crop central part
392           //      roi(0, 210, 540, 540), then resize to (512x512)
393           // E.g. for 540x960->768x320, we first crop central part
394           //      roi(0, 367, 540, 225), then resize to (768x320)
395           int offset_y = (int)round(0.5 * ((float)orig_height -
396               ((float)orig_width * (float)c.inHeight / (float)c.inWidth)));
397           cv::resize(image(Rect(0, offset_y, orig_width, orig_height -
398                                 2 * offset_y)), s_image,
399                      Size(c.inWidth, c.inHeight), 0, 0, cv::INTER_AREA);
400         }
401     }
403     #ifdef DEBUG_FILES
404     {
405         // Image files can be converted into video using, example script
406         // (on desktop Ubuntu, with ffmpeg installed):
407         // ffmpeg -i netin_%04d.png -vf "scale=(iw*sar)*max(768/(iw*sar)\,320/ih):ih*max(768/(iw*sar)\,320/ih), crop=768:320" -b:v 4000k out.mp4
408         // Update width 768, height 320, if necessary
409         char netin_name[80];
410         sprintf(netin_name, "netin_%04d.png", frame_idx);
411         cv::imwrite(netin_name, s_image);
412         std::cout << "Video input, width:" << orig_width << " height:"
413                   << orig_height << " Network width:" << c.inWidth
414                   << " height:" << c.inHeight << std::endl;
415     }
416     #endif
418     cv::split(s_image, bgr_frames);
419     memcpy(frame_buffer,                bgr_frames[0].ptr(), channel_size);
420     memcpy(frame_buffer+1*channel_size, bgr_frames[1].ptr(), channel_size);
421     memcpy(frame_buffer+2*channel_size, bgr_frames[2].ptr(), channel_size);
422     return true;
425 // Create frame with boxes drawn around classified objects
426 bool WriteFrameOutput(const ExecutionObjectPipeline& eop,
427                       const Configuration& c, const cmdline_opts_t& opts,
428                       float confidence_value)
430     // Asseembly original frame
431     int width  = c.inWidth;
432     int height = c.inHeight;
433     int channel_size = width * height;
434     Mat frame, bgr[3];
436     unsigned char *in = (unsigned char *) eop.GetInputBufferPtr();
437     bgr[0] = Mat(height, width, CV_8UC(1), in);
438     bgr[1] = Mat(height, width, CV_8UC(1), in + channel_size);
439     bgr[2] = Mat(height, width, CV_8UC(1), in + channel_size*2);
440     cv::merge(bgr, 3, frame);
442     int frame_index = eop.GetFrameIndex();
443     char outfile_name[64];
444     if (opts.is_preprocessed_input)
445     {
446         snprintf(outfile_name, 64, "frame_%d.png", frame_index);
447         cv::imwrite(outfile_name, frame);
448         printf("Saving frame %d to: %s\n", frame_index, outfile_name);
449     }
451     // Draw boxes around classified objects
452     float *out = (float *) eop.GetOutputBufferPtr();
453     int num_floats = eop.GetOutputBufferSizeInBytes() / sizeof(float);
454     for (int i = 0; i < num_floats / 7; i++)
455     {
456         int index = (int)    out[i * 7 + 0];
457         if (index < 0)  break;
459         float score =        out[i * 7 + 2];
460         if (score * 100 < confidence_value)  continue;
462         int   label = (int)  out[i * 7 + 1];
463         int   xmin  = (int) (out[i * 7 + 3] * width);
464         int   ymin  = (int) (out[i * 7 + 4] * height);
465         int   xmax  = (int) (out[i * 7 + 5] * width);
466         int   ymax  = (int) (out[i * 7 + 6] * height);
468         const ObjectClass& object_class = object_classes->At(label);
470         if(opts.verbose) {
471             printf("%2d: (%d, %d) -> (%d, %d): %s, score=%f\n",
472                i, xmin, ymin, xmax, ymax, object_class.label.c_str(), score);
473         }
475         if (xmin < 0)       xmin = 0;
476         if (ymin < 0)       ymin = 0;
477         if (xmax > width)   xmax = width;
478         if (ymax > height)  ymax = height;
479         cv::rectangle(frame, Point(xmin, ymin), Point(xmax, ymax),
480                       Scalar(object_class.color.blue,
481                              object_class.color.green,
482                              object_class.color.red), 2);
483     }
485     if (opts.is_camera_input || opts.is_video_input)
486     {
487         cv::imshow("SSD_Multibox", frame);
488 #ifdef DEBUG_FILES
489         // Image files can be converted into video using, example script
490         // (on desktop Ubuntu, with ffmpeg installed):
491         // ffmpeg -i multibox_%04d.png -vf "scale=(iw*sar)*max(768/(iw*sar)\,320/ih):ih*max(768/(iw*sar)\,320/ih), crop=768:320" -b:v 4000k out.mp4
492         // Update width 768, height 320, if necessary
493         snprintf(outfile_name, 64, "multibox_%04d.png", frame_index);
494         cv::imwrite(outfile_name, r_frame);
495 #endif
496         waitKey(1);
497     }
498     else
499     {
500         // Resize to output width/height, keep aspect ratio
501         Mat r_frame;
502         uint32_t output_width = opts.output_width;
503         if (output_width == 0)  output_width = orig_width;
504         uint32_t output_height = (output_width*1.0f) / orig_width * orig_height;
505         cv::resize(frame, r_frame, Size(output_width, output_height));
507         snprintf(outfile_name, 64, "multibox_%d.png", frame_index);
508         cv::imwrite(outfile_name, frame);
509         printf("Saving frame %d with SSD multiboxes to: %s\n",
510                frame_index, outfile_name);
511     }
513     return true;
516 void DisplayHelp()
518     std::cout <<
519     "Usage: ssd_multibox\n"
520     "  Will run partitioned ssd_multibox network to perform "
521     "multi-objects detection\n"
522     "  and classification.  First part of network "
523     "(layersGroupId 1) runs on EVE,\n"
524     "  second part (layersGroupId 2) runs on DSP.\n"
525     "  Use -c to run a different segmentation network.  Default is jdetnet_voc.\n"
526     "Optional arguments:\n"
527     " -c <config>          Valid configs: jdetnet_voc, jdetnet \n"
528     " -d <number>          Number of dsp cores to use\n"
529     " -e <number>          Number of eve cores to use\n"
530     " -i <image>           Path to the image file as input\n"
531     "                      Default are 9 frames in testvecs\n"
532     " -i camera<number>    Use camera as input\n"
533     "                      video input port: /dev/video<number>\n"
534     " -i <name>.{mp4,mov,avi}  Use video file as input\n"
535     " -l <objects_list>    Path to the object classes list file\n"
536     " -f <number>          Number of frames to process\n"
537     " -w <number>          Output image/video width\n"
538     " -p <number>          Output probability threshold in percentage\n"
539     "                      Default is 25 percent or higher\n"
540     " -v                   Verbose output during execution\n"
541     " -h                   Help\n";