Merge branch 'hotfix/v01.05.01'
[tidl/tidl-api.git] / examples / ssd_multibox / main.cpp
1 /******************************************************************************
2  * Copyright (c) 2018, Texas Instruments Incorporated - http://www.ti.com/
3  *   All rights reserved.
4  *
5  *   Redistribution and use in source and binary forms, with or without
6  *   modification, are permitted provided that the following conditions are met:
7  *       * Redistributions of source code must retain the above copyright
8  *         notice, this list of conditions and the following disclaimer.
9  *       * Redistributions in binary form must reproduce the above copyright
10  *         notice, this list of conditions and the following disclaimer in the
11  *         documentation and/or other materials provided with the distribution.
12  *       * Neither the name of Texas Instruments Incorporated nor the
13  *         names of its contributors may be used to endorse or promote products
14  *         derived from this software without specific prior written permission.
15  *
16  *   THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
17  *   AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
18  *   IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
19  *   ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE
20  *   LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
21  *   CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
22  *   SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
23  *   INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
24  *   CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
25  *   ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF
26  *   THE POSSIBILITY OF SUCH DAMAGE.
27  *****************************************************************************/
28 #include <signal.h>
29 #include <iostream>
30 #include <iomanip>
31 #include <fstream>
32 #include <cassert>
33 #include <string>
34 #include <functional>
35 #include <algorithm>
36 #include <time.h>
37 #include <unistd.h>
39 #include <queue>
40 #include <vector>
41 #include <cstdio>
42 #include <string>
43 #include <chrono>
45 #include "executor.h"
46 #include "execution_object.h"
47 #include "execution_object_pipeline.h"
48 #include "configuration.h"
49 #include "../common/object_classes.h"
50 #include "../common/utils.h"
51 #include "../common/video_utils.h"
53 using namespace std;
54 using namespace tidl;
55 using namespace cv;
58 #define NUM_VIDEO_FRAMES  100
59 #define DEFAULT_CONFIG    "jdetnet_voc"
60 #define DEFAULT_INPUT     "../test/testvecs/input/horse_768x320.y"
61 #define DEFAULT_INPUT_FRAMES (1)
62 #define DEFAULT_OBJECT_CLASSES_LIST_FILE "./jdetnet_voc_objects.json"
63 #define DEFAULT_OUTPUT_PROB_THRESHOLD  25
65 /* Enable this macro to record individual output files and */
66 /* resized, cropped network input files                    */
67 //#define DEBUG_FILES
69 std::unique_ptr<ObjectClasses> object_classes;
70 uint32_t orig_width;
71 uint32_t orig_height;
72 uint32_t num_frames_file;
74 bool RunConfiguration(const cmdline_opts_t& opts);
75 Executor* CreateExecutor(DeviceType dt, uint32_t num, const Configuration& c,
76                          int layers_group_id);
77 bool ReadFrame(ExecutionObjectPipeline& eop, uint32_t frame_idx,
78                const Configuration& c, const cmdline_opts_t& opts,
79                VideoCapture &cap, ifstream &ifs);
80 bool WriteFrameOutput(const ExecutionObjectPipeline& eop,
81                       const Configuration& c, const cmdline_opts_t& opts,
82                       float confidence_value);
83 static void DisplayHelp();
85 /***************************************************************/
86 /* Slider to control detection confidence level                */
87 /***************************************************************/
88 static void on_trackbar( int slider_id, void *inst )
89 {
90   //This function is invoked on every slider move.
91   //No action required, since prob_slider is automatically updated.
92   //But, for any additional operation on slider move, this is the place to insert code.
93 }
96 int main(int argc, char *argv[])
97 {
98     // Catch ctrl-c to ensure a clean exit
99     signal(SIGABRT, exit);
100     signal(SIGTERM, exit);
102     // If there are no devices capable of offloading TIDL on the SoC, exit
103     uint32_t num_eves = Executor::GetNumDevices(DeviceType::EVE);
104     uint32_t num_dsps = Executor::GetNumDevices(DeviceType::DSP);
105     if (num_eves == 0 && num_dsps == 0)
106     {
107         cout << "ssd_multibox requires EVE or DSP for execution." << endl;
108         return EXIT_SUCCESS;
109     }
111     // Process arguments
112     cmdline_opts_t opts;
113     opts.config = DEFAULT_CONFIG;
114     opts.object_classes_list_file = DEFAULT_OBJECT_CLASSES_LIST_FILE;
115     opts.num_eves = num_eves > 0 ? 1 : 0;
116     opts.num_dsps = num_dsps > 0 ? 1 : 0;
117     opts.input_file = DEFAULT_INPUT;
118     opts.output_prob_threshold = DEFAULT_OUTPUT_PROB_THRESHOLD;
119     if (! ProcessArgs(argc, argv, opts))
120     {
121         DisplayHelp();
122         exit(EXIT_SUCCESS);
123     }
124     assert(opts.num_dsps != 0 || opts.num_eves != 0);
125     if (opts.num_frames == 0)
126         opts.num_frames = (opts.is_camera_input || opts.is_video_input) ?
127                           NUM_VIDEO_FRAMES :
128                           ((opts.input_file == DEFAULT_INPUT) ?
129                            DEFAULT_INPUT_FRAMES : 1);
130     cout << "Input: " << opts.input_file << endl;
132     // Get object classes list
133     object_classes = std::unique_ptr<ObjectClasses>(
134                              new ObjectClasses(opts.object_classes_list_file));
135     if (object_classes->GetNumClasses() == 0)
136     {
137         cout << "No object classes defined for this config." << endl;
138         return EXIT_FAILURE;
139     }
141     // Run network
142     bool status = RunConfiguration(opts);
143     if (!status)
144     {
145         cout << "ssd_multibox FAILED" << endl;
146         return EXIT_FAILURE;
147     }
149     cout << "ssd_multibox PASSED" << endl;
150     return EXIT_SUCCESS;
153 bool RunConfiguration(const cmdline_opts_t& opts)
155     int prob_slider     = opts.output_prob_threshold;
156     // Read the TI DL configuration file
157     Configuration c;
158     std::string config_file = "../test/testvecs/config/infer/tidl_config_"
159                               + opts.config + ".txt";
160     bool status = c.ReadFromFile(config_file);
161     if (!status)
162     {
163         cerr << "Error in configuration file: " << config_file << endl;
164         return false;
165     }
166     c.enableApiTrace = opts.verbose;
167     if (opts.num_eves == 0 || opts.num_dsps == 0)
168         c.runFullNet = true;
170     // setup camera/video input
171     VideoCapture cap;
172     if (! SetVideoInputOutput(cap, opts, "SSD_Multibox"))  return false;
174     if (opts.is_camera_input || opts.is_video_input)
175     {
176         std::string TrackbarName("Confidence(%):");
177         createTrackbar( TrackbarName.c_str(), "SSD_Multibox",
178                         &prob_slider, 100, on_trackbar );
179         std::cout << TrackbarName << std::endl;
180     }
182     // setup preprocessed input
183     ifstream ifs;
184     if (opts.is_preprocessed_input)
185     {
186         ifs.open(opts.input_file, ios::binary | ios::ate);
187         if (! ifs.good())
188         {
189             cerr << "Cannot open " << opts.input_file << endl;
190             return false;
191         }
192         num_frames_file = ((int) ifs.tellg()) /
193                           (c.inWidth * c.inHeight * c.inNumChannels);
194     }
196     try
197     {
198         // Create Executors with the approriate core type, number of cores
199         // and configuration specified
200         // EVE will run layersGroupId 1 in the network, while
201         // DSP will run layersGroupId 2 in the network
202         Executor* e_eve = CreateExecutor(DeviceType::EVE, opts.num_eves, c, 1);
203         Executor* e_dsp = CreateExecutor(DeviceType::DSP, opts.num_dsps, c, 2);
204         vector<ExecutionObjectPipeline *> eops;
206         if (e_eve != nullptr && e_dsp != nullptr)
207         {
208             // Construct ExecutionObjectPipeline that utilizes multiple
209             // ExecutionObjects to process a single frame, each ExecutionObject
210             // processes one layerGroup of the network
211             //
212             // Pipeline depth can enable more optimized pipeline execution:
213             // Given one EVE and one DSP as an example, with different
214             //     pipeline_depth, we have different execution behavior:
215             // If pipeline_depth is set to 1,
216             //    we create one EOP: eop0 (eve0, dsp0)
217             //    pipeline execution of multiple frames over time is as follows:
218             //    --------------------- time ------------------->
219             //    eop0: [eve0...][dsp0]
220             //    eop0:                [eve0...][dsp0]
221             //    eop0:                               [eve0...][dsp0]
222             //    eop0:                                              [eve0...][dsp0]
223             // If pipeline_depth is set to 2,
224             //    we create two EOPs: eop0 (eve0, dsp0), eop1(eve0, dsp0)
225             //    pipeline execution of multiple frames over time is as follows:
226             //    --------------------- time ------------------->
227             //    eop0: [eve0...][dsp0]
228             //    eop1:          [eve0...][dsp0]
229             //    eop0:                   [eve0...][dsp0]
230             //    eop1:                            [eve0...][dsp0]
231             // Additional benefit of setting pipeline_depth to 2 is that
232             //    it can also overlap host ReadFrame() with device processing:
233             //    --------------------- time ------------------->
234             //    eop0: [RF][eve0...][dsp0]
235             //    eop1:     [RF]     [eve0...][dsp0]
236             //    eop0:                    [RF][eve0...][dsp0]
237             //    eop1:                             [RF][eve0...][dsp0]
238             uint32_t pipeline_depth = 2;  // 2 EOs in EOP -> depth 2
239             for (uint32_t j = 0; j < pipeline_depth; j++)
240                 for (uint32_t i = 0; i < max(opts.num_eves, opts.num_dsps); i++)
241                     eops.push_back(new ExecutionObjectPipeline(
242                       {(*e_eve)[i%opts.num_eves], (*e_dsp)[i%opts.num_dsps]}));
243         }
244         else
245         {
246             // Construct ExecutionObjectPipeline that utilizes a
247             // ExecutionObject to process a single frame, each ExecutionObject
248             // processes the full network
249             //
250             // Use duplicate EOPs to do double buffering on frame input/output
251             //    because each EOP has its own set of input/output buffers,
252             //    so that host ReadFrame() can overlap device processing
253             // Use one EO as an example, with different buffer_factor,
254             //    we have different execution behavior:
255             // If buffer_factor is set to 1 -> single buffering
256             //    we create one EOP: eop0 (eo0)
257             //    pipeline execution of multiple frames over time is as follows:
258             //    --------------------- time ------------------->
259             //    eop0: [RF][eo0.....][WF]
260             //    eop0:                   [RF][eo0.....][WF]
261             //    eop0:                                     [RF][eo0.....][WF]
262             // If buffer_factor is set to 2 -> double buffering
263             //    we create two EOPs: eop0 (eo0), eop1(eo0)
264             //    pipeline execution of multiple frames over time is as follows:
265             //    --------------------- time ------------------->
266             //    eop0: [RF][eo0.....][WF]
267             //    eop1:     [RF]      [eo0.....][WF]
268             //    eop0:                   [RF]  [eo0.....][WF]
269             //    eop1:                             [RF]  [eo0.....][WF]
270             uint32_t buffer_factor = 2;  // set to 1 for single buffering
271             for (uint32_t j = 0; j < buffer_factor; j++)
272             {
273                 for (uint32_t i = 0; i < opts.num_eves; i++)
274                     eops.push_back(new ExecutionObjectPipeline({(*e_eve)[i]}));
275                 for (uint32_t i = 0; i < opts.num_dsps; i++)
276                     eops.push_back(new ExecutionObjectPipeline({(*e_dsp)[i]}));
277             }
278         }
279         uint32_t num_eops = eops.size();
281         // Allocate input/output memory for each EOP
282         AllocateMemory(eops);
284         chrono::time_point<chrono::steady_clock> tloop0, tloop1;
285         tloop0 = chrono::steady_clock::now();
287         // Process frames with available eops in a pipelined manner
288         // additional num_eops iterations to flush pipeline (epilogue)
289         for (uint32_t frame_idx = 0;
290              frame_idx < opts.num_frames + num_eops; frame_idx++)
291         {
292             ExecutionObjectPipeline* eop = eops[frame_idx % num_eops];
294             // Wait for previous frame on the same eop to finish processing
295             if (eop->ProcessFrameWait())
296                 WriteFrameOutput(*eop, c, opts, (float)prob_slider);
298             // Read a frame and start processing it with current eo
299             if (ReadFrame(*eop, frame_idx, c, opts, cap, ifs))
300                 eop->ProcessFrameStartAsync();
301         }
303         tloop1 = chrono::steady_clock::now();
304         chrono::duration<float> elapsed = tloop1 - tloop0;
305         cout << "Loop total time (including read/write/opencv/print/etc): "
306                   << setw(6) << setprecision(4)
307                   << (elapsed.count() * 1000) << "ms" << endl;
309         FreeMemory(eops);
310         for (auto eop : eops)  delete eop;
311         delete e_eve;
312         delete e_dsp;
313     }
314     catch (tidl::Exception &e)
315     {
316         cerr << e.what() << endl;
317         status = false;
318     }
320     return status;
323 // Create an Executor with the specified type and number of EOs
324 Executor* CreateExecutor(DeviceType dt, uint32_t num, const Configuration& c,
325                          int layers_group_id)
327     if (num == 0) return nullptr;
329     DeviceIds ids;
330     for (uint32_t i = 0; i < num; i++)
331         ids.insert(static_cast<DeviceId>(i));
333     Executor* e = new Executor(dt, ids, c, layers_group_id);
334     assert(e != nullptr);
335     return e;
338 bool ReadFrame(ExecutionObjectPipeline& eop, uint32_t frame_idx,
339                const Configuration& c, const cmdline_opts_t& opts,
340                VideoCapture &cap, ifstream &ifs)
342     if ((uint32_t)frame_idx >= opts.num_frames)
343         return false;
345     eop.SetFrameIndex(frame_idx);
347     char*  frame_buffer = eop.GetInputBufferPtr();
348     assert (frame_buffer != nullptr);
349     int channel_size = c.inWidth * c.inHeight;
350     int frame_size   = channel_size * c.inNumChannels;
352     Mat image;
353     if (!opts.is_camera_input && !opts.is_video_input)
354     {
355         if (opts.is_preprocessed_input)
356         {
357             orig_width  = c.inWidth;
358             orig_height = c.inHeight;
359             ifs.seekg((frame_idx % num_frames_file) * frame_size);
360             ifs.read(frame_buffer, frame_size);
361             return ifs.good();
362         }
363         else
364         {
365             image = cv::imread(opts.input_file, CV_LOAD_IMAGE_COLOR);
366             if (image.empty())
367             {
368                 cerr << "Unable to read from: " << opts.input_file << endl;
369                 return false;
370             }
371         }
372     }
373     else
374     {
375         if(opts.is_camera_input)
376         {
377            if (! cap.grab()) return false;
378            if (! cap.retrieve(image)) return false;
379         }
380         else
381         { // Video clip
382            if (cap.grab())
383            {
384              if (! cap.retrieve(image)) return false;
385            } else {
386              //Rewind!
387              std::cout << "Video clip rewinded!" << std::endl;
388              cap.set(CAP_PROP_POS_FRAMES, 0);
389              if (! cap.grab()) return false;
390              if (! cap.retrieve(image)) return false;
391            }
392         }
393     }
395     // Scale to network input size:
396     Mat s_image, bgr_frames[3];
397     orig_width  = image.cols;
398     orig_height = image.rows;
399     if (!opts.is_camera_input && !opts.is_video_input)
400     {
401         cv::resize(image, s_image, Size(c.inWidth, c.inHeight),
402                    0, 0, cv::INTER_AREA);
403     }
404     else
405     {
406         // Preserve aspect ratio, by doing central cropping
407         // Choose vertical or horizontal central cropping
408         // based on dimension reduction
409         if(orig_width > orig_height)
410         {
411             float change_width  = (float)c.inWidth / (float)orig_width;
412             float change_height = (float)c.inHeight / (float)orig_height;
413             if(change_width < change_height)
414             {
415                 // E.g. for 1920x1080->512x512, we first crop central part
416                 // roi(420, 0, 1080, 1080), then resize to (512x512)
417                 int offset_x = (int)round(0.5 * ((float)orig_width -
418                   ((float)orig_height * (float)c.inWidth / (float)c.inHeight)));
419                 cv::resize(image(Rect(offset_x, 0, orig_width - 2 * offset_x,
420                                       orig_height)), s_image,
421                            Size(c.inWidth, c.inHeight), 0, 0, cv::INTER_AREA);
422             } else {
423                 // E.g. for 1920x1080->768x320, we first crop central part
424                 // roi(0, 140, 1920, 800), then resize to (768x320)
425                 int offset_y = (int)round(0.5 * ((float)orig_height -
426                   ((float)orig_width * (float)c.inHeight / (float)c.inWidth)));
427                 cv::resize(image(Rect(0, offset_y, orig_width,
428                                       orig_height - 2 * offset_y)), s_image,
429                            Size(c.inWidth, c.inHeight), 0, 0, cv::INTER_AREA);
430             }
431         } else {
432           // E.g. for 540x960->512x512, we first crop central part
433           //      roi(0, 210, 540, 540), then resize to (512x512)
434           // E.g. for 540x960->768x320, we first crop central part
435           //      roi(0, 367, 540, 225), then resize to (768x320)
436           int offset_y = (int)round(0.5 * ((float)orig_height -
437               ((float)orig_width * (float)c.inHeight / (float)c.inWidth)));
438           cv::resize(image(Rect(0, offset_y, orig_width, orig_height -
439                                 2 * offset_y)), s_image,
440                      Size(c.inWidth, c.inHeight), 0, 0, cv::INTER_AREA);
441         }
442     }
444     #ifdef DEBUG_FILES
445     {
446         // Image files can be converted into video using, example script
447         // (on desktop Ubuntu, with ffmpeg installed):
448         // ffmpeg -i netin_%04d.png -vf "scale=(iw*sar)*max(768/(iw*sar)\,320/ih):ih*max(768/(iw*sar)\,320/ih), crop=768:320" -b:v 4000k out.mp4
449         // Update width 768, height 320, if necessary
450         char netin_name[80];
451         sprintf(netin_name, "netin_%04d.png", frame_idx);
452         cv::imwrite(netin_name, s_image);
453         std::cout << "Video input, width:" << orig_width << " height:"
454                   << orig_height << " Network width:" << c.inWidth
455                   << " height:" << c.inHeight << std::endl;
456     }
457     #endif
459     cv::split(s_image, bgr_frames);
460     memcpy(frame_buffer,                bgr_frames[0].ptr(), channel_size);
461     memcpy(frame_buffer+1*channel_size, bgr_frames[1].ptr(), channel_size);
462     memcpy(frame_buffer+2*channel_size, bgr_frames[2].ptr(), channel_size);
463     return true;
466 // Create frame with boxes drawn around classified objects
467 bool WriteFrameOutput(const ExecutionObjectPipeline& eop,
468                       const Configuration& c, const cmdline_opts_t& opts,
469                       float confidence_value)
471     // Asseembly original frame
472     int width  = c.inWidth;
473     int height = c.inHeight;
474     int channel_size = width * height;
475     Mat frame, bgr[3];
477     unsigned char *in = (unsigned char *) eop.GetInputBufferPtr();
478     bgr[0] = Mat(height, width, CV_8UC(1), in);
479     bgr[1] = Mat(height, width, CV_8UC(1), in + channel_size);
480     bgr[2] = Mat(height, width, CV_8UC(1), in + channel_size*2);
481     cv::merge(bgr, 3, frame);
483     int frame_index = eop.GetFrameIndex();
484     char outfile_name[64];
485     if (opts.is_preprocessed_input)
486     {
487         snprintf(outfile_name, 64, "frame_%d.png", frame_index);
488         cv::imwrite(outfile_name, frame);
489         printf("Saving frame %d to: %s\n", frame_index, outfile_name);
490     }
492     // Draw boxes around classified objects
493     float *out = (float *) eop.GetOutputBufferPtr();
494     int num_floats = eop.GetOutputBufferSizeInBytes() / sizeof(float);
495     for (int i = 0; i < num_floats / 7; i++)
496     {
497         int index = (int)    out[i * 7 + 0];
498         if (index < 0)  break;
500         float score =        out[i * 7 + 2];
501         if (score * 100 < confidence_value)  continue;
503         int   label = (int)  out[i * 7 + 1];
504         int   xmin  = (int) (out[i * 7 + 3] * width);
505         int   ymin  = (int) (out[i * 7 + 4] * height);
506         int   xmax  = (int) (out[i * 7 + 5] * width);
507         int   ymax  = (int) (out[i * 7 + 6] * height);
509         const ObjectClass& object_class = object_classes->At(label);
511         if(opts.verbose) {
512             printf("%2d: (%d, %d) -> (%d, %d): %s, score=%f\n",
513                i, xmin, ymin, xmax, ymax, object_class.label.c_str(), score);
514         }
516         if (xmin < 0)       xmin = 0;
517         if (ymin < 0)       ymin = 0;
518         if (xmax > width)   xmax = width;
519         if (ymax > height)  ymax = height;
520         cv::rectangle(frame, Point(xmin, ymin), Point(xmax, ymax),
521                       Scalar(object_class.color.blue,
522                              object_class.color.green,
523                              object_class.color.red), 2);
524     }
526     if (opts.is_camera_input || opts.is_video_input)
527     {
528         cv::imshow("SSD_Multibox", frame);
529 #ifdef DEBUG_FILES
530         // Image files can be converted into video using, example script
531         // (on desktop Ubuntu, with ffmpeg installed):
532         // ffmpeg -i multibox_%04d.png -vf "scale=(iw*sar)*max(768/(iw*sar)\,320/ih):ih*max(768/(iw*sar)\,320/ih), crop=768:320" -b:v 4000k out.mp4
533         // Update width 768, height 320, if necessary
534         snprintf(outfile_name, 64, "multibox_%04d.png", frame_index);
535         cv::imwrite(outfile_name, r_frame);
536 #endif
537         waitKey(1);
538     }
539     else
540     {
541         // Resize to output width/height, keep aspect ratio
542         Mat r_frame;
543         uint32_t output_width = opts.output_width;
544         if (output_width == 0)  output_width = orig_width;
545         uint32_t output_height = (output_width*1.0f) / orig_width * orig_height;
546         cv::resize(frame, r_frame, Size(output_width, output_height));
548         snprintf(outfile_name, 64, "multibox_%d.png", frame_index);
549         cv::imwrite(outfile_name, frame);
550         printf("Saving frame %d with SSD multiboxes to: %s\n",
551                frame_index, outfile_name);
552     }
554     return true;
557 void DisplayHelp()
559     std::cout <<
560     "Usage: ssd_multibox\n"
561     "  Will run partitioned ssd_multibox network to perform "
562     "multi-objects detection\n"
563     "  and classification.  First part of network "
564     "(layersGroupId 1) runs on EVE,\n"
565     "  second part (layersGroupId 2) runs on DSP.\n"
566     "  Use -c to run a different segmentation network.  Default is jdetnet_voc.\n"
567     "Optional arguments:\n"
568     " -c <config>          Valid configs: jdetnet_voc, jdetnet \n"
569     " -d <number>          Number of dsp cores to use\n"
570     " -e <number>          Number of eve cores to use\n"
571     " -i <image>           Path to the image file as input\n"
572     "                      Default are 9 frames in testvecs\n"
573     " -i camera<number>    Use camera as input\n"
574     "                      video input port: /dev/video<number>\n"
575     " -i <name>.{mp4,mov,avi}  Use video file as input\n"
576     " -l <objects_list>    Path to the object classes list file\n"
577     " -f <number>          Number of frames to process\n"
578     " -w <number>          Output image/video width\n"
579     " -p <number>          Output probability threshold in percentage\n"
580     "                      Default is 25 percent or higher\n"
581     " -v                   Verbose output during execution\n"
582     " -h                   Help\n";