ExecutionObjectPipeline for executing layersGroups
[tidl/tidl-api.git] / examples / ssd_multibox / main.cpp
1 /******************************************************************************
2  * Copyright (c) 2018, Texas Instruments Incorporated - http://www.ti.com/
3  *   All rights reserved.
4  *
5  *   Redistribution and use in source and binary forms, with or without
6  *   modification, are permitted provided that the following conditions are met:
7  *       * Redistributions of source code must retain the above copyright
8  *         notice, this list of conditions and the following disclaimer.
9  *       * Redistributions in binary form must reproduce the above copyright
10  *         notice, this list of conditions and the following disclaimer in the
11  *         documentation and/or other materials provided with the distribution.
12  *       * Neither the name of Texas Instruments Incorporated nor the
13  *         names of its contributors may be used to endorse or promote products
14  *         derived from this software without specific prior written permission.
15  *
16  *   THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
17  *   AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
18  *   IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
19  *   ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE
20  *   LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
21  *   CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
22  *   SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
23  *   INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
24  *   CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
25  *   ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF
26  *   THE POSSIBILITY OF SUCH DAMAGE.
27  *****************************************************************************/
28 #include <signal.h>
29 #include <getopt.h>
30 #include <iostream>
31 #include <iomanip>
32 #include <fstream>
33 #include <cassert>
34 #include <string>
35 #include <functional>
36 #include <algorithm>
37 #include <time.h>
38 #include <unistd.h>
40 #include <queue>
41 #include <vector>
42 #include <cstdio>
44 #include "executor.h"
45 #include "execution_object.h"
46 #include "execution_object_pipeline.h"
47 #include "configuration.h"
48 #include "../segmentation/object_classes.h"
50 #include "opencv2/core.hpp"
51 #include "opencv2/imgproc.hpp"
52 #include "opencv2/highgui.hpp"
53 #include "opencv2/videoio.hpp"
55 #define NUM_VIDEO_FRAMES  100
56 #define DEFAULT_CONFIG    "jdetnet"
57 #define DEFAULT_INPUT     "../test/testvecs/input/preproc_0_768x320.y"
59 bool __TI_show_debug_ = false;
60 bool is_default_input = false;
61 bool is_preprocessed_input = false;
62 bool is_camera_input       = false;
63 int  orig_width;
64 int  orig_height;
65 object_class_table_t *object_class_table;
67 using namespace tidl;
68 using namespace cv;
71 bool RunConfiguration(const std::string& config_file,
72                       uint32_t num_dsps, uint32_t num_eves,
73                       DeviceType device_type, std::string& input_file);
74 bool ReadFrame(ExecutionObjectPipeline& eop, int frame_idx,
75                const Configuration& configuration, int num_frames,
76                std::string& image_file, VideoCapture &cap);
77 bool WriteFrameOutput(const ExecutionObjectPipeline& eop,
78                       const Configuration& configuration);
80 void ReportTime(int frame_index, std::string device_name, double elapsed_host,
81                 double elapsed_device);
83 static void ProcessArgs(int argc, char *argv[],
84                         std::string& config,
85                         uint32_t& num_dsps,
86                         uint32_t& num_eves,
87                         DeviceType& device_type,
88                         std::string& input_file);
90 static void DisplayHelp();
92 static double ms_diff(struct timespec &t0, struct timespec &t1)
93 { return (t1.tv_sec - t0.tv_sec) * 1e3 + (t1.tv_nsec - t0.tv_nsec) / 1e6; }
96 int main(int argc, char *argv[])
97 {
98     // Catch ctrl-c to ensure a clean exit
99     signal(SIGABRT, exit);
100     signal(SIGTERM, exit);
102     // If there are no devices capable of offloading TIDL on the SoC, exit
103     uint32_t num_eve = Executor::GetNumDevices(DeviceType::EVE);
104     uint32_t num_dsp = Executor::GetNumDevices(DeviceType::DSP);
105     if (num_eve == 0 || num_dsp == 0)
106     {
107         std::cout << "ssd_multibox requires both EVE and DSP for execution."
108                   << std::endl;
109         return EXIT_SUCCESS;
110     }
112     // Process arguments
113     std::string config      = DEFAULT_CONFIG;
114     std::string input_file  = DEFAULT_INPUT;
115     uint32_t num_dsps    = 1;
116     uint32_t num_eves    = 1;
117     DeviceType  device_type = DeviceType::EVE;
118     ProcessArgs(argc, argv, config, num_dsps, num_eves,
119                 device_type, input_file);
121     if ((object_class_table = GetObjectClassTable(config)) == nullptr)
122     {
123         std::cout << "No object classes defined for this config." << std::endl;
124         return EXIT_FAILURE;
125     }
127     if (input_file == DEFAULT_INPUT)  is_default_input = true;
128     if (input_file == "camera")       is_camera_input = true;
129     if (input_file.length() > 2 &&
130         input_file.compare(input_file.length() - 2, 2, ".y") == 0)
131         is_preprocessed_input = true;
132     std::cout << "Input: " << input_file << std::endl;
133     std::string config_file = "../test/testvecs/config/infer/tidl_config_"
134                               + config + ".txt";
135     bool status = RunConfiguration(config_file, num_dsps, num_eves,
136                                    device_type, input_file);
138     if (!status)
139     {
140         std::cout << "ssd_multibox FAILED" << std::endl;
141         return EXIT_FAILURE;
142     }
144     std::cout << "ssd_multibox PASSED" << std::endl;
145     return EXIT_SUCCESS;
148 bool RunConfiguration(const std::string& config_file,
149                       uint32_t num_dsps, uint32_t num_eves,
150                       DeviceType device_type, std::string& input_file)
152     DeviceIds ids_eve, ids_dsp;
153     for (int i = 0; i < num_eves; i++)
154         ids_eve.insert(static_cast<DeviceId>(i));
155     for (int i = 0; i < num_dsps; i++)
156         ids_dsp.insert(static_cast<DeviceId>(i));
158     // Read the TI DL configuration file
159     Configuration configuration;
160     bool status = configuration.ReadFromFile(config_file);
161     if (!status)
162     {
163         std::cerr << "Error in configuration file: " << config_file
164                   << std::endl;
165         return false;
166     }
168     // setup input
169     int num_frames = is_default_input ? 9 : 9;
170     VideoCapture cap;
171     std::string image_file;
172     if (is_camera_input)
173     {
174         cap = VideoCapture(1);  // cap = VideoCapture("test.mp4");
175         if (! cap.isOpened())
176         {
177             std::cerr << "Cannot open camera input." << std::endl;
178             return false;
179         }
180         num_frames = NUM_VIDEO_FRAMES;
181         namedWindow("SSD_Multibox", WINDOW_AUTOSIZE | CV_GUI_NORMAL);
182     }
183     else
184     {
185         image_file = input_file;
186     }
188     try
189     {
190         // Create a executor with the approriate core type, number of cores
191         // and configuration specified
192         // EVE will run layersGroupId 1 in the network, while
193         // DSP will run layersGroupId 2 in the network
194         Executor exe_eve(DeviceType::EVE, ids_eve, configuration, 1);
195         Executor exe_dsp(DeviceType::DSP, ids_dsp, configuration, 2);
197         // Construct ExecutionObjectPipeline that utilizes multiple
198         // ExecutionObjects to process a single frame, each ExecutionObject
199         // processes one layerGroup of the network
200         int num_eops = std::max(num_eves, num_dsps);
201         std::vector<ExecutionObjectPipeline *> eops;
202         for (int i = 0; i < num_eops; i++)
203             eops.push_back(new ExecutionObjectPipeline({exe_eve[i%num_eves],
204                                                         exe_dsp[i%num_dsps]}));
206         // Allocate input/output memory for each EOP
207         std::vector<void *> buffers;
208         for (auto eop : eops)
209         {
210             size_t in_size  = eop->GetInputBufferSizeInBytes();
211             size_t out_size = eop->GetOutputBufferSizeInBytes();
212             void*  in_ptr   = malloc(in_size);
213             void*  out_ptr  = malloc(out_size);
214             assert(in_ptr != nullptr && out_ptr != nullptr);
215             buffers.push_back(in_ptr);
216             buffers.push_back(out_ptr);
218             ArgInfo in(in_ptr,   in_size);
219             ArgInfo out(out_ptr, out_size);
220             eop->SetInputOutputBuffer(in, out);
221         }
223         struct timespec tloop0, tloop1;
224         clock_gettime(CLOCK_MONOTONIC, &tloop0);
226         // Process frames with ExecutionObjectPipelines in a pipelined manner
227         // additional num_eops iterations to flush pipeline (epilogue)
228         for (int frame_idx = 0; frame_idx < num_frames + num_eops; frame_idx++)
229         {
230             ExecutionObjectPipeline* eop = eops[frame_idx % num_eops];
232             // Wait for previous frame on the same eop to finish processing
233             if (eop->ProcessFrameWait())
234             {
235                 ReportTime(eop->GetFrameIndex(), eop->GetDeviceName(),
236                            eop->GetHostProcessTimeInMilliSeconds(),
237                            eop->GetProcessTimeInMilliSeconds());
238                 WriteFrameOutput(*eop, configuration);
239             }
241             // Read a frame and start processing it with current eo
242             if (ReadFrame(*eop, frame_idx, configuration, num_frames,
243                           image_file, cap))
244             {
245                 eop->ProcessFrameStartAsync();
246             }
247         }
249         clock_gettime(CLOCK_MONOTONIC, &tloop1);
250         std::cout << "Loop total time (including read/write/print/etc): "
251                   << std::setw(6) << std::setprecision(4)
252                   << ms_diff(tloop0, tloop1) << "ms" << std::endl;
254         for (auto eop : eops)
255             delete eop;
256         for (auto b : buffers)
257             free(b);
258     }
259     catch (tidl::Exception &e)
260     {
261         std::cerr << e.what() << std::endl;
262         status = false;
263     }
265     return status;
268 void ReportTime(int frame_index, std::string device_name, double elapsed_host,
269                 double elapsed_device)
271     double overhead = 100 - (elapsed_device/elapsed_host*100);
272     std::cout << "frame[" << frame_index << "]: "
273               << "Time on " << device_name << ": "
274               << std::setw(6) << std::setprecision(4)
275               << elapsed_device << "ms, "
276               << "host: "
277               << std::setw(6) << std::setprecision(4)
278               << elapsed_host << "ms ";
279     std::cout << "API overhead: "
280               << std::setw(6) << std::setprecision(3)
281               << overhead << " %" << std::endl;
285 bool ReadFrame(ExecutionObjectPipeline& eop, int frame_idx,
286                const Configuration& configuration, int num_frames,
287                std::string& image_file, VideoCapture &cap)
289     if (frame_idx >= num_frames)
290         return false;
291     eop.SetFrameIndex(frame_idx);
293     char*  frame_buffer = eop.GetInputBufferPtr();
294     assert (frame_buffer != nullptr);
295     int channel_size = configuration.inWidth * configuration.inHeight;
297     Mat image;
298     if (! image_file.empty())
299     {
300         if (is_preprocessed_input)
301         {
302             std::ifstream ifs(image_file, std::ios::binary);
303             //ifs.seekg(frame_idx * channel_size * 3);
304             ifs.read(frame_buffer, channel_size * 3);
305             bool ifs_status = ifs.good();
306             ifs.close();
307             orig_width  = configuration.inWidth;
308             orig_height = configuration.inHeight;
309             return ifs_status;  // already PreProc-ed
310         }
311         else
312         {
313             image = cv::imread(image_file, CV_LOAD_IMAGE_COLOR);
314             if (image.empty())
315             {
316                 std::cerr << "Unable to read from: " << image_file << std::endl;
317                 return false;
318             }
319         }
320     }
321     else
322     {
323         // 640x480 camera input, process one in every 5 frames,
324         // can adjust number of skipped frames to match real time processing
325         if (! cap.grab())  return false;
326         if (! cap.grab())  return false;
327         if (! cap.grab())  return false;
328         if (! cap.grab())  return false;
329         if (! cap.grab())  return false;
330         if (! cap.retrieve(image)) return false;
331     }
333     // scale to network input size
334     Mat s_image, bgr_frames[3];
335     orig_width  = image.cols;
336     orig_height = image.rows;
337     cv::resize(image, s_image,
338                Size(configuration.inWidth, configuration.inHeight),
339                0, 0, cv::INTER_AREA);
340     cv::split(s_image, bgr_frames);
341     memcpy(frame_buffer,                bgr_frames[0].ptr(), channel_size);
342     memcpy(frame_buffer+1*channel_size, bgr_frames[1].ptr(), channel_size);
343     memcpy(frame_buffer+2*channel_size, bgr_frames[2].ptr(), channel_size);
344     return true;
347 // Create frame with boxes drawn around classified objects
348 bool WriteFrameOutput(const ExecutionObjectPipeline& eop,
349                       const Configuration& configuration)
351     // Asseembly original frame
352     int width  = configuration.inWidth;
353     int height = configuration.inHeight;
354     int channel_size = width * height;
355     Mat frame, r_frame, bgr[3];
357     unsigned char *in = (unsigned char *) eop.GetInputBufferPtr();
358     bgr[0] = Mat(height, width, CV_8UC(1), in);
359     bgr[1] = Mat(height, width, CV_8UC(1), in + channel_size);
360     bgr[2] = Mat(height, width, CV_8UC(1), in + channel_size*2);
361     cv::merge(bgr, 3, frame);
363     int frame_index = eop.GetFrameIndex();
364     char outfile_name[64];
365     if (! is_camera_input && is_preprocessed_input)
366     {
367         snprintf(outfile_name, 64, "frame_%d.png", frame_index);
368         cv::imwrite(outfile_name, frame);
369         printf("Saving frame %d to: %s\n", frame_index, outfile_name);
370     }
372     // Draw boxes around classified objects
373     float *out = (float *) eop.GetOutputBufferPtr();
374     int num_floats = eop.GetOutputBufferSizeInBytes() / sizeof(float);
375     for (int i = 0; i < num_floats / 7; i++)
376     {
377         int index = (int)    out[i * 7 + 0];
378         if (index < 0)  break;
380         int   label = (int)  out[i * 7 + 1];
381         float score =        out[i * 7 + 2];
382         int   xmin  = (int) (out[i * 7 + 3] * width);
383         int   ymin  = (int) (out[i * 7 + 4] * height);
384         int   xmax  = (int) (out[i * 7 + 5] * width);
385         int   ymax  = (int) (out[i * 7 + 6] * height);
387         object_class_t *object_class = GetObjectClass(object_class_table,
388                                                       label);
389         if (object_class == nullptr)  continue;
391 #if 0
392         printf("(%d, %d) -> (%d, %d): %s, score=%f\n",
393                xmin, ymin, xmax, ymax, object_class->label, score);
394 #endif
396         cv::rectangle(frame, Point(xmin, ymin), Point(xmax, ymax),
397                       Scalar(object_class->color.blue,
398                              object_class->color.green,
399                              object_class->color.red), 2);
400     }
402     // output
403     cv::resize(frame, r_frame, Size(orig_width, orig_height));
404     if (is_camera_input)
405     {
406         cv::imshow("SSD_Multibox", r_frame);
407         waitKey(1);
408     }
409     else
410     {
411         snprintf(outfile_name, 64, "multibox_%d.png", frame_index);
412         cv::imwrite(outfile_name, r_frame);
413         printf("Saving frame %d with SSD multiboxes to: %s\n",
414                frame_index, outfile_name);
415     }
417     return true;
421 void ProcessArgs(int argc, char *argv[], std::string& config,
422                  uint32_t& num_dsps, uint32_t& num_eves,
423                  DeviceType& device_type, std::string& input_file)
425     const struct option long_options[] =
426     {
427         {"config",      required_argument, 0, 'c'},
428         {"num_dsps",    required_argument, 0, 'd'},
429         {"num_eves",    required_argument, 0, 'e'},
430         {"image_file",  required_argument, 0, 'i'},
431         {"help",        no_argument,       0, 'h'},
432         {"verbose",     no_argument,       0, 'v'},
433         {0, 0, 0, 0}
434     };
436     int option_index = 0;
438     while (true)
439     {
440         int c = getopt_long(argc, argv, "c:d:e:i:hv", long_options,
441                             &option_index);
443         if (c == -1)
444             break;
446         switch (c)
447         {
448             case 'c': config = optarg;
449                       break;
451             case 'd': num_dsps = atoi(optarg);
452                       assert (num_dsps > 0 && num_dsps <= 
453                                      Executor::GetNumDevices(DeviceType::DSP));
454                       break;
456             case 'e': num_eves = atoi(optarg);
457                       assert (num_eves > 0 && num_eves <=
458                                      Executor::GetNumDevices(DeviceType::EVE));
459                       break;
461             case 'i': input_file = optarg;
462                       break;
464             case 'v': __TI_show_debug_ = true;
465                       break;
467             case 'h': DisplayHelp();
468                       exit(EXIT_SUCCESS);
469                       break;
471             case '?': // Error in getopt_long
472                       exit(EXIT_FAILURE);
473                       break;
475             default:
476                       std::cerr << "Unsupported option: " << c << std::endl;
477                       break;
478         }
479     }
482 void DisplayHelp()
484     std::cout << "Usage: ssd_multibox\n"
485                  "  Will run partitioned ssd_multibox network to perform "
486                  "multi-objects detection\n"
487                  "  and classification.  First part of network "
488                  "(layersGroupId 1) runs on EVE,\n"
489                  "  second part (layersGroupId 2) runs on DSP.\n"
490                  "  Use -c to run a different segmentation network. "
491                  "Default is jdetnet.\n"
492                  "Optional arguments:\n"
493                  " -c <config>          Valid configs: jdetnet \n"
494                  " -d <number>          Number of dsp cores to use\n"
495                  " -e <number>          Number of eve cores to use\n"
496                  " -i <image>           Path to the image file\n"
497                  "                      Default is 1 frame in testvecs\n"
498                  " -i camera            Use camera as input\n"
499                  " -v                   Verbose output during execution\n"
500                  " -h                   Help\n";