]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - tidl/tidl-api.git/blob - examples/ssd_multibox/main.cpp
Merge branch 'release/v01.03.01'
[tidl/tidl-api.git] / examples / ssd_multibox / main.cpp
1 /******************************************************************************
2  * Copyright (c) 2018, Texas Instruments Incorporated - http://www.ti.com/
3  *   All rights reserved.
4  *
5  *   Redistribution and use in source and binary forms, with or without
6  *   modification, are permitted provided that the following conditions are met:
7  *       * Redistributions of source code must retain the above copyright
8  *         notice, this list of conditions and the following disclaimer.
9  *       * Redistributions in binary form must reproduce the above copyright
10  *         notice, this list of conditions and the following disclaimer in the
11  *         documentation and/or other materials provided with the distribution.
12  *       * Neither the name of Texas Instruments Incorporated nor the
13  *         names of its contributors may be used to endorse or promote products
14  *         derived from this software without specific prior written permission.
15  *
16  *   THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
17  *   AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
18  *   IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
19  *   ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE
20  *   LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
21  *   CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
22  *   SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
23  *   INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
24  *   CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
25  *   ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF
26  *   THE POSSIBILITY OF SUCH DAMAGE.
27  *****************************************************************************/
28 #include <signal.h>
29 #include <iostream>
30 #include <iomanip>
31 #include <fstream>
32 #include <cassert>
33 #include <string>
34 #include <functional>
35 #include <algorithm>
36 #include <time.h>
37 #include <unistd.h>
39 #include <queue>
40 #include <vector>
41 #include <cstdio>
42 #include <string>
43 #include <chrono>
45 #include "executor.h"
46 #include "execution_object.h"
47 #include "execution_object_pipeline.h"
48 #include "configuration.h"
49 #include "../common/object_classes.h"
50 #include "../common/utils.h"
51 #include "../common/video_utils.h"
53 using namespace std;
54 using namespace tidl;
55 using namespace cv;
58 #define NUM_VIDEO_FRAMES  100
59 #define DEFAULT_CONFIG    "jdetnet_voc"
60 #define DEFAULT_INPUT     "../test/testvecs/input/horse_768x320.y"
61 #define DEFAULT_INPUT_FRAMES (1)
62 #define DEFAULT_OBJECT_CLASSES_LIST_FILE "./jdetnet_voc_objects.json"
63 #define DEFAULT_OUTPUT_PROB_THRESHOLD  25
65 /* Enable this macro to record individual output files and */
66 /* resized, cropped network input files                    */
67 //#define DEBUG_FILES
69 std::unique_ptr<ObjectClasses> object_classes;
70 uint32_t orig_width;
71 uint32_t orig_height;
72 uint32_t num_frames_file;
74 bool RunConfiguration(const cmdline_opts_t& opts);
75 Executor* CreateExecutor(DeviceType dt, uint32_t num, const Configuration& c,
76                          int layers_group_id);
77 bool ReadFrame(ExecutionObjectPipeline& eop, uint32_t frame_idx,
78                const Configuration& c, const cmdline_opts_t& opts,
79                VideoCapture &cap, ifstream &ifs);
80 bool WriteFrameOutput(const ExecutionObjectPipeline& eop,
81                       const Configuration& c, const cmdline_opts_t& opts,
82                       float confidence_value);
83 static void DisplayHelp();
85 /***************************************************************/
86 /* Slider to control detection confidence level                */
87 /***************************************************************/
88 static void on_trackbar( int slider_id, void *inst )
89 {
90   //This function is invoked on every slider move.
91   //No action required, since prob_slider is automatically updated.
92   //But, for any additional operation on slider move, this is the place to insert code.
93 }
96 int main(int argc, char *argv[])
97 {
98     // Catch ctrl-c to ensure a clean exit
99     signal(SIGABRT, exit);
100     signal(SIGTERM, exit);
102     // If there are no devices capable of offloading TIDL on the SoC, exit
103     uint32_t num_eves = Executor::GetNumDevices(DeviceType::EVE);
104     uint32_t num_dsps = Executor::GetNumDevices(DeviceType::DSP);
105     if (num_eves == 0 && num_dsps == 0)
106     {
107         cout << "ssd_multibox requires EVE or DSP for execution." << endl;
108         return EXIT_SUCCESS;
109     }
111     // Process arguments
112     cmdline_opts_t opts;
113     opts.config = DEFAULT_CONFIG;
114     opts.object_classes_list_file = DEFAULT_OBJECT_CLASSES_LIST_FILE;
115     opts.num_eves = num_eves > 0 ? 1 : 0;
116     opts.num_dsps = num_dsps > 0 ? 1 : 0;
117     opts.input_file = DEFAULT_INPUT;
118     opts.output_prob_threshold = DEFAULT_OUTPUT_PROB_THRESHOLD;
119     if (! ProcessArgs(argc, argv, opts))
120     {
121         DisplayHelp();
122         exit(EXIT_SUCCESS);
123     }
124     assert(opts.num_dsps != 0 || opts.num_eves != 0);
125     if (opts.num_frames == 0)
126         opts.num_frames = (opts.is_camera_input || opts.is_video_input) ?
127                           NUM_VIDEO_FRAMES :
128                           ((opts.input_file == DEFAULT_INPUT) ?
129                            DEFAULT_INPUT_FRAMES : 1);
130     cout << "Input: " << opts.input_file << endl;
132     // Get object classes list
133     object_classes = std::unique_ptr<ObjectClasses>(
134                              new ObjectClasses(opts.object_classes_list_file));
135     if (object_classes->GetNumClasses() == 0)
136     {
137         cout << "No object classes defined for this config." << endl;
138         return EXIT_FAILURE;
139     }
141     // Run network
142     bool status = RunConfiguration(opts);
143     if (!status)
144     {
145         cout << "ssd_multibox FAILED" << endl;
146         return EXIT_FAILURE;
147     }
149     cout << "ssd_multibox PASSED" << endl;
150     return EXIT_SUCCESS;
153 bool RunConfiguration(const cmdline_opts_t& opts)
155     int prob_slider     = opts.output_prob_threshold;
156     // Read the TI DL configuration file
157     Configuration c;
158     std::string config_file = "../test/testvecs/config/infer/tidl_config_"
159                               + opts.config + ".txt";
160     bool status = c.ReadFromFile(config_file);
161     if (!status)
162     {
163         cerr << "Error in configuration file: " << config_file << endl;
164         return false;
165     }
166     c.enableApiTrace = opts.verbose;
167     if (opts.num_eves == 0 || opts.num_dsps == 0)
168         c.runFullNet = true;
169     // DSP only execution requires larger NETWORK HEAP size
170     if (opts.num_eves == 0)
171         c.NETWORK_HEAP_SIZE = 75000000;
173     // setup camera/video input
174     VideoCapture cap;
175     if (! SetVideoInputOutput(cap, opts, "SSD_Multibox"))  return false;
177     if (opts.is_camera_input || opts.is_video_input)
178     {
179         std::string TrackbarName("Confidence(%):");
180         createTrackbar( TrackbarName.c_str(), "SSD_Multibox",
181                         &prob_slider, 100, on_trackbar );
182         std::cout << TrackbarName << std::endl;
183     }
185     // setup preprocessed input
186     ifstream ifs;
187     if (opts.is_preprocessed_input)
188     {
189         ifs.open(opts.input_file, ios::binary | ios::ate);
190         if (! ifs.good())
191         {
192             cerr << "Cannot open " << opts.input_file << endl;
193             return false;
194         }
195         num_frames_file = ((int) ifs.tellg()) /
196                           (c.inWidth * c.inHeight * c.inNumChannels);
197     }
199     try
200     {
201         // Create Executors with the approriate core type, number of cores
202         // and configuration specified
203         // EVE will run layersGroupId 1 in the network, while
204         // DSP will run layersGroupId 2 in the network
205         Executor* e_eve = CreateExecutor(DeviceType::EVE, opts.num_eves, c, 1);
206         Executor* e_dsp = CreateExecutor(DeviceType::DSP, opts.num_dsps, c, 2);
207         vector<ExecutionObjectPipeline *> eops;
209         if (e_eve != nullptr && e_dsp != nullptr)
210         {
211             // Construct ExecutionObjectPipeline that utilizes multiple
212             // ExecutionObjects to process a single frame, each ExecutionObject
213             // processes one layerGroup of the network
214             //
215             // Pipeline depth can enable more optimized pipeline execution:
216             // Given one EVE and one DSP as an example, with different
217             //     pipeline_depth, we have different execution behavior:
218             // If pipeline_depth is set to 1,
219             //    we create one EOP: eop0 (eve0, dsp0)
220             //    pipeline execution of multiple frames over time is as follows:
221             //    --------------------- time ------------------->
222             //    eop0: [eve0...][dsp0]
223             //    eop0:                [eve0...][dsp0]
224             //    eop0:                               [eve0...][dsp0]
225             //    eop0:                                              [eve0...][dsp0]
226             // If pipeline_depth is set to 2,
227             //    we create two EOPs: eop0 (eve0, dsp0), eop1(eve0, dsp0)
228             //    pipeline execution of multiple frames over time is as follows:
229             //    --------------------- time ------------------->
230             //    eop0: [eve0...][dsp0]
231             //    eop1:          [eve0...][dsp0]
232             //    eop0:                   [eve0...][dsp0]
233             //    eop1:                            [eve0...][dsp0]
234             // Additional benefit of setting pipeline_depth to 2 is that
235             //    it can also overlap host ReadFrame() with device processing:
236             //    --------------------- time ------------------->
237             //    eop0: [RF][eve0...][dsp0]
238             //    eop1:     [RF]     [eve0...][dsp0]
239             //    eop0:                    [RF][eve0...][dsp0]
240             //    eop1:                             [RF][eve0...][dsp0]
241             uint32_t pipeline_depth = 2;  // 2 EOs in EOP -> depth 2
242             for (uint32_t j = 0; j < pipeline_depth; j++)
243                 for (uint32_t i = 0; i < max(opts.num_eves, opts.num_dsps); i++)
244                     eops.push_back(new ExecutionObjectPipeline(
245                       {(*e_eve)[i%opts.num_eves], (*e_dsp)[i%opts.num_dsps]}));
246         }
247         else
248         {
249             // Construct ExecutionObjectPipeline that utilizes a
250             // ExecutionObject to process a single frame, each ExecutionObject
251             // processes the full network
252             //
253             // Use duplicate EOPs to do double buffering on frame input/output
254             //    because each EOP has its own set of input/output buffers,
255             //    so that host ReadFrame() can overlap device processing
256             // Use one EO as an example, with different buffer_factor,
257             //    we have different execution behavior:
258             // If buffer_factor is set to 1 -> single buffering
259             //    we create one EOP: eop0 (eo0)
260             //    pipeline execution of multiple frames over time is as follows:
261             //    --------------------- time ------------------->
262             //    eop0: [RF][eo0.....][WF]
263             //    eop0:                   [RF][eo0.....][WF]
264             //    eop0:                                     [RF][eo0.....][WF]
265             // If buffer_factor is set to 2 -> double buffering
266             //    we create two EOPs: eop0 (eo0), eop1(eo0)
267             //    pipeline execution of multiple frames over time is as follows:
268             //    --------------------- time ------------------->
269             //    eop0: [RF][eo0.....][WF]
270             //    eop1:     [RF]      [eo0.....][WF]
271             //    eop0:                   [RF]  [eo0.....][WF]
272             //    eop1:                             [RF]  [eo0.....][WF]
273             uint32_t buffer_factor = 2;  // set to 1 for single buffering
274             for (uint32_t j = 0; j < buffer_factor; j++)
275             {
276                 for (uint32_t i = 0; i < opts.num_eves; i++)
277                     eops.push_back(new ExecutionObjectPipeline({(*e_eve)[i]}));
278                 for (uint32_t i = 0; i < opts.num_dsps; i++)
279                     eops.push_back(new ExecutionObjectPipeline({(*e_dsp)[i]}));
280             }
281         }
282         uint32_t num_eops = eops.size();
284         // Allocate input/output memory for each EOP
285         AllocateMemory(eops);
287         chrono::time_point<chrono::steady_clock> tloop0, tloop1;
288         tloop0 = chrono::steady_clock::now();
290         // Process frames with available eops in a pipelined manner
291         // additional num_eops iterations to flush pipeline (epilogue)
292         for (uint32_t frame_idx = 0;
293              frame_idx < opts.num_frames + num_eops; frame_idx++)
294         {
295             ExecutionObjectPipeline* eop = eops[frame_idx % num_eops];
297             // Wait for previous frame on the same eop to finish processing
298             if (eop->ProcessFrameWait())
299                 WriteFrameOutput(*eop, c, opts, (float)prob_slider);
301             // Read a frame and start processing it with current eo
302             if (ReadFrame(*eop, frame_idx, c, opts, cap, ifs))
303                 eop->ProcessFrameStartAsync();
304         }
306         tloop1 = chrono::steady_clock::now();
307         chrono::duration<float> elapsed = tloop1 - tloop0;
308         cout << "Loop total time (including read/write/opencv/print/etc): "
309                   << setw(6) << setprecision(4)
310                   << (elapsed.count() * 1000) << "ms" << endl;
312         FreeMemory(eops);
313         for (auto eop : eops)  delete eop;
314         delete e_eve;
315         delete e_dsp;
316     }
317     catch (tidl::Exception &e)
318     {
319         cerr << e.what() << endl;
320         status = false;
321     }
323     return status;
326 // Create an Executor with the specified type and number of EOs
327 Executor* CreateExecutor(DeviceType dt, uint32_t num, const Configuration& c,
328                          int layers_group_id)
330     if (num == 0) return nullptr;
332     DeviceIds ids;
333     for (uint32_t i = 0; i < num; i++)
334         ids.insert(static_cast<DeviceId>(i));
336     Executor* e = new Executor(dt, ids, c, layers_group_id);
337     assert(e != nullptr);
338     return e;
341 bool ReadFrame(ExecutionObjectPipeline& eop, uint32_t frame_idx,
342                const Configuration& c, const cmdline_opts_t& opts,
343                VideoCapture &cap, ifstream &ifs)
345     if ((uint32_t)frame_idx >= opts.num_frames)
346         return false;
348     eop.SetFrameIndex(frame_idx);
350     char*  frame_buffer = eop.GetInputBufferPtr();
351     assert (frame_buffer != nullptr);
352     int channel_size = c.inWidth * c.inHeight;
353     int frame_size   = channel_size * c.inNumChannels;
355     Mat image;
356     if (!opts.is_camera_input && !opts.is_video_input)
357     {
358         if (opts.is_preprocessed_input)
359         {
360             orig_width  = c.inWidth;
361             orig_height = c.inHeight;
362             ifs.seekg((frame_idx % num_frames_file) * frame_size);
363             ifs.read(frame_buffer, frame_size);
364             return ifs.good();
365         }
366         else
367         {
368             image = cv::imread(opts.input_file, CV_LOAD_IMAGE_COLOR);
369             if (image.empty())
370             {
371                 cerr << "Unable to read from: " << opts.input_file << endl;
372                 return false;
373             }
374         }
375     }
376     else
377     {
378         if(opts.is_camera_input)
379         {
380            if (! cap.grab()) return false;
381            if (! cap.retrieve(image)) return false;
382         }
383         else
384         { // Video clip
385            if (cap.grab())
386            {
387              if (! cap.retrieve(image)) return false;
388            } else {
389              //Rewind!
390              std::cout << "Video clip rewinded!" << std::endl;
391              cap.set(CAP_PROP_POS_FRAMES, 0);
392              if (! cap.grab()) return false;
393              if (! cap.retrieve(image)) return false;
394            }
395         }
396     }
398     // Scale to network input size:
399     Mat s_image, bgr_frames[3];
400     orig_width  = image.cols;
401     orig_height = image.rows;
402     if (!opts.is_camera_input && !opts.is_video_input)
403     {
404         cv::resize(image, s_image, Size(c.inWidth, c.inHeight),
405                    0, 0, cv::INTER_AREA);
406     }
407     else
408     {
409         // Preserve aspect ratio, by doing central cropping
410         // Choose vertical or horizontal central cropping
411         // based on dimension reduction
412         if(orig_width > orig_height)
413         {
414             float change_width  = (float)c.inWidth / (float)orig_width;
415             float change_height = (float)c.inHeight / (float)orig_height;
416             if(change_width < change_height)
417             {
418                 // E.g. for 1920x1080->512x512, we first crop central part
419                 // roi(420, 0, 1080, 1080), then resize to (512x512)
420                 int offset_x = (int)round(0.5 * ((float)orig_width -
421                   ((float)orig_height * (float)c.inWidth / (float)c.inHeight)));
422                 cv::resize(image(Rect(offset_x, 0, orig_width - 2 * offset_x,
423                                       orig_height)), s_image,
424                            Size(c.inWidth, c.inHeight), 0, 0, cv::INTER_AREA);
425             } else {
426                 // E.g. for 1920x1080->768x320, we first crop central part
427                 // roi(0, 140, 1920, 800), then resize to (768x320)
428                 int offset_y = (int)round(0.5 * ((float)orig_height -
429                   ((float)orig_width * (float)c.inHeight / (float)c.inWidth)));
430                 cv::resize(image(Rect(0, offset_y, orig_width,
431                                       orig_height - 2 * offset_y)), s_image,
432                            Size(c.inWidth, c.inHeight), 0, 0, cv::INTER_AREA);
433             }
434         } else {
435           // E.g. for 540x960->512x512, we first crop central part
436           //      roi(0, 210, 540, 540), then resize to (512x512)
437           // E.g. for 540x960->768x320, we first crop central part
438           //      roi(0, 367, 540, 225), then resize to (768x320)
439           int offset_y = (int)round(0.5 * ((float)orig_height -
440               ((float)orig_width * (float)c.inHeight / (float)c.inWidth)));
441           cv::resize(image(Rect(0, offset_y, orig_width, orig_height -
442                                 2 * offset_y)), s_image,
443                      Size(c.inWidth, c.inHeight), 0, 0, cv::INTER_AREA);
444         }
445     }
447     #ifdef DEBUG_FILES
448     {
449         // Image files can be converted into video using, example script
450         // (on desktop Ubuntu, with ffmpeg installed):
451         // ffmpeg -i netin_%04d.png -vf "scale=(iw*sar)*max(768/(iw*sar)\,320/ih):ih*max(768/(iw*sar)\,320/ih), crop=768:320" -b:v 4000k out.mp4
452         // Update width 768, height 320, if necessary
453         char netin_name[80];
454         sprintf(netin_name, "netin_%04d.png", frame_idx);
455         cv::imwrite(netin_name, s_image);
456         std::cout << "Video input, width:" << orig_width << " height:"
457                   << orig_height << " Network width:" << c.inWidth
458                   << " height:" << c.inHeight << std::endl;
459     }
460     #endif
462     cv::split(s_image, bgr_frames);
463     memcpy(frame_buffer,                bgr_frames[0].ptr(), channel_size);
464     memcpy(frame_buffer+1*channel_size, bgr_frames[1].ptr(), channel_size);
465     memcpy(frame_buffer+2*channel_size, bgr_frames[2].ptr(), channel_size);
466     return true;
469 // Create frame with boxes drawn around classified objects
470 bool WriteFrameOutput(const ExecutionObjectPipeline& eop,
471                       const Configuration& c, const cmdline_opts_t& opts,
472                       float confidence_value)
474     // Asseembly original frame
475     int width  = c.inWidth;
476     int height = c.inHeight;
477     int channel_size = width * height;
478     Mat frame, bgr[3];
480     unsigned char *in = (unsigned char *) eop.GetInputBufferPtr();
481     bgr[0] = Mat(height, width, CV_8UC(1), in);
482     bgr[1] = Mat(height, width, CV_8UC(1), in + channel_size);
483     bgr[2] = Mat(height, width, CV_8UC(1), in + channel_size*2);
484     cv::merge(bgr, 3, frame);
486     int frame_index = eop.GetFrameIndex();
487     char outfile_name[64];
488     if (opts.is_preprocessed_input)
489     {
490         snprintf(outfile_name, 64, "frame_%d.png", frame_index);
491         cv::imwrite(outfile_name, frame);
492         printf("Saving frame %d to: %s\n", frame_index, outfile_name);
493     }
495     // Draw boxes around classified objects
496     float *out = (float *) eop.GetOutputBufferPtr();
497     int num_floats = eop.GetOutputBufferSizeInBytes() / sizeof(float);
498     for (int i = 0; i < num_floats / 7; i++)
499     {
500         int index = (int)    out[i * 7 + 0];
501         if (index < 0)  break;
503         float score =        out[i * 7 + 2];
504         if (score * 100 < confidence_value)  continue;
506         int   label = (int)  out[i * 7 + 1];
507         int   xmin  = (int) (out[i * 7 + 3] * width);
508         int   ymin  = (int) (out[i * 7 + 4] * height);
509         int   xmax  = (int) (out[i * 7 + 5] * width);
510         int   ymax  = (int) (out[i * 7 + 6] * height);
512         const ObjectClass& object_class = object_classes->At(label);
514         if(opts.verbose) {
515             printf("%2d: (%d, %d) -> (%d, %d): %s, score=%f\n",
516                i, xmin, ymin, xmax, ymax, object_class.label.c_str(), score);
517         }
519         if (xmin < 0)       xmin = 0;
520         if (ymin < 0)       ymin = 0;
521         if (xmax > width)   xmax = width;
522         if (ymax > height)  ymax = height;
523         cv::rectangle(frame, Point(xmin, ymin), Point(xmax, ymax),
524                       Scalar(object_class.color.blue,
525                              object_class.color.green,
526                              object_class.color.red), 2);
527     }
529     if (opts.is_camera_input || opts.is_video_input)
530     {
531         cv::imshow("SSD_Multibox", frame);
532 #ifdef DEBUG_FILES
533         // Image files can be converted into video using, example script
534         // (on desktop Ubuntu, with ffmpeg installed):
535         // ffmpeg -i multibox_%04d.png -vf "scale=(iw*sar)*max(768/(iw*sar)\,320/ih):ih*max(768/(iw*sar)\,320/ih), crop=768:320" -b:v 4000k out.mp4
536         // Update width 768, height 320, if necessary
537         snprintf(outfile_name, 64, "multibox_%04d.png", frame_index);
538         cv::imwrite(outfile_name, r_frame);
539 #endif
540         waitKey(1);
541     }
542     else
543     {
544         // Resize to output width/height, keep aspect ratio
545         Mat r_frame;
546         uint32_t output_width = opts.output_width;
547         if (output_width == 0)  output_width = orig_width;
548         uint32_t output_height = (output_width*1.0f) / orig_width * orig_height;
549         cv::resize(frame, r_frame, Size(output_width, output_height));
551         snprintf(outfile_name, 64, "multibox_%d.png", frame_index);
552         cv::imwrite(outfile_name, frame);
553         printf("Saving frame %d with SSD multiboxes to: %s\n",
554                frame_index, outfile_name);
555     }
557     return true;
560 void DisplayHelp()
562     std::cout <<
563     "Usage: ssd_multibox\n"
564     "  Will run partitioned ssd_multibox network to perform "
565     "multi-objects detection\n"
566     "  and classification.  First part of network "
567     "(layersGroupId 1) runs on EVE,\n"
568     "  second part (layersGroupId 2) runs on DSP.\n"
569     "  Use -c to run a different segmentation network.  Default is jdetnet_voc.\n"
570     "Optional arguments:\n"
571     " -c <config>          Valid configs: jdetnet_voc, jdetnet \n"
572     " -d <number>          Number of dsp cores to use\n"
573     " -e <number>          Number of eve cores to use\n"
574     " -i <image>           Path to the image file as input\n"
575     "                      Default are 9 frames in testvecs\n"
576     " -i camera<number>    Use camera as input\n"
577     "                      video input port: /dev/video<number>\n"
578     " -i <name>.{mp4,mov,avi}  Use video file as input\n"
579     " -l <objects_list>    Path to the object classes list file\n"
580     " -f <number>          Number of frames to process\n"
581     " -w <number>          Output image/video width\n"
582     " -p <number>          Output probability threshold in percentage\n"
583     "                      Default is 25 percent or higher\n"
584     " -v                   Verbose output during execution\n"
585     " -h                   Help\n";