Partitioned execution of TI DL network
[tidl/tidl-api.git] / examples / ssd_multibox / main.cpp
1 /******************************************************************************
2  * Copyright (c) 2018, Texas Instruments Incorporated - http://www.ti.com/
3  *   All rights reserved.
4  *
5  *   Redistribution and use in source and binary forms, with or without
6  *   modification, are permitted provided that the following conditions are met:
7  *       * Redistributions of source code must retain the above copyright
8  *         notice, this list of conditions and the following disclaimer.
9  *       * Redistributions in binary form must reproduce the above copyright
10  *         notice, this list of conditions and the following disclaimer in the
11  *         documentation and/or other materials provided with the distribution.
12  *       * Neither the name of Texas Instruments Incorporated nor the
13  *         names of its contributors may be used to endorse or promote products
14  *         derived from this software without specific prior written permission.
15  *
16  *   THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
17  *   AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
18  *   IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
19  *   ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE
20  *   LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
21  *   CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
22  *   SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
23  *   INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
24  *   CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
25  *   ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF
26  *   THE POSSIBILITY OF SUCH DAMAGE.
27  *****************************************************************************/
28 #include <signal.h>
29 #include <getopt.h>
30 #include <iostream>
31 #include <iomanip>
32 #include <fstream>
33 #include <cassert>
34 #include <string>
35 #include <functional>
36 #include <algorithm>
37 #include <time.h>
38 #include <unistd.h>
40 #include <queue>
41 #include <vector>
42 #include <cstdio>
44 #include "executor.h"
45 #include "execution_object.h"
46 #include "configuration.h"
47 #include "../segmentation/object_classes.h"
49 #include "opencv2/core.hpp"
50 #include "opencv2/imgproc.hpp"
51 #include "opencv2/highgui.hpp"
52 #include "opencv2/videoio.hpp"
54 #define NUM_VIDEO_FRAMES  100
55 #define DEFAULT_CONFIG    "jdetnet"
56 #define DEFAULT_INPUT     "../test/testvecs/input/preproc_0_768x320.y"
58 bool __TI_show_debug_ = false;
59 bool is_default_input = false;
60 bool is_preprocessed_input = false;
61 bool is_camera_input       = false;
62 bool is_partitioned        = true;
63 int  orig_width;
64 int  orig_height;
65 object_class_table_t *object_class_table;
67 using namespace tinn;
68 using namespace cv;
71 bool RunConfiguration(const std::string& config_file, uint32_t num_devices,
72                       DeviceType device_type, std::string& input_file);
73 bool ReadFrame(ExecutionObject& eo, int frame_idx,
74                const Configuration& configuration, int num_frames,
75                std::string& image_file, VideoCapture &cap);
76 bool WriteFrameOutput(const ExecutionObject &eo_in,
77                       const ExecutionObject &eo_out,
78                       const Configuration& configuration);
80 void ReportTime(int frame_index, std::string device_name, double elapsed_host,
81                 double elapsed_device);
83 static void ProcessArgs(int argc, char *argv[],
84                         std::string& config,
85                         uint32_t& num_devices,
86                         DeviceType& device_type,
87                         std::string& input_file);
89 static void DisplayHelp();
91 static double ms_diff(struct timespec &t0, struct timespec &t1)
92 { return (t1.tv_sec - t0.tv_sec) * 1e3 + (t1.tv_nsec - t0.tv_nsec) / 1e6; }
95 int main(int argc, char *argv[])
96 {
97     // Catch ctrl-c to ensure a clean exit
98     signal(SIGABRT, exit);
99     signal(SIGTERM, exit);
101     // If there are no devices capable of offloading TIDL on the SoC, exit
102     uint32_t num_dla = Executor::GetNumDevices(DeviceType::DLA);
103     uint32_t num_dsp = Executor::GetNumDevices(DeviceType::DSP);
104     if (num_dla == 0 && num_dsp == 0)
105     {
106         std::cout << "TI DL not supported on this SoC." << std::endl;
107         return EXIT_SUCCESS;
108     }
110     // Process arguments
111     std::string config      = DEFAULT_CONFIG;
112     std::string input_file  = DEFAULT_INPUT;
113     uint32_t num_devices    = 1;
114     DeviceType  device_type = DeviceType::DLA;
115     ProcessArgs(argc, argv, config, num_devices, device_type, input_file);
117     if (is_partitioned)
118         num_devices = std::min(num_devices, std::min(num_dla, num_dsp));
119     if (num_devices == 0)
120     {
121         std::cout << "Partitioned execution requires at least 1 DLA and 1 DSP."
122                   << std::endl;
123         return EXIT_FAILURE;
124     }
125     if ((object_class_table = GetObjectClassTable(config)) == nullptr)
126     {
127         std::cout << "No object classes defined for this config." << std::endl;
128         return EXIT_FAILURE;
129     }
131     if (input_file == DEFAULT_INPUT)  is_default_input = true;
132     if (input_file == "camera")       is_camera_input = true;
133     if (input_file.length() > 2 &&
134         input_file.compare(input_file.length() - 2, 2, ".y") == 0)
135         is_preprocessed_input = true;
136     std::cout << "Input: " << input_file << std::endl;
137     std::string config_file = "../test/testvecs/config/infer/tidl_config_"
138                               + config + ".txt";
139     bool status = RunConfiguration(config_file, num_devices, device_type,
140                                    input_file);
142     if (!status)
143     {
144         std::cout << "ssd_multibox FAILED" << std::endl;
145         return EXIT_FAILURE;
146     }
148     std::cout << "ssd_multibox PASSED" << std::endl;
149     return EXIT_SUCCESS;
152 bool RunConfiguration(const std::string& config_file, uint32_t num_devices,
153                       DeviceType device_type, std::string& input_file)
155     DeviceIds ids;
156     for (int i = 0; i < num_devices; i++)
157         ids.insert(static_cast<DeviceId>(i));
159     // Read the TI DL configuration file
160     Configuration configuration;
161     bool status = configuration.ReadFromFile(config_file);
162     if (!status)
163     {
164         std::cerr << "Error in configuration file: " << config_file
165                   << std::endl;
166         return false;
167     }
168     configuration.runFullNet = is_partitioned ? 0 : 1;
170     // setup input
171     int num_frames = is_default_input ? 3 : 1;
172     VideoCapture cap;
173     std::string image_file;
174     if (is_camera_input)
175     {
176         cap = VideoCapture(1);  // cap = VideoCapture("test.mp4");
177         if (! cap.isOpened())
178         {
179             std::cerr << "Cannot open camera input." << std::endl;
180             return false;
181         }
182         num_frames = NUM_VIDEO_FRAMES;
183         namedWindow("SSD_Multibox", WINDOW_AUTOSIZE | CV_GUI_NORMAL);
184     }
185     else
186     {
187         image_file = input_file;
188     }
190     try
191     {
192         // Create a executor with the approriate core type, number of cores
193         // and configuration specified
194         configuration.layersGroupId = 1;
195         Executor *executor_1 = new Executor(device_type, ids, configuration);
196         Executor *executor_2 = nullptr;
197         if (is_partitioned)
198         {
199             configuration.layersGroupId       = 2;
200             configuration.enableInternalInput = 1;  // 0 is also valid
201             executor_2 = new Executor(DeviceType::DSP, ids, configuration);
202         }
204         // Query Executor for set of ExecutionObjects created
205         const ExecutionObjects *execution_objects_1, *execution_objects_2;
206         execution_objects_1 = & executor_1->GetExecutionObjects();
207         int num_eos = execution_objects_1->size();
208         if (is_partitioned)
209             execution_objects_2 = & executor_2->GetExecutionObjects();
211         // Allocate input and output buffers for each execution object
212         std::vector<void *> buffers;
213         for (int i = 0; i < num_eos; i++)
214         {
215             ExecutionObject *eo1 = execution_objects_1->at(i).get();
216             size_t in_size  = eo1->GetInputBufferSizeInBytes();
217             size_t out_size = eo1->GetOutputBufferSizeInBytes();
218             ArgInfo in  = { ArgInfo(malloc(in_size),  in_size)};
219             ArgInfo out = { ArgInfo(nullptr, 0) };
220             if (configuration.enableInternalInput == 0)
221                 out = ArgInfo(malloc(out_size), out_size);
222             eo1->SetInputOutputBuffer(in, out);
224             buffers.push_back(in.ptr());
225             buffers.push_back(out.ptr());
227             if (is_partitioned)
228             {
229                 ExecutionObject *eo2 = execution_objects_2->at(i).get();
230                 size_t out2_size = eo2->GetOutputBufferSizeInBytes();
231                 ArgInfo out2 = { ArgInfo(malloc(out2_size), out2_size) };
232                 eo2->SetInputOutputBuffer(out, out2);
233                 buffers.push_back(out2.ptr());
234             }
235         }
237         #define MAX_NUM_EOS  4
238         struct timespec t0[MAX_NUM_EOS], t1, tloop0, tloop1;
239         clock_gettime(CLOCK_MONOTONIC, &tloop0);
241         // Process frames with available execution objects in a pipelined manner
242         // additional num_eos iterations to flush the pipeline (epilogue)
243         ExecutionObject *eo1, *eo2, *eo_wait, *eo_input;
244         for (int frame_idx = 0;
245              frame_idx < num_frames + num_eos; frame_idx++)
246         {
247             eo1 = execution_objects_1->at(frame_idx % num_eos).get();
248             eo_wait = eo1;
249             if (is_partitioned)
250             {
251                 eo2 = execution_objects_2->at(frame_idx % num_eos).get();
252                 eo_wait = eo2;
253             }
255             // Wait for previous frame on the same eo to finish processing
256             if (eo_wait->ProcessFrameWait())
257             {
258                 int finished_idx = eo_wait->GetFrameIndex();
259                 clock_gettime(CLOCK_MONOTONIC, &t1);
260                 ReportTime(finished_idx,
261                            (is_partitioned || device_type == DeviceType::DSP) ?
262                            "DSP" : "DLA",
263                            ms_diff(t0[finished_idx % num_eos], t1),
264                            eo_wait->GetProcessTimeInMilliSeconds());
266                 eo_input = execution_objects_1->at(finished_idx %num_eos).get();
267                 WriteFrameOutput(*eo_input, *eo_wait, configuration);
268             }
270             // Read a frame and start processing it with current eo
271             if (ReadFrame(*eo1, frame_idx, configuration, num_frames,
272                           image_file, cap))
273             {
274                 clock_gettime(CLOCK_MONOTONIC, &t0[frame_idx % num_eos]);
275                 eo1->ProcessFrameStartAsync();
277                 if (is_partitioned && eo1->ProcessFrameWait())
278                 {
279                     clock_gettime(CLOCK_MONOTONIC, &t1);
280                     ReportTime(frame_idx, "DLA",
281                            ms_diff(t0[frame_idx % num_eos], t1),
282                            eo1->GetProcessTimeInMilliSeconds());
284                     clock_gettime(CLOCK_MONOTONIC, &t0[frame_idx % num_eos]);
285                     eo2->ProcessFrameStartAsync();
286                 }
287             }
288         }
290         clock_gettime(CLOCK_MONOTONIC, &tloop1);
291         std::cout << "Loop total time (including read/write/print/etc): "
292                   << std::setw(6) << std::setprecision(4)
293                   << ms_diff(tloop0, tloop1) << "ms" << std::endl;
295         delete executor_1;
296         delete executor_2;
297         for (auto b : buffers)
298             free(b);
299     }
300     catch (tinn::Exception &e)
301     {
302         std::cerr << e.what() << std::endl;
303         status = false;
304     }
306     return status;
309 void ReportTime(int frame_index, std::string device_name, double elapsed_host,
310                 double elapsed_device)
312     double overhead = 100 - (elapsed_device/elapsed_host*100);
313     std::cout << "frame[" << frame_index << "]: "
314               << "Time on " << device_name << ": "
315               << std::setw(6) << std::setprecision(4)
316               << elapsed_device << "ms, "
317               << "host: "
318               << std::setw(6) << std::setprecision(4)
319               << elapsed_host << "ms ";
320     std::cout << "API overhead: "
321               << std::setw(6) << std::setprecision(3)
322               << overhead << " %" << std::endl;
326 bool ReadFrame(ExecutionObject &eo, int frame_idx,
327                const Configuration& configuration, int num_frames,
328                std::string& image_file, VideoCapture &cap)
330     if (frame_idx >= num_frames)
331         return false;
332     eo.SetFrameIndex(frame_idx);
334     char*  frame_buffer = eo.GetInputBufferPtr();
335     assert (frame_buffer != nullptr);
336     int channel_size = configuration.inWidth * configuration.inHeight;
338     Mat image;
339     if (! image_file.empty())
340     {
341         if (is_preprocessed_input)
342         {
343             std::ifstream ifs(image_file, std::ios::binary);
344             ifs.seekg(frame_idx * channel_size * 3);
345             ifs.read(frame_buffer, channel_size * 3);
346             bool ifs_status = ifs.good();
347             ifs.close();
348             orig_width  = configuration.inWidth;
349             orig_height = configuration.inHeight;
350             return ifs_status;  // already PreProc-ed
351         }
352         else
353         {
354             image = cv::imread(image_file, CV_LOAD_IMAGE_COLOR);
355             if (image.empty())
356             {
357                 std::cerr << "Unable to read from: " << image_file << std::endl;
358                 return false;
359             }
360         }
361     }
362     else
363     {
364         // 640x480 camera input, process one in every 5 frames,
365         // can adjust number of skipped frames to match real time processing
366         if (! cap.grab())  return false;
367         if (! cap.grab())  return false;
368         if (! cap.grab())  return false;
369         if (! cap.grab())  return false;
370         if (! cap.grab())  return false;
371         if (! cap.retrieve(image)) return false;
372     }
374     // scale to network input size
375     Mat s_image, bgr_frames[3];
376     orig_width  = image.cols;
377     orig_height = image.rows;
378     cv::resize(image, s_image,
379                Size(configuration.inWidth, configuration.inHeight),
380                0, 0, cv::INTER_AREA);
381     cv::split(s_image, bgr_frames);
382     memcpy(frame_buffer,                bgr_frames[0].ptr(), channel_size);
383     memcpy(frame_buffer+1*channel_size, bgr_frames[1].ptr(), channel_size);
384     memcpy(frame_buffer+2*channel_size, bgr_frames[2].ptr(), channel_size);
385     return true;
388 // Create frame with boxes drawn around classified objects
389 bool WriteFrameOutput(const ExecutionObject &eo_in,
390                       const ExecutionObject &eo_out,
391                       const Configuration& configuration)
393     // Asseembly original frame
394     int width  = configuration.inWidth;
395     int height = configuration.inHeight;
396     int channel_size = width * height;
397     Mat frame, r_frame, bgr[3];
399     unsigned char *in = (unsigned char *) eo_in.GetInputBufferPtr();
400     bgr[0] = Mat(height, width, CV_8UC(1), in);
401     bgr[1] = Mat(height, width, CV_8UC(1), in + channel_size);
402     bgr[2] = Mat(height, width, CV_8UC(1), in + channel_size*2);
403     cv::merge(bgr, 3, frame);
405     int frame_index = eo_in.GetFrameIndex();
406     char outfile_name[64];
407     if (! is_camera_input && is_preprocessed_input)
408     {
409         snprintf(outfile_name, 64, "frame_%d.png", frame_index);
410         cv::imwrite(outfile_name, frame);
411         printf("Saving frame %d to: %s\n", frame_index, outfile_name);
412     }
414     // Draw boxes around classified objects
415     float *out = (float *) eo_out.GetOutputBufferPtr();
416     int num_floats = eo_out.GetOutputBufferSizeInBytes() / sizeof(float);
417     for (int i = 0; i < num_floats / 7; i++)
418     {
419         int index = (int)    out[i * 7 + 0];
420         if (index < 0)  break;
422         int   label = (int)  out[i * 7 + 1];
423         float score =        out[i * 7 + 2];
424         int   xmin  = (int) (out[i * 7 + 3] * width);
425         int   ymin  = (int) (out[i * 7 + 4] * height);
426         int   xmax  = (int) (out[i * 7 + 5] * width);
427         int   ymax  = (int) (out[i * 7 + 6] * height);
429         object_class_t *object_class = GetObjectClass(object_class_table,
430                                                       label);
431         if (object_class == nullptr)  continue;
433 #if 0
434         printf("(%d, %d) -> (%d, %d): %s, score=%f\n",
435                xmin, ymin, xmax, ymax, object_class->label, score);
436 #endif
438         cv::rectangle(frame, Point(xmin, ymin), Point(xmax, ymax),
439                       Scalar(object_class->color.blue,
440                              object_class->color.green,
441                              object_class->color.red), 2);
442     }
444     // output
445     cv::resize(frame, r_frame, Size(orig_width, orig_height));
446     if (is_camera_input)
447     {
448         cv::imshow("SSD_Multibox", r_frame);
449         waitKey(1);
450     }
451     else
452     {
453         snprintf(outfile_name, 64, "multibox_%d.png", frame_index);
454         cv::imwrite(outfile_name, r_frame);
455         printf("Saving frame %d with SSD multiboxes to: %s\n",
456                frame_index, outfile_name);
457     }
459     return true;
463 void ProcessArgs(int argc, char *argv[], std::string& config,
464                  uint32_t& num_devices, DeviceType& device_type,
465                  std::string& input_file)
467     const struct option long_options[] =
468     {
469         {"config",      required_argument, 0, 'c'},
470         {"num_devices", required_argument, 0, 'n'},
471         {"device_type", required_argument, 0, 't'},
472         {"image_file",  required_argument, 0, 'i'},
473         {"help",        no_argument,       0, 'h'},
474         {"verbose",     no_argument,       0, 'v'},
475         {0, 0, 0, 0}
476     };
478     int option_index = 0;
480     while (true)
481     {
482         int c = getopt_long(argc, argv, "c:n:t:i:hv", long_options, &option_index);
484         if (c == -1)
485             break;
487         switch (c)
488         {
489             case 'c': config = optarg;
490                       break;
492             case 'n': num_devices = atoi(optarg);
493                       assert (num_devices > 0 && num_devices <= 4);
494                       break;
496             case 't': if (*optarg == 'e')
497                       {
498                           device_type = DeviceType::DLA;
499                           is_partitioned = false;
500                       }
501 #if 0
502                       else if (*optarg == 'd')
503                       {
504                           device_type = DeviceType::DSP;
505                           is_partitioned = false;
506                       }
507 #endif
508                       else
509                       {
510                           //std::cerr << "Invalid argument to -t, only e or d"
511                           std::cerr << "Invalid argument to -t, only e"
512                                        " allowed" << std::endl;
513                           exit(EXIT_FAILURE);
514                       }
515                       break;
517             case 'i': input_file = optarg;
518                       break;
520             case 'v': __TI_show_debug_ = true;
521                       break;
523             case 'h': DisplayHelp();
524                       exit(EXIT_SUCCESS);
525                       break;
527             case '?': // Error in getopt_long
528                       exit(EXIT_FAILURE);
529                       break;
531             default:
532                       std::cerr << "Unsupported option: " << c << std::endl;
533                       break;
534         }
535     }
538 void DisplayHelp()
540     std::cout << "Usage: ssd_multibox\n"
541                  "  Will run ssd_multibox network to perform multi-objects"
542                  " classification.\n  Use -c to run a different"
543                  "  segmentation network. Default is jdetnet.\n"
544                  "Optional arguments:\n"
545                  " -c <config>          Valid configs: jdetnet, jdetnet_512x256\n"
546                  " -n <number of cores> Number of cores to use (1 - 4)\n"
547                  " -t <d|e>             Type of core. d -> DSP, e -> DLA\n"
548                  "                      DSP not supported at this time\n"
549                  "                      Default to partitioned execution: \n"
550                  "                          part 1 on DLA, part 2 on DSP\n"
551                  " -i <image>           Path to the image file\n"
552                  "                      Default is 1 frame in testvecs\n"
553                  " -i camera            Use camera as input\n"
554                  " -v                   Verbose output during execution\n"
555                  " -h                   Help\n";