1 /******************************************************************************
2 * Copyright (c) 2018, Texas Instruments Incorporated - http://www.ti.com/
3 * All rights reserved.
4 *
5 * Redistribution and use in source and binary forms, with or without
6 * modification, are permitted provided that the following conditions are met:
7 * * Redistributions of source code must retain the above copyright
8 * notice, this list of conditions and the following disclaimer.
9 * * Redistributions in binary form must reproduce the above copyright
10 * notice, this list of conditions and the following disclaimer in the
11 * documentation and/or other materials provided with the distribution.
12 * * Neither the name of Texas Instruments Incorporated nor the
13 * names of its contributors may be used to endorse or promote products
14 * derived from this software without specific prior written permission.
15 *
16 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
17 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
18 * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
19 * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE
20 * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
21 * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
22 * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
23 * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
24 * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
25 * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF
26 * THE POSSIBILITY OF SUCH DAMAGE.
27 *****************************************************************************/
28 #include <signal.h>
29 #include <getopt.h>
30 #include <iostream>
31 #include <iomanip>
32 #include <fstream>
33 #include <cassert>
34 #include <string>
35 #include <functional>
36 #include <algorithm>
37 #include <time.h>
38 #include <unistd.h>
40 #include <queue>
41 #include <vector>
42 #include <cstdio>
44 #include "executor.h"
45 #include "execution_object.h"
46 #include "configuration.h"
47 #include "../segmentation/object_classes.h"
49 #include "opencv2/core.hpp"
50 #include "opencv2/imgproc.hpp"
51 #include "opencv2/highgui.hpp"
52 #include "opencv2/videoio.hpp"
54 #define NUM_VIDEO_FRAMES 100
55 #define DEFAULT_CONFIG "jdetnet"
56 #define DEFAULT_INPUT "../test/testvecs/input/preproc_0_768x320.y"
58 bool __TI_show_debug_ = false;
59 bool is_default_input = false;
60 bool is_preprocessed_input = false;
61 bool is_camera_input = false;
62 int orig_width;
63 int orig_height;
64 object_class_table_t *object_class_table;
66 using namespace tinn;
67 using namespace cv;
70 bool RunConfiguration(const std::string& config_file, uint32_t num_devices,
71 DeviceType device_type, std::string& input_file);
72 bool ReadFrame(ExecutionObject& eo, int frame_idx,
73 const Configuration& configuration, int num_frames,
74 std::string& image_file, VideoCapture &cap);
75 bool WriteFrameOutput(const ExecutionObject &eo_in,
76 const ExecutionObject &eo_out,
77 const Configuration& configuration);
79 void ReportTime(int frame_index, std::string device_name, double elapsed_host,
80 double elapsed_device);
82 static void ProcessArgs(int argc, char *argv[],
83 std::string& config,
84 uint32_t& num_devices,
85 DeviceType& device_type,
86 std::string& input_file);
88 static void DisplayHelp();
90 static double ms_diff(struct timespec &t0, struct timespec &t1)
91 { return (t1.tv_sec - t0.tv_sec) * 1e3 + (t1.tv_nsec - t0.tv_nsec) / 1e6; }
94 int main(int argc, char *argv[])
95 {
96 // Catch ctrl-c to ensure a clean exit
97 signal(SIGABRT, exit);
98 signal(SIGTERM, exit);
100 // If there are no devices capable of offloading TIDL on the SoC, exit
101 uint32_t num_dla = Executor::GetNumDevices(DeviceType::DLA);
102 uint32_t num_dsp = Executor::GetNumDevices(DeviceType::DSP);
103 if (num_dla == 0 && num_dsp == 0)
104 {
105 std::cout << "TI DL not supported on this SoC." << std::endl;
106 return EXIT_SUCCESS;
107 }
109 // Process arguments
110 std::string config = DEFAULT_CONFIG;
111 std::string input_file = DEFAULT_INPUT;
112 uint32_t num_devices = 1;
113 DeviceType device_type = DeviceType::DLA;
114 ProcessArgs(argc, argv, config, num_devices, device_type, input_file);
116 // Use same number of DLAs and DSPs
117 num_devices = std::min(num_devices, std::min(num_dla, num_dsp));
118 if (num_devices == 0)
119 {
120 std::cout << "Partitioned execution requires at least 1 DLA and 1 DSP."
121 << std::endl;
122 return EXIT_FAILURE;
123 }
124 if ((object_class_table = GetObjectClassTable(config)) == nullptr)
125 {
126 std::cout << "No object classes defined for this config." << std::endl;
127 return EXIT_FAILURE;
128 }
130 if (input_file == DEFAULT_INPUT) is_default_input = true;
131 if (input_file == "camera") is_camera_input = true;
132 if (input_file.length() > 2 &&
133 input_file.compare(input_file.length() - 2, 2, ".y") == 0)
134 is_preprocessed_input = true;
135 std::cout << "Input: " << input_file << std::endl;
136 std::string config_file = "../test/testvecs/config/infer/tidl_config_"
137 + config + ".txt";
138 bool status = RunConfiguration(config_file, num_devices, device_type,
139 input_file);
141 if (!status)
142 {
143 std::cout << "ssd_multibox FAILED" << std::endl;
144 return EXIT_FAILURE;
145 }
147 std::cout << "ssd_multibox PASSED" << std::endl;
148 return EXIT_SUCCESS;
149 }
151 bool RunConfiguration(const std::string& config_file, uint32_t num_devices,
152 DeviceType device_type, std::string& input_file)
153 {
154 DeviceIds ids;
155 for (int i = 0; i < num_devices; i++)
156 ids.insert(static_cast<DeviceId>(i));
158 // Read the TI DL configuration file
159 Configuration configuration;
160 bool status = configuration.ReadFromFile(config_file);
161 if (!status)
162 {
163 std::cerr << "Error in configuration file: " << config_file
164 << std::endl;
165 return false;
166 }
168 // setup input
169 int num_frames = is_default_input ? 3 : 1;
170 VideoCapture cap;
171 std::string image_file;
172 if (is_camera_input)
173 {
174 cap = VideoCapture(1); // cap = VideoCapture("test.mp4");
175 if (! cap.isOpened())
176 {
177 std::cerr << "Cannot open camera input." << std::endl;
178 return false;
179 }
180 num_frames = NUM_VIDEO_FRAMES;
181 namedWindow("SSD_Multibox", WINDOW_AUTOSIZE | CV_GUI_NORMAL);
182 }
183 else
184 {
185 image_file = input_file;
186 }
188 try
189 {
190 // Create a executor with the approriate core type, number of cores
191 // and configuration specified
192 // DLA will run layersGroupId 1 in the network, while
193 // DSP will run layersGroupId 2 in the network
194 Executor executor_dla(DeviceType::DLA, ids, configuration, 1);
195 Executor executor_dsp(DeviceType::DSP, ids, configuration, 2);
197 // Query Executor for set of ExecutionObjects created
198 const ExecutionObjects& execution_objects_dla =
199 executor_dla.GetExecutionObjects();
200 const ExecutionObjects& execution_objects_dsp =
201 executor_dsp.GetExecutionObjects();
202 int num_eos = execution_objects_dla.size();
204 // Allocate input and output buffers for each execution object
205 // Note that "out" is both the output of eo_dla and the input of eo_dsp
206 // This is how two layersGroupIds, 1 and 2, are tied together
207 std::vector<void *> buffers;
208 for (int i = 0; i < num_eos; i++)
209 {
210 ExecutionObject *eo_dla = execution_objects_dla[i].get();
211 size_t in_size = eo_dla->GetInputBufferSizeInBytes();
212 size_t out_size = eo_dla->GetOutputBufferSizeInBytes();
213 ArgInfo in = { ArgInfo(malloc(in_size), in_size) };
214 ArgInfo out = { ArgInfo(malloc(out_size), out_size) };
215 eo_dla->SetInputOutputBuffer(in, out);
217 ExecutionObject *eo_dsp = execution_objects_dsp[i].get();
218 size_t out2_size = eo_dsp->GetOutputBufferSizeInBytes();
219 ArgInfo out2 = { ArgInfo(malloc(out2_size), out2_size) };
220 eo_dsp->SetInputOutputBuffer(out, out2);
222 buffers.push_back(in.ptr());
223 buffers.push_back(out.ptr());
224 buffers.push_back(out2.ptr());
225 }
227 #define MAX_NUM_EOS 4
228 struct timespec t0[MAX_NUM_EOS], t1, tloop0, tloop1;
229 clock_gettime(CLOCK_MONOTONIC, &tloop0);
231 // Process frames with available execution objects in a pipelined manner
232 // additional num_eos iterations to flush the pipeline (epilogue)
233 ExecutionObject *eo_dla, *eo_dsp, *eo_input;
234 for (int frame_idx = 0;
235 frame_idx < num_frames + num_eos; frame_idx++)
236 {
237 eo_dla = execution_objects_dla[frame_idx % num_eos].get();
238 eo_dsp = execution_objects_dsp[frame_idx % num_eos].get();
240 // Wait for previous frame on the same eo to finish processing
241 if (eo_dsp->ProcessFrameWait())
242 {
243 int finished_idx = eo_dsp->GetFrameIndex();
244 clock_gettime(CLOCK_MONOTONIC, &t1);
245 ReportTime(finished_idx, "DSP",
246 ms_diff(t0[finished_idx % num_eos], t1),
247 eo_dsp->GetProcessTimeInMilliSeconds());
249 eo_input = execution_objects_dla[finished_idx % num_eos].get();
250 WriteFrameOutput(*eo_input, *eo_dsp, configuration);
251 }
253 // Read a frame and start processing it with current eo
254 if (ReadFrame(*eo_dla, frame_idx, configuration, num_frames,
255 image_file, cap))
256 {
257 clock_gettime(CLOCK_MONOTONIC, &t0[frame_idx % num_eos]);
258 eo_dla->ProcessFrameStartAsync();
260 if (eo_dla->ProcessFrameWait())
261 {
262 clock_gettime(CLOCK_MONOTONIC, &t1);
263 ReportTime(frame_idx, "DLA",
264 ms_diff(t0[frame_idx % num_eos], t1),
265 eo_dla->GetProcessTimeInMilliSeconds());
267 clock_gettime(CLOCK_MONOTONIC, &t0[frame_idx % num_eos]);
268 eo_dsp->ProcessFrameStartAsync();
269 }
270 }
271 }
273 clock_gettime(CLOCK_MONOTONIC, &tloop1);
274 std::cout << "Loop total time (including read/write/print/etc): "
275 << std::setw(6) << std::setprecision(4)
276 << ms_diff(tloop0, tloop1) << "ms" << std::endl;
278 for (auto b : buffers)
279 free(b);
280 }
281 catch (tinn::Exception &e)
282 {
283 std::cerr << e.what() << std::endl;
284 status = false;
285 }
287 return status;
288 }
290 void ReportTime(int frame_index, std::string device_name, double elapsed_host,
291 double elapsed_device)
292 {
293 double overhead = 100 - (elapsed_device/elapsed_host*100);
294 std::cout << "frame[" << frame_index << "]: "
295 << "Time on " << device_name << ": "
296 << std::setw(6) << std::setprecision(4)
297 << elapsed_device << "ms, "
298 << "host: "
299 << std::setw(6) << std::setprecision(4)
300 << elapsed_host << "ms ";
301 std::cout << "API overhead: "
302 << std::setw(6) << std::setprecision(3)
303 << overhead << " %" << std::endl;
304 }
307 bool ReadFrame(ExecutionObject &eo, int frame_idx,
308 const Configuration& configuration, int num_frames,
309 std::string& image_file, VideoCapture &cap)
310 {
311 if (frame_idx >= num_frames)
312 return false;
313 eo.SetFrameIndex(frame_idx);
315 char* frame_buffer = eo.GetInputBufferPtr();
316 assert (frame_buffer != nullptr);
317 int channel_size = configuration.inWidth * configuration.inHeight;
319 Mat image;
320 if (! image_file.empty())
321 {
322 if (is_preprocessed_input)
323 {
324 std::ifstream ifs(image_file, std::ios::binary);
325 ifs.seekg(frame_idx * channel_size * 3);
326 ifs.read(frame_buffer, channel_size * 3);
327 bool ifs_status = ifs.good();
328 ifs.close();
329 orig_width = configuration.inWidth;
330 orig_height = configuration.inHeight;
331 return ifs_status; // already PreProc-ed
332 }
333 else
334 {
335 image = cv::imread(image_file, CV_LOAD_IMAGE_COLOR);
336 if (image.empty())
337 {
338 std::cerr << "Unable to read from: " << image_file << std::endl;
339 return false;
340 }
341 }
342 }
343 else
344 {
345 // 640x480 camera input, process one in every 5 frames,
346 // can adjust number of skipped frames to match real time processing
347 if (! cap.grab()) return false;
348 if (! cap.grab()) return false;
349 if (! cap.grab()) return false;
350 if (! cap.grab()) return false;
351 if (! cap.grab()) return false;
352 if (! cap.retrieve(image)) return false;
353 }
355 // scale to network input size
356 Mat s_image, bgr_frames[3];
357 orig_width = image.cols;
358 orig_height = image.rows;
359 cv::resize(image, s_image,
360 Size(configuration.inWidth, configuration.inHeight),
361 0, 0, cv::INTER_AREA);
362 cv::split(s_image, bgr_frames);
363 memcpy(frame_buffer, bgr_frames[0].ptr(), channel_size);
364 memcpy(frame_buffer+1*channel_size, bgr_frames[1].ptr(), channel_size);
365 memcpy(frame_buffer+2*channel_size, bgr_frames[2].ptr(), channel_size);
366 return true;
367 }
369 // Create frame with boxes drawn around classified objects
370 bool WriteFrameOutput(const ExecutionObject &eo_in,
371 const ExecutionObject &eo_out,
372 const Configuration& configuration)
373 {
374 // Asseembly original frame
375 int width = configuration.inWidth;
376 int height = configuration.inHeight;
377 int channel_size = width * height;
378 Mat frame, r_frame, bgr[3];
380 unsigned char *in = (unsigned char *) eo_in.GetInputBufferPtr();
381 bgr[0] = Mat(height, width, CV_8UC(1), in);
382 bgr[1] = Mat(height, width, CV_8UC(1), in + channel_size);
383 bgr[2] = Mat(height, width, CV_8UC(1), in + channel_size*2);
384 cv::merge(bgr, 3, frame);
386 int frame_index = eo_in.GetFrameIndex();
387 char outfile_name[64];
388 if (! is_camera_input && is_preprocessed_input)
389 {
390 snprintf(outfile_name, 64, "frame_%d.png", frame_index);
391 cv::imwrite(outfile_name, frame);
392 printf("Saving frame %d to: %s\n", frame_index, outfile_name);
393 }
395 // Draw boxes around classified objects
396 float *out = (float *) eo_out.GetOutputBufferPtr();
397 int num_floats = eo_out.GetOutputBufferSizeInBytes() / sizeof(float);
398 for (int i = 0; i < num_floats / 7; i++)
399 {
400 int index = (int) out[i * 7 + 0];
401 if (index < 0) break;
403 int label = (int) out[i * 7 + 1];
404 float score = out[i * 7 + 2];
405 int xmin = (int) (out[i * 7 + 3] * width);
406 int ymin = (int) (out[i * 7 + 4] * height);
407 int xmax = (int) (out[i * 7 + 5] * width);
408 int ymax = (int) (out[i * 7 + 6] * height);
410 object_class_t *object_class = GetObjectClass(object_class_table,
411 label);
412 if (object_class == nullptr) continue;
414 #if 0
415 printf("(%d, %d) -> (%d, %d): %s, score=%f\n",
416 xmin, ymin, xmax, ymax, object_class->label, score);
417 #endif
419 cv::rectangle(frame, Point(xmin, ymin), Point(xmax, ymax),
420 Scalar(object_class->color.blue,
421 object_class->color.green,
422 object_class->color.red), 2);
423 }
425 // output
426 cv::resize(frame, r_frame, Size(orig_width, orig_height));
427 if (is_camera_input)
428 {
429 cv::imshow("SSD_Multibox", r_frame);
430 waitKey(1);
431 }
432 else
433 {
434 snprintf(outfile_name, 64, "multibox_%d.png", frame_index);
435 cv::imwrite(outfile_name, r_frame);
436 printf("Saving frame %d with SSD multiboxes to: %s\n",
437 frame_index, outfile_name);
438 }
440 return true;
441 }
444 void ProcessArgs(int argc, char *argv[], std::string& config,
445 uint32_t& num_devices, DeviceType& device_type,
446 std::string& input_file)
447 {
448 const struct option long_options[] =
449 {
450 {"config", required_argument, 0, 'c'},
451 {"num_devices", required_argument, 0, 'n'},
452 {"image_file", required_argument, 0, 'i'},
453 {"help", no_argument, 0, 'h'},
454 {"verbose", no_argument, 0, 'v'},
455 {0, 0, 0, 0}
456 };
458 int option_index = 0;
460 while (true)
461 {
462 int c = getopt_long(argc, argv, "c:n:i:hv", long_options, &option_index);
464 if (c == -1)
465 break;
467 switch (c)
468 {
469 case 'c': config = optarg;
470 break;
472 case 'n': num_devices = atoi(optarg);
473 assert (num_devices > 0 && num_devices <= 4);
474 break;
476 case 'i': input_file = optarg;
477 break;
479 case 'v': __TI_show_debug_ = true;
480 break;
482 case 'h': DisplayHelp();
483 exit(EXIT_SUCCESS);
484 break;
486 case '?': // Error in getopt_long
487 exit(EXIT_FAILURE);
488 break;
490 default:
491 std::cerr << "Unsupported option: " << c << std::endl;
492 break;
493 }
494 }
495 }
497 void DisplayHelp()
498 {
499 std::cout << "Usage: ssd_multibox\n"
500 " Will run partitioned ssd_multibox network to perform "
501 "multi-objects detection\n"
502 " and classification. First part of network "
503 "(layersGroupId 1) runs on DLA,\n"
504 " second part (layersGroupId 2) runs on DSP.\n"
505 " Use -c to run a different segmentation network. "
506 "Default is jdetnet.\n"
507 "Optional arguments:\n"
508 " -c <config> Valid configs: jdetnet \n"
509 " -n <number of cores> Number of cores to use (1 - 4)\n"
510 " -i <image> Path to the image file\n"
511 " Default is 1 frame in testvecs\n"
512 " -i camera Use camera as input\n"
513 " -v Verbose output during execution\n"
514 " -h Help\n";
515 }