Add ssd_multibox example to tinn (Part 1)
[tidl/tidl-api.git] / examples / ssd_multibox / main.cpp
1 /******************************************************************************
2  * Copyright (c) 2018, Texas Instruments Incorporated - http://www.ti.com/
3  *   All rights reserved.
4  *
5  *   Redistribution and use in source and binary forms, with or without
6  *   modification, are permitted provided that the following conditions are met:
7  *       * Redistributions of source code must retain the above copyright
8  *         notice, this list of conditions and the following disclaimer.
9  *       * Redistributions in binary form must reproduce the above copyright
10  *         notice, this list of conditions and the following disclaimer in the
11  *         documentation and/or other materials provided with the distribution.
12  *       * Neither the name of Texas Instruments Incorporated nor the
13  *         names of its contributors may be used to endorse or promote products
14  *         derived from this software without specific prior written permission.
15  *
16  *   THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
17  *   AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
18  *   IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
19  *   ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE
20  *   LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
21  *   CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
22  *   SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
23  *   INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
24  *   CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
25  *   ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF
26  *   THE POSSIBILITY OF SUCH DAMAGE.
27  *****************************************************************************/
28 #include <signal.h>
29 #include <getopt.h>
30 #include <iostream>
31 #include <iomanip>
32 #include <fstream>
33 #include <cassert>
34 #include <string>
35 #include <functional>
36 #include <algorithm>
37 #include <time.h>
38 #include <unistd.h>
40 #include <queue>
41 #include <vector>
42 #include <cstdio>
44 #include "executor.h"
45 #include "execution_object.h"
46 #include "configuration.h"
47 #include "../segmentation/object_classes.h"
49 #include "opencv2/core.hpp"
50 #include "opencv2/imgproc.hpp"
51 #include "opencv2/highgui.hpp"
52 #include "opencv2/videoio.hpp"
54 #define NUM_VIDEO_FRAMES  100
55 #define DEFAULT_CONFIG    "jdetnet"
56 #define DEFAULT_INPUT     "../test/testvecs/input/preproc_0_768x320.y"
58 bool __TI_show_debug_ = false;
59 bool is_default_input = false;
60 bool is_preprocessed_input = false;
61 bool is_camera_input       = false;
62 int  orig_width;
63 int  orig_height;
64 object_class_table_t *object_class_table;
66 using namespace tinn;
67 using namespace cv;
70 bool RunConfiguration(const std::string& config_file, int num_devices,
71                       DeviceType device_type, std::string& input_file);
72 bool RunAllConfigurations(int32_t num_devices, DeviceType device_type);
74 bool ReadFrame(ExecutionObject& eo, int frame_idx,
75                const Configuration& configuration, int num_frames,
76                std::string& image_file, VideoCapture &cap);
77 bool WriteFrameOutput(const ExecutionObject &eo,
78                       const Configuration& configuration);
80 static void ProcessArgs(int argc, char *argv[],
81                         std::string& config,
82                         int& num_devices,
83                         DeviceType& device_type,
84                         std::string& input_file);
86 static void DisplayHelp();
88 static double ms_diff(struct timespec &t0, struct timespec &t1)
89 { return (t1.tv_sec - t0.tv_sec) * 1e3 + (t1.tv_nsec - t0.tv_nsec) / 1e6; }
92 int main(int argc, char *argv[])
93 {
94     // Catch ctrl-c to ensure a clean exit
95     signal(SIGABRT, exit);
96     signal(SIGTERM, exit);
98     // If there are no devices capable of offloading TIDL on the SoC, exit
99     uint32_t num_dla = Executor::GetNumDevices(DeviceType::DLA);
100     uint32_t num_dsp = Executor::GetNumDevices(DeviceType::DSP);
101     if (num_dla == 0 && num_dsp == 0)
102     {
103         std::cout << "TI DL not supported on this SoC." << std::endl;
104         return EXIT_SUCCESS;
105     }
107     // Process arguments
108     std::string config      = DEFAULT_CONFIG;
109     std::string input_file  = DEFAULT_INPUT;
110     int         num_devices = 1;
111     DeviceType  device_type = DeviceType::DLA;
112     ProcessArgs(argc, argv, config, num_devices, device_type, input_file);
114     if ((object_class_table = GetObjectClassTable(config)) == nullptr)
115     {
116         std::cout << "No object classes defined for this config." << std::endl;
117         return EXIT_FAILURE;
118     }
120     if (input_file == DEFAULT_INPUT)  is_default_input = true;
121     if (input_file == "camera")       is_camera_input = true;
122     if (input_file.length() > 2 &&
123         input_file.compare(input_file.length() - 2, 2, ".y") == 0)
124         is_preprocessed_input = true;
125     std::cout << "Input: " << input_file << std::endl;
126     std::string config_file = "../test/testvecs/config/infer/tidl_config_"
127                               + config + ".txt";
128     bool status = RunConfiguration(config_file, num_devices, device_type,
129                                    input_file);
131     if (!status)
132     {
133         std::cout << "ssd_multibox FAILED" << std::endl;
134         return EXIT_FAILURE;
135     }
137     std::cout << "ssd_multibox PASSED" << std::endl;
138     return EXIT_SUCCESS;
141 bool RunConfiguration(const std::string& config_file, int num_devices,
142                       DeviceType device_type, std::string& input_file)
144     DeviceIds ids;
145     for (int i = 0; i < num_devices; i++)
146         ids.insert(static_cast<DeviceId>(i));
148     // Read the TI DL configuration file
149     Configuration configuration;
150     bool status = configuration.ReadFromFile(config_file);
151     if (!status)
152     {
153         std::cerr << "Error in configuration file: " << config_file
154                   << std::endl;
155         return false;
156     }
157     if (device_type == DeviceType::DLA || device_type == DeviceType::DSP)
158         configuration.runFullNet = 1;
160     // setup input
161     int num_frames = is_default_input ? 3 : 1;
162     VideoCapture cap;
163     std::string image_file;
164     if (is_camera_input)
165     {
166         cap = VideoCapture(1);  // cap = VideoCapture("test.mp4");
167         if (! cap.isOpened())
168         {
169             std::cerr << "Cannot open camera input." << std::endl;
170             return false;
171         }
172         num_frames = NUM_VIDEO_FRAMES;
173         namedWindow("SSD_Multibox", WINDOW_AUTOSIZE | CV_GUI_NORMAL);
174     }
175     else
176     {
177         image_file = input_file;
178     }
180     // Determine input frame size from configuration
181     size_t frame_sz = configuration.inWidth * configuration.inHeight *
182                       configuration.inNumChannels;
184     try
185     {
186         // Create a executor with the approriate core type, number of cores
187         // and configuration specified
188         Executor executor(device_type, ids, configuration);
190         // Query Executor for set of ExecutionObjects created
191         const ExecutionObjects& execution_objects =
192                                                 executor.GetExecutionObjects();
193         int num_eos = execution_objects.size();
195         // Allocate input and output buffers for each execution object
196         std::vector<void *> buffers;
197         for (auto &eo : execution_objects)
198         {
199             ArgInfo in  = { ArgInfo(malloc(frame_sz), frame_sz)};
200             ArgInfo out = { ArgInfo(malloc(frame_sz), frame_sz)};
201             eo->SetInputOutputBuffer(in, out);
203             buffers.push_back(in.ptr());
204             buffers.push_back(out.ptr());
205         }
207         #define MAX_NUM_EOS  4
208         struct timespec t0[MAX_NUM_EOS], t1;
210         // Process frames with available execution objects in a pipelined manner
211         // additional num_eos iterations to flush the pipeline (epilogue)
212         for (int frame_idx = 0;
213              frame_idx < num_frames + num_eos; frame_idx++)
214         {
215             ExecutionObject* eo = execution_objects[frame_idx % num_eos].get();
217             // Wait for previous frame on the same eo to finish processing
218             if (eo->ProcessFrameWait())
219             {
220                 clock_gettime(CLOCK_MONOTONIC, &t1);
221                 double elapsed_host =
222                                 ms_diff(t0[eo->GetFrameIndex() % num_eos], t1);
223                 double elapsed_device = eo->GetProcessTimeInMilliSeconds();
224                 double overhead = 100 - (elapsed_device/elapsed_host*100);
226                 std::cout << "frame[" << eo->GetFrameIndex() << "]: "
227                           << "Time on device: "
228                           << std::setw(6) << std::setprecision(4)
229                           << elapsed_device << "ms, "
230                           << "host: "
231                           << std::setw(6) << std::setprecision(4)
232                           << elapsed_host << "ms ";
233                 std::cout << "API overhead: "
234                           << std::setw(6) << std::setprecision(3)
235                           << overhead << " %" << std::endl;
237                 WriteFrameOutput(*eo, configuration);
238             }
240             // Read a frame and start processing it with current eo
241             if (ReadFrame(*eo, frame_idx, configuration, num_frames,
242                           image_file, cap))
243             {
244                 clock_gettime(CLOCK_MONOTONIC, &t0[frame_idx % num_eos]);
245                 eo->ProcessFrameStartAsync();
246             }
247         }
249         for (auto b : buffers)
250             free(b);
252     }
253     catch (tinn::Exception &e)
254     {
255         std::cerr << e.what() << std::endl;
256         status = false;
257     }
259     return status;
263 bool ReadFrame(ExecutionObject &eo, int frame_idx,
264                const Configuration& configuration, int num_frames,
265                std::string& image_file, VideoCapture &cap)
267     if (frame_idx >= num_frames)
268         return false;
269     eo.SetFrameIndex(frame_idx);
271     char*  frame_buffer = eo.GetInputBufferPtr();
272     assert (frame_buffer != nullptr);
273     int channel_size = configuration.inWidth * configuration.inHeight;
275     Mat image;
276     if (! image_file.empty())
277     {
278         if (is_preprocessed_input)
279         {
280             std::ifstream ifs(image_file, std::ios::binary);
281             ifs.seekg(frame_idx * channel_size * 3);
282             ifs.read(frame_buffer, channel_size * 3);
283             bool ifs_status = ifs.good();
284             ifs.close();
285             orig_width  = configuration.inWidth;
286             orig_height = configuration.inHeight;
287             return ifs_status;  // already PreProc-ed
288         }
289         else
290         {
291             image = cv::imread(image_file, CV_LOAD_IMAGE_COLOR);
292             if (image.empty())
293             {
294                 std::cerr << "Unable to read from: " << image_file << std::endl;
295                 return false;
296             }
297         }
298     }
299     else
300     {
301         // 640x480 camera input, process one in every 5 frames,
302         // can adjust number of skipped frames to match real time processing
303         if (! cap.grab())  return false;
304         if (! cap.grab())  return false;
305         if (! cap.grab())  return false;
306         if (! cap.grab())  return false;
307         if (! cap.grab())  return false;
308         if (! cap.retrieve(image)) return false;
309     }
311     // scale to network input size
312     Mat s_image, bgr_frames[3];
313     orig_width  = image.cols;
314     orig_height = image.rows;
315     cv::resize(image, s_image,
316                Size(configuration.inWidth, configuration.inHeight),
317                0, 0, cv::INTER_AREA);
318     cv::split(s_image, bgr_frames);
319     memcpy(frame_buffer,                bgr_frames[0].ptr(), channel_size);
320     memcpy(frame_buffer+1*channel_size, bgr_frames[1].ptr(), channel_size);
321     memcpy(frame_buffer+2*channel_size, bgr_frames[2].ptr(), channel_size);
322     return true;
325 // Create frame with boxes drawn around classified objects
326 bool WriteFrameOutput(const ExecutionObject &eo,
327                       const Configuration& configuration)
329     // Asseembly original frame
330     int width  = configuration.inWidth;
331     int height = configuration.inHeight;
332     int channel_size = width * height;
333     Mat frame, r_frame, bgr[3];
335     unsigned char *in = (unsigned char *) eo.GetInputBufferPtr();
336     bgr[0] = Mat(height, width, CV_8UC(1), in);
337     bgr[1] = Mat(height, width, CV_8UC(1), in + channel_size);
338     bgr[2] = Mat(height, width, CV_8UC(1), in + channel_size*2);
339     cv::merge(bgr, 3, frame);
341     int frame_index = eo.GetFrameIndex();
342     char outfile_name[64];
343     if (! is_camera_input && is_preprocessed_input)
344     {
345         snprintf(outfile_name, 64, "frame_%d.png", frame_index);
346         cv::imwrite(outfile_name, frame);
347         printf("Saving frame %d to: %s\n", frame_index, outfile_name);
348     }
350     // Draw boxes around classified objects
351     float *out = (float *) eo.GetOutputBufferPtr();
352     int num_floats = eo.GetOutputBufferSizeInBytes() / sizeof(float);
353     for (int i = 0; i < num_floats / 7; i++)
354     {
355         int index = (int)    out[i * 7 + 0];
356         if (index < 0)  break;
358         int   label = (int)  out[i * 7 + 1];
359         float score =        out[i * 7 + 2];
360         int   xmin  = (int) (out[i * 7 + 3] * width);
361         int   ymin  = (int) (out[i * 7 + 4] * height);
362         int   xmax  = (int) (out[i * 7 + 5] * width);
363         int   ymax  = (int) (out[i * 7 + 6] * height);
365         object_class_t *object_class = GetObjectClass(object_class_table,
366                                                       label);
367         if (object_class == nullptr)  continue;
369 #if 0
370         printf("(%d, %d) -> (%d, %d): %s, score=%f\n",
371                xmin, ymin, xmax, ymax, object_class->label, score);
372 #endif
374         cv::rectangle(frame, Point(xmin, ymin), Point(xmax, ymax),
375                       Scalar(object_class->color[0], object_class->color[1],
376                              object_class->color[2]), 2);
377     }
379     // output
380     cv::resize(frame, r_frame, Size(orig_width, orig_height));
381     if (is_camera_input)
382     {
383         cv::imshow("SSD_Multibox", r_frame);
384         waitKey(1);
385     }
386     else
387     {
388         snprintf(outfile_name, 64, "multibox_%d.png", frame_index);
389         cv::imwrite(outfile_name, r_frame);
390         printf("Saving frame %d with SSD multiboxes to: %s\n",
391                frame_index, outfile_name);
392     }
394     return true;
398 void ProcessArgs(int argc, char *argv[], std::string& config,
399                  int& num_devices, DeviceType& device_type,
400                  std::string& input_file)
402     const struct option long_options[] =
403     {
404         {"config",      required_argument, 0, 'c'},
405         {"num_devices", required_argument, 0, 'n'},
406         {"device_type", required_argument, 0, 't'},
407         {"image_file",  required_argument, 0, 'i'},
408         {"help",        no_argument,       0, 'h'},
409         {"verbose",     no_argument,       0, 'v'},
410         {0, 0, 0, 0}
411     };
413     int option_index = 0;
415     while (true)
416     {
417         int c = getopt_long(argc, argv, "c:n:t:i:hv", long_options, &option_index);
419         if (c == -1)
420             break;
422         switch (c)
423         {
424             case 'c': config = optarg;
425                       break;
427             case 'n': num_devices = atoi(optarg);
428                       assert (num_devices > 0 && num_devices <= 4);
429                       break;
431             case 't': if (*optarg == 'e')
432                           device_type = DeviceType::DLA;
433 #if 0
434                       else if (*optarg == 'd')
435                           device_type = DeviceType::DSP;
436 #endif
437                       else
438                       {
439                           //std::cerr << "Invalid argument to -t, only e or d"
440                           std::cerr << "Invalid argument to -t, only e"
441                                        " allowed" << std::endl;
442                           exit(EXIT_FAILURE);
443                       }
444                       break;
446             case 'i': input_file = optarg;
447                       break;
449             case 'v': __TI_show_debug_ = true;
450                       break;
452             case 'h': DisplayHelp();
453                       exit(EXIT_SUCCESS);
454                       break;
456             case '?': // Error in getopt_long
457                       exit(EXIT_FAILURE);
458                       break;
460             default:
461                       std::cerr << "Unsupported option: " << c << std::endl;
462                       break;
463         }
464     }
467 void DisplayHelp()
469     std::cout << "Usage: ssd_multibox\n"
470                  "  Will run ssd_multibox network to perform multi-objects"
471                  " classification.\n  Use -c to run a different"
472                  "  segmentation network. Default is jdetnet.\n"
473                  "Optional arguments:\n"
474                  " -c <config>          Valid configs: jdetnet, jdetnet_512x256\n"
475                  " -n <number of cores> Number of cores to use (1 - 4)\n"
476                  " -t <d|e>             Type of core. d -> DSP, e -> DLA\n"
477                  "                      Only support DLA for now\n"
478                  " -i <image>           Path to the image file\n"
479                  "                      Default is 1 frame in testvecs\n"
480                  " -i camera            Use camera as input\n"
481                  " -v                   Verbose output during execution\n"
482                  " -h                   Help\n";