a289507d4b050a9d9418b8424de26397e16b7f87
[tidl/tidl-api.git] / examples / two_eo_per_frame / main.cpp
1 /******************************************************************************
2  * Copyright (c) 2017-2018  Texas Instruments Incorporated - http://www.ti.com/
3  *  All rights reserved.
4  *
5  *  Redistribution and use in source and binary forms, with or without
6  *  modification, are permitted provided that the following conditions are met:
7  *      * Redistributions of source code must retain the above copyright
8  *        notice, this list of conditions and the following disclaimer.
9  *      * Redistributions in binary form must reproduce the above copyright
10  *        notice, this list of conditions and the following disclaimer in the
11  *        documentation and/or other materials provided with the distribution.
12  *      * Neither the name of Texas Instruments Incorporated nor the
13  *        names of its contributors may be used to endorse or promote products
14  *        derived from this software without specific prior written permission.
15  *
16  *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
17  *  AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
18  *  IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
19  *  ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE
20  *  LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
21  *  CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
22  *  SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
23  *  INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
24  *  CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
25  *  ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF
26  *  THE POSSIBILITY OF SUCH DAMAGE.
27  *****************************************************************************/
29 //
30 // This example illustrates using multiple EOs to process a single frame
31 // For details, refer http://downloads.ti.com/mctools/esd/docs/tidl-api/
32 //
33 #include <signal.h>
34 #include <iostream>
35 #include <fstream>
36 #include <cassert>
37 #include <string>
39 #include "executor.h"
40 #include "execution_object.h"
41 #include "execution_object_pipeline.h"
42 #include "configuration.h"
43 #include "utils.h"
45 using namespace tidl;
46 using std::string;
47 using std::unique_ptr;
48 using std::vector;
50 using EOP = tidl::ExecutionObjectPipeline;
52 bool Run(int num_eve,int num_dsp, const char* ref_output);
54 Executor* CreateExecutor(DeviceType dt, int num, const Configuration& c,
55                          int layer_group_id);
57 void AllocateMemory(const vector<EOP *>& EOPs);
58 void FreeMemory    (const vector<EOP *>& EOPs);
61 int main(int argc, char *argv[])
62 {
63     // Catch ctrl-c to ensure a clean exit
64     signal(SIGABRT, exit);
65     signal(SIGTERM, exit);
67     // This example requires both EVE and C66x
68     uint32_t num_eve = Executor::GetNumDevices(DeviceType::EVE);
69     uint32_t num_dsp = Executor::GetNumDevices(DeviceType::DSP);
70     if (num_eve == 0 || num_dsp == 0)
71     {
72         std::cout << "TI DL not supported on this SoC." << std::endl;
73         return EXIT_SUCCESS;
74     }
76     string ref_file ="../test/testvecs/reference/j11_v2_ref.bin";
77     unique_ptr<const char> reference_output(ReadReferenceOutput(ref_file));
79     bool status = Run(num_eve, num_dsp, reference_output.get());
81     if (!status)
82     {
83         std::cout << "FAILED" << std::endl;
84         return EXIT_FAILURE;
85     }
87     std::cout << "PASSED" << std::endl;
88     return EXIT_SUCCESS;
89 }
91 bool Run(int num_eve, int num_dsp, const char* ref_output)
92 {
93     string config_file ="../test/testvecs/config/infer/tidl_config_j11_v2.txt";
95     Configuration c;
96     if (!c.ReadFromFile(config_file))
97         return false;
99     // Heap sizes for this network determined using Configuration::showHeapStats
100     c.PARAM_HEAP_SIZE   = (3 << 20); // 3MB
101     c.NETWORK_HEAP_SIZE = (20 << 20); // 20MB
103     c.numFrames = 16;
105     // Assign layers 12, 13 and 14 to layer group 2
106     c.layerIndex2LayerGroupId = { {12, 2}, {13, 2}, {14, 2} };
108     // Open input file for reading
109     std::ifstream input(c.inData, std::ios::binary);
111     bool status = true;
112     try
113     {
114         // Create Executors - use all the DSP and EVE cores available
115         // Layer group 1 will be executed on EVE, 2 on DSP
116         unique_ptr<Executor> eve(CreateExecutor(DeviceType::EVE,num_eve,c,1));
117         unique_ptr<Executor> dsp(CreateExecutor(DeviceType::DSP,num_dsp,c,2));
119         // Create pipelines. Each pipeline has 1 EVE and 1 DSP. If there are
120         // more EVEs than DSPs, the DSPs are shared across multiple
121         // pipelines. E.g.
122         // 2 EVE, 2 DSP: EVE1 -> DSP1, EVE2 -> DSP2
123         // 4 EVE, 2 DSP: EVE1 -> DSP1, EVE2 -> DSP2, EVE3 -> DSP1, EVE4 ->DSP2
124         std::vector<EOP *> EOPs;
125         uint32_t num_pipe = std::max(num_eve, num_dsp);
126         for (uint32_t i = 0; i < num_pipe; i++)
127               EOPs.push_back(new EOP( { (*eve)[i % num_eve],
128                                         (*dsp)[i % num_dsp] } ));
130         AllocateMemory(EOPs);
132         // Process frames with EOs in a pipelined manner
133         // additional num_eos iterations to flush the pipeline (epilogue)
134         int num_eops = EOPs.size();
135         for (int frame_idx = 0; frame_idx < c.numFrames + num_eops; frame_idx++)
136         {
137             EOP* eop = EOPs[frame_idx % num_eops];
139             // Wait for previous frame on the same eo to finish processing
140             if (eop->ProcessFrameWait())
141             {
142                 ReportTime(eop);
144                 // The reference output is valid only for the first frame
145                 // processed on each EOP
146                 if (frame_idx < num_eops && !CheckFrame(eop, ref_output))
147                     status = false;
148             }
150             // Read a frame and start processing it with current eo
151             if (ReadFrame(eop, frame_idx, c, input))
152                 eop->ProcessFrameStartAsync();
153         }
155         FreeMemory(EOPs);
157     }
158     catch (tidl::Exception &e)
159     {
160         std::cerr << e.what() << std::endl;
161         status = false;
162     }
164     input.close();
166     return status;
169 // Create an Executor with the specified type and number of EOs
170 Executor* CreateExecutor(DeviceType dt, int num, const Configuration& c,
171                          int layer_group_id)
173     if (num == 0) return nullptr;
175     DeviceIds ids;
176     for (int i = 0; i < num; i++)
177         ids.insert(static_cast<DeviceId>(i));
179     return new Executor(dt, ids, c, layer_group_id);
182 // Allocate input and output memory for each EO
183 void AllocateMemory(const vector<EOP *>& EOPs)
185     // Allocate input and output buffers for each execution object
186     for (auto eop : EOPs)
187     {
188         size_t in_size  = eop->GetInputBufferSizeInBytes();
189         size_t out_size = eop->GetOutputBufferSizeInBytes();
190         ArgInfo in  = { ArgInfo(malloc(in_size),  in_size)};
191         ArgInfo out = { ArgInfo(malloc(out_size), out_size)};
192         eop->SetInputOutputBuffer(in, out);
193     }
196 // Free the input and output memory associated with each EO
197 void FreeMemory(const vector<EOP *>& EOPs)
199     for (auto eop : EOPs)
200     {
201         free(eop->GetInputBufferPtr());
202         free(eop->GetOutputBufferPtr());
203     }