1 /******************************************************************************
2 * Copyright (c) 2017 Texas Instruments Incorporated - http://www.ti.com/
3 * All rights reserved.
4 *
5 * Redistribution and use in source and binary forms, with or without
6 * modification, are permitted provided that the following conditions are met:
7 * * Redistributions of source code must retain the above copyright
8 * notice, this list of conditions and the following disclaimer.
9 * * Redistributions in binary form must reproduce the above copyright
10 * notice, this list of conditions and the following disclaimer in the
11 * documentation and/or other materials provided with the distribution.
12 * * Neither the name of Texas Instruments Incorporated nor the
13 * names of its contributors may be used to endorse or promote products
14 * derived from this software without specific prior written permission.
15 *
16 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
17 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
18 * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
19 * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE
20 * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
21 * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
22 * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
23 * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
24 * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
25 * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF
26 * THE POSSIBILITY OF SUCH DAMAGE.
27 *****************************************************************************/
29 #pragma once
31 //! @file configuration.h
33 #include <string>
34 #include <iostream>
36 namespace tidl {
38 /*! @class Configuration
39 @brief Specifies the configuration required for a network
40 */
41 class Configuration
42 {
43 public:
45 //! Number of frames of input data (can be 0 if data is not read from file)
46 int numFrames;
48 //! Height of the input frame
49 int inHeight;
51 //! Width of the input frame
52 int inWidth;
54 //! Number of channels in the input frame (e.g. 3 for BGR)
55 int inNumChannels;
56 int noZeroCoeffsPercentage;
58 //! Pre-processing type applied to the input frame
59 //! Specific to each network, can take values from 0 to 4, default is 0
60 int preProcType;
62 //! Force to run all layers, regardless of layersGroupId partitioning
63 int runFullNet;
65 //! When set, inputs are taken from TIDL internal buffers that contain
66 //! outputs of previous layersGroupId, instead of from user application
67 int enableInternalInput;
69 //! Size of the TI DL per Execution Object heap
70 size_t EXTMEM_HEAP_SIZE;
72 //! Size of the heap used for paramter data
73 size_t PARAM_HEAP_SIZE;
75 //! @brief Location of the input file
76 //! Can be empty if input data is provided by frameworks such as OpenCV.
77 std::string inData;
79 //! Location of the output file
80 //! Can be empty if output data is consumed by frameworks such as OpenCV.
81 std::string outData;
83 //! Path to the TIDL network binary file
84 std::string netBinFile;
86 //! Path to the TIDL parameter binary file
87 std::string paramsBinFile;
89 //! Default constructor.
90 Configuration();
92 //! Validate the fields in the configuration object
93 bool Validate() const;
95 //! Print the configuration
96 void Print(std::ostream& os = std::cout) const;
98 //! Read a configuration from the specified file and validate
99 bool ReadFromFile(const std::string& file_name);
100 };
102 }