TIDL-API docu update: time, probability
[tidl/tidl-api.git] / tidl_api / inc / configuration.h
1 /******************************************************************************
2  * Copyright (c) 2017-2018 Texas Instruments Incorporated - http://www.ti.com/
3  *  All rights reserved.
4  *
5  *  Redistribution and use in source and binary forms, with or without
6  *  modification, are permitted provided that the following conditions are met:
7  *      * Redistributions of source code must retain the above copyright
8  *        notice, this list of conditions and the following disclaimer.
9  *      * Redistributions in binary form must reproduce the above copyright
10  *        notice, this list of conditions and the following disclaimer in the
11  *        documentation and/or other materials provided with the distribution.
12  *      * Neither the name of Texas Instruments Incorporated nor the
13  *        names of its contributors may be used to endorse or promote products
14  *        derived from this software without specific prior written permission.
15  *
16  *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
17  *  AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
18  *  IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
19  *  ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE
20  *  LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
21  *  CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
22  *  SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
23  *  INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
24  *  CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
25  *  ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF
26  *  THE POSSIBILITY OF SUCH DAMAGE.
27  *****************************************************************************/
29 #pragma once
31 //! @file configuration.h
33 #include <string>
34 #include <iostream>
36 namespace tidl {
38 /*! @class Configuration
39     @brief Specifies the configuration required for a network
40 */
41 class Configuration
42 {
43   public:
45     //! Number of frames of input data (can be 0 if data is not read from file)
46     int     numFrames;
48     //! Height of the input frame
49     int     inHeight;
51     //! Width of the input frame
52     int     inWidth;
54     //! Number of channels in the input frame (e.g. 3 for BGR)
55     int     inNumChannels;
56     int     noZeroCoeffsPercentage;
58     //! Pre-processing type applied to the input frame
59     //! Specific to each network, can take values from 0 to 4, default is 0
60     int     preProcType;
62     //! Force to run all layers, regardless of layersGroupId partitioning
63     int     runFullNet;
65     //! When set, inputs are taken from TIDL internal buffers that contain
66     //! outputs of previous layersGroupId, instead of from user application
67     int     enableInternalInput;
69     //! Size of the TI DL per Execution Object heap
70     size_t EXTMEM_HEAP_SIZE;
72     //! Size of the heap used for paramter data
73     size_t PARAM_HEAP_SIZE;
75     //! @brief Location of the input file
76     //! Can be empty if input data is provided by frameworks such as OpenCV.
77     std::string inData;
79     //! Location of the output file
80     //! Can be empty if output data is consumed by frameworks such as OpenCV.
81     std::string outData;
83     //! Path to the TIDL network binary file
84     std::string netBinFile;
86     //! Path to the TIDL parameter binary file
87     std::string paramsBinFile;
89     //! Default constructor.
90     Configuration();
92     //! Validate the fields in the configuration object
93     bool Validate() const;
95     //! Print the configuration
96     void Print(std::ostream& os = std::cout) const;
98     //! Read a configuration from the specified file and validate
99     bool ReadFromFile(const std::string& file_name);
100 };