1 /******************************************************************************
2 * Copyright (c) 2017 Texas Instruments Incorporated - http://www.ti.com/
3 * All rights reserved.
4 *
5 * Redistribution and use in source and binary forms, with or without
6 * modification, are permitted provided that the following conditions are met:
7 * * Redistributions of source code must retain the above copyright
8 * notice, this list of conditions and the following disclaimer.
9 * * Redistributions in binary form must reproduce the above copyright
10 * notice, this list of conditions and the following disclaimer in the
11 * documentation and/or other materials provided with the distribution.
12 * * Neither the name of Texas Instruments Incorporated nor the
13 * names of its contributors may be used to endorse or promote products
14 * derived from this software without specific prior written permission.
15 *
16 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
17 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
18 * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
19 * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE
20 * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
21 * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
22 * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
23 * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
24 * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
25 * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF
26 * THE POSSIBILITY OF SUCH DAMAGE.
27 *****************************************************************************/
29 /*! @file execution_object.h */
31 #pragma once
33 #include <memory>
35 namespace tidl {
37 class Kernel;
38 class Device;
40 /*! @class ExecutionObject
41 @brief Runs the TIDL network on an OpenCL device
42 */
44 class ExecutionObject
45 {
46 public:
48 //! @private
49 // Used by the Executor to construct an ExecutionObject
50 ExecutionObject(Device* d, uint8_t device_index,
51 const ArgInfo& create_arg,
52 const ArgInfo& param_heap_arg,
53 size_t extmem_heap_size,
54 bool internal_input);
55 //! @private
56 ~ExecutionObject();
58 //! Specify the input and output buffers used by the EO
59 //! @param in buffer used for input.
60 //! @param out buffer used for output.
61 void SetInputOutputBuffer (const ArgInfo& in, const ArgInfo& out);
63 //! Returns a pointer to the input buffer set via SetInputOutputBuffer
64 char* GetInputBufferPtr() const;
66 //! Returns size of the input buffer
67 size_t GetInputBufferSizeInBytes() const;
69 //! @brief Set the frame index of the frame currently processed by the
70 //! ExecutionObject. Used for trace/debug messages
71 //! @param idx index of the frame
72 void SetFrameIndex(int idx);
74 //! Returns the index of a frame being processed (set by SetFrameIndex)
75 int GetFrameIndex() const;
77 //! Returns a pointer to the output buffer
78 char* GetOutputBufferPtr() const;
80 //! Returns the number of bytes written to the output buffer
81 size_t GetOutputBufferSizeInBytes() const;
83 //! @brief Start processing a frame. The call is asynchronous and returns
84 //! immediately. Use ExecutionObject::ProcessFrameWait to wait
85 bool ProcessFrameStartAsync();
87 //! Wait for the execution object to complete processing a frame
88 //! @return false if ExecutionObject::ProcessFrameWait was called
89 //! without a corresponding call to
90 //! ExecutionObject::ProcessFrameStartAsync.
91 bool ProcessFrameWait();
93 //! @brief return the number of cycles taken *on the device* to
94 //! execute the process call
95 //! @return Number of cycles to process a frame on the device.
96 uint64_t GetProcessCycles() const;
98 //! @brief return the number of milliseconds taken *on the device* to
99 //! execute the process call
100 //! @return Number of milliseconds to process a frame on the device.
101 float GetProcessTimeInMilliSeconds() const;
103 //! @private
104 // Used by the Executor
105 enum class CallType { INIT, PROCESS, CLEANUP };
106 bool RunAsync(CallType ct);
107 bool Wait (CallType ct);
109 ExecutionObject() = delete;
110 ExecutionObject(const ExecutionObject&) = delete;
111 ExecutionObject& operator=(const ExecutionObject&) = delete;
113 private:
114 class Impl;
115 std::unique_ptr<Impl> pimpl_m;
116 };
118 } // namespace tidl