Quantization history configuration parameters
[tidl/tidl-api.git] / tidl_api / inc / execution_object_pipeline.h
1 /******************************************************************************
2  * Copyright (c) 2018 Texas Instruments Incorporated - http://www.ti.com/
3  *  All rights reserved.
4  *
5  *  Redistribution and use in source and binary forms, with or without
6  *  modification, are permitted provided that the following conditions are met:
7  *      * Redistributions of source code must retain the above copyright
8  *        notice, this list of conditions and the following disclaimer.
9  *      * Redistributions in binary form must reproduce the above copyright
10  *        notice, this list of conditions and the following disclaimer in the
11  *        documentation and/or other materials provided with the distribution.
12  *      * Neither the name of Texas Instruments Incorporated nor the
13  *        names of its contributors may be used to endorse or promote products
14  *        derived from this software without specific prior written permission.
15  *
16  *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
17  *  AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
18  *  IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
19  *  ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE
20  *  LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
21  *  CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
22  *  SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
23  *  INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
24  *  CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
25  *  ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF
26  *  THE POSSIBILITY OF SUCH DAMAGE.
27  *****************************************************************************/
29 //! @file execution_object_pipeline.h
31 #pragma once
32 #include <string>
33 #include <vector>
34 #include <cstdint>
35 #include <cassert>
37 #include "executor.h"
38 #include "execution_object_internal.h"
39 #include "execution_object.h"
41 namespace tidl {
43 /*! @class ExecutionObjectPipeline
44     @brief Manages the pipelined execution using multiple ExecutionObjects.
45     Each executor runs one layersGroup of the network.  ExecutionObjects
46     must run consecutive layersGroups to form a pipelined execution.
47 */
48 class ExecutionObjectPipeline : public ExecutionObjectInternalInterface
49 {
50     public:
51         //! @brief Create an ExecutionObjectPipeline object.
52         //!
53         //! The ExecutionObjectPipeline will take the provided ExecutionObjects
54         //! to create an execution pipeline.  E.g.
55         //! @code
56         //!   Configuration config("path to configuration file");
57         //!   DeviceIds ids = {DeviceId::ID0, DeviceId::ID1};
58         //!   Executor exe_eve(DeviceType::EVE, ids, config, 1);
59         //!   Executor exe_dsp(DeviceType::DSP, ids, config, 2);
60         //!   ExecutionObjectPipeline ep0({exe_eve[0], exe_dsp[0]});
61         //!   ExecutionObjectPipeline ep1({exe_eve[1], exe_dsp[1]});
62         //! @endcode
63         //!
64         //! @param eos DSP or EVE ExecutionObjects forming a pipeline
65         ExecutionObjectPipeline(std::vector<ExecutionObject*> eos);
67         //! @brief Tear down an ExecutionObjectPipeline and free used resources
68         ~ExecutionObjectPipeline();
70         //! Returns the number of ExecutionObjects associated with the
71         //! ExecutionObjectPipeline
72         uint32_t GetNumExecutionObjects() const;
74         //! Specify the input and output buffers used by the EOP
75         //! @param in buffer used for input.
76         //! @param out buffer used for output.
77         void SetInputOutputBuffer (const ArgInfo& in,
78                                    const ArgInfo& out) override;
80         //! Returns a pointer to the input buffer
81         char* GetInputBufferPtr() const override;
83         //! Returns size of the input buffer
84         size_t GetInputBufferSizeInBytes() const override;
86         //! Returns a pointer to the output buffer
87         char* GetOutputBufferPtr() const override;
89         //! Returns the number of bytes written to the output buffer
90         size_t GetOutputBufferSizeInBytes() const override;
92         //! @brief Set the frame index of the frame currently processed by the
93         //! ExecutionObjectPipeline. Used for trace/debug messages
94         //! @param idx index of the frame
95         void SetFrameIndex(int idx) override;
97         //! Returns the index of a frame being processed (set by SetFrameIndex)
98         int  GetFrameIndex() const override;
100         //! @brief Start processing a frame. The call is asynchronous and
101         //! returns immediately. Use ProcessFrameWait() to wait
102         bool ProcessFrameStartAsync() override;
104         //! Wait for the executor pipeline to complete processing a frame
105         //! @return false if ProcessFrameWait() was called
106         //! without a corresponding call to
107         //! ExecutionObjectPipeline::ProcessFrameStartAsync().
108         bool ProcessFrameWait() override;
110         //! @brief return the number of milliseconds taken *on the device* to
111         //! execute the process call
112         //! @return Number of milliseconds to process a frame on the device.
113         float GetProcessTimeInMilliSeconds() const override;
115         //! @brief return the number of milliseconds taken *on the device*
116         //! to process a layersGroup by a componenet ExecutionObject
117         //! @return Number of milliseconds to process a layersGroup on the
118         //! device by a component ExecutionObject.
119         float GetProcessTimeInMilliSeconds(uint32_t eo_index) const;
121         //! @brief return the number of milliseconds taken *on the host* to
122         //! execute the process call
123         //! @return Number of milliseconds to process a frame on the host.
124         float GetHostProcessTimeInMilliSeconds() const override;
126         //! @brief return the number of milliseconds taken *on the host*
127         //! to process a layersGroup by a componenet ExecutionObject
128         //! @return Number of milliseconds to process a layersGroup on the
129         //! host by a component ExecutionObject.
130         float GetHostProcessTimeInMilliSeconds(uint32_t eo_index) const;
132         //! Return the combined device names that this pipeline runs on
133         const std::string& GetDeviceName() const override;
135         //! Write the output buffer for each layer to a file
136         //! \<filename_prefix>_<ID>_HxW.bin
137         void WriteLayerOutputsToFile(const std::string& filename_prefix=
138                                      "trace_dump_") const override;
140         //! Returns a LayerOutput object corresponding to a layer.
141         //! Caller is responsible for deleting the LayerOutput object.
142         //! @see LayerOutput
143         //! @param layer_index The layer index of the layer
144         //! @param output_index The output index of the buffer for a given
145         //!                     layer. Defaults to 0.
146         const LayerOutput* GetOutputFromLayer(uint32_t layer_index,
147                                        uint32_t output_index=0) const override;
149         //! Get output buffers from all layers
150         const LayerOutputs* GetOutputsFromAllLayers() const override;
152         //! @private Used by runtime
153         //! @brief callback function at the completion of each ExecutionObject,
154         //! to chain the next ExectionObject for execution
155         void RunAsyncNext();
157         ExecutionObjectPipeline()                                     = delete;
158         ExecutionObjectPipeline(const ExecutionObjectPipeline&)       = delete;
159         ExecutionObjectPipeline& operator=(const ExecutionObjectPipeline&)
160                                                                       = delete;
162     private:
163         class Impl;
164         std::unique_ptr<Impl> pimpl_m;
165 };
167 } // namespace tidl