1 /******************************************************************************
2 * Copyright (c) 2018 Texas Instruments Incorporated - http://www.ti.com/
3 * All rights reserved.
4 *
5 * Redistribution and use in source and binary forms, with or without
6 * modification, are permitted provided that the following conditions are met:
7 * * Redistributions of source code must retain the above copyright
8 * notice, this list of conditions and the following disclaimer.
9 * * Redistributions in binary form must reproduce the above copyright
10 * notice, this list of conditions and the following disclaimer in the
11 * documentation and/or other materials provided with the distribution.
12 * * Neither the name of Texas Instruments Incorporated nor the
13 * names of its contributors may be used to endorse or promote products
14 * derived from this software without specific prior written permission.
15 *
16 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
17 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
18 * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
19 * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE
20 * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
21 * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
22 * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
23 * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
24 * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
25 * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF
26 * THE POSSIBILITY OF SUCH DAMAGE.
27 *****************************************************************************/
29 //! @file execution_object_pipeline.h
31 #pragma once
32 #include <string>
33 #include <vector>
34 #include <cstdint>
35 #include <cassert>
37 #include "executor.h"
38 #include "execution_object_internal.h"
39 #include "execution_object.h"
41 namespace tidl {
43 /*! @class ExecutionObjectPipeline
44 @brief Manages the pipelined execution using multiple ExecutionObjects.
45 Each executor runs one layersGroup of the network. ExecutionObjects
46 must run consecutive layersGroups to form a pipelined execution.
47 */
48 class ExecutionObjectPipeline : public ExecutionObjectInternalInterface
49 {
50 public:
51 //! @brief Create an ExecutionObjectPipeline object.
52 //!
53 //! The ExecutionObjectPipeline will take the provided ExecutionObjects
54 //! to create an execution pipeline. E.g.
55 //! @code
56 //! Configuration config("path to configuration file");
57 //! DeviceIds ids = {DeviceId::ID0, DeviceId::ID1};
58 //! Executor exe_eve(DeviceType::EVE, ids, config, 1);
59 //! Executor exe_dsp(DeviceType::DSP, ids, config, 2);
60 //! ExecutionObjectPipeline ep0({exe_eve[0], exe_dsp[0]});
61 //! ExecutionObjectPipeline ep1({exe_eve[1], exe_dsp[1]});
62 //! @endcode
63 //!
64 //! @param eos DSP or EVE ExecutionObjects forming a pipeline
65 ExecutionObjectPipeline(std::vector<ExecutionObject*> eos);
67 //! @brief Tear down an ExecutionObjectPipeline and free used resources
68 ~ExecutionObjectPipeline();
70 //! Specify the input and output buffers used by the EOP
71 //! @param in buffer used for input.
72 //! @param out buffer used for output.
73 void SetInputOutputBuffer (const ArgInfo& in,
74 const ArgInfo& out) override;
76 //! Returns a pointer to the input buffer
77 char* GetInputBufferPtr() const override;
79 //! Returns size of the input buffer
80 size_t GetInputBufferSizeInBytes() const override;
82 //! Returns a pointer to the output buffer
83 char* GetOutputBufferPtr() const override;
85 //! Returns the number of bytes written to the output buffer
86 size_t GetOutputBufferSizeInBytes() const override;
88 //! @brief Set the frame index of the frame currently processed by the
89 //! ExecutionObjectPipeline. Used for trace/debug messages
90 //! @param idx index of the frame
91 void SetFrameIndex(int idx) override;
93 //! Returns the index of a frame being processed (set by SetFrameIndex)
94 int GetFrameIndex() const override;
96 //! @brief Start processing a frame. The call is asynchronous and
97 //! returns immediately. Use ProcessFrameWait() to wait
98 bool ProcessFrameStartAsync() override;
100 //! Wait for the executor pipeline to complete processing a frame
101 //! @return false if ProcessFrameWait() was called
102 //! without a corresponding call to
103 //! ExecutionObjectPipeline::ProcessFrameStartAsync().
104 bool ProcessFrameWait() override;
106 //! @brief return the number of milliseconds taken *on the device* to
107 //! execute the process call
108 //! @return Number of milliseconds to process a frame on the device.
109 float GetProcessTimeInMilliSeconds() const override;
111 //! @brief return the number of milliseconds taken *on the host* to
112 //! execute the process call
113 //! @return Number of milliseconds to process a frame on the host.
114 float GetHostProcessTimeInMilliSeconds() const override;
116 //! Return the combined device names that this pipeline runs on
117 const std::string& GetDeviceName() const override;
119 //! Write the output buffer for each layer to a file
120 //! \<filename_prefix>_<ID>_HxW.bin
121 void WriteLayerOutputsToFile(const std::string& filename_prefix=
122 "trace_dump_") const override;
124 //! Returns a LayerOutput object corresponding to a layer.
125 //! Caller is responsible for deleting the LayerOutput object.
126 //! @see LayerOutput
127 //! @param layer_index The layer index of the layer
128 //! @param output_index The output index of the buffer for a given
129 //! layer. Defaults to 0.
130 const LayerOutput* GetOutputFromLayer(uint32_t layer_index,
131 uint32_t output_index=0) const override;
133 //! Get output buffers from all layers
134 const LayerOutputs* GetOutputsFromAllLayers() const override;
136 //! @private Used by runtime
137 //! @brief callback function at the completion of each ExecutionObject,
138 //! to chain the next ExectionObject for execution
139 void RunAsyncNext();
141 ExecutionObjectPipeline() = delete;
142 ExecutionObjectPipeline(const ExecutionObjectPipeline&) = delete;
143 ExecutionObjectPipeline& operator=(const ExecutionObjectPipeline&)
144 = delete;
146 private:
147 class Impl;
148 std::unique_ptr<Impl> pimpl_m;
149 };
151 } // namespace tidl