Merge branch 'release/v01.02.00'
[tidl/tidl-api.git] / tidl_api / pybind11 / CONTRIBUTING.md
1 Thank you for your interest in this project! Please refer to the following
2 sections on how to contribute code and bug reports.
4 ### Reporting bugs
6 At the moment, this project is run in the spare time of a single person
7 ([Wenzel Jakob](http://rgl.epfl.ch/people/wjakob)) with very limited resources
8 for issue tracker tickets. Thus, before submitting a question or bug report,
9 please take a moment of your time and ensure that your issue isn't already
10 discussed in the project documentation provided at
11 [http://pybind11.readthedocs.org/en/latest](http://pybind11.readthedocs.org/en/latest).
13 Assuming that you have identified a previously unknown problem or an important
14 question, it's essential that you submit a self-contained and minimal piece of
15 code that reproduces the problem. In other words: no external dependencies,
16 isolate the function(s) that cause breakage, submit matched and complete C++
17 and Python snippets that can be easily compiled and run on my end.
19 ## Pull requests
20 Contributions are submitted, reviewed, and accepted using Github pull requests.
21 Please refer to [this
22 article](https://help.github.com/articles/using-pull-requests) for details and
23 adhere to the following rules to make the process as smooth as possible:
25 * Make a new branch for every feature you're working on.
26 * Make small and clean pull requests that are easy to review but make sure they
27   do add value by themselves.
28 * Add tests for any new functionality and run the test suite (``make pytest``)
29   to ensure that no existing features break.
30 * This project has a strong focus on providing general solutions using a
31   minimal amount of code, thus small pull requests are greatly preferred.
33 ### Licensing of contributions
35 pybind11 is provided under a BSD-style license that can be found in the
36 ``LICENSE`` file. By using, distributing, or contributing to this project, you
37 agree to the terms and conditions of this license.
39 You are under no obligation whatsoever to provide any bug fixes, patches, or
40 upgrades to the features, functionality or performance of the source code
41 ("Enhancements") to anyone; however, if you choose to make your Enhancements
42 available either publicly, or directly to the author of this software, without
43 imposing a separate written license agreement for such Enhancements, then you
44 hereby grant the following license: a non-exclusive, royalty-free perpetual
45 license to install, use, modify, prepare derivative works, incorporate into
46 other computer software, distribute, and sublicense such enhancements or
47 derivative works thereof, in binary and source code form.