1 /*
2 pybind11/chrono.h: Transparent conversion between std::chrono and python's datetime
4 Copyright (c) 2016 Trent Houliston <trent@houliston.me> and
5 Wenzel Jakob <wenzel.jakob@epfl.ch>
7 All rights reserved. Use of this source code is governed by a
8 BSD-style license that can be found in the LICENSE file.
9 */
11 #pragma once
13 #include "pybind11.h"
14 #include <cmath>
15 #include <ctime>
16 #include <chrono>
17 #include <datetime.h>
19 // Backport the PyDateTime_DELTA functions from Python3.3 if required
20 #ifndef PyDateTime_DELTA_GET_DAYS
21 #define PyDateTime_DELTA_GET_DAYS(o) (((PyDateTime_Delta*)o)->days)
22 #endif
23 #ifndef PyDateTime_DELTA_GET_SECONDS
24 #define PyDateTime_DELTA_GET_SECONDS(o) (((PyDateTime_Delta*)o)->seconds)
25 #endif
26 #ifndef PyDateTime_DELTA_GET_MICROSECONDS
27 #define PyDateTime_DELTA_GET_MICROSECONDS(o) (((PyDateTime_Delta*)o)->microseconds)
28 #endif
30 NAMESPACE_BEGIN(PYBIND11_NAMESPACE)
31 NAMESPACE_BEGIN(detail)
33 template <typename type> class duration_caster {
34 public:
35 typedef typename type::rep rep;
36 typedef typename type::period period;
38 typedef std::chrono::duration<uint_fast32_t, std::ratio<86400>> days;
40 bool load(handle src, bool) {
41 using namespace std::chrono;
43 // Lazy initialise the PyDateTime import
44 if (!PyDateTimeAPI) { PyDateTime_IMPORT; }
46 if (!src) return false;
47 // If invoked with datetime.delta object
48 if (PyDelta_Check(src.ptr())) {
49 value = type(duration_cast<duration<rep, period>>(
50 days(PyDateTime_DELTA_GET_DAYS(src.ptr()))
51 + seconds(PyDateTime_DELTA_GET_SECONDS(src.ptr()))
52 + microseconds(PyDateTime_DELTA_GET_MICROSECONDS(src.ptr()))));
53 return true;
54 }
55 // If invoked with a float we assume it is seconds and convert
56 else if (PyFloat_Check(src.ptr())) {
57 value = type(duration_cast<duration<rep, period>>(duration<double>(PyFloat_AsDouble(src.ptr()))));
58 return true;
59 }
60 else return false;
61 }
63 // If this is a duration just return it back
64 static const std::chrono::duration<rep, period>& get_duration(const std::chrono::duration<rep, period> &src) {
65 return src;
66 }
68 // If this is a time_point get the time_since_epoch
69 template <typename Clock> static std::chrono::duration<rep, period> get_duration(const std::chrono::time_point<Clock, std::chrono::duration<rep, period>> &src) {
70 return src.time_since_epoch();
71 }
73 static handle cast(const type &src, return_value_policy /* policy */, handle /* parent */) {
74 using namespace std::chrono;
76 // Use overloaded function to get our duration from our source
77 // Works out if it is a duration or time_point and get the duration
78 auto d = get_duration(src);
80 // Lazy initialise the PyDateTime import
81 if (!PyDateTimeAPI) { PyDateTime_IMPORT; }
83 // Declare these special duration types so the conversions happen with the correct primitive types (int)
84 using dd_t = duration<int, std::ratio<86400>>;
85 using ss_t = duration<int, std::ratio<1>>;
86 using us_t = duration<int, std::micro>;
88 auto dd = duration_cast<dd_t>(d);
89 auto subd = d - dd;
90 auto ss = duration_cast<ss_t>(subd);
91 auto us = duration_cast<us_t>(subd - ss);
92 return PyDelta_FromDSU(dd.count(), ss.count(), us.count());
93 }
95 PYBIND11_TYPE_CASTER(type, _("datetime.timedelta"));
96 };
98 // This is for casting times on the system clock into datetime.datetime instances
99 template <typename Duration> class type_caster<std::chrono::time_point<std::chrono::system_clock, Duration>> {
100 public:
101 typedef std::chrono::time_point<std::chrono::system_clock, Duration> type;
102 bool load(handle src, bool) {
103 using namespace std::chrono;
105 // Lazy initialise the PyDateTime import
106 if (!PyDateTimeAPI) { PyDateTime_IMPORT; }
108 if (!src) return false;
109 if (PyDateTime_Check(src.ptr())) {
110 std::tm cal;
111 cal.tm_sec = PyDateTime_DATE_GET_SECOND(src.ptr());
112 cal.tm_min = PyDateTime_DATE_GET_MINUTE(src.ptr());
113 cal.tm_hour = PyDateTime_DATE_GET_HOUR(src.ptr());
114 cal.tm_mday = PyDateTime_GET_DAY(src.ptr());
115 cal.tm_mon = PyDateTime_GET_MONTH(src.ptr()) - 1;
116 cal.tm_year = PyDateTime_GET_YEAR(src.ptr()) - 1900;
117 cal.tm_isdst = -1;
119 value = system_clock::from_time_t(std::mktime(&cal)) + microseconds(PyDateTime_DATE_GET_MICROSECOND(src.ptr()));
120 return true;
121 }
122 else return false;
123 }
125 static handle cast(const std::chrono::time_point<std::chrono::system_clock, Duration> &src, return_value_policy /* policy */, handle /* parent */) {
126 using namespace std::chrono;
128 // Lazy initialise the PyDateTime import
129 if (!PyDateTimeAPI) { PyDateTime_IMPORT; }
131 std::time_t tt = system_clock::to_time_t(src);
132 // this function uses static memory so it's best to copy it out asap just in case
133 // otherwise other code that is using localtime may break this (not just python code)
134 std::tm localtime = *std::localtime(&tt);
136 // Declare these special duration types so the conversions happen with the correct primitive types (int)
137 using us_t = duration<int, std::micro>;
139 return PyDateTime_FromDateAndTime(localtime.tm_year + 1900,
140 localtime.tm_mon + 1,
141 localtime.tm_mday,
142 localtime.tm_hour,
143 localtime.tm_min,
144 localtime.tm_sec,
145 (duration_cast<us_t>(src.time_since_epoch() % seconds(1))).count());
146 }
147 PYBIND11_TYPE_CASTER(type, _("datetime.datetime"));
148 };
150 // Other clocks that are not the system clock are not measured as datetime.datetime objects
151 // since they are not measured on calendar time. So instead we just make them timedeltas
152 // Or if they have passed us a time as a float we convert that
153 template <typename Clock, typename Duration> class type_caster<std::chrono::time_point<Clock, Duration>>
154 : public duration_caster<std::chrono::time_point<Clock, Duration>> {
155 };
157 template <typename Rep, typename Period> class type_caster<std::chrono::duration<Rep, Period>>
158 : public duration_caster<std::chrono::duration<Rep, Period>> {
159 };
161 NAMESPACE_END(detail)
162 NAMESPACE_END(PYBIND11_NAMESPACE)