1 /*
2 pybind11/operator.h: Metatemplates for operator overloading
4 Copyright (c) 2016 Wenzel Jakob <wenzel.jakob@epfl.ch>
6 All rights reserved. Use of this source code is governed by a
7 BSD-style license that can be found in the LICENSE file.
8 */
10 #pragma once
12 #include "pybind11.h"
14 #if defined(__clang__) && !defined(__INTEL_COMPILER)
15 # pragma clang diagnostic ignored "-Wunsequenced" // multiple unsequenced modifications to 'self' (when using def(py::self OP Type()))
16 #elif defined(_MSC_VER)
17 # pragma warning(push)
18 # pragma warning(disable: 4127) // warning C4127: Conditional expression is constant
19 #endif
21 NAMESPACE_BEGIN(PYBIND11_NAMESPACE)
22 NAMESPACE_BEGIN(detail)
24 /// Enumeration with all supported operator types
25 enum op_id : int {
26 op_add, op_sub, op_mul, op_div, op_mod, op_divmod, op_pow, op_lshift,
27 op_rshift, op_and, op_xor, op_or, op_neg, op_pos, op_abs, op_invert,
28 op_int, op_long, op_float, op_str, op_cmp, op_gt, op_ge, op_lt, op_le,
29 op_eq, op_ne, op_iadd, op_isub, op_imul, op_idiv, op_imod, op_ilshift,
30 op_irshift, op_iand, op_ixor, op_ior, op_complex, op_bool, op_nonzero,
31 op_repr, op_truediv, op_itruediv, op_hash
32 };
34 enum op_type : int {
35 op_l, /* base type on left */
36 op_r, /* base type on right */
37 op_u /* unary operator */
38 };
40 struct self_t { };
41 static const self_t self = self_t();
43 /// Type for an unused type slot
44 struct undefined_t { };
46 /// Don't warn about an unused variable
47 inline self_t __self() { return self; }
49 /// base template of operator implementations
50 template <op_id, op_type, typename B, typename L, typename R> struct op_impl { };
52 /// Operator implementation generator
53 template <op_id id, op_type ot, typename L, typename R> struct op_ {
54 template <typename Class, typename... Extra> void execute(Class &cl, const Extra&... extra) const {
55 using Base = typename Class::type;
56 using L_type = conditional_t<std::is_same<L, self_t>::value, Base, L>;
57 using R_type = conditional_t<std::is_same<R, self_t>::value, Base, R>;
58 using op = op_impl<id, ot, Base, L_type, R_type>;
59 cl.def(op::name(), &op::execute, is_operator(), extra...);
60 #if PY_MAJOR_VERSION < 3
61 if (id == op_truediv || id == op_itruediv)
62 cl.def(id == op_itruediv ? "__idiv__" : ot == op_l ? "__div__" : "__rdiv__",
63 &op::execute, is_operator(), extra...);
64 #endif
65 }
66 template <typename Class, typename... Extra> void execute_cast(Class &cl, const Extra&... extra) const {
67 using Base = typename Class::type;
68 using L_type = conditional_t<std::is_same<L, self_t>::value, Base, L>;
69 using R_type = conditional_t<std::is_same<R, self_t>::value, Base, R>;
70 using op = op_impl<id, ot, Base, L_type, R_type>;
71 cl.def(op::name(), &op::execute_cast, is_operator(), extra...);
72 #if PY_MAJOR_VERSION < 3
73 if (id == op_truediv || id == op_itruediv)
74 cl.def(id == op_itruediv ? "__idiv__" : ot == op_l ? "__div__" : "__rdiv__",
75 &op::execute, is_operator(), extra...);
76 #endif
77 }
78 };
80 #define PYBIND11_BINARY_OPERATOR(id, rid, op, expr) \
81 template <typename B, typename L, typename R> struct op_impl<op_##id, op_l, B, L, R> { \
82 static char const* name() { return "__" #id "__"; } \
83 static auto execute(const L &l, const R &r) -> decltype(expr) { return (expr); } \
84 static B execute_cast(const L &l, const R &r) { return B(expr); } \
85 }; \
86 template <typename B, typename L, typename R> struct op_impl<op_##id, op_r, B, L, R> { \
87 static char const* name() { return "__" #rid "__"; } \
88 static auto execute(const R &r, const L &l) -> decltype(expr) { return (expr); } \
89 static B execute_cast(const R &r, const L &l) { return B(expr); } \
90 }; \
91 inline op_<op_##id, op_l, self_t, self_t> op(const self_t &, const self_t &) { \
92 return op_<op_##id, op_l, self_t, self_t>(); \
93 } \
94 template <typename T> op_<op_##id, op_l, self_t, T> op(const self_t &, const T &) { \
95 return op_<op_##id, op_l, self_t, T>(); \
96 } \
97 template <typename T> op_<op_##id, op_r, T, self_t> op(const T &, const self_t &) { \
98 return op_<op_##id, op_r, T, self_t>(); \
99 }
101 #define PYBIND11_INPLACE_OPERATOR(id, op, expr) \
102 template <typename B, typename L, typename R> struct op_impl<op_##id, op_l, B, L, R> { \
103 static char const* name() { return "__" #id "__"; } \
104 static auto execute(L &l, const R &r) -> decltype(expr) { return expr; } \
105 static B execute_cast(L &l, const R &r) { return B(expr); } \
106 }; \
107 template <typename T> op_<op_##id, op_l, self_t, T> op(const self_t &, const T &) { \
108 return op_<op_##id, op_l, self_t, T>(); \
109 }
111 #define PYBIND11_UNARY_OPERATOR(id, op, expr) \
112 template <typename B, typename L> struct op_impl<op_##id, op_u, B, L, undefined_t> { \
113 static char const* name() { return "__" #id "__"; } \
114 static auto execute(const L &l) -> decltype(expr) { return expr; } \
115 static B execute_cast(const L &l) { return B(expr); } \
116 }; \
117 inline op_<op_##id, op_u, self_t, undefined_t> op(const self_t &) { \
118 return op_<op_##id, op_u, self_t, undefined_t>(); \
119 }
121 PYBIND11_BINARY_OPERATOR(sub, rsub, operator-, l - r)
122 PYBIND11_BINARY_OPERATOR(add, radd, operator+, l + r)
123 PYBIND11_BINARY_OPERATOR(mul, rmul, operator*, l * r)
124 PYBIND11_BINARY_OPERATOR(truediv, rtruediv, operator/, l / r)
125 PYBIND11_BINARY_OPERATOR(mod, rmod, operator%, l % r)
126 PYBIND11_BINARY_OPERATOR(lshift, rlshift, operator<<, l << r)
127 PYBIND11_BINARY_OPERATOR(rshift, rrshift, operator>>, l >> r)
128 PYBIND11_BINARY_OPERATOR(and, rand, operator&, l & r)
129 PYBIND11_BINARY_OPERATOR(xor, rxor, operator^, l ^ r)
130 PYBIND11_BINARY_OPERATOR(eq, eq, operator==, l == r)
131 PYBIND11_BINARY_OPERATOR(ne, ne, operator!=, l != r)
132 PYBIND11_BINARY_OPERATOR(or, ror, operator|, l | r)
133 PYBIND11_BINARY_OPERATOR(gt, lt, operator>, l > r)
134 PYBIND11_BINARY_OPERATOR(ge, le, operator>=, l >= r)
135 PYBIND11_BINARY_OPERATOR(lt, gt, operator<, l < r)
136 PYBIND11_BINARY_OPERATOR(le, ge, operator<=, l <= r)
137 //PYBIND11_BINARY_OPERATOR(pow, rpow, pow, std::pow(l, r))
138 PYBIND11_INPLACE_OPERATOR(iadd, operator+=, l += r)
139 PYBIND11_INPLACE_OPERATOR(isub, operator-=, l -= r)
140 PYBIND11_INPLACE_OPERATOR(imul, operator*=, l *= r)
141 PYBIND11_INPLACE_OPERATOR(itruediv, operator/=, l /= r)
142 PYBIND11_INPLACE_OPERATOR(imod, operator%=, l %= r)
143 PYBIND11_INPLACE_OPERATOR(ilshift, operator<<=, l <<= r)
144 PYBIND11_INPLACE_OPERATOR(irshift, operator>>=, l >>= r)
145 PYBIND11_INPLACE_OPERATOR(iand, operator&=, l &= r)
146 PYBIND11_INPLACE_OPERATOR(ixor, operator^=, l ^= r)
147 PYBIND11_INPLACE_OPERATOR(ior, operator|=, l |= r)
148 PYBIND11_UNARY_OPERATOR(neg, operator-, -l)
149 PYBIND11_UNARY_OPERATOR(pos, operator+, +l)
150 PYBIND11_UNARY_OPERATOR(abs, abs, std::abs(l))
151 PYBIND11_UNARY_OPERATOR(hash, hash, std::hash<L>()(l))
152 PYBIND11_UNARY_OPERATOR(invert, operator~, (~l))
153 PYBIND11_UNARY_OPERATOR(bool, operator!, !!l)
154 PYBIND11_UNARY_OPERATOR(int, int_, (int) l)
155 PYBIND11_UNARY_OPERATOR(float, float_, (double) l)
157 #undef PYBIND11_BINARY_OPERATOR
158 #undef PYBIND11_INPLACE_OPERATOR
159 #undef PYBIND11_UNARY_OPERATOR
160 NAMESPACE_END(detail)
162 using detail::self;
164 NAMESPACE_END(PYBIND11_NAMESPACE)
166 #if defined(_MSC_VER)
167 # pragma warning(pop)
168 #endif