1 #include <assert.h>
2 #include "executor.h"
3 #include "executor_impl.h"
4 #include "parameters.h"
5 #include "util.h"
6 #include "trace.h"
9 using namespace tidl;
11 using std::unique_ptr;
13 Executor::Executor(DeviceType core_type, const DeviceIds& ids,
14 const Configuration& configuration, int layers_group_id)
15 {
16 pimpl_m = unique_ptr<ExecutorImpl>
17 { new ExecutorImpl(core_type, ids, layers_group_id) };
18 pimpl_m->Initialize(configuration);
19 }
23 // Pointer to implementation idiom: https://herbsutter.com/gotw/_100/:
24 // Both unique_ptr and shared_ptr can be instantiated with an incomplete type
25 // unique_ptr's destructor requires a complete type in order to invoke delete
26 // By writing it yourself in the implementation file, you force it to be
27 // defined in a place where impl is already defined, and this successfully
28 // prevents the compiler from trying to automatically generate the destructor
29 // on demand in the caller’s code where impl is not defined.
30 Executor::~Executor() = default;
32 uint32_t Executor::GetNumDevices(DeviceType device_type)
33 {
34 return Device::GetNumDevices(device_type);
35 }
37 #define STRING(S) XSTRING(S)
38 #define XSTRING(S) #S
39 std::string Executor::GetAPIVersion()
40 {
41 static std::string version = STRING(_BUILD_VER);
42 version += ".";
43 version += STRING(_BUILD_SHA);
44 return version;
45 }
48 ExecutorImpl::ExecutorImpl(DeviceType core_type, const DeviceIds& ids,
49 int layers_group_id):
50 configuration_m(),
51 shared_networkparam_heap_m(nullptr, &__free_ddr),
52 device_ids_m(ids),
53 core_type_m(core_type),
54 layers_group_id_m(layers_group_id)
55 {
56 std::string name;
57 if (core_type_m == DeviceType::DSP)
58 name = "";
59 else if (core_type_m == DeviceType::DLA)
60 name = STRING(SETUP_KERNEL) ";" STRING(INIT_KERNEL) ";" STRING(PROCESS_KERNEL) ";" STRING(CLEANUP_KERNEL);
62 device_m = Device::Create(core_type_m, ids, name);
63 }
66 const ExecutionObjects& Executor::GetExecutionObjects() const
67 {
68 return pimpl_m->execution_objects_m;
69 }
71 bool ExecutorImpl::Initialize(const Configuration& configuration)
72 {
73 configuration_m = configuration;
75 // Allocate, initialize TIDL_CreateParams object
76 up_malloc_ddr<TIDL_CreateParams> shared_createparam(
77 malloc_ddr<TIDL_CreateParams>(),
78 &__free_ddr);
79 InitializeNetworkCreateParam(shared_createparam.get(), configuration);
81 // Read network from file into network struct in TIDL_CreateParams
82 sTIDL_Network_t *net = &(shared_createparam.get())->net;
84 bool status = ReadBinary(configuration_m.netBinFile,
85 reinterpret_cast<char *>(net),
86 sizeof(sTIDL_Network_t));
87 assert(status != false);
89 //TODO: Why is this set here?
90 net->interElementSize = 4;
92 // Force to run full network if runFullNet is set
93 if (configuration.runFullNet)
94 {
95 for (int i = 0; i < net->numLayers; i++)
96 if (net->TIDLLayers[i].layerType != TIDL_DataLayer)
97 net->TIDLLayers[i].layersGroupId = layers_group_id_m;
98 }
100 // Call a setup kernel to allocate and fill network parameters
101 InitializeNetworkParams(shared_createparam.get());
103 const ArgInfo create_arg(shared_createparam.get(),
104 sizeof(TIDL_CreateParams));
105 const ArgInfo param_heap_arg(shared_networkparam_heap_m.get(),
106 configuration_m.PARAM_HEAP_SIZE);
107 for (auto ids : device_ids_m)
108 {
109 uint8_t index = static_cast<uint8_t>(ids);
110 execution_objects_m.push_back(
111 unique_ptr<ExecutionObject>
112 {new ExecutionObject(device_m.get(), index,
113 create_arg, param_heap_arg,
114 configuration_m.EXTMEM_HEAP_SIZE,
115 configuration_m.enableInternalInput)} );
116 }
118 for (auto &eo : execution_objects_m)
119 eo->RunAsync(ExecutionObject::CallType::INIT);
121 for (auto &eo : execution_objects_m)
122 eo->Wait(ExecutionObject::CallType::INIT);
124 return true;
125 }
128 bool ExecutorImpl::InitializeNetworkParams(TIDL_CreateParams *cp)
129 {
130 // Determine size of network parameters buffer, allocate it
131 size_t networkparam_size =
132 GetBinaryFileSize(configuration_m.paramsBinFile);
134 up_malloc_ddr<char> networkparam(malloc_ddr<char>(networkparam_size),
135 &__free_ddr);
137 // Read network parameters from bin file into buffer
138 bool status = ReadBinary(configuration_m.paramsBinFile,
139 networkparam.get(),
140 networkparam_size);
141 assert(status != false);
143 // Allocate a buffer for passing parameters to the kernel
144 up_malloc_ddr<OCL_TIDL_SetupParams> setupParams(
145 malloc_ddr<OCL_TIDL_SetupParams>(),
146 &__free_ddr);
148 setupParams->enableTrace = OCL_TIDL_TRACE_OFF;
149 setupParams->networkParamHeapSize = configuration_m.PARAM_HEAP_SIZE;
150 setupParams->noZeroCoeffsPercentage = configuration_m.noZeroCoeffsPercentage;
151 setupParams->sizeofTIDL_CreateParams = sizeof(TIDL_CreateParams);
152 setupParams->offsetofNet = offsetof(TIDL_CreateParams, net);
154 // Allocate buffer for a network parameter heap. Used by the setup
155 // kernel to allocate and initialize network parameters for the layers
156 shared_networkparam_heap_m.reset(malloc_ddr<char>(setupParams->networkParamHeapSize));
158 KernelArgs args = { ArgInfo(cp, sizeof(TIDL_CreateParams)),
159 ArgInfo(networkparam.get(), networkparam_size),
160 ArgInfo(shared_networkparam_heap_m.get(),
161 setupParams->networkParamHeapSize),
162 ArgInfo(setupParams.get(),
163 sizeof(OCL_TIDL_SetupParams)) };
165 // Execute kernel on first available device in the Executor
166 uint8_t id = static_cast<uint8_t>(*(device_ids_m.cbegin()));
167 unique_ptr<Kernel> K {new Kernel(device_m.get(), STRING(SETUP_KERNEL),
168 args, id)};
169 K->RunAsync();
170 K->Wait();
172 if (setupParams->errorCode != OCL_TIDL_SUCCESS)
173 throw Exception(setupParams->errorCode,
174 __FILE__, __FUNCTION__, __LINE__);
176 return status;
177 }
180 void ExecutorImpl::Cleanup()
181 {
182 for (auto &eo : execution_objects_m)
183 eo->RunAsync(ExecutionObject::CallType::CLEANUP);
185 for (auto &eo : execution_objects_m)
186 eo->Wait(ExecutionObject::CallType::CLEANUP);
187 }
190 void ExecutorImpl::InitializeNetworkCreateParam(TIDL_CreateParams *CP,
191 const Configuration& configuration)
192 {
193 CP->currCoreId = layers_group_id_m;
194 CP->currLayersGroupId = layers_group_id_m;
195 CP->l1MemSize = tidl::internal::DMEM0_SIZE;
196 CP->l2MemSize = tidl::internal::DMEM1_SIZE;
197 CP->l3MemSize = tidl::internal::OCMC_SIZE;
199 CP->quantHistoryParam1 = tidl::internal::QUANT_HISTORY_PARAM1;
200 CP->quantHistoryParam2 = tidl::internal::QUANT_HISTORY_PARAM2;
201 CP->quantMargin = tidl::internal::QUANT_MARGIN;
202 CP->optimiseExtMem = TIDL_optimiseExtMemL1;
203 }
205 Exception::Exception(const std::string& error, const std::string& file,
206 const std::string& func, uint32_t line_no)
207 {
209 message_m = "TIDL Error: [";
210 message_m += file;
211 message_m += ", ";
212 message_m += func;
213 message_m += ", ";
214 message_m += std::to_string(line_no);
215 message_m += "]: ";
216 message_m += error;
217 }
219 Exception::Exception(int32_t errorCode, const std::string& file,
220 const std::string& func, uint32_t line_no)
221 {
222 message_m = "TIDL Error: [";
223 message_m += file;
224 message_m += ", ";
225 message_m += func;
226 message_m += ", ";
227 message_m += std::to_string(line_no);
228 message_m += "]: ";
230 if (errorCode == OCL_TIDL_ERROR)
231 message_m += "";
232 else if (errorCode == OCL_TIDL_ALLOC_FAIL)
233 message_m += "Allocation failed on device";
234 else if (errorCode == OCL_TIDL_MEMREC_ALLOC_FAIL)
235 message_m += "Memrec allocation failed on device";
236 else if (errorCode == OCL_TIDL_PROCESS_FAIL)
237 message_m += "Process call failed on device";
238 else if (errorCode == OCL_TIDL_CREATE_PARAMS_MISMATCH)
239 message_m += "TIDL_CreateParams definition inconsistent across host"
240 "and device.";
241 else
242 message_m += std::to_string(errorCode);
244 }
246 const char* Exception::what() const noexcept
247 {
248 return message_m.c_str();
249 }