Renamed namespace (tidl -> tinn), updated documentation
[tidl/tidl-api.git] / tinn_api / src / executor.cpp
1 #include <assert.h>
2 #include "executor.h"
3 #include "executor_impl.h"
4 #include "parameters.h"
5 #include "util.h"
6 #include "trace.h"
9 using namespace tinn;
11 using std::unique_ptr;
13 Executor::Executor(DeviceType core_type, const DeviceIds& ids,
14                    const Configuration& configuration)
15 {
16     pimpl_m = unique_ptr<ExecutorImpl>
17               { new ExecutorImpl(core_type, ids) };
18     pimpl_m->Initialize(configuration);
19 }
23 // Pointer to implementation idiom: https://herbsutter.com/gotw/_100/:
24 // Both unique_ptr and shared_ptr can be instantiated with an incomplete type
25 // unique_ptr's destructor requires a complete type in order to invoke delete
26 // By writing it yourself in the implementation file, you force it to be
27 // defined in a place where impl is already defined, and this successfully
28 // prevents the compiler from trying to automatically generate the destructor
29 // on demand in the caller’s code where impl is not defined.
30 Executor::~Executor() = default;
32 uint32_t Executor::GetNumDevices(DeviceType device_type)
33 {
34     return Device::GetNumDevices(device_type);
35 }
37 #define STRING(S)  XSTRING(S)
38 #define XSTRING(S) #S
39 std::string Executor::GetAPIVersion()
40 {
41     static std::string version = STRING(_BUILD_VER);
42     version += ".";
43     version += STRING(_BUILD_SHA);
44     return version;
45 }
48 ExecutorImpl::ExecutorImpl(DeviceType core_type, const DeviceIds& ids):
49     configuration_m(),
50     shared_networkparam_heap_m(nullptr, &__free_ddr),
51     device_ids_m(ids),
52     core_type_m(core_type)
53 {
54     std::string name;
55     if (core_type_m == DeviceType::DSP)
56         name  = "ocl_wrapper.out";
57     else if (core_type_m == DeviceType::DLA)
58         name = STRING(SETUP_KERNEL) ";" STRING(INIT_KERNEL) ";" STRING(PROCESS_KERNEL) ";" STRING(CLEANUP_KERNEL);
60     device_m = Device::Create(core_type_m, ids, name);
61 }
64 const ExecutionObjects& Executor::GetExecutionObjects() const
65 {
66     return pimpl_m->execution_objects_m;
67 }
69 bool ExecutorImpl::Initialize(const Configuration& configuration)
70 {
71     configuration_m = configuration;
73     // Allocate, initialize TIDL_CreateParams object
74     up_malloc_ddr<TIDL_CreateParams> shared_createparam(
75                                             malloc_ddr<TIDL_CreateParams>(),
76                                             &__free_ddr);
77     InitializeNetworkCreateParam(shared_createparam.get());
79     // Read network from file into network struct in TIDL_CreateParams
80     sTIDL_Network_t *net = &(shared_createparam.get())->net;
82     bool status = ReadBinary(configuration_m.netBinFile,
83                              reinterpret_cast<char *>(net),
84                              sizeof(sTIDL_Network_t));
85     assert(status != false);
87     //TODO: Why is this set here?
88     net->interElementSize = 4;
90     // Call a setup kernel to allocate and fill network parameters
91     InitializeNetworkParams(shared_createparam.get());
93     const ArgInfo create_arg(shared_createparam.get(),
94                              sizeof(TIDL_CreateParams));
95     const ArgInfo param_heap_arg(shared_networkparam_heap_m.get(),
96                                  configuration_m.PARAM_HEAP_SIZE);
97     for (auto ids : device_ids_m)
98     {
99         uint8_t index = static_cast<uint8_t>(ids);
100         execution_objects_m.push_back(
101              unique_ptr<ExecutionObject>
102              {new ExecutionObject(device_m.get(), index,
103                                   create_arg, param_heap_arg,
104                                   configuration_m.EXTMEM_HEAP_SIZE)} );
105     }
107     for (auto &eo : execution_objects_m)
108         eo->RunAsync(ExecutionObject::CallType::INIT);
110     for (auto &eo : execution_objects_m)
111         eo->Wait(ExecutionObject::CallType::INIT);
113     return true;
117 bool ExecutorImpl::InitializeNetworkParams(TIDL_CreateParams *cp)
119     // Determine size of network parameters buffer, allocate it
120     size_t networkparam_size =
121                         GetBinaryFileSize(configuration_m.paramsBinFile);
123     up_malloc_ddr<char> networkparam(malloc_ddr<char>(networkparam_size),
124                                 &__free_ddr);
126     // Read network parameters from bin file into buffer
127     bool status = ReadBinary(configuration_m.paramsBinFile,
128                              networkparam.get(),
129                              networkparam_size);
130     assert(status != false);
132     // Allocate a buffer for passing parameters to the kernel
133     up_malloc_ddr<OCL_TIDL_SetupParams> setupParams(
134                                             malloc_ddr<OCL_TIDL_SetupParams>(),
135                                             &__free_ddr);
137     setupParams->enableTrace = OCL_TIDL_TRACE_OFF;
138     setupParams->networkParamHeapSize = configuration_m.PARAM_HEAP_SIZE;
139     setupParams->noZeroCoeffsPercentage = configuration_m.noZeroCoeffsPercentage;
140     setupParams->sizeofTIDL_CreateParams = sizeof(TIDL_CreateParams);
141     setupParams->offsetofNet = offsetof(TIDL_CreateParams, net);
143     // Allocate buffer for a network parameter heap. Used by the setup
144     // kernel to allocate and initialize network parameters for the layers
145     shared_networkparam_heap_m.reset(malloc_ddr<char>(setupParams->networkParamHeapSize));
147     KernelArgs args = { ArgInfo(cp, sizeof(TIDL_CreateParams)),
148                         ArgInfo(networkparam.get(), networkparam_size),
149                         ArgInfo(shared_networkparam_heap_m.get(),
150                                 setupParams->networkParamHeapSize),
151                         ArgInfo(setupParams.get(),
152                                 sizeof(OCL_TIDL_SetupParams)) };
154     // Execute kernel on first available device in the Executor
155     uint8_t id = static_cast<uint8_t>(*(device_ids_m.cbegin()));
156     unique_ptr<Kernel> K {new Kernel(device_m.get(), STRING(SETUP_KERNEL),
157                                      args, id)};
158     K->RunAsync();
159     K->Wait();
161     if (setupParams->errorCode != OCL_TIDL_SUCCESS)
162         throw Exception(setupParams->errorCode,
163                         __FILE__, __FUNCTION__, __LINE__);
165     return status;
169 void ExecutorImpl::Cleanup()
171     for (auto &eo : execution_objects_m)
172         eo->RunAsync(ExecutionObject::CallType::CLEANUP);
174     for (auto &eo : execution_objects_m)
175         eo->Wait(ExecutionObject::CallType::CLEANUP);
179 void ExecutorImpl::InitializeNetworkCreateParam(TIDL_CreateParams *CP)
181     CP->currCoreId           = tinn::internal::CURR_CORE_ID;
182     CP->currLayersGroupId    = tinn::internal::CURR_LAYERS_GROUP_ID;
183     CP->l1MemSize            = tinn::internal::DMEM0_SIZE;
184     CP->l2MemSize            = tinn::internal::DMEM1_SIZE;
185     CP->l3MemSize            = tinn::internal::OCMC_SIZE;
187     CP->quantHistoryParam1   = tinn::internal::QUANT_HISTORY_PARAM1;
188     CP->quantHistoryParam2   = tinn::internal::QUANT_HISTORY_PARAM2;
189     CP->quantMargin          = tinn::internal::QUANT_MARGIN;
190     CP->optimiseExtMem       = TIDL_optimiseExtMemL1;
193 Exception::Exception(const std::string& error, const std::string& file,
194                      const std::string& func, uint32_t line_no)
197     message_m = "TIDL Error: [";
198     message_m += file;
199     message_m += ", ";
200     message_m += func;
201     message_m += ", ";
202     message_m += std::to_string(line_no);
203     message_m += "]: ";
204     message_m += error;
207 Exception::Exception(int32_t errorCode, const std::string& file,
208                      const std::string& func, uint32_t line_no)
210     message_m = "TIDL Error: [";
211     message_m += file;
212     message_m += ", ";
213     message_m += func;
214     message_m += ", ";
215     message_m += std::to_string(line_no);
216     message_m += "]: ";
218     if (errorCode == OCL_TIDL_ERROR)
219         message_m += "";
220     else if (errorCode == OCL_TIDL_ALLOC_FAIL)
221         message_m += "Allocation failed on device";
222     else if (errorCode == OCL_TIDL_MEMREC_ALLOC_FAIL)
223         message_m += "Memrec allocation failed on device";
224     else if (errorCode == OCL_TIDL_PROCESS_FAIL)
225         message_m += "Process call failed on device";
226     else if (errorCode == OCL_TIDL_CREATE_PARAMS_MISMATCH)
227         message_m += "TIDL_CreateParams definition inconsistent across host"
228                      "and device.";
229     else
230         message_m += std::to_string(errorCode);
234 const char* Exception::what() const noexcept
236     return message_m.c_str();